Data Fields

IIMGENC1_Params Struct Reference
[IIMGENC1 - XDM Image Encoder Interface]

Defines the creation time parameters for all IIMGENC1 instance objects. More...

#include <iimgenc1.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 maxHeight
XDAS_Int32 maxWidth
XDAS_Int32 maxScans
XDAS_Int32 dataEndianness
XDAS_Int32 forceChromaFormat

Detailed Description

Defines the creation time parameters for all IIMGENC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Maximum height.

Maximum width.

Maximum number of scans.

Endianness of output data.

See also:
XDM_DataFormat

Force encoding in given Chroma format.

See also:
XDM_ChromaFormat

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated