Data Fields

Engine_Attrs Struct Reference
[Codec Engine Runtime]

Attributes of an Engine. More...

#include <Engine.h>

Data Fields

String procId

Detailed Description

Attributes of an Engine.

See also:
Engine_open() and Engine_ATTRS.

Field Documentation

id of the processor that runs the server; only needed in the case that there's more than one processor that can provide the same server.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated