Data Structures | Defines | Typedefs | Enumerations

IVIDEO - XDM Video Interface

Data Structures

struct  IVIDEO_BufDesc
 Buffer descriptor for video buffers. More...
struct  IVIDEO1_BufDescIn
 Buffer descriptor for input video buffers. More...
struct  IVIDEO1_BufDesc
 Detailed buffer descriptor for video buffers. More...
struct  IVIDEO2_BufDesc
 Detailed buffer descriptor for video buffers. More...

Defines

#define IVIDEO2_MAX_IO_BUFFERS   20
 Maximum I/O Buffers.
#define IVIDEO_MAX_YUV_BUFFERS   3
 Max YUV buffers - one each for 'Y', 'U', and 'V'.
#define IVIDEO_MAX_NUM_PLANES   3
 Max YUV buffers - one each for 'Y', 'U', and 'V'.
#define IVIDEO_MAX_NUM_METADATA_PLANES   3

Typedefs

typedef struct IVIDEO_BufDesc IVIDEO_BufDesc
 Buffer descriptor for video buffers.
typedef struct IVIDEO1_BufDescIn IVIDEO1_BufDescIn
 Buffer descriptor for input video buffers.
typedef struct IVIDEO1_BufDesc IVIDEO1_BufDesc
 Detailed buffer descriptor for video buffers.
typedef struct IVIDEO2_BufDesc IVIDEO2_BufDesc
 Detailed buffer descriptor for video buffers.

Enumerations

enum  IVIDEO_FrameSkip {
  IVIDEO_NO_SKIP = 0,
  IVIDEO_SKIP_P = 1,
  IVIDEO_SKIP_B = 2,
  IVIDEO_SKIP_I = 3,
  IVIDEO_SKIP_IP = 4,
  IVIDEO_SKIP_IB = 5,
  IVIDEO_SKIP_PB = 6,
  IVIDEO_SKIP_IPB = 7,
  IVIDEO_SKIP_IDR = 8,
  IVIDEO_SKIP_NONREFERENCE = 9,
  IVIDEO_SKIP_DEFAULT = IVIDEO_NO_SKIP
}
 

Video frame skip features for video decoder.

More...
enum  IVIDEO_FrameType {
  IVIDEO_NA_FRAME = -1,
  IVIDEO_I_FRAME = 0,
  IVIDEO_P_FRAME = 1,
  IVIDEO_B_FRAME = 2,
  IVIDEO_IDR_FRAME = 3,
  IVIDEO_II_FRAME = 4,
  IVIDEO_IP_FRAME = 5,
  IVIDEO_IB_FRAME = 6,
  IVIDEO_PI_FRAME = 7,
  IVIDEO_PP_FRAME = 8,
  IVIDEO_PB_FRAME = 9,
  IVIDEO_BI_FRAME = 10,
  IVIDEO_BP_FRAME = 11,
  IVIDEO_BB_FRAME = 12,
  IVIDEO_MBAFF_I_FRAME = 13,
  IVIDEO_MBAFF_P_FRAME = 14,
  IVIDEO_MBAFF_B_FRAME = 15,
  IVIDEO_MBAFF_IDR_FRAME = 16,
  IVIDEO_FRAMETYPE_DEFAULT = IVIDEO_I_FRAME
}
 

Video frame types.

More...
enum  IVIDEO_ContentType {
  IVIDEO_CONTENTTYPE_NA = -1,
  IVIDEO_PROGRESSIVE = 0,
  IVIDEO_PROGRESSIVE_FRAME = IVIDEO_PROGRESSIVE,
  IVIDEO_INTERLACED = 1,
  IVIDEO_INTERLACED_FRAME = IVIDEO_INTERLACED,
  IVIDEO_INTERLACED_TOPFIELD = 2,
  IVIDEO_INTERLACED_BOTTOMFIELD = 3,
  IVIDEO_CONTENTTYPE_DEFAULT = IVIDEO_PROGRESSIVE
}
 

Video content types.

More...
enum  IVIDEO_RateControlPreset {
  IVIDEO_LOW_DELAY = 1,
  IVIDEO_STORAGE = 2,
  IVIDEO_TWOPASS = 3,
  IVIDEO_NONE = 4,
  IVIDEO_USER_DEFINED = 5,
  IVIDEO_RATECONTROLPRESET_DEFAULT = IVIDEO_LOW_DELAY
}
 

Video rate control presets.

More...
enum  IVIDEO_SkipMode {
  IVIDEO_FRAME_ENCODED = 0,
  IVIDEO_FRAME_SKIPPED = 1,
  IVIDEO_SKIPMODE_DEFAULT = IVIDEO_FRAME_ENCODED
}
 

Video frame skipping modes.

More...
enum  IVIDEO_OutputFrameStatus {
  IVIDEO_FRAME_NOERROR = 0,
  IVIDEO_FRAME_NOTAVAILABLE = 1,
  IVIDEO_FRAME_ERROR = 2,
  IVIDEO_FRAME_OUTPUTSKIP = 3,
  IVIDEO_OUTPUTFRAMESTATUS_DEFAULT = IVIDEO_FRAME_NOERROR
}
 

Video output buffer status.

More...
enum  IVIDEO_PictureType {
  IVIDEO_NA_PICTURE = -1,
  IVIDEO_I_PICTURE = 0,
  IVIDEO_P_PICTURE = 1,
  IVIDEO_B_PICTURE = 2,
  IVIDEO_PICTURE_TYPE_DEFAULT = IVIDEO_I_PICTURE
}
 

Video Picture types.

More...
enum  IVIDEO_Format {
  IVIDEO_MPEG1 = 1,
  IVIDEO_MPEG2SP = 2,
  IVIDEO_MPEG2MP = 3,
  IVIDEO_MPEG2HP = 4,
  IVIDEO_MPEG4SP = 5,
  IVIDEO_MPEG4ASP = 6,
  IVIDEO_H264BP = 7,
  IVIDEO_H264MP = 8,
  IVIDEO_H264HP = 9,
  IVIDEO_VC1SP = 10,
  IVIDEO_VC1MP = 11,
  IVIDEO_VC1AP = 12,
  IVIDEO_H264RCDO = 13,
  IVIDEO_RV8 = 14,
  IVIDEO_RV9 = 15,
  IVIDEO_RV10 = IVIDEO_RV9,
  IVIDEO_ON2VP6 = 16,
  IVIDEO_ON2VP7 = 17,
  IVIDEO_AVS10 = 18,
  IVIDEO_SORENSONSPARK = 19,
  IVIDEO_H263_PROFILE0 = 20,
  IVIDEO_H263_PROFILE3 = 21,
  IVIDEO_H264SVC = 22,
  IVIDEO_MULTIVIEW = 23,
  IVIDEO_MJPEG = 24
}
 

Video Format types.

More...
enum  IVIDEO_VideoLayout {
  IVIDEO_FIELD_INTERLEAVED = 0,
  IVIDEO_FIELD_SEPARATED = 1,
  IVIDEO_TOP_ONLY = 2,
  IVIDEO_BOTTOM_ONLY = 3
}
 

Video buffer layout.

More...
enum  IVIDEO_OperatingMode {
  IVIDEO_DECODE_ONLY = 0,
  IVIDEO_ENCODE_ONLY = 1,
  IVIDEO_TRANSCODE_FRAMELEVEL = 2,
  IVIDEO_TRANSCODE_MBLEVEL = 3,
  IVIDEO_TRANSRATE_FRAMELEVEL = 4,
  IVIDEO_TRANSRATE_MBLEVEL = 5
}
 

Video coding mode of operation.

More...
enum  IVIDEO_BitRange {
  IVIDEO_YUVRANGE_FULL = 0,
  IVIDEO_YUVRANGE_ITU = 1
}
 

Video bit range.

More...
enum  IVIDEO_DataMode {
  IVIDEO_FIXEDLENGTH = 0,
  IVIDEO_SLICEMODE = 1,
  IVIDEO_NUMROWS = 2,
  IVIDEO_ENTIREFRAME = 3
}
 

input/output data mode

More...
enum  IVIDEO_ErrorInfoMode {
  IVIDEO_ERRORINFO_OFF = 0,
  IVIDEO_ERRORINFO_ON_INPUT = 1,
  IVIDEO_ERRORINFO_ON_OUTPUT = 2,
  IVIDEO_ERRORINFO_ON_BOTH = 3,
  IVIDEO_ERRORINFO_MODE_DEFAULT = IVIDEO_ERRORINFO_OFF
}
 

Configuration for providing/receiving packet error information.

More...
enum  IVIDEO_MetadataType {
  IVIDEO_METADATAPLANE_NONE = -1,
  IVIDEO_METADATAPLANE_MBINFO = 0,
  IVIDEO_METADATAPLANE_EINFO = 1,
  IVIDEO_METADATAPLANE_ALPHA = 2
}

Detailed Description

This is the XDM video interface shared between the various codecs.


Define Documentation

#define IVIDEO2_MAX_IO_BUFFERS   20

Maximum I/O Buffers.

See also:
IVIDDEC2_OutArgs
IVIDDEC3_OutArgs
IVIDENC2_OutArgs
#define IVIDEO_MAX_YUV_BUFFERS   3

Max YUV buffers - one each for 'Y', 'U', and 'V'.

#define IVIDEO_MAX_NUM_PLANES   3

Max YUV buffers - one each for 'Y', 'U', and 'V'.

Luma followed by chroma.

#define IVIDEO_MAX_NUM_METADATA_PLANES   3

MBINFO , packet error info and alpha planes.

See also:
IVIDEO_METADATAPLANE_MBINFO
IVIDEO_METADATAPLANE_EINFO
IVIDEO_METADATAPLANE_ALPHA

Typedef Documentation

Buffer descriptor for video buffers.

Buffer descriptor for input video buffers.

Detailed buffer descriptor for video buffers.

Detailed buffer descriptor for video buffers.


Enumeration Type Documentation

Video frame skip features for video decoder.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Enumerator:
IVIDEO_NO_SKIP 

Do not skip any frame types.

IVIDEO_SKIP_P 

Decode the P frame/skip frames internally, but do not copy the decoded output to the output buffers. This should be indicated by setting the output buffers to NULL.

Remarks:
For example, if a B frame is dependant on the previously decoded P frame, the B frame shall be decoded and displayed successfully. For this, the P frame needs to be decoded, but not copied to the output buffer.
IVIDEO_SKIP_B 

Skip B, BI frames. For B frames, the decoder will decode the frame bitstream, and return as soon as the frame type is decisively decoded. Internally, the algorithm will modify its state, so that subsequent decoding of other frames is possible.

IVIDEO_SKIP_I 

Skip intra coded frame.

IVIDEO_SKIP_IP 

Skip I and P frame/field(s).

IVIDEO_SKIP_IB 

Skip I and B frame/field(s).

IVIDEO_SKIP_PB 

Skip P and B frame/field(s).

IVIDEO_SKIP_IPB 

Skip I/P/B/BI frames.

IVIDEO_SKIP_IDR 

Skip IDR Frame.

IVIDEO_SKIP_NONREFERENCE 
Todo:
add documentation
IVIDEO_SKIP_DEFAULT 

Default settings.

Video frame types.

Remarks:
For the various IVIDEO_xy_FRAME values, this frame type is interlaced where both top and bottom fields are provided in a single frame. The first field is an "x" frame, the second field is "y" field.
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Enumerator:
IVIDEO_NA_FRAME 

Frame type not available.

IVIDEO_I_FRAME 

Intra coded frame.

IVIDEO_P_FRAME 

Forward inter coded frame.

IVIDEO_B_FRAME 

Bi-directional inter coded frame.

IVIDEO_IDR_FRAME 

Intra coded frame that can be used for refreshing video content.

IVIDEO_II_FRAME 

Interlaced Frame, both fields are I frames

IVIDEO_IP_FRAME 

Interlaced Frame, first field is an I frame, second field is a P frame.

IVIDEO_IB_FRAME 

Interlaced Frame, first field is an I frame, second field is a B frame.

IVIDEO_PI_FRAME 

Interlaced Frame, first field is a P frame, second field is a I frame.

IVIDEO_PP_FRAME 

Interlaced Frame, both fields are P frames.

IVIDEO_PB_FRAME 

Interlaced Frame, first field is a P frame, second field is a B frame.

IVIDEO_BI_FRAME 

Interlaced Frame, first field is a B frame, second field is an I frame.

IVIDEO_BP_FRAME 

Interlaced Frame, first field is a B frame, second field is a P frame.

IVIDEO_BB_FRAME 

Interlaced Frame, both fields are B frames.

IVIDEO_MBAFF_I_FRAME 

Intra coded MBAFF frame.

IVIDEO_MBAFF_P_FRAME 

Forward inter coded MBAFF frame.

IVIDEO_MBAFF_B_FRAME 

Bi-directional inter coded MBAFF frame.

IVIDEO_MBAFF_IDR_FRAME 

Intra coded MBAFF frame that can be used for refreshing video content.

IVIDEO_FRAMETYPE_DEFAULT 

Default setting.

Video content types.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Enumerator:
IVIDEO_CONTENTTYPE_NA 

Frame type is not available.

IVIDEO_PROGRESSIVE 

Progressive frame.

IVIDEO_PROGRESSIVE_FRAME 

Progressive Frame.

IVIDEO_INTERLACED 

Interlaced frame.

IVIDEO_INTERLACED_FRAME 

Interlaced frame.

IVIDEO_INTERLACED_TOPFIELD 

Interlaced picture, top field.

IVIDEO_INTERLACED_BOTTOMFIELD 

Interlaced picture, bottom field.

IVIDEO_CONTENTTYPE_DEFAULT 

Default setting.

Video rate control presets.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Enumerator:
IVIDEO_LOW_DELAY 

CBR rate control for video conferencing.

IVIDEO_STORAGE 

VBR rate control for local storage (DVD) recording.

IVIDEO_TWOPASS 

Two pass rate control for non real time applications.

IVIDEO_NONE 

No configurable video rate control mechanism.

IVIDEO_USER_DEFINED 

User defined configuration using extended parameters.

IVIDEO_RATECONTROLPRESET_DEFAULT 

Default setting.

Video frame skipping modes.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Enumerator:
IVIDEO_FRAME_ENCODED 

Input video frame successfully encoded.

IVIDEO_FRAME_SKIPPED 

Input video frame dropped. There is no encoded bitstream corresponding to the input frame.

IVIDEO_SKIPMODE_DEFAULT 

Default setting.

Video output buffer status.

Remarks:
Ownership of the buffers, either by application or algorithm, is conveyed via these values.
This reflects the status of ALL output buffers. For example, if video decoded output is in 4:2:0 format, all the 3 output buffers' status is described by this value. Similarly, for 4:2:2 formatted buffers, this value describes the single buffer's status.
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Enumerator:
IVIDEO_FRAME_NOERROR 

The output buffer is available.

IVIDEO_FRAME_NOTAVAILABLE 

The codec doesn't have any output buffers.

IVIDEO_FRAME_ERROR 

The output buffer is available and corrupted.

Remarks:
For example, if a bitstream is erroneous and partially decoded, a portion of the decoded image may be available for display. Another example is if the bitstream for a given frame decode may be decoded without error, but the previously decoded dependant frames weren't successfully decoded. This would result in an incorrectly decoded frame.
IVIDEO_FRAME_OUTPUTSKIP 

The video frame was skipped (i.e. not decoded).

IVIDEO_OUTPUTFRAMESTATUS_DEFAULT 

Default setting.

Video Picture types.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Enumerator:
IVIDEO_NA_PICTURE 

Frame type not available.

IVIDEO_I_PICTURE 

Intra coded picture.

IVIDEO_P_PICTURE 

Forward inter coded picture.

IVIDEO_B_PICTURE 

Bi-directional inter coded picture.

IVIDEO_PICTURE_TYPE_DEFAULT 

Default setting.

Video Format types.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Enumerator:
IVIDEO_MPEG1 

Video format is Mpeg1 stream

IVIDEO_MPEG2SP 

Video format is Mpeg2/H.262 stream, Simple Profile

IVIDEO_MPEG2MP 

Video format is Mpeg2/H.262 stream, Main Profile

IVIDEO_MPEG2HP 

Video format is Mpeg2/H.262 stream, High Profile

IVIDEO_MPEG4SP 

Video format is Mpeg4 stream, Simple Profile

IVIDEO_MPEG4ASP 

Video format is Mpeg4 stream, Advanced Simple Profile

IVIDEO_H264BP 

Video format is H.264 stream, Base Profile

IVIDEO_H264MP 

Video format is H.264 stream, Main Profile

IVIDEO_H264HP 

Video format is H.264 stream, High Profile

IVIDEO_VC1SP 

Video format is VC1/WMV9 stream, Simple Profile

IVIDEO_VC1MP 

Video format is VC1/WMV9 stream, Main Profile

IVIDEO_VC1AP 

Video format is VC1 stream, Advanced Profile

IVIDEO_H264RCDO 

Video format is H.264 stream, Fast profile/RCDO

IVIDEO_RV8 

Video format is Real Video 8 stream

IVIDEO_RV9 

Video format is Real Video 9 stream

IVIDEO_RV10 

Video format is Real Video 10 stream, same as RV9

IVIDEO_ON2VP6 

Video format is ON2, VP6.x

IVIDEO_ON2VP7 

Video format is ON2, VP7.x

IVIDEO_AVS10 

Video format is AVS 1.0

IVIDEO_SORENSONSPARK 

Video format is SorensonSpark V0/V1

IVIDEO_H263_PROFILE0 

Video format is H263 Base line profile

IVIDEO_H263_PROFILE3 

Video format is H263 and Annex IJKT

IVIDEO_H264SVC 

Video format is SVC

IVIDEO_MULTIVIEW 

Video format is Multiview coding

IVIDEO_MJPEG 

Video format is motion JPEG

Video buffer layout.

Todo:
Do we need a default value for this enum?
Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Enumerator:
IVIDEO_FIELD_INTERLEAVED 

Buffer layout is interleaved.

IVIDEO_FIELD_SEPARATED 

Buffer layout is field separated.

IVIDEO_TOP_ONLY 

Buffer contains only top field.

IVIDEO_BOTTOM_ONLY 

Buffer contains only bottom field.

Video coding mode of operation.

Todo:
Do we need a default value for this enum?
Todo:
Should "decode" and "encode" modes change to "process full frame"? For example, setting DECODE_ONLY for an encoder is wrong - can we make it impossible for codecs/apps to make this error?
Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Enumerator:
IVIDEO_DECODE_ONLY 

Decoding mode.

IVIDEO_ENCODE_ONLY 

Encoding mode.

IVIDEO_TRANSCODE_FRAMELEVEL 

Transcode mode of operation (encode/decode) which consumes/generates transcode information at the frame level.

IVIDEO_TRANSCODE_MBLEVEL 

Transcode mode of operation (encode/decode) which consumes/generates transcode information at the MB level.

IVIDEO_TRANSRATE_FRAMELEVEL 

Transrate mode of operation for encoder which consumes transrate information at the frame level.

IVIDEO_TRANSRATE_MBLEVEL 

Transrate mode of operation for encoder which consumes transrate information at the MB level.

Video bit range.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Todo:
Do we need a default value for this enum?
Enumerator:
IVIDEO_YUVRANGE_FULL 

Pixel range for YUV is 0-255.

IVIDEO_YUVRANGE_ITU 

Pixel range for YUV is as per ITU-T.

input/output data mode

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE
Todo:
Do we need a default value for this enum?
Todo:
Request from DM365 team to split IVIDEO_SLICEMODE into IVIDEO_SLICEMODE_BYTE and IVIDEO_SLICEMODE_NAL.
Enumerator:
IVIDEO_FIXEDLENGTH 

In terms of multiples of 2K

IVIDEO_SLICEMODE 

Slice mode

IVIDEO_NUMROWS 

Number of rows, each row is 16 lines of video

IVIDEO_ENTIREFRAME 

Processing of entire frame data

Configuration for providing/receiving packet error information.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
Enumerator:
IVIDEO_ERRORINFO_OFF 

Packet error information is unsupported.

IVIDEO_ERRORINFO_ON_INPUT 

Packet error information is supported for input data.

IVIDEO_ERRORINFO_ON_OUTPUT 

Packet error information is supported for output data.

IVIDEO_ERRORINFO_ON_BOTH 

Packet error information is supported for both input and output data.

IVIDEO_ERRORINFO_MODE_DEFAULT 

Default setting.

Enumerator:
IVIDEO_METADATAPLANE_NONE 

Used to indicate no metadata is requested or available.

IVIDEO_METADATAPLANE_MBINFO 

Offset into IVIDEO_MAX_NUM_METADATA_PLANES array for MB Info.

See also:
IVIDEO_MAX_NUM_METADATA_PLANES
IVIDEO_METADATAPLANE_EINFO 

Offset into IVIDEO_MAX_NUM_METADATA_PLANES array for Error Info.

See also:
IVIDEO_MAX_NUM_METADATA_PLANES
IVIDEO_METADATAPLANE_ALPHA 

Offset into IVIDEO_MAX_NUM_METADATA_PLANES array for Alpha Data.

See also:
IVIDEO_MAX_NUM_METADATA_PLANES
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated