![]() |
![]() |
This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
#include <ividanalytics.h>
Data Fields | |
XDAS_Int32 | size |
IVIDANALYTICS_Grid * | grid |
XDM_Date | date |
IVIDANALYTICS_Rule | rule |
This structure defines the algorithm parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
New overlay grid with analytics enable mask
Set the current time.
Rule associated with this command (if applicable).