![]() |
![]() |
Defines the creation time parameters for all ISPHENC instance objects. More...
#include <isphenc.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | frameSize |
XDAS_Int32 | compandingLaw |
XDAS_Int32 | packingType |
XDAS_Int32 | vadSelection |
Defines the creation time parameters for all ISPHENC instance objects.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details. Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Input frame size in bytes for sample based codecs.
Companding Law.
Packing Format Option (for codecs that support multiple packing formats - used for selection, 0, 1, 2...)
VAD A/VAD B, VAD 1/ VAD 2 etc