ISPHDEC_OutArgs Struct Reference
[XDM ISPHDEC Speech/Voice Decoder Interface]

Defines the run time output arguments for all ISPHDEC instance objects. More...

#include <isphdec.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 mode

Detailed Description

Defines the run time output arguments for all ISPHDEC instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
ISPHDEC_Fxns::process()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Speech voice mode. See ISPEECH_VoiceMode.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated