![]() |
![]() |
Data Structures | |
struct | IVIDANALYTICS_Grid |
Access modes used to declare how the algorithm accessed buffers. More... | |
struct | IVIDANALYTICS_Rule |
Analytics rule. More... | |
struct | IVIDANALYTICS_Obj |
This must be the first field of all IVIDANALYTICS instance objects. More... | |
struct | IVIDANALYTICS_Params |
Defines the creation time parameters for all IVIDANALYTICS instance objects. More... | |
struct | IVIDANALYTICS_DynamicParams |
This structure defines the algorithm parameters that can be modified after creation via control() calls. More... | |
struct | IVIDANALYTICS_InArgs |
Defines the input arguments for all IVIDANALYTICS instance process function. More... | |
struct | IVIDANALYTICS_Status |
Defines instance status parameters. More... | |
struct | IVIDANALYTICS_OutArgs |
Defines the run time output arguments for all IVIDANALYTICS instance objects. More... | |
struct | IVIDANALYTICS_Fxns |
Defines all of the operations on IVIDANALYTICS objects. More... | |
Defines | |
#define | IVIDANALYTICS_EOK XDM_EOK |
#define | IVIDANALYTICS_EFAIL XDM_EFAIL |
#define | IVIDANALYTICS_EUNSUPPORTED XDM_EUNSUPPORTED |
#define | IVIDANALYTICS_SETRULE XDM_CLASSCMDBASE |
Set a new rule. | |
#define | IVIDANALYTICS_CLEARRULE XDM_CLASSCMDBASE + 1 |
Clear a rule. | |
#define | IVIDANALYTICS_MAXTARGETS 128 |
Maximum targets that can be detected per process() call. | |
#define | IVIDANALYTICS_MAXEVENTS 128 |
Maximum number of events that can be detected per process() call. | |
Typedefs | |
typedef struct IVIDANALYTICS_Obj * | IVIDANALYTICS_Handle |
Opaque handle to an IVIDANALYTICS objects. | |
typedef IALG_Cmd | IVIDANALYTICS_Cmd |
Defines the control commands for the IVIDANALYTICS module. | |
Enumerations | |
enum | IVIDANALYTICS_AnalysisMask { IVIDANALYTICS_MOTIONDETECT = 0, IVIDANALYTICS_OBJECTTRACKING = 1, IVIDANALYTICS_USERBASE = 16 } |
Access modes used to declare how the algorithm accessed buffers. More... | |
enum | IVIDANALYTICS_ObjectType { IVIDANALYTICS_OBJECTTYPE_VEHICLE = 0, IVIDANALYTICS_OBJECTTYPE_HUMAN = 1, IVIDANALYTICS_OBJECTTYPE_USERBASE = 256 } |
Types of objects. More... | |
enum | IVIDANALYTICS_ActionType { IVIDANALYTICS_ACTIONTYPE_LOITER = 0, IVIDANALYTICS_ACTIONTYPE_ENTER = 1, IVIDANALYTICS_ACTIONTYPE_EXIT = 2, IVIDANALYTICS_ACTIONTYPE_APPEAR = 3, IVIDANALYTICS_ACTIONTYPE_DISAPPEAR = 4, IVIDANALYTICS_ACTIONTYPE_CROSSL2R = 5, IVIDANALYTICS_ACTIONTYPE_CROSSR2L = 6, IVIDANALYTICS_ACTIONTYPE_CROSSU2D = 7, IVIDANALYTICS_ACTIONTYPE_CROSSD2U = 8, IVIDANALYTICS_ACTIONTYPE_USERBASE = 256 } |
Types of objects. More... | |
enum | IVIDANALYTICS_ViewState { IVIDANALYTICS_VIEWSTATE_BAD = 0, IVIDANALYTICS_VIEWSTATE_GOOD = 1 } |
View state of the analytics engine. More... |
This is the XDM Beta Video Analytics Interface.
#define IVIDANALYTICS_EOK XDM_EOK |
Success.
#define IVIDANALYTICS_EFAIL XDM_EFAIL |
General failure.
#define IVIDANALYTICS_EUNSUPPORTED XDM_EUNSUPPORTED |
Request is unsupported.
#define IVIDANALYTICS_SETRULE XDM_CLASSCMDBASE |
Set a new rule.
#define IVIDANALYTICS_CLEARRULE XDM_CLASSCMDBASE + 1 |
Clear a rule.
#define IVIDANALYTICS_MAXTARGETS 128 |
Maximum targets that can be detected per process() call.
#define IVIDANALYTICS_MAXEVENTS 128 |
Maximum number of events that can be detected per process() call.
typedef struct IVIDANALYTICS_Obj* IVIDANALYTICS_Handle |
Opaque handle to an IVIDANALYTICS objects.
typedef IALG_Cmd IVIDANALYTICS_Cmd |
Defines the control commands for the IVIDANALYTICS module.
Access modes used to declare how the algorithm accessed buffers.
Types of objects.
Types of objects.
View state of the analytics engine.