![]() |
![]() |
Defines | |
#define | TRACEUTIL_SUCCESS 0 |
#define | TRACEUTIL_FAILURE -1 |
Functions | |
Int | TraceUtil_start (String engineName) |
Begin using the TraceUtil module; create thread that periodically collects DSP trace. | |
Int | TraceUtil_stop (Void) |
Finish using the TraceUtil module, stop the collecting thread. |
#define TRACEUTIL_SUCCESS 0 |
Success.
#define TRACEUTIL_FAILURE -1 |
General system error.
Int TraceUtil_start | ( | String | engineName | ) |
Begin using the TraceUtil module; create thread that periodically collects DSP trace.
[in] | engineName | Name of the engine. This uses the same name conventions as Engine_open()'s name. |
TRACEUTIL_SUCCESS | Success. | |
TRACEUTIL_FAILURE | Failed to initialize the necessary tracing resources. |
Int TraceUtil_stop | ( | Void | ) |
Finish using the TraceUtil module, stop the collecting thread.
TRACEUTIL_SUCCESS | Success. | |
TRACEUTIL_FAILURE | Failed to free the necessary tracing resources. |