![]() |
![]() |
#define LAD_MAXLENGTHIMAGENAME 512 |
max size for DSP server path name
#define LAD_MAXLENGTHCONFIGNAME 32 |
max size Link config name
typedef Uns LAD_ClientHandle |
handle for communicating with LAD
enum LAD_Status |
enum LAD_DspState |
LAD_Status LAD_connect | ( | LAD_ClientHandle * | handle | ) |
Connect to LAD.
[out] | handle | The new client handle, as defined by LAD. |
LAD_SUCCESS | Success. | |
LAD_INVALIDARG | The handle pointer is NULL. | |
LAD_ACCESSDENIED | Returned on either of two conditions: this client is trying to establish a second active connection to LAD, and the request is denied; or, the total number of simultaneous client connections to LAD has been reached, and no more client handles are available. | |
LAD_IOFAILURE | Unable to communicate with LAD, due to an OS-level I/O failure. A full system reboot may be necessary. | |
LAD_INVALIDVERSION | Unable to communicate with LAD due to a mismatch in the communication protocol between the client and LAD. |
LAD_Status LAD_disconnect | ( | LAD_ClientHandle | handle | ) |
Disconnect from LAD.
[in] | handle | The client handle, as returned from previous call to LAD_connect(). |
LAD_SUCCESS | Success. | |
LAD_INVALIDARG | Invalid client handle. | |
LAD_NOTCONNECTED | Not currently connected to LAD. | |
LAD_STILLRUNNING | This client has previously started the DSP via a call to LAD_startupDsp, and must call LAD_releaseDsp before attempting to disconnect from LAD. | |
LAD_IOFAILURE | Unable to communicate with LAD, due to an OS-level I/O failure, or timeout. A full system reboot may be necessary. |
LAD_Status LAD_getDspStatus | ( | LAD_ClientHandle | handle, | |
Int | cpuId, | |||
LAD_DspStatus * | statusInfo | |||
) |
Get DSP status from LAD.
[in] | handle | The client handle, as returned from previous call to LAD_connect(). |
[in] | cpuId | The CPU for which status is to be returned. |
[out] | statusInfo | The DSP status structure to be filled in by LAD. |
LAD_SUCCESS | Success. | |
LAD_INVALIDARG | Invalid handle or statusInfo pointer. | |
LAD_NOTCONNECTED | Not currently connected to LAD. | |
LAD_FAILURE | Failure occurred when querying DSP state. | |
LAD_IOFAILURE | Unable to communicate with LAD, due to an OS-level I/O failure. A full system reboot may be necessary. |
LAD_Status LAD_releaseDsp | ( | LAD_ClientHandle | handle | ) |
Release control of the DSP. This call is only appropriate if the client previously made a successful call to LAD_startupDsp().
[in] | handle | The client handle, as returned from LAD_connect(). |
LAD_SUCCESS | Success, the DSP has been stopped. | |
LAD_STILLRUNNING | Success, the DSP is continuing to run due to other client connection(s). | |
LAD_INVALIDARG | Invalid client handle. | |
LAD_NOTCONNECTED | Not currently connected to LAD. | |
LAD_ACCESSDENIED | This client not allowed to stop the DSP because it didn't successfully start it. | |
LAD_FAILURE | LAD was unable to stop and detach from the DSP. | |
LAD_IOFAILURE | Unable to communicate with LAD, due to an OS-level I/O failure. A full system reboot may be necessary. |
LAD_Status LAD_startupDsp | ( | LAD_ClientHandle | handle, | |
Int | cpuId, | |||
String | linkConfigName, | |||
String | imageName | |||
) |
Load and start the DSP running.
[in] | handle | The client handle, as returned from LAD_connect(). |
[in] | cpuId | The DSP to be loaded and started. |
[in] | linkConfigName | The pre-defined Link configuration known to LAD. |
[in] | imageName | The name to the DSP server executable. If an environment variable named "LAD_SERVERPATH" is defined, indicting a repository for server executable files, then this path will be pre-pended to the imageName to form the location of the DSP executable file; if "LAD_SERVERPATH" is not defined, then imageName will be considered to be the full path name of the DSP executable file. |
LAD_SUCCESS | Success, DSP has been started. | |
LAD_ALREADYRUNNING | Success, the DSP was already running with the same Link configuration and server executable. | |
LAD_INVALIDARG | Invalid client handle, cpuId, or linkConfigName. | |
LAD_NOTCONNECTED | Not currently connected to LAD. | |
LAD_ACCESSDENIED | LAD has refused the request because the DSP is already running, with a linkConfigName or imageName that does not match this request. | |
LAD_FAILURE | LAD is unable to start the DSP. | |
LAD_IOFAILURE | Unable to communicate with LAD, due to an OS-level I/O failure. A full system reboot may be necessary. |