IVIDTRANSCODE_Params Struct Reference
[XDM IVIDTRANSCODE Video Transcoder Interface]

Defines the creation time parameters for all IVIDTRANSCODE instance objects. More...

#include <ividtranscode.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 numOutputStreams
XDAS_Int32 formatInput
XDAS_Int32 formatOutput [2]
XDAS_Int32 maxHeightInput
XDAS_Int32 maxWidthInput
XDAS_Int32 maxFrameRateInput
XDAS_Int32 maxBitRateInput
XDAS_Int32 maxHeightOutput [2]
XDAS_Int32 maxWidthOutput [2]
XDAS_Int32 maxFrameRateOutput [2]
XDAS_Int32 maxBitRateOutput [2]
XDAS_Int32 dataEndianness

Detailed Description

Defines the creation time parameters for all IVIDTRANSCODE instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Number of output transcoded streams This allows the possibility of generating more than one transcoded bit-streams from a single incoming bit-stream.

Video Format types.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE

See also:
IVIDEO_Format
Remarks:
This is the video standard of incoming bit stream.

Video Format types.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
This enumeration defines a base set of values. Algorithms which require proprietary enumeration values may define them - much like extended fields in base structures. These extended enums should be between XDM_CUSTOMENUMBASE and 0x7FFF.
See also:
XDM_CUSTOMENUMBASE

See also:
IVIDEO_Format
Remarks:
This array indicates the video standard for each of the transcoded bit streams.

Maximum video height in pixels.

Maximum video width in pixels.

Maximum frame rate in fps * 1000. For example, if max frame rate is 30 frames per second, set this field to 30000.

Maximum bit rate, bits per second. For example, if bit rate is 10 Mbps, set this field to 10000000

Maximum output video height in pixels for each of the transcoded output.

Maximum output video width in pixels for each of the transcoded output.

Maximum frame rate in fps * 1000. for each out the output bitstreams For example, if max frame rate is 30 frames per second, set this field to 30000.

Maximum bit rate, in bits per second for each of the transcoded bitstreams. For example, if bit rate is 10 Mbps, set this field to 10000000

Endianness of output data.

See also:
XDM_DataFormat

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated