![]() |
![]() |
Defines the input arguments for all ISPHENC1 instance process function. More...
#include <isphenc1.h>
Data Fields | |
XDAS_Int16 | size |
XDAS_Int16 | nullTrafficChannel |
XDM1_SingleBufDesc | data |
Defines the input arguments for all ISPHENC1 instance process function.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details. Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Enable/disable the null traffic channel.
Raw data input for data transmission.