This structure defines the codec parameters that can be modified after creation via control() calls. More...
#include <iimgdec1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numAU |
XDAS_Int32 | decodeHeader |
XDAS_Int32 | displayWidth |
This structure defines the codec parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Number of Access unit to decode. Set to XDM_DEFAULT to decode the entire frame.
Decode entire access unit or only header.
Pitch. If set to zero, imageWidth is used; else, this field (assuming it's larger than imageWidth) is used.