module ti.sysbios.hal.MemProtect |
 |
 |
 |
Memory protection manager
SYS/BIOS Memory Protection Extensions (MPE) add memory protection capability
to the SYS/BIOS kernel. With this extension enabled
(see
BIOS.mpeEnabled), an application can
restrict the memory and peripherals a Task can access, thereby creating a
sandbox. The access restricted tasks run in unprivileged mode and are
therefore also restricted in terms of the type of CPU instructions they can
execute. For example, an access restricted or unprivileged task cannot
disable interrupts directly.
[
more ... ]
#include <ti/sysbios/hal/MemProtect.h>
Functions common to all target modules |
|
|
DETAILS
SYS/BIOS Memory Protection Extensions (MPE) add memory protection capability
to the SYS/BIOS kernel. With this extension enabled
(see
BIOS.mpeEnabled), an application can
restrict the memory and peripherals a Task can access, thereby creating a
sandbox. The access restricted tasks run in unprivileged mode and are
therefore also restricted in terms of the type of CPU instructions they can
execute. For example, an access restricted or unprivileged task cannot
disable interrupts directly.
SYS/BIOS MPE can be used to enhance the security of applications by
compartmentalizing the application into mutually isolated tasks. In the
simplest configuration, the security critical portions of the application
can be moved to privileged tasks and the rest of the application can be run
as unprivileged tasks. In a more advanced configuration, multiple mutually
isolated tasks may be used to compartmentalize the application at a finer
level of granularity.
SYS/BIOS MPE introduces the notion of execution domains. A Domain is a
protected environment for the kernel and tasks to execute within and has
an Access Control List (ACL) that is defined at the time of creating the
domain. The kernel and privileged tasks execute in a special domain that
allows them to access the entire address space. User Task domains are more
restrictive and allow a user task to only access memory regions explicitly
owned by the domain or memory regions that are public and accessible to all
domains.
A domain can be created in main() or a privileged task only. A User Task is
assigned to an existing domain at the time of its creation. A User Task may
create more threads which inherit its domain. A User Task cannot assign any
other domain to the tasks it creates.
This module contains APIs used to create and/or construct domains at
runtime.
Calling Context
Function | Hwi | Swi |
Task | Main | Startup |
MemProtect_constructDomain | N | N |
Y | Y | N |
MemProtect_destructDomain | N | N |
Y | Y | N |
Definitions:
- Hwi: API is callable from a Hwi thread.
- Swi: API is callable from a Swi thread.
- Task: API is callable from a Task thread.
- Main: API is callable during any of these phases:
- In your module startup after this module is started
(e.g. Hwi_Module_startupDone() returns TRUE).
- During xdc.runtime.Startup.lastFxns.
- During main().
- During BIOS.startupFxns.
- Startup: API is callable during any of these phases:
- During xdc.runtime.Startup.firstFxns.
|
C SYNOPSIS
#include <ti/sysbios/hal/MemProtect.h>
Macros
// Access Privilege Flags
#define MemProtect_USER_READ
#define MemProtect_USER_WRITE
#define MemProtect_USER_EXEC
#define MemProtect_PRIV_READ
#define MemProtect_PRIV_WRITE
#define MemProtect_PRIV_EXEC
// Memory Type Flags
#define MemProtect_DEVICE
#define MemProtect_DEVICE_UNBUFFERED
#define MemProtect_NONCACHEABLE
#define MemProtect_WRITEBACK
#define MemProtect_WRITETHROUGH
#define MemProtect_WRITEALLOCATE
#define MemProtect_SHAREABLE
// ACL Helper Macros
#define MemProtect_NUM_KERNEL_ACL_ENTRIES
#define MemProtect_NUM_USER_ACL_ENTRIES
#define MemProtect_NUM_ACL_ENTRIES
Typedefs
typedef struct MemProtect_Acl {
Ptr baseAddress;
SizeT length;
UInt32 flags;
} MemProtect_Acl;
typedef MemProtect_Struct *MemProtect_Handle;
Functions
Int MemProtect_constructDomain(MemProtect_Struct *obj, struct MemProtect_Acl *acl, UInt16 aclLength)
Int MemProtect_destructDomain(MemProtect_Struct *obj)
MEMPROTECT FUNCTIONS
MemProtect_constructDomain()
Construct an execution domain with given access control permissions
Int MemProtect_constructDomain(MemProtect_Struct *obj, struct MemProtect_Acl *acl, UInt16 aclLength)
ARGUMENTS
obj - Pointer to a statically created MemProtect object of type MemProtect_Struct
acl - Pointer to an array of ACL entries. ACL entries are of type MemProtect_Acl
aclLength - Length of ACL entry array
RETURNS
Returns 0 on success. A negative return value indicates an error occurred.
DETAILS
This function constructs an execution domain with the access permissions
specified by the Access Control List (ACL) passed to it.
MemProtect_destructDomain()
Destruct execution domain
Int MemProtect_destructDomain(MemProtect_Struct *obj)
ARGUMENTS
obj - Pointer to a statically created MemProtect object of type MemProtect_Struct
RETURNS
Returns 0 on success. A negative return value indicates an error occurred.
DETAILS
This function destructs a previously constructed execution domain.
Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool MemProtect_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool MemProtect_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 MemProtect_Module_getMask();
// Returns the diagnostics mask for this module
Void MemProtect_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var MemProtect = xdc.useModule('ti.sysbios.hal.MemProtect');
module-wide config parameters
generated on Tue, 28 Jul 2020 21:22:41 GMT