enum ICache.Type |
![](../../../Arrow_up.png) |
Lists of bitmask cache types
enum Type {
Type_L1P,
// Level 1 Program cache
Type_L1D,
// Level 1 Data cache
Type_L1,
// Level 1 caches
Type_L2P,
// Level 2 Program cache
Type_L2D,
// Level 2 Data cache
Type_L2,
// Level 2 caches
Type_ALLP,
// All Program caches
Type_ALLD,
// All Data caches
Type_ALL
// All caches
};
config ICache.enableCache // module-wide |
![](../../../Arrow_up.png) |
Enable supported caches during startup
config Bool enableCache = true;
DETAILS
Not implemented by all architectures. Refer to specific
architecture Cache module for details.
metaonly config ICache.common$ // module-wide |
![](../../../Arrow_up.png) |
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
ICache.disable() // module-wide |
![](../../../Arrow_up.png) |
Disables the 'type' cache(s)
Void disable(Bits16 type);
ARGUMENTS
type
bit mask of Cache type
ICache.enable() // module-wide |
![](../../../Arrow_up.png) |
Enables all cache(s)
Void enable(Bits16 type);
ARGUMENTS
type
bit mask of Cache type
ICache.inv() // module-wide |
![](../../../Arrow_up.png) |
Invalidate the range of memory within the specified starting
address and byte count. The range of addresses operated on
gets quantized to whole cache lines in each cache. All lines
in range are invalidated for all the 'type' caches
Void inv(Ptr blockPtr, SizeT byteCnt, Bits16 type, Bool wait);
ARGUMENTS
blockPtr
start address of range to be invalidated
byteCnt
number of bytes to be invalidated
type
bit mask of Cache type
wait
wait until the operation is completed
ICache.wait() // module-wide |
![](../../../Arrow_up.png) |
Wait for a previous cache operation to complete
DETAILS
Wait for the cache wb/wbInv/inv operation to complete. A cache
operation is not truly complete until it has worked its way
through all buffering and all memory writes have landed in the
source memory.
ICache.wb() // module-wide |
![](../../../Arrow_up.png) |
Writes back a range of memory from all cache(s)
Void wb(Ptr blockPtr, SizeT byteCnt, Bits16 type, Bool wait);
ARGUMENTS
blockPtr
start address of range to be invalidated
byteCnt
number of bytes to be invalidated
type
bit mask of Cache type
wait
wait until the operation is completed
DETAILS
Writes back the range of memory within the specified starting
address and byte count. The range of addresses operated on
gets quantized to whole cache lines in each cache. All lines
within the range are left valid in the 'type' caches and the data
within the range will be written back to the source memory.
ICache.wbAll() // module-wide |
![](../../../Arrow_up.png) |
Write back all caches
DETAILS
Perform a global write back. There is no effect on program cache.
All data cache lines are left valid.
ICache.wbInv() // module-wide |
![](../../../Arrow_up.png) |
Writes back and invalidates the range of memory within the
specified starting address and byte count. The range of
addresses operated on gets quantized to whole cache lines in
each cache. All lines within the range are written back to the
source memory and then invalidated for all 'type' caches
Void wbInv(Ptr blockPtr, SizeT byteCnt, Bits16 type, Bool wait);
ARGUMENTS
blockPtr
start address of range to be invalidated
byteCnt
number of bytes to be invalidated
type
bit mask of Cache type
wait
wait until the operation is completed
ICache.wbInvAll() // module-wide |
![](../../../Arrow_up.png) |
Write back invalidate all caches
DETAILS
Performs a global write back and invalidate. All cache lines
are written out to physical memory and then invalidated.