Additional ARM device-specific APIs are also provided.
const Hwi_NUM_INTERRUPTS |
![](../../../../../../Arrow_up.png) |
intcps supports 128 interrupts
#define Hwi_NUM_INTERRUPTS (Int)128
enum Hwi_MaskingOption |
![](../../../../../../Arrow_up.png) |
Shorthand interrupt masking options
typedef enum Hwi_MaskingOption {
Hwi_MaskingOption_NONE,
Hwi_MaskingOption_ALL,
Hwi_MaskingOption_SELF,
Hwi_MaskingOption_BITMASK,
Hwi_MaskingOption_LOWER
} Hwi_MaskingOption;
VALUES
MaskingOption_NONE
No interrupts are disabled
MaskingOption_ALL
All interrupts are disabled
MaskingOption_SELF
Only this interrupt is disabled
MaskingOption_BITMASK
User supplies interrupt enable masks
MaskingOption_LOWER
All current and lower priority
interrupts are disabled.
Only a few targets/devices truly
support this masking option. For those
that don't, this setting is treated
the same as MaskingOption_SELF.
enum Hwi_Type |
![](../../../../../../Arrow_up.png) |
Interrupt type. IRQ or FIQ
typedef enum Hwi_Type {
Hwi_Type_IRQ,
// IRQ interrupt
Hwi_Type_FIQ
// FIQ interrupt
} Hwi_Type;
typedef Hwi_FuncPtr |
![](../../../../../../Arrow_up.png) |
Hwi create function type definition
typedef Void (*Hwi_FuncPtr)(UArg);
typedef Hwi_Irp |
![](../../../../../../Arrow_up.png) |
Interrupt Return Pointer
DETAILS
This is the address of the interrupted instruction.
typedef Hwi_VectorFuncPtr |
![](../../../../../../Arrow_up.png) |
Hwi vector function type definition
typedef Void (*Hwi_VectorFuncPtr)(Void);
struct Hwi_HookSet |
![](../../../../../../Arrow_up.png) |
Hwi hook set type definition
typedef struct Hwi_HookSet {
Void (*registerFxn)(Int);
} Hwi_HookSet;
DETAILS
The functions that make up a hookSet have certain restrictions. They
cannot call any Hwi instance functions other than Hwi_getHookContext()
and Hwi_setHookContext(). For all practical purposes, they should treat
the Hwi_Handle passed to these functions as an opaque handle.
struct Hwi_Intc |
![](../../../../../../Arrow_up.png) |
Interrupt Controller. Symbol "Hwi_intc" is physical device
typedef struct Hwi_Intc {
UInt32 REVISION;
// 0x00 Config Register
UInt32 hole0[3];
// 0x04-0x0C
UInt32 SYSCONFIG;
// 0x10 Config Register
UInt32 SYSSTATUS;
// 0x14 Status Register
UInt32 hole1[10];
// 0x18-0x3c
UInt32 SIR_IRQ;
// 0x40 Source IRQ Register
UInt32 SIR_FIQ;
// 0x44 Source FIQ Register
UInt32 CONTROL;
// 0x48 Control Register
UInt32 PROTECTION;
// 0x4C Protection Register
UInt32 IDLE;
// 0x50 Idle Register
UInt32 hole2[3];
// 0x54-0x5C
UInt32 IRQ_PRIORITY;
// 0x60 IRQ Priority Register
UInt32 FIQ_PRIORITY;
// 0x64 IRQ Priority Register
UInt32 THRESHOLD;
// 0x68 Threshold Register
UInt32 hole3[5];
// 0x6C-0x7C
UInt32 ITR0;
// 0x80 Interrupt Input Register
UInt32 MIR0;
// 0x84 Mask Interrupt Register
UInt32 MIR_CLEAR0;
// 0x88 MIR Clear Register
UInt32 MIR_SET0;
// 0x8C MIR Set Register
UInt32 ISR_SET0;
// 0x90 Interrupt Set Register
UInt32 ISR_CLEAR0;
// 0x94 Interrupt Clear Register
UInt32 PENDING_IRQ0;
// 0x98 Pending IRQ Register
UInt32 PENDING_FIQ0;
// 0x9C Pending FIQ Register
UInt32 ITR1;
// 0xA0 Interrupt Input Register
UInt32 MIR1;
// 0xA4 Mask Interrupt Register
UInt32 MIR_CLEAR1;
// 0xA8 MIR Clear Register
UInt32 MIR_SET1;
// 0xAC MIR Set Register
UInt32 ISR_SET1;
// 0xB0 Interrupt Set Register
UInt32 ISR_CLEAR1;
// 0xB4 Interrupt Clear Register
UInt32 PENDING_IRQ1;
// 0xB8 Pending IRQ Register
UInt32 PENDING_FIQ1;
// 0xBC Pending FIQ Register
UInt32 ITR2;
// 0xC0 Interrupt Input Register
UInt32 MIR2;
// 0xC4 Mask Interrupt Register
UInt32 MIR_CLEAR2;
// 0xC8 MIR Clear Register
UInt32 MIR_SET2;
// 0xCC MIR Set Register
UInt32 ISR_SET2;
// 0xD0 Interrupt Set Register
UInt32 ISR_CLEAR2;
// 0xD4 Interrupt Clear Register
UInt32 PENDING_IRQ2;
// 0xD8 Pending IRQ Register
UInt32 PENDING_FIQ2;
// 0xDC Pending FIQ Register
UInt32 ITR3;
// 0xE0 Interrupt Input Register
UInt32 MIR3;
// 0xE4 Mask Interrupt Register
UInt32 MIR_CLEAR3;
// 0xE8 MIR Clear Register
UInt32 MIR_SET3;
// 0xEC MIR Set Register
UInt32 ISR_SET3;
// 0xF0 Interrupt Set Register
UInt32 ISR_CLEAR3;
// 0xF4 Interrupt Clear Register
UInt32 PENDING_IRQ3;
// 0xF8 Pending IRQ Register
UInt32 PENDING_FIQ3;
// 0xFC Pending FIQ Register
UInt32 ILR[128];
// 0x100 thru 0x2FC
} Hwi_Intc;
struct Hwi_StackInfo |
![](../../../../../../Arrow_up.png) |
Structure contains Hwi stack usage info
typedef struct Hwi_StackInfo {
SizeT hwiStackPeak;
SizeT hwiStackSize;
Ptr hwiStackBase;
} Hwi_StackInfo;
DETAILS
Used by getStackInfo() and viewGetStackInfo() functions
config Hwi_E_alreadyDefined // module-wide |
![](../../../../../../Arrow_up.png) |
Error raised when an attempt is made to create a Hwi
that has already been created
extern const Error_Id Hwi_E_alreadyDefined;
config Hwi_E_badIntNum // module-wide |
![](../../../../../../Arrow_up.png) |
Error raised if an attempt is made to create a Hwi
with an interrupt number greater than NUM_INTERRUPTS - 1
config Hwi_E_handleNotFound // module-wide |
![](../../../../../../Arrow_up.png) |
Error raised when Hwi handle referenced in Hwi_delete()
is not found in the Hwi dispatch table
extern const Error_Id Hwi_E_handleNotFound;
config Hwi_E_invalidPriority // module-wide |
![](../../../../../../Arrow_up.png) |
Error raised if an attempt is made to create a Hwi
with a priority of 0
extern const Error_Id Hwi_E_invalidPriority;
config Hwi_E_undefined // module-wide |
![](../../../../../../Arrow_up.png) |
Error raised when an undefined interrupt has fired
config Hwi_LD_end // module-wide |
![](../../../../../../Arrow_up.png) |
Issued just after return from Hwi function (with interrupts disabled)
config Hwi_LM_begin // module-wide |
![](../../../../../../Arrow_up.png) |
Issued just prior to Hwi function invocation (with interrupts disabled)
config Hwi_NUM_PRIORITIES // module-wide |
![](../../../../../../Arrow_up.png) |
The device-specific number of priorities supported
extern const Int Hwi_NUM_PRIORITIES;
DETAILS
The actual number supported is device specific and provided by
the catalog device specification.
config Hwi_dispatcherAutoNestingSupport // module-wide |
![](../../../../../../Arrow_up.png) |
Include interrupt nesting logic in interrupt dispatcher?
extern const Bool Hwi_dispatcherAutoNestingSupport;
DETAILS
Default is true.
This option provides the user with the ability to optimize
interrupt dispatcher performance when support for interrupt
nesting is not required.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that manipulates interrupt mask
registers and enables and disables interrupts before and
after invoking the user's Hwi function.
Set this parameter to false if you don't need interrupts
enabled during the execution of your Hwi functions.
config Hwi_dispatcherIrpTrackingSupport // module-wide |
![](../../../../../../Arrow_up.png) |
Controls whether the
dispatcher retains the interrupted thread's return address
extern const Bool Hwi_dispatcherIrpTrackingSupport;
DETAILS
This option is enabled by default.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that keeps track of the interrupt's
return address and provide a small savings in interrupt latency.
The application can get an interrupt's most recent return
address using the
getIrp API.
config Hwi_dispatcherSwiSupport // module-wide |
![](../../../../../../Arrow_up.png) |
Include Swi scheduling logic in interrupt dispatcher?
extern const Bool Hwi_dispatcherSwiSupport;
DETAILS
Default is inherited from
BIOS.swiEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that Swis
will not be posted from any of their Hwi threads.
WARNING
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Swi scheduler
prior to returning from an interrupt.
With this setting, Swis MUST NOT be posted from Hwi functions!
config Hwi_dispatcherTaskSupport // module-wide |
![](../../../../../../Arrow_up.png) |
Include Task scheduling logic in interrupt dispatcher?
extern const Bool Hwi_dispatcherTaskSupport;
DETAILS
Default is inherited from
BIOS.taskEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that no
Task scheduling APIs (ie
Semaphore_post()) will be executed from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Task scheduler
prior to returning from an interrupt.
config Hwi_fiqStack // module-wide |
![](../../../../../../Arrow_up.png) |
FIQ stack pointer. Default = null.
(Indicates that stack is to be created internally)
extern const Ptr Hwi_fiqStack;
config Hwi_mir0Mask // module-wide |
![](../../../../../../Arrow_up.png) |
Initial MIR0 Interrupt Mask. Default is 0xffffffff
extern const Bits32 Hwi_mir0Mask;
config Hwi_mir1Mask // module-wide |
![](../../../../../../Arrow_up.png) |
Initial MIR1 Interrupt Mask. Default is 0xffffffff
extern const Bits32 Hwi_mir1Mask;
config Hwi_mir2Mask // module-wide |
![](../../../../../../Arrow_up.png) |
Initial MIR2 Interrupt Mask. Default is 0xffffffff
extern const Bits32 Hwi_mir2Mask;
config Hwi_mir3Mask // module-wide |
![](../../../../../../Arrow_up.png) |
Initial MIR3 Interrupt Mask. Default is 0xffffffff
extern const Bits32 Hwi_mir3Mask;
extern Hwi_intc |
![](../../../../../../Arrow_up.png) |
Hwi_Intc Hwi_intc; // linked as extern ti_sysbios_family_arm_a8_intcps_Hwi_intc
Hwi_clearInterrupt() // module-wide |
![](../../../../../../Arrow_up.png) |
Clear a specific interrupt
Void Hwi_clearInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to clear
DETAILS
Clears a specific interrupt's pending status.
The implementation is family-specific.
Hwi_clearPostedInterrupt() // module-wide |
![](../../../../../../Arrow_up.png) |
Clear a specific software generated interrupt
triggered by Hwi_post(intNum);
Void Hwi_clearPostedInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to clear
Hwi_disable() // module-wide |
![](../../../../../../Arrow_up.png) |
Globally disable interrupts
macro UInt Hwi_disable();
RETURNS
opaque key for use by Hwi_restore()
DETAILS
Hwi_disable globally disables hardware interrupts and returns an
opaque key indicating whether interrupts were globally enabled or
disabled on entry to Hwi_disable().
The actual value of the key is target/device specific and is meant
to be passed to Hwi_restore().
Call Hwi_disable before a portion of a function that needs
to run without interruption. When critical processing is complete, call
Hwi_restore or Hwi_enable to reenable hardware interrupts.
Servicing of interrupts that occur while interrupts are disabled is
postponed until interrupts are reenabled. However, if the same type
of interrupt occurs several times while interrupts are disabled,
the interrupt's function is executed only once when interrupts are
reenabled.
A context switch can occur when calling Hwi_enable or Hwi_restore if
an enabled interrupt occurred while interrupts are disabled.
Hwi_disable may be called from main(). However, since Hwi interrupts
are already disabled in main(), such a call has no effect.
CONSTRAINTS
If a Task switching API such as
Semaphore_pend(),
Semaphore_post(),
Task_sleep(), or
Task_yield()
is invoked which results in a context switch while
interrupts are disabled, an embedded call to
Hwi_enable occurs
on the way to the new thread context which unconditionally re-enables
interrupts. Interrupts will remain enabled until a subsequent
Hwi_disable
invocation.
Swis always run with interrupts enabled.
See
Swi_post() for a discussion Swis and
interrupts.
Hwi_disableFIQ() // module-wide |
![](../../../../../../Arrow_up.png) |
Disable FIQ interrupts
RETURNS
previous FIQ interrupt enable/disable state
Hwi_disableIRQ() // module-wide |
![](../../../../../../Arrow_up.png) |
Disable IRQ interrupts
RETURNS
previous IRQ interrupt enable/disable state
Hwi_disableInterrupt() // module-wide |
![](../../../../../../Arrow_up.png) |
Disable a specific interrupt
UInt Hwi_disableInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to disable
RETURNS
key to restore previous enable/disable state
DETAILS
Disable a specific interrupt identified by an interrupt number.
Hwi_disableMIR0() // module-wide |
![](../../../../../../Arrow_up.png) |
Disable specific interrupts
Bits32 Hwi_disableMIR0(Bits32 mask);
ARGUMENTS
mask
bitmask of interrupts to disable
RETURNS
previous MIR0 settings bitmask
DETAILS
Disables specific interrupts by setting the bits specified by
mask in the Mask Interrupts Register (MIR).
Hwi_disableMIR1() // module-wide |
![](../../../../../../Arrow_up.png) |
Bits32 Hwi_disableMIR1(Bits32 mask);
Hwi_disableMIR2() // module-wide |
![](../../../../../../Arrow_up.png) |
Bits32 Hwi_disableMIR2(Bits32 mask);
Hwi_disableMIR3() // module-wide |
![](../../../../../../Arrow_up.png) |
Bits32 Hwi_disableMIR3(Bits32 mask);
Hwi_enable() // module-wide |
![](../../../../../../Arrow_up.png) |
Globally enable interrupts
RETURNS
opaque key for use by Hwi_restore()
DETAILS
Hwi_enable globally enables hardware interrupts and returns an
opaque key indicating whether interrupts were globally enabled or
disabled on entry to Hwi_enable().
The actual value of the key is target/device specific and is meant
to be passed to Hwi_restore().
This function is
called as part of SYS/BIOS Startup_POST_APP_MAIN phase.
Hardware interrupts are enabled unless a call to Hwi_disable disables
them.
Servicing of interrupts that occur while interrupts are disabled is
postponed until interrupts are reenabled. However, if the same type
of interrupt occurs several times while interrupts are disabled,
the interrupt's function is executed only once when interrupts are
reenabled.
A context switch can occur when calling Hwi_enable or Hwi_restore if
an enabled interrupt occurred while interrupts are disabled.
Any call to Hwi_enable enables interrupts, even if Hwi_disable has
been called several times.
Hwi_enable must not be called from main().
Hwi_enableFIQ() // module-wide |
![](../../../../../../Arrow_up.png) |
Enable FIQ interrupts
RETURNS
previous FIQ interrupt enable/disable state
Hwi_enableIRQ() // module-wide |
![](../../../../../../Arrow_up.png) |
Enable IRQ interrupts
ARGUMENTS
key
enable/disable state to restore
Hwi_enableInterrupt() // module-wide |
![](../../../../../../Arrow_up.png) |
Enable a specific interrupt
UInt Hwi_enableInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to enable
RETURNS
key to restore previous enable/disable state
DETAILS
Enables a specific interrupt identified by an interrupt number.
Hwi_enableMIR0() // module-wide |
![](../../../../../../Arrow_up.png) |
Enable specific interrupts
Bits32 Hwi_enableMIR0(Bits32 mask);
ARGUMENTS
mask
bitmask of interrupts to enable
RETURNS
previous MIR settings bitmask
DETAILS
Enables specific interrupts by clearing the bits specified by
mask in the Mask Interrupts Register (MIR).
Hwi_enableMIR1() // module-wide |
![](../../../../../../Arrow_up.png) |
Bits32 Hwi_enableMIR1(Bits32 mask);
Hwi_enableMIR2() // module-wide |
![](../../../../../../Arrow_up.png) |
Bits32 Hwi_enableMIR2(Bits32 mask);
Hwi_enableMIR3() // module-wide |
![](../../../../../../Arrow_up.png) |
Bits32 Hwi_enableMIR3(Bits32 mask);
Hwi_getCoreStackInfo() // module-wide |
![](../../../../../../Arrow_up.png) |
Get Hwi stack usage Info for the specified coreId
Bool Hwi_getCoreStackInfo(
IHwi_StackInfo *
stkInfo,
Bool computeStackDepth,
UInt coreId);
ARGUMENTS
stkInfo
pointer to structure of type StackInfo
computeStackDepth
decides whether to compute stack depth
coreId
core whose stack info needs to be retrieved
RETURNS
boolean to indicate a stack overflow
DETAILS
getCoreStackInfo returns the Hwi stack usage info for the specified
coreId to its calling function by filling stack base address,
stack size and stack peak fields in the
StackInfo structure.
This function should be used only in applications built with
ti.sysbios.BIOS.smpEnabled set to true.
getCoreStackInfo accepts three arguments, a pointer to a structure
of type
StackInfo, a boolean and a coreId. If the boolean
is set to true, the function computes the stack depth and fills the
stack peak field in the StackInfo structure. If a stack overflow
is detected, the stack depth is not computed. If the boolean is
set to false, the function only checks for a stack overflow.
The isr stack is always checked for an overflow and a boolean
is returned to indicate whether an overflow occured.
Below is an example of calling getCoreStackInfo() API:
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/hal/Hwi.h>
#include <ti/sysbios/hal/Core.h>
#include <ti/sysbios/knl/Task.h>
...
Void idleTask()
{
UInt idx;
Hwi_StackInfo stkInfo;
Bool stackOverflow = FALSE;
// Request stack depth for each core's Hwi stack and check for
// overflow
for (idx = 0; idx < Core_numCores; idx++) {
stackOverflow = Hwi_getCoreStackInfo(&stkInfo, TRUE, idx);
// Alternately, we can omit the request for stack depth and
// request only the stack base and stack size (the check for
// stack overflow is always performed):
//
// stackOverflow = Hwi_getCoreStackInfo(&stkInfo, FALSE, idx);
if (stackOverflow) {
// isr Stack Overflow detected
}
}
}
Int main(Int argc, char* argv[])
{
...
BIOS_start();
return (0);
}
Hwi_getHandle() // module-wide |
![](../../../../../../Arrow_up.png) |
Returns Hwi_Handle associated with intNum
ARGUMENTS
intNum
interrupt number
Hwi_getStackInfo() // module-wide |
![](../../../../../../Arrow_up.png) |
Get Hwi stack usage Info
Bool Hwi_getStackInfo(
IHwi_StackInfo *
stkInfo,
Bool computeStackDepth);
ARGUMENTS
stkInfo
pointer to structure of type StackInfo
computeStackDepth
decides whether to compute stack depth
RETURNS
boolean to indicate a stack overflow
DETAILS
getStackInfo returns the Hwi stack usage info to its calling
function by filling stack base address, stack size and stack
peak fields in the
StackInfo structure.
getStackInfo accepts two arguments, a pointer to a structure
of type
StackInfo and a boolean. If the boolean is set
to true, the function computes the stack depth and fills the
stack peak field in the StackInfo structure. If a stack overflow
is detected, the stack depth is not computed. If the boolean is
set to false, the function only checks for a stack overflow.
The isr stack is always checked for an overflow and a boolean
is returned to indicate whether an overflow occured.
Below is an example of calling getStackInfo() API:
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/hal/Hwi.h>
#include <ti/sysbios/knl/Swi.h>
#include <ti/sysbios/knl/Task.h>
Swi_Handle swi0;
volatile Bool swiStackOverflow = FALSE;
Void swi0Fxn(UArg arg1, UArg arg2)
{
Hwi_StackInfo stkInfo;
// Request stack depth
swiStackOverflow = Hwi_getStackInfo(&stkInfo, TRUE);
// Alternately, we can omit the request for stack depth and
// request only the stack base and stack size (the check for
// stack overflow is always performed):
//
// swiStackOverflow = Hwi_getStackInfo(&stkInfo, FALSE);
if (swiStackOverflow) {
// isr Stack Overflow detected
}
}
Void idleTask()
{
Swi_post(swi0);
}
Int main(Int argc, char* argv[])
{
swi0 = Swi_create(swi0Fxn, NULL, NULL);
BIOS_start();
return (0);
}
Hwi_post() // module-wide |
![](../../../../../../Arrow_up.png) |
Generate an interrupt for test purposes
Void Hwi_post(UInt intNum);
ARGUMENTS
intNum
ID of interrupt to generate
ID of interrupt to generate
DETAILS
The INTCPS ISR_SETx registers are used
to trigger a software generated interrupt.
To clear a software generated interrupt, the user
must call
Hwi_clearPostedInterrupt(intNum).
Hwi_restore() // module-wide |
![](../../../../../../Arrow_up.png) |
Globally restore interrupts
macro Void Hwi_restore(UInt key);
ARGUMENTS
key
enable/disable state to restore
DETAILS
Hwi_restore globally restores interrupts to the state determined
by the key argument provided by a previous invocation of Hwi_disable.
A context switch may occur when calling Hwi_restore if Hwi_restore
reenables interrupts and another Hwi occurred while interrupts were
disabled.
Hwi_restore may be called from main(). However, since Hwi_enable
cannot be called from main(), interrupts are always disabled in
main(), and a call to Hwi_restore has no effect.
NOTE
When using TI compiler, Hwi_restore() uses the key to restore all
the bits in the processor status register. This has the effect that
both IRQ and FIQ interrupts are restored to their original status.
Therefore, if FIQ interrupts are disabled but a key obtained when
FIQ interrupts were still enabled is passed to Hwi_restore(), FIQ
interrupts will be re-enabled. Care must be taken to avoid this.
When using GCC compiler, Hwi_restore() only toggles the control bits
corresponding to IRQ interrupts and therefore, FIQ interrupts are not
affected.
Hwi_restoreFIQ() // module-wide |
![](../../../../../../Arrow_up.png) |
Restore FIQ interrupts
Void Hwi_restoreFIQ(UInt key);
ARGUMENTS
key
enable/disable state to restore
Hwi_restoreIRQ() // module-wide |
![](../../../../../../Arrow_up.png) |
Restore IRQ interrupts
Void Hwi_restoreIRQ(UInt key);
ARGUMENTS
key
enable/disable state to restore
Hwi_restoreInterrupt() // module-wide |
![](../../../../../../Arrow_up.png) |
Restore a specific interrupt's enabled/disabled state
Void Hwi_restoreInterrupt(UInt intNum, UInt key);
ARGUMENTS
intNum
interrupt number to restore
key
key returned from enableInt or disableInt
DETAILS
Restores a specific interrupt identified by an interrupt number.
restoreInterrupt is generally used to restore an interrupt to its state
before
disableInterrupt or
enableInterrupt was
invoked
Hwi_restoreMIR0() // module-wide |
![](../../../../../../Arrow_up.png) |
Restore maskable interrupts to the state they were in
when either disableMIR0() or enableMIR0() was called
Bits32 Hwi_restoreMIR0(Bits32 mask);
ARGUMENTS
mask
bitmask of interrupts to restore
RETURNS
previous MIR0 settings bitmask
DETAILS
Simply writes mask to the MIR register.
Hwi_restoreMIR1() // module-wide |
![](../../../../../../Arrow_up.png) |
Bits32 Hwi_restoreMIR1(Bits32 mask);
Hwi_restoreMIR2() // module-wide |
![](../../../../../../Arrow_up.png) |
Bits32 Hwi_restoreMIR2(Bits32 mask);
Hwi_restoreMIR3() // module-wide |
![](../../../../../../Arrow_up.png) |
Bits32 Hwi_restoreMIR3(Bits32 mask);
Hwi_setPriority() // module-wide |
![](../../../../../../Arrow_up.png) |
Set an interrupt's priority
Void Hwi_setPriority(UInt intNum, UInt priority);
ARGUMENTS
intNum
ID of interrupt
priority
priority
DETAILS
Valid priority values range from 1 to
(
NUM_PRIORITIES - 1),
1 is the highest priority.
Hwi_setType() // module-wide |
![](../../../../../../Arrow_up.png) |
Set an interrupt's type (FIQ/IRQ)
Void Hwi_setType(
UInt intNum,
Hwi_Type type);
ARGUMENTS
intNum
ID of interrupt
type
type = FIQ/IRQ
Hwi_startup() // module-wide |
![](../../../../../../Arrow_up.png) |
Initially enable interrupts
DETAILS
Called within BIOS_start
Module-Wide Built-Ins |
![](../../../../../../Arrow_up.png) |
// Get this module's unique id
Bool Hwi_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Hwi_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Hwi_Module_getMask();
// Returns the diagnostics mask for this module
Void Hwi_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
![](../../../../../../Arrow_up.png) |
typedef struct Hwi_Object Hwi_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct Hwi_Struct Hwi_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
![](../../../../../../Arrow_up.png) |
typedef struct Hwi_Params {
// Instance config-params structure
// Common per-instance configs
UArg arg;
// ISR function argument. Default is 0
Bool enableInt;
// Enable this interrupt when object is created? Default is true
Int eventId;
// Interrupt event ID (Interrupt Selection Number)
// The maskSetting parameter is ignored.
Only Hwi_MaskingOption_LOWER is supported
Int priority;
// Interrupt priority
// Interrupt type (IRQ/FIQ). Default is IRQ
} Hwi_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config Hwi_Params.arg // instance |
![](../../../../../../Arrow_up.png) |
ISR function argument. Default is 0
config Hwi_Params.enableInt // instance |
![](../../../../../../Arrow_up.png) |
Enable this interrupt when object is created? Default is true
config Hwi_Params.eventId // instance |
![](../../../../../../Arrow_up.png) |
Interrupt event ID (Interrupt Selection Number)
DETAILS
Default is -1.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored.
config Hwi_Params.maskSetting // instance |
![](../../../../../../Arrow_up.png) |
The maskSetting parameter is ignored.
Only Hwi_MaskingOption_LOWER is supported
DETAILS
The interrupt controller is designed for priority based interrupts
config Hwi_Params.priority // instance |
![](../../../../../../Arrow_up.png) |
Interrupt priority
DETAILS
The default value of -1 is used as a flag to indicate
the lowest (logical) device-specific priority value.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored.
config Hwi_Params.type // instance |
![](../../../../../../Arrow_up.png) |
Interrupt type (IRQ/FIQ). Default is IRQ
Runtime Instance Creation |
![](../../../../../../Arrow_up.png) |
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
intNum
interrupt number
hwiFxn
pointer to ISR function
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Hwi dispatcher table entry is created and filled with the
function specified by the fxn parameter and the attributes
specified by the params parameter.
If params is NULL, the Hwi's dispatcher properties are assigned a
default set of values. Otherwise, the following properties
are specified by a structure of type Hwi_Params.
- The arg element is a generic argument that is passed to the plugged
function as its only parameter. The default value is 0.
- The enableInt element determines whether the interrupt should be
enabled in the IER by create.
- The maskSetting element defines the dispatcherAutoNestingSupport
behavior of the interrupt.
Hwi_create returns a pointer to the created Hwi object.
Instance Deletion |
![](../../../../../../Arrow_up.png) |
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
Hwi_getFunc() // instance |
![](../../../../../../Arrow_up.png) |
Get Hwi function and arg
ARGUMENTS
handle
handle of a previously-created Hwi instance object
arg
pointer for returning hwi's ISR function argument
RETURNS
hwi's ISR function
Hwi_getHookContext() // instance |
![](../../../../../../Arrow_up.png) |
Get hook instance's context for a Hwi
Ptr Hwi_getHookContext(
Hwi_Handle handle,
Int id);
ARGUMENTS
handle
handle of a previously-created Hwi instance object
RETURNS
hook instance's context for hwi
Hwi_getIrp() // instance |
![](../../../../../../Arrow_up.png) |
Get address of interrupted instruction
ARGUMENTS
handle
handle of a previously-created Hwi instance object
RETURNS
most current IRP of a Hwi
Hwi_reconfig() // instance |
![](../../../../../../Arrow_up.png) |
Reconfigure a dispatched interrupt
ARGUMENTS
handle
handle of a previously-created Hwi instance object
Hwi_setFunc() // instance |
![](../../../../../../Arrow_up.png) |
Overwrite Hwi function and arg
ARGUMENTS
handle
handle of a previously-created Hwi instance object
fxn
pointer to ISR function
arg
argument to ISR function
DETAILS
Replaces a Hwi object's hwiFxn function originally
provided in
create.
CONSTRAINTS
Hwi_setFunc() is not thread safe. This means that the new value for
for 'fxn' may be temporarily paired with the previous value for 'arg'
if pre-emption occurs within the execution of Hwi_setFunc().
To guard against this condition, surround the Hwi_setFunc() call with
calls to Hwi_disable() and Hwi_restore():
key = Hwi_disable();
Hwi_setFunc(newFunc, newArg);
Hwi_restore(key);
Hwi_setHookContext() // instance |
![](../../../../../../Arrow_up.png) |
Set hook instance's context for a Hwi
Void Hwi_setHookContext(
Hwi_Handle handle,
Int id,
Ptr hookContext);
ARGUMENTS
handle
handle of a previously-created Hwi instance object
id
hook instance's ID
hookContext
value to write to context
Instance Convertors |
![](../../../../../../Arrow_up.png) |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins |
![](../../../../../../Arrow_up.png) |
Int Hwi_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
const Hwi.NUM_INTERRUPTS |
![](../../../../../../Arrow_up.png) |
intcps supports 128 interrupts
const Hwi.NUM_INTERRUPTS = 128;
C SYNOPSIS
enum Hwi.MaskingOption |
![](../../../../../../Arrow_up.png) |
Shorthand interrupt masking options
values of type Hwi.MaskingOption
const Hwi.MaskingOption_NONE;
const Hwi.MaskingOption_ALL;
const Hwi.MaskingOption_SELF;
const Hwi.MaskingOption_BITMASK;
const Hwi.MaskingOption_LOWER;
VALUES
MaskingOption_NONE
No interrupts are disabled
MaskingOption_ALL
All interrupts are disabled
MaskingOption_SELF
Only this interrupt is disabled
MaskingOption_BITMASK
User supplies interrupt enable masks
MaskingOption_LOWER
All current and lower priority
interrupts are disabled.
Only a few targets/devices truly
support this masking option. For those
that don't, this setting is treated
the same as MaskingOption_SELF.
C SYNOPSIS
enum Hwi.Type |
![](../../../../../../Arrow_up.png) |
Interrupt type. IRQ or FIQ
values of type Hwi.Type
const Hwi.Type_IRQ;
// IRQ interrupt
const Hwi.Type_FIQ;
// FIQ interrupt
C SYNOPSIS
struct Hwi.HookSet |
![](../../../../../../Arrow_up.png) |
Hwi hook set type definition
var obj = new Hwi.HookSet;
obj.registerFxn = Void(*)(Int) ...
DETAILS
The functions that make up a hookSet have certain restrictions. They
cannot call any Hwi instance functions other than Hwi_getHookContext()
and Hwi_setHookContext(). For all practical purposes, they should treat
the Hwi_Handle passed to these functions as an opaque handle.
C SYNOPSIS
struct Hwi.Intc |
![](../../../../../../Arrow_up.png) |
Interrupt Controller. Symbol "Hwi_intc" is physical device
var obj = new Hwi.Intc;
obj.REVISION = UInt32 ...
// 0x00 Config Register
obj.hole0 = UInt32[3] ...
// 0x04-0x0C
obj.SYSCONFIG = UInt32 ...
// 0x10 Config Register
obj.SYSSTATUS = UInt32 ...
// 0x14 Status Register
obj.hole1 = UInt32[10] ...
// 0x18-0x3c
obj.SIR_IRQ = UInt32 ...
// 0x40 Source IRQ Register
obj.SIR_FIQ = UInt32 ...
// 0x44 Source FIQ Register
obj.CONTROL = UInt32 ...
// 0x48 Control Register
obj.PROTECTION = UInt32 ...
// 0x4C Protection Register
obj.IDLE = UInt32 ...
// 0x50 Idle Register
obj.hole2 = UInt32[3] ...
// 0x54-0x5C
obj.IRQ_PRIORITY = UInt32 ...
// 0x60 IRQ Priority Register
obj.FIQ_PRIORITY = UInt32 ...
// 0x64 IRQ Priority Register
obj.THRESHOLD = UInt32 ...
// 0x68 Threshold Register
obj.hole3 = UInt32[5] ...
// 0x6C-0x7C
obj.ITR0 = UInt32 ...
// 0x80 Interrupt Input Register
obj.MIR0 = UInt32 ...
// 0x84 Mask Interrupt Register
obj.MIR_CLEAR0 = UInt32 ...
// 0x88 MIR Clear Register
obj.MIR_SET0 = UInt32 ...
// 0x8C MIR Set Register
obj.ISR_SET0 = UInt32 ...
// 0x90 Interrupt Set Register
obj.ISR_CLEAR0 = UInt32 ...
// 0x94 Interrupt Clear Register
obj.PENDING_IRQ0 = UInt32 ...
// 0x98 Pending IRQ Register
obj.PENDING_FIQ0 = UInt32 ...
// 0x9C Pending FIQ Register
obj.ITR1 = UInt32 ...
// 0xA0 Interrupt Input Register
obj.MIR1 = UInt32 ...
// 0xA4 Mask Interrupt Register
obj.MIR_CLEAR1 = UInt32 ...
// 0xA8 MIR Clear Register
obj.MIR_SET1 = UInt32 ...
// 0xAC MIR Set Register
obj.ISR_SET1 = UInt32 ...
// 0xB0 Interrupt Set Register
obj.ISR_CLEAR1 = UInt32 ...
// 0xB4 Interrupt Clear Register
obj.PENDING_IRQ1 = UInt32 ...
// 0xB8 Pending IRQ Register
obj.PENDING_FIQ1 = UInt32 ...
// 0xBC Pending FIQ Register
obj.ITR2 = UInt32 ...
// 0xC0 Interrupt Input Register
obj.MIR2 = UInt32 ...
// 0xC4 Mask Interrupt Register
obj.MIR_CLEAR2 = UInt32 ...
// 0xC8 MIR Clear Register
obj.MIR_SET2 = UInt32 ...
// 0xCC MIR Set Register
obj.ISR_SET2 = UInt32 ...
// 0xD0 Interrupt Set Register
obj.ISR_CLEAR2 = UInt32 ...
// 0xD4 Interrupt Clear Register
obj.PENDING_IRQ2 = UInt32 ...
// 0xD8 Pending IRQ Register
obj.PENDING_FIQ2 = UInt32 ...
// 0xDC Pending FIQ Register
obj.ITR3 = UInt32 ...
// 0xE0 Interrupt Input Register
obj.MIR3 = UInt32 ...
// 0xE4 Mask Interrupt Register
obj.MIR_CLEAR3 = UInt32 ...
// 0xE8 MIR Clear Register
obj.MIR_SET3 = UInt32 ...
// 0xEC MIR Set Register
obj.ISR_SET3 = UInt32 ...
// 0xF0 Interrupt Set Register
obj.ISR_CLEAR3 = UInt32 ...
// 0xF4 Interrupt Clear Register
obj.PENDING_IRQ3 = UInt32 ...
// 0xF8 Pending IRQ Register
obj.PENDING_FIQ3 = UInt32 ...
// 0xFC Pending FIQ Register
obj.ILR = UInt32[128] ...
// 0x100 thru 0x2FC
C SYNOPSIS
struct Hwi.StackInfo |
![](../../../../../../Arrow_up.png) |
Structure contains Hwi stack usage info
var obj = new Hwi.StackInfo;
obj.hwiStackPeak = SizeT ...
obj.hwiStackSize = SizeT ...
obj.hwiStackBase = Ptr ...
DETAILS
Used by getStackInfo() and viewGetStackInfo() functions
C SYNOPSIS
config Hwi.E_alreadyDefined // module-wide |
![](../../../../../../Arrow_up.png) |
Error raised when an attempt is made to create a Hwi
that has already been created
msg: "E_alreadyDefined: Hwi already defined, intnum: %d"
};
C SYNOPSIS
config Hwi.E_badIntNum // module-wide |
![](../../../../../../Arrow_up.png) |
Error raised if an attempt is made to create a Hwi
with an interrupt number greater than NUM_INTERRUPTS - 1
msg: "E_badIntNum, intnum: %d is out of range"
};
C SYNOPSIS
config Hwi.E_handleNotFound // module-wide |
![](../../../../../../Arrow_up.png) |
Error raised when Hwi handle referenced in Hwi_delete()
is not found in the Hwi dispatch table
msg: "E_handleNotFound: Hwi handle not found: 0x%x"
};
C SYNOPSIS
config Hwi.E_invalidPriority // module-wide |
![](../../../../../../Arrow_up.png) |
Error raised if an attempt is made to create a Hwi
with a priority of 0
msg: "E_invalidPriority, priority: %d is either invalid or not supported"
};
C SYNOPSIS
config Hwi.E_undefined // module-wide |
![](../../../../../../Arrow_up.png) |
Error raised when an undefined interrupt has fired
msg: "E_undefined: Hwi undefined, intnum: %d"
};
C SYNOPSIS
config Hwi.LD_end // module-wide |
![](../../../../../../Arrow_up.png) |
Issued just after return from Hwi function (with interrupts disabled)
msg: "LD_end: hwi: 0x%x"
};
C SYNOPSIS
config Hwi.LM_begin // module-wide |
![](../../../../../../Arrow_up.png) |
Issued just prior to Hwi function invocation (with interrupts disabled)
msg: "LM_begin: hwi: 0x%x, func: 0x%x, preThread: %d, intNum: %d, irp: 0x%x"
};
C SYNOPSIS
config Hwi.NUM_PRIORITIES // module-wide |
![](../../../../../../Arrow_up.png) |
The device-specific number of priorities supported
Hwi.NUM_PRIORITIES = Int undefined;
DETAILS
The actual number supported is device specific and provided by
the catalog device specification.
C SYNOPSIS
config Hwi.dispatcherAutoNestingSupport // module-wide |
![](../../../../../../Arrow_up.png) |
Include interrupt nesting logic in interrupt dispatcher?
Hwi.dispatcherAutoNestingSupport = Bool true;
DETAILS
Default is true.
This option provides the user with the ability to optimize
interrupt dispatcher performance when support for interrupt
nesting is not required.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that manipulates interrupt mask
registers and enables and disables interrupts before and
after invoking the user's Hwi function.
Set this parameter to false if you don't need interrupts
enabled during the execution of your Hwi functions.
C SYNOPSIS
config Hwi.dispatcherIrpTrackingSupport // module-wide |
![](../../../../../../Arrow_up.png) |
Controls whether the
dispatcher retains the interrupted thread's return address
Hwi.dispatcherIrpTrackingSupport = Bool true;
DETAILS
This option is enabled by default.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that keeps track of the interrupt's
return address and provide a small savings in interrupt latency.
The application can get an interrupt's most recent return
address using the
getIrp API.
C SYNOPSIS
config Hwi.dispatcherSwiSupport // module-wide |
![](../../../../../../Arrow_up.png) |
Include Swi scheduling logic in interrupt dispatcher?
Hwi.dispatcherSwiSupport = Bool undefined;
DETAILS
Default is inherited from
BIOS.swiEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that Swis
will not be posted from any of their Hwi threads.
WARNING
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Swi scheduler
prior to returning from an interrupt.
With this setting, Swis MUST NOT be posted from Hwi functions!
C SYNOPSIS
config Hwi.dispatcherTaskSupport // module-wide |
![](../../../../../../Arrow_up.png) |
Include Task scheduling logic in interrupt dispatcher?
Hwi.dispatcherTaskSupport = Bool undefined;
DETAILS
Default is inherited from
BIOS.taskEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that no
Task scheduling APIs (ie
Semaphore_post()) will be executed from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Task scheduler
prior to returning from an interrupt.
C SYNOPSIS
config Hwi.fiqStack // module-wide |
![](../../../../../../Arrow_up.png) |
FIQ stack pointer. Default = null.
(Indicates that stack is to be created internally)
C SYNOPSIS
config Hwi.mir0Mask // module-wide |
![](../../../../../../Arrow_up.png) |
Initial MIR0 Interrupt Mask. Default is 0xffffffff
Hwi.mir0Mask = Bits32 0xffffffff;
C SYNOPSIS
config Hwi.mir1Mask // module-wide |
![](../../../../../../Arrow_up.png) |
Initial MIR1 Interrupt Mask. Default is 0xffffffff
Hwi.mir1Mask = Bits32 0xffffffff;
C SYNOPSIS
config Hwi.mir2Mask // module-wide |
![](../../../../../../Arrow_up.png) |
Initial MIR2 Interrupt Mask. Default is 0xffffffff
Hwi.mir2Mask = Bits32 0xffffffff;
C SYNOPSIS
config Hwi.mir3Mask // module-wide |
![](../../../../../../Arrow_up.png) |
Initial MIR3 Interrupt Mask. Default is 0xffffffff
Hwi.mir3Mask = Bits32 0xffffffff;
C SYNOPSIS
metaonly config Hwi.common$ // module-wide |
![](../../../../../../Arrow_up.png) |
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly config Hwi.dataAbortFunc // module-wide |
![](../../../../../../Arrow_up.png) |
Data abort exception handler.
Default is an internal exception handler
Hwi.dataAbortFunc = Void(*)(Void) undefined;
metaonly config Hwi.fiqFunc // module-wide |
![](../../../../../../Arrow_up.png) |
FIQ interrupt handler. Default is internal FIQ dispatcher
Hwi.fiqFunc = Void(*)(Void) undefined;
metaonly config Hwi.fiqStackSection // module-wide |
![](../../../../../../Arrow_up.png) |
Memory section used for FIQ stack
Default is null
Hwi.fiqStackSection = String null;
metaonly config Hwi.fiqStackSize // module-wide |
![](../../../../../../Arrow_up.png) |
FIQ stack size in MAUs.
Default is 1024 bytes
Hwi.fiqStackSize = SizeT 1024;
metaonly config Hwi.irqFunc // module-wide |
![](../../../../../../Arrow_up.png) |
IRQ interrupt handler. Default is internal IRQ dispatcher
Hwi.irqFunc = Void(*)(Void) undefined;
metaonly config Hwi.prefetchAbortFunc // module-wide |
![](../../../../../../Arrow_up.png) |
Prefetch abort exception handler.
Default is an internal exception handler
Hwi.prefetchAbortFunc = Void(*)(Void) undefined;
metaonly config Hwi.reservedFunc // module-wide |
![](../../../../../../Arrow_up.png) |
Reserved exception handler.
Default is an internal exception handler
Hwi.reservedFunc = Void(*)(Void) undefined;
metaonly config Hwi.resetFunc // module-wide |
![](../../../../../../Arrow_up.png) |
Reset Handler. Default is c_int00
Hwi.resetFunc = Void(*)(Void) undefined;
metaonly config Hwi.swiFunc // module-wide |
![](../../../../../../Arrow_up.png) |
SWI Handler. Default is internal SWI handler.
Default is an internal exception handler
Hwi.swiFunc = Void(*)(Void) undefined;
metaonly config Hwi.undefinedInstFunc // module-wide |
![](../../../../../../Arrow_up.png) |
Undefined instruction exception handler.
Default is an internal exception handler
Hwi.undefinedInstFunc = Void(*)(Void) undefined;
metaonly Hwi.addHookSet() // module-wide |
![](../../../../../../Arrow_up.png) |
addHookSet is used in a config file to add a hook set (defined
by struct HookSet)
ARGUMENTS
hook
structure of type HookSet
DETAILS
HookSet structure elements may be omitted, in which case those
elements will not exist.
Instance Config Parameters |
![](../../../../../../Arrow_up.png) |
var params = new Hwi.Params;
// Instance config-params object
params.arg = UArg 0;
// ISR function argument. Default is 0
params.enableInt = Bool true;
// Enable this interrupt when object is created? Default is true
params.eventId = Int -1;
// Interrupt event ID (Interrupt Selection Number)
// The maskSetting parameter is ignored.
Only Hwi_MaskingOption_LOWER is supported
params.priority = Int -1;
// Interrupt priority
// Interrupt type (IRQ/FIQ). Default is IRQ
config Hwi.Params.arg // instance |
![](../../../../../../Arrow_up.png) |
ISR function argument. Default is 0
var params = new Hwi.Params;
...
params.arg = UArg 0;
C SYNOPSIS
config Hwi.Params.enableInt // instance |
![](../../../../../../Arrow_up.png) |
Enable this interrupt when object is created? Default is true
var params = new Hwi.Params;
...
params.enableInt = Bool true;
C SYNOPSIS
config Hwi.Params.eventId // instance |
![](../../../../../../Arrow_up.png) |
Interrupt event ID (Interrupt Selection Number)
var params = new Hwi.Params;
...
params.eventId = Int -1;
DETAILS
Default is -1.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored.
C SYNOPSIS
config Hwi.Params.maskSetting // instance |
![](../../../../../../Arrow_up.png) |
The maskSetting parameter is ignored.
Only Hwi_MaskingOption_LOWER is supported
var params = new Hwi.Params;
...
DETAILS
The interrupt controller is designed for priority based interrupts
C SYNOPSIS
config Hwi.Params.priority // instance |
![](../../../../../../Arrow_up.png) |
Interrupt priority
var params = new Hwi.Params;
...
params.priority = Int -1;
DETAILS
The default value of -1 is used as a flag to indicate
the lowest (logical) device-specific priority value.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored.
C SYNOPSIS
config Hwi.Params.type // instance |
![](../../../../../../Arrow_up.png) |
Interrupt type (IRQ/FIQ). Default is IRQ
var params = new Hwi.Params;
...
C SYNOPSIS
Static Instance Creation |
![](../../../../../../Arrow_up.png) |
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = Hwi.create(Int intNum, Void(*)(UArg) hwiFxn, params);
// Create an instance-object
ARGUMENTS
intNum
interrupt number
hwiFxn
pointer to ISR function
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Hwi dispatcher table entry is created and filled with the
function specified by the fxn parameter and the attributes
specified by the params parameter.
If params is NULL, the Hwi's dispatcher properties are assigned a
default set of values. Otherwise, the following properties
are specified by a structure of type Hwi_Params.
- The arg element is a generic argument that is passed to the plugged
function as its only parameter. The default value is 0.
- The enableInt element determines whether the interrupt should be
enabled in the IER by create.
- The maskSetting element defines the dispatcherAutoNestingSupport
behavior of the interrupt.
Hwi_create returns a pointer to the created Hwi object.