module ti.sysbios.family.arm.gic.Hwi

Hardware Interrupt Support Module

This Hwi module provides ARM cortex-A Generic Interrupt Controller(GIC) v2.0 specific implementations and extensions of the APIs defined in IHwi. [ more ... ]
C synopsis target-domain sourced in ti/sysbios/family/arm/gic/Hwi.xdc
#include <ti/sysbios/family/arm/gic/Hwi.h>
Functions
Void
Void
Void
macro UInt 
macro UInt 
macro UInt 
macro UInt 
Void
Void 
macro Void 
macro Void 
Void 
Hwi_setPriority// Set an interrupt's priority(UInt intNum, UInt priority);
Functions common to all IHwi modules
Void 
macro UInt 
UInt 
macro UInt 
UInt 
Bool 
Ptr 
Bool 
Void 
macro Void 
Void 
Void 
Void 
Void 
Functions common to all target instances
Functions common to all target modules
Typedefs
typedef Void 
typedef struct
typedef struct
typedef Hwi_Object *
typedef struct
typedef UArg 
typedef enum
typedef struct
typedef struct
typedef struct
typedef struct
typedef enum
typedef Void 
Constants
extern const UInt 
extern const Assert_Id 
extern const UInt 
extern const UInt 
extern const Bool 
extern const Bool 
extern const Bool 
extern const Bool 
extern const Bool 
extern const Error_Id 
extern const Error_Id 
extern const Error_Id 
extern const Error_Id 
extern const Bool 
extern const Log_Event 
extern const Log_Event 
extern const UInt 
extern const UInt 
extern const UInt 
Variables
Hwi_gicc// ; // linked as extern ti_sysbios_family_arm_gic_Hwi_gicc
Hwi_gicd// ; // linked as extern ti_sysbios_family_arm_gic_Hwi_gicd
 
DETAILS
This Hwi module provides ARM cortex-A Generic Interrupt Controller(GIC) v2.0 specific implementations and extensions of the APIs defined in IHwi.
The GIC is logically partitioned into 2 blocks, the Distributor block and CPU interface block. The Distributor block interfaces with the interrupt sources, prioritizes interrupts and distributes them to the CPU interface block. The CPU interface block connects to the processors in the system and is responsible for priority masking and preemption handling for the processor it is connected to.
The GIC can implement up to 8 CPU interfaces with each CPU interface being able to see up to 1020 interrupts. The GIC assigns interrupt ID numbers 0-1019 as follows: - Interrupt numbers 0-31 are used for interrupts private to a CPU interface. These private interrupts are banked in the Distributor. - Banked interrupt number 0-15 are used for Software Generated Interrupts or SGIs. - Banked interrupt number 16-31 are used for Private Peripheral Interrupts or PPIs. - Interrupt numbers 32-1019 are used for Shared Peripheral Interrupts or SPIs. - Interrupt numbers 1020-1023 are reserved.
NOTE
In the SoC Technical Reference Manual, the MPU IRQs 0 to N map to GIC interrupt numbers 32 to (N+32) where (N+1) is the total number of Shared Peripheral Interrupts implemented. For instance on OMAP5430, MPU IRQ 0 to 159 maps to GIC interrupt number 32 to 191.
In this Hwi module implementation, the instance config parameter value MaskingOption_LOWER is equivalent to MaskingOption_SELF. Statically configuring a Hwi object's Params.maskSetting to MaskingOption_LOWER will result in the generation of a benign build warning. Dynamic usages of MaskingOption_LOWER will be silently converted to MaskingOption_SELF.
This module is written for GIC v2.0, however it is backwards compatible with GIC v1.0
INTERRUPT GROUPING
GIC allows configuring an interrupt as a Group 0 or a Group 1 interrupt. Group 0 interrupts are Secure interrupts and Group 1 interrupts are Non-secure interrupts.
If enableSecureMode is set to true, this module supports both Group0 and Group 1 interrupts. Group 0 interrupts are delivered to the CPU using FIQ signal whereas Group 1 interrupts are delivered using IRQ signal.
If enableSecureMode is set to false, this module only supports Group 1 interrupts which are delivered to the target CPU using IRQ signal.
INTERRUPT PRIORITIES
In general GIC supports priority values 0 thru 255.
In practice valid priority values depend on the particular device used, security mode and the Binary Point Register (see BPR and ABPR) value.
The device implementation and security mode decide the number of priority bits that are implemented (see NUM_PRIORITY_BITS). Group 0 interrupts always implement one more priority bit than Group 1 interrupts.
In GIC, interrupts with lower priority numbers have higher priority.
ZERO LATENCY INTERRUPTS
On Keystone2 devices, this module supports zero-latency interrupts. A zero-latency interrupt does not go through the SYS/BIOS dispatcher and thus has a faster response time. Since zero-latency interrupts bypass the dispatcher, their handler function cannot call any SYS/BIOS APIs.
This module implements zero-latency interrupts by forwarding the interrupt to the target CPU using FIQ signal. Therefore, in order to configure an interrupt as a zero-latency interrupt, the Hwi type needs to be changed to FIQ when creating or constructing a Hwi.
Example showing how to create a zero-latency Hwi:
  Void main(Void)
  {
      Hwi_Params hwiParams;
      Hwi_Params_init(&hwiParams);
      // Default Hwi type is IRQ
      hwiParams.type = Hwi_Type_FIQ;
      Hwi_create(INT_NUM_FIQ, myIsrFIQ, &hwiParams, NULL);
      ...
  }
FIQs run on their own stack. See fiqStack and fiqStackSize for more info on how to control the FIQ stack.
 
enum Hwi_MaskingOption

Shorthand interrupt masking options

C synopsis target-domain
typedef enum Hwi_MaskingOption {
    Hwi_MaskingOption_NONE,
    Hwi_MaskingOption_ALL,
    Hwi_MaskingOption_SELF,
    Hwi_MaskingOption_BITMASK,
    Hwi_MaskingOption_LOWER
} Hwi_MaskingOption;
 
VALUES
MaskingOption_NONE — No interrupts are disabled
MaskingOption_ALL — All interrupts are disabled
MaskingOption_SELF — Only this interrupt is disabled
MaskingOption_BITMASK — User supplies interrupt enable masks
MaskingOption_LOWER — All current and lower priority interrupts are disabled.
Only a few targets/devices truly support this masking option. For those that don't, this setting is treated the same as MaskingOption_SELF.
 
enum Hwi_Type

Interrupt type. IRQ or FIQ

C synopsis target-domain
typedef enum Hwi_Type {
    Hwi_Type_IRQ,
    // IRQ interrupt
    Hwi_Type_FIQ
    // FIQ interrupt
} Hwi_Type;
 
 
typedef Hwi_FuncPtr

Hwi create function type definition

C synopsis target-domain
typedef Void (*Hwi_FuncPtr)(UArg);
 
 
typedef Hwi_Irp

Interrupt Return Pointer

C synopsis target-domain
typedef UArg Hwi_Irp;
 
DETAILS
This is the address of the interrupted instruction.
 
typedef Hwi_VectorFuncPtr

Hwi vector function type definition

C synopsis target-domain
typedef Void (*Hwi_VectorFuncPtr)(Void);
 
 
struct Hwi_Gicc

Generic Interrupt Controller CPU Interface. Symbol "Hwi_gicc" is a physical device

C synopsis target-domain
typedef struct Hwi_Gicc {
    UInt32 CTLR;
    // 0x0000 CPU Interface Control Register
    UInt32 PMR;
    // 0x0004 Interrupt Priority Mask Register
    UInt32 BPR;
    // 0x0008 Binary Point Register
    UInt32 IAR;
    // 0x000C Interrupt Acknowledge Register
    UInt32 EOIR;
    // 0x0010 End Of Interrupt Register
    UInt32 RPR;
    // 0x0014 Running Priority Register
    UInt32 HPPIR;
    // 0x0018 Highest Priority Pending Interrupt Register
    UInt32 ABPR;
    // 0x001C Aliased Binary Point Register
    UInt32 AIAR;
    // 0x0020 Aliased IAR Register
    UInt32 AEOIR;
    // 0x0024 Aliased EOI Register
    UInt32 AHPPIR;
    // 0x0028 Aliased HPPI Register
    UInt32 hole0[41];
    // 0x002C-0x00CC
    UInt32 APR0;
    // 0x00D0 Active Priority Register
    UInt32 hole1[3];
    // 0x00D4-0x00DC
    UInt32 NSAPR0;
    // 0x00E0 Non-secure Active Priority Register
    UInt32 hole2[6];
    // 0x00E4-0x00F8
    UInt32 IIDR;
    // 0x00FC CPU Interface Id Register
    UInt32 hole3[960];
    // 0x0100-0x0FFC
    UInt32 DIR;
    // 0x1000 Deactivate Interrupt Register
} Hwi_Gicc;
 
 
struct Hwi_Gicd

Generic Interrupt Controller Distributor. Symbol "Hwi_gicd" is a physical device

C synopsis target-domain
typedef struct Hwi_Gicd {
    UInt32 CTLR;
    // 0x000 Distributor Control Register
    UInt32 TYPER;
    // 0x004 Interrupt Controller Type Register
    UInt32 IIDR;
    // 0x008 Distributor Implementor Id Register
    UInt32 hole0[29];
    // 0x00C-0x07C
    UInt32 IGROUPR[32];
    // 0x080 Interrupt Group Registers
    UInt32 ISENABLER[32];
    // 0x100 Interrupt Set-Enable Registers
    UInt32 ICENABLER[32];
    // 0x180 Interrupt Clear-Enable Registers
    UInt32 ISPENDR[32];
    // 0x200 Interrupt Set-Pending Registers
    UInt32 ICPENDR[32];
    // 0x280 Interrupt Clear-Pending Registers
    UInt32 ISACTIVER[32];
    // 0x300 Interrupt Set-Active Registers
    UInt32 ICACTIVER[32];
    // 0x380 Interrupt Clear-Active Registers
    UInt32 IPRIORITYR[255];
    // 0x400 Interrupt Priority Registers
    UInt32 hole1[1];
    // 0x7FC
    UInt32 ITARGETSR[255];
    // 0x800 Interrupt Processor Targets Register
    UInt32 hole2[1];
    // 0xBFC
    UInt32 ICFGR[64];
    // 0xC00 Interrupt Configuration Registers
    UInt32 PPISR;
    // 0xD00 PPI Status Register
    UInt32 SPISR[7];
    // 0xD04 SPI Status Registers
    UInt32 hole3[120];
    // 0xD20-0xEFC
    UInt32 SGIR;
    // 0xF00 Software Generated Interrupt Registers
    UInt32 hole4[3];
    // 0xF04-0xF0C
    UInt32 CPENDSGIR[4];
    // 0xF10 SGI Clear-Pending Registers
    UInt32 SPENDSGIR[4];
    // 0xF20 SGI Set-Pending Registers
    UInt32 hole5[40];
    // 0xF30-0xFCC
    UInt32 PIDR4;
    // 0xFD0 Peripheral ID4 Register
    UInt32 PIDR5;
    // 0xFD4 Peripheral ID5 Register
    UInt32 PIDR6;
    // 0xFD8 Peripheral ID6 Register
    UInt32 PIDR7;
    // 0xFDC Peripheral ID7 Register
    UInt32 PIDR0;
    // 0xFE0 Peripheral ID0 Register
    UInt32 PIDR1;
    // 0xFE4 Peripheral ID1 Register
    UInt32 PIDR2;
    // 0xFE8 Peripheral ID2 Register
    UInt32 PIDR3;
    // 0xFEC Peripheral ID3 Register
    UInt32 CIDR0;
    // 0xFF0 Component ID0 Register
    UInt32 CIDR1;
    // 0xFF4 Component ID1 Register
    UInt32 CIDR2;
    // 0xFF8 Component ID2 Register
    UInt32 CIDR3;
    // 0xFFC Component ID3 Register
} Hwi_Gicd;
 
 
struct Hwi_HookSet

Hwi hook set type definition

C synopsis target-domain
typedef struct Hwi_HookSet {
    Void (*registerFxn)(Int);
    Void (*createFxn)(IHwi_Handle,Error_Block*);
    Void (*beginFxn)(IHwi_Handle);
    Void (*endFxn)(IHwi_Handle);
    Void (*deleteFxn)(IHwi_Handle);
} Hwi_HookSet;
 
DETAILS
The functions that make up a hookSet have certain restrictions. They cannot call any Hwi instance functions other than Hwi_getHookContext() and Hwi_setHookContext(). For all practical purposes, they should treat the Hwi_Handle passed to these functions as an opaque handle.
 
struct Hwi_StackInfo

Structure contains Hwi stack usage info

C synopsis target-domain
typedef struct Hwi_StackInfo {
    SizeT hwiStackPeak;
    SizeT hwiStackSize;
    Ptr hwiStackBase;
} Hwi_StackInfo;
 
DETAILS
Used by getStackInfo() and viewGetStackInfo() functions
 
config Hwi_ABPR  // module-wide

GIC Aliased Binary Point Register value for Grourp 1 interrupts

C synopsis target-domain
extern const UInt Hwi_ABPR;
 
DETAILS
Defines the point at which the priority value fields split into two parts, the group priority field and the sub-priority field. ABPR is used only when enableSecureMode set to true and is ignored when security mode is set to false. ABPR applies to Group 1 interrupts.
The group priority field determines interrupt preemption in case of nested interrupts whereas sub-priority field is used to determine priority within a group when multiple interrrupts belonging to the same group are pending.
Valid ABPR values are from 1-7 with the minimum value supported being implementation defined and in the range 1-4. Minimum ABPR value is 1 more than the minimum BPR value.
   --------------------------------------------------------
  | ABPR value | Group priority field | Sub-priority field |
   --------------------------------------------------------
  |     0      |          --          |         --         |
  |     1      |         [7:1]        |         [0]        |
  |     2      |         [7:2]        |        [1:0]       |
  |     3      |         [7:3]        |        [2:0]       |
  |     4      |         [7:4]        |        [3:0]       |
  |     5      |         [7:5]        |        [4:0]       |
  |     6      |         [7:6]        |        [5:0]       |
  |     7      |          [7]         |        [6:0]       |
   --------------------------------------------------------
 
config Hwi_A_badSGIIntNum  // module-wide

Assert raised when an interrupt number >= 16 is passed to Hwi_raiseSGI() function

C synopsis target-domain
extern const Assert_Id Hwi_A_badSGIIntNum;
 
 
config Hwi_BPR  // module-wide

GIC Binary Point Register value

C synopsis target-domain
extern const UInt Hwi_BPR;
 
DETAILS
Defines the point at which the priority value fields split into two parts, the group priority field and the sub-priority field. When running in SECURE mode, BPR applies to Group 0 interrupts and when running in NON-SECURE mode, BPR applies to Group 1 interrupts.
The group priority field determines interrupt preemption in case of nested interrupts whereas sub-priority field is used to determine priority within a group when multiple interrrupts belonging to the same group are pending.
Valid BPR values are from 0-7 with the minimum value supported being implementation defined and in the range 0-3.
   -------------------------------------------------------
  | BPR value | Group priority field | Sub-priority field |
   -------------------------------------------------------
  |     0     |         [7:1]        |         [0]        |
  |     1     |         [7:2]        |        [1:0]       |
  |     2     |         [7:3]        |        [2:0]       |
  |     3     |         [7:4]        |        [3:0]       |
  |     4     |         [7:5]        |        [4:0]       |
  |     5     |         [7:6]        |        [5:0]       |
  |     6     |          [7]         |        [6:0]       |
  |     7     |     No preemption    |        [7:0]       |
   -------------------------------------------------------
 
config Hwi_DEFAULT_INT_PRIORITY  // module-wide

Default Interrupt Priority

C synopsis target-domain
extern const UInt Hwi_DEFAULT_INT_PRIORITY;
 
DETAILS
Set to one level higher than minimum supported priority.
 
config Hwi_E_alreadyDefined  // module-wide

Error raised when an attempt is made to create a Hwi that has already been created

C synopsis target-domain
extern const Error_Id Hwi_E_alreadyDefined;
 
 
config Hwi_E_badIntNum  // module-wide

Error raised if an attempt is made to create a Hwi with an interrupt number greater than Hwi_NUM_INTERRUPTS - 1

C synopsis target-domain
extern const Error_Id Hwi_E_badIntNum;
 
 
config Hwi_E_handleNotFound  // module-wide

Error raised when Hwi handle referenced in Hwi_delete() is not found in the Hwi dispatch table

C synopsis target-domain
extern const Error_Id Hwi_E_handleNotFound;
 
 
config Hwi_E_undefined  // module-wide

Error raised when an undefined interrupt has fired

C synopsis target-domain
extern const Error_Id Hwi_E_undefined;
 
 
config Hwi_LD_end  // module-wide

Issued just after return from Hwi function (with interrupts disabled)

C synopsis target-domain
extern const Log_Event Hwi_LD_end;
 
 
config Hwi_LM_begin  // module-wide

Issued just prior to Hwi function invocation (with interrupts disabled)

C synopsis target-domain
extern const Log_Event Hwi_LM_begin;
 
 
config Hwi_MIN_INT_PRIORITY  // module-wide

Minimum Interrupt Priority

C synopsis target-domain
extern const UInt Hwi_MIN_INT_PRIORITY;
 
 
config Hwi_NUM_INTERRUPTS  // module-wide

Number of interrupts implemented in GIC

C synopsis target-domain
extern const UInt Hwi_NUM_INTERRUPTS;
 
DETAILS
On OMAP543x GIC implements 192 interrupts.
See the OMAP543x_ES1 Technical Reference Manual pg 5280 for more details.
 
config Hwi_NUM_PRIORITY_BITS  // module-wide

Number of Priority bits implemented

C synopsis target-domain
extern const UInt Hwi_NUM_PRIORITY_BITS;
 
DETAILS
On OMAP543x running in non-secure mode, only most significant 4 priority bits are available for use. The least significant 4 bits are always 0.
 
config Hwi_dispatcherAutoNestingSupport  // module-wide

Include interrupt nesting logic in interrupt dispatcher?

C synopsis target-domain
extern const Bool Hwi_dispatcherAutoNestingSupport;
 
DETAILS
Default is true.
This option provides the user with the ability to optimize interrupt dispatcher performance when support for interrupt nesting is not required.
Setting this parameter to false will disable the logic in the interrupt dispatcher that manipulates interrupt mask registers and enables and disables interrupts before and after invoking the user's Hwi function.
Set this parameter to false if you don't need interrupts enabled during the execution of your Hwi functions.
 
config Hwi_dispatcherIrpTrackingSupport  // module-wide

Controls whether the dispatcher retains the interrupted thread's return address

C synopsis target-domain
extern const Bool Hwi_dispatcherIrpTrackingSupport;
 
DETAILS
This option is enabled by default.
Setting this parameter to false will disable the logic in the interrupt dispatcher that keeps track of the interrupt's return address and provide a small savings in interrupt latency.
The application can get an interrupt's most recent return address using the getIrp API.
 
config Hwi_dispatcherSwiSupport  // module-wide

Include Swi scheduling logic in interrupt dispatcher?

C synopsis target-domain
extern const Bool Hwi_dispatcherSwiSupport;
 
DETAILS
Default is inherited from BIOS.swiEnabled, which is true by default.
This option provides the user with the ability to optimize interrupt dispatcher performance when it is known that Swis will not be posted from any of their Hwi threads.
WARNING
Setting this parameter to false will disable the logic in the interrupt dispatcher that invokes the Swi scheduler prior to returning from an interrupt. With this setting, Swis MUST NOT be posted from Hwi functions!
 
config Hwi_dispatcherTaskSupport  // module-wide

Include Task scheduling logic in interrupt dispatcher?

C synopsis target-domain
extern const Bool Hwi_dispatcherTaskSupport;
 
DETAILS
Default is inherited from BIOS.taskEnabled, which is true by default.
This option provides the user with the ability to optimize interrupt dispatcher performance when it is known that no Task scheduling APIs (ie Semaphore_post()) will be executed from any of their Hwi threads.
Setting this parameter to false will disable the logic in the interrupt dispatcher that invokes the Task scheduler prior to returning from an interrupt.
 
config Hwi_enableSecureMode  // module-wide

Security Mode

C synopsis target-domain
extern const Bool Hwi_enableSecureMode;
 
DETAILS
This field specifies the MPU's security mode. The MPU's security mode determines the type of accesses to the GIC i.e. if the MPU is in secure mode, all accesses to the GIC are secure and if the MPU is in non-secure mode, all accesses to the GIC are non-secure.
An exception to the above rule can be seen on certain devices like Keystone 2, where all GIC acceses are secure irrespective of the MPU's security state. enableSecureMode should be set to true for such devices.
 
config Hwi_initGicd  // module-wide

Initialize all GIC Distributor registers. True by default

C synopsis target-domain
extern const Bool Hwi_initGicd;
 
DETAILS
Flag determines whether to initialize certain global GIC distributor registers. It is set to false when running under a hypervisor and should be true if not running under a hypervisor.
 
extern Hwi_gicc
C synopsis target-domain
Hwi_Gicc Hwi_gicc; // linked as extern ti_sysbios_family_arm_gic_Hwi_gicc
 
 
extern Hwi_gicd
C synopsis target-domain
Hwi_Gicd Hwi_gicd; // linked as extern ti_sysbios_family_arm_gic_Hwi_gicd
 
 
Hwi_clearInterrupt()  // module-wide

Clear a specific interrupt

C synopsis target-domain
Void Hwi_clearInterrupt(UInt intNum);
 
ARGUMENTS
intNum — interrupt number to clear
DETAILS
Clears a specific interrupt's pending status. The implementation is family-specific.
 
Hwi_disable()  // module-wide

Globally disable interrupts

C synopsis target-domain
macro UInt Hwi_disable();
 
RETURNS
opaque key for use by Hwi_restore()
DETAILS
Hwi_disable globally disables hardware interrupts and returns an opaque key indicating whether interrupts were globally enabled or disabled on entry to Hwi_disable(). The actual value of the key is target/device specific and is meant to be passed to Hwi_restore().
Call Hwi_disable before a portion of a function that needs to run without interruption. When critical processing is complete, call Hwi_restore or Hwi_enable to reenable hardware interrupts.
Servicing of interrupts that occur while interrupts are disabled is postponed until interrupts are reenabled. However, if the same type of interrupt occurs several times while interrupts are disabled, the interrupt's function is executed only once when interrupts are reenabled.
A context switch can occur when calling Hwi_enable or Hwi_restore if an enabled interrupt occurred while interrupts are disabled.
Hwi_disable may be called from main(). However, since Hwi interrupts are already disabled in main(), such a call has no effect.
NOTE
Disables only IRQ interrupts
CONSTRAINTS
If a Task switching API such as Semaphore_pend(), Semaphore_post(), Task_sleep(), or Task_yield() is invoked which results in a context switch while interrupts are disabled, an embedded call to Hwi_enable occurs on the way to the new thread context which unconditionally re-enables interrupts. Interrupts will remain enabled until a subsequent Hwi_disable invocation.
Swis always run with interrupts enabled. See Swi_post() for a discussion Swis and interrupts.
 
Hwi_disableFIQ()  // module-wide

Disable FIQ interrupts

C synopsis target-domain
macro UInt Hwi_disableFIQ();
 
RETURNS
previous FIQ interrupt enable/disable state
 
Hwi_disableIRQ()  // module-wide

Disable IRQ interrupts

C synopsis target-domain
macro UInt Hwi_disableIRQ();
 
RETURNS
previous IRQ interrupt enable/disable state
NOTE
Same as Hwi_disable()
 
Hwi_disableInterrupt()  // module-wide

Disable a specific interrupt

C synopsis target-domain
UInt Hwi_disableInterrupt(UInt intNum);
 
ARGUMENTS
intNum — interrupt number to disable
RETURNS
key to restore previous enable/disable state
DETAILS
Disable a specific interrupt identified by an interrupt number.
 
Hwi_enable()  // module-wide

Globally enable interrupts

C synopsis target-domain
macro UInt Hwi_enable();
 
RETURNS
opaque key for use by Hwi_restore()
DETAILS
Hwi_enable globally enables hardware interrupts and returns an opaque key indicating whether interrupts were globally enabled or disabled on entry to Hwi_enable(). The actual value of the key is target/device specific and is meant to be passed to Hwi_restore().
This function is called as part of SYS/BIOS Startup_POST_APP_MAIN phase.
Hardware interrupts are enabled unless a call to Hwi_disable disables them.
Servicing of interrupts that occur while interrupts are disabled is postponed until interrupts are reenabled. However, if the same type of interrupt occurs several times while interrupts are disabled, the interrupt's function is executed only once when interrupts are reenabled.
A context switch can occur when calling Hwi_enable or Hwi_restore if an enabled interrupt occurred while interrupts are disabled.
Any call to Hwi_enable enables interrupts, even if Hwi_disable has been called several times.
Hwi_enable must not be called from main().
NOTE
Enables only IRQ interrupts
 
Hwi_enableFIQ()  // module-wide

Enable FIQ interrupts

C synopsis target-domain
macro UInt Hwi_enableFIQ();
 
RETURNS
previous FIQ interrupt enable/disable state
 
Hwi_enableIRQ()  // module-wide

Enable IRQ interrupts

C synopsis target-domain
macro UInt Hwi_enableIRQ();
 
RETURNS
previous IRQ interrupt enable/disable state
NOTE
Same as Hwi_enable()
 
Hwi_enableInterrupt()  // module-wide

Enable a specific interrupt

C synopsis target-domain
UInt Hwi_enableInterrupt(UInt intNum);
 
ARGUMENTS
intNum — interrupt number to enable
RETURNS
key to restore previous enable/disable state
DETAILS
Enables a specific interrupt identified by an interrupt number.
 
Hwi_getCoreStackInfo()  // module-wide

Get Hwi stack usage Info for the specified coreId

C synopsis target-domain
Bool Hwi_getCoreStackInfo(IHwi_StackInfo *stkInfo, Bool computeStackDepth, UInt coreId);
 
ARGUMENTS
stkInfo — pointer to structure of type StackInfo
computeStackDepth — decides whether to compute stack depth
coreId — core whose stack info needs to be retrieved
RETURNS
boolean to indicate a stack overflow
DETAILS
getCoreStackInfo returns the Hwi stack usage info for the specified coreId to its calling function by filling stack base address, stack size and stack peak fields in the StackInfo structure.
This function should be used only in applications built with ti.sysbios.BIOS.smpEnabled set to true.
getCoreStackInfo accepts three arguments, a pointer to a structure of type StackInfo, a boolean and a coreId. If the boolean is set to true, the function computes the stack depth and fills the stack peak field in the StackInfo structure. If a stack overflow is detected, the stack depth is not computed. If the boolean is set to false, the function only checks for a stack overflow.
The isr stack is always checked for an overflow and a boolean is returned to indicate whether an overflow occured.
Below is an example of calling getCoreStackInfo() API:
  #include <ti/sysbios/BIOS.h>
  #include <ti/sysbios/hal/Hwi.h>
  #include <ti/sysbios/hal/Core.h>
  #include <ti/sysbios/knl/Task.h>

  ...

  Void idleTask()
  {
      UInt idx;
      Hwi_StackInfo stkInfo;
      Bool stackOverflow = FALSE;

      // Request stack depth for each core's Hwi stack and check for
      // overflow
      for (idx = 0; idx < Core_numCores; idx++) {
          stackOverflow = Hwi_getCoreStackInfo(&stkInfo, TRUE, idx);

          // Alternately, we can omit the request for stack depth and
          // request only the stack base and stack size (the check for
          // stack overflow is always performed):
          //
          // stackOverflow = Hwi_getCoreStackInfo(&stkInfo, FALSE, idx);

          if (stackOverflow) {
              // isr Stack Overflow detected
          }
      }
  }

  Int main(Int argc, char* argv[])
  {
      ...
      BIOS_start();
      return (0);
  }
 
Hwi_getHandle()  // module-wide

Returns Hwi_Handle associated with intNum

C synopsis target-domain
Hwi_Handle Hwi_getHandle(UInt intNum);
 
ARGUMENTS
intNum — interrupt number
 
Hwi_getStackInfo()  // module-wide

Get Hwi stack usage Info

C synopsis target-domain
Bool Hwi_getStackInfo(IHwi_StackInfo *stkInfo, Bool computeStackDepth);
 
ARGUMENTS
stkInfo — pointer to structure of type StackInfo
computeStackDepth — decides whether to compute stack depth
RETURNS
boolean to indicate a stack overflow
DETAILS
getStackInfo returns the Hwi stack usage info to its calling function by filling stack base address, stack size and stack peak fields in the StackInfo structure.
getStackInfo accepts two arguments, a pointer to a structure of type StackInfo and a boolean. If the boolean is set to true, the function computes the stack depth and fills the stack peak field in the StackInfo structure. If a stack overflow is detected, the stack depth is not computed. If the boolean is set to false, the function only checks for a stack overflow.
The isr stack is always checked for an overflow and a boolean is returned to indicate whether an overflow occured.
Below is an example of calling getStackInfo() API:
  #include <ti/sysbios/BIOS.h>
  #include <ti/sysbios/hal/Hwi.h>
  #include <ti/sysbios/knl/Swi.h>
  #include <ti/sysbios/knl/Task.h>

  Swi_Handle swi0;
  volatile Bool swiStackOverflow = FALSE;

  Void swi0Fxn(UArg arg1, UArg arg2)
  {
      Hwi_StackInfo stkInfo;

      // Request stack depth
      swiStackOverflow = Hwi_getStackInfo(&stkInfo, TRUE);
 
      // Alternately, we can omit the request for stack depth and 
      // request only the stack base and stack size (the check for
      // stack overflow is always performed):
      //
      // swiStackOverflow = Hwi_getStackInfo(&stkInfo, FALSE);

      if (swiStackOverflow) {
          // isr Stack Overflow detected
      }
  }

  Void idleTask()
  {
      Swi_post(swi0);
  }

  Int main(Int argc, char* argv[])
  {
      swi0 = Swi_create(swi0Fxn, NULL, NULL);

      BIOS_start();
      return (0);
  }
 
Hwi_post()  // module-wide

Generate an interrupt for test purposes

C synopsis target-domain
Void Hwi_post(UInt intNum);
 
ARGUMENTS
intNum — ID of interrupt to generate
 
Hwi_restore()  // module-wide

Globally restore interrupts

C synopsis target-domain
macro Void Hwi_restore(UInt key);
 
ARGUMENTS
key — enable/disable state to restore
DETAILS
Hwi_restore globally restores interrupts to the state determined by the key argument provided by a previous invocation of Hwi_disable.
A context switch may occur when calling Hwi_restore if Hwi_restore reenables interrupts and another Hwi occurred while interrupts were disabled.
Hwi_restore may be called from main(). However, since Hwi_enable cannot be called from main(), interrupts are always disabled in main(), and a call to Hwi_restore has no effect.
NOTE
Restores only IRQ interrupts
 
Hwi_restoreFIQ()  // module-wide

Restore FIQ interrupts

C synopsis target-domain
macro Void Hwi_restoreFIQ(UInt key);
 
ARGUMENTS
key — enable/disable state to restore
 
Hwi_restoreIRQ()  // module-wide

Restore IRQ interrupts

C synopsis target-domain
macro Void Hwi_restoreIRQ(UInt key);
 
ARGUMENTS
key — enable/disable state to restore
NOTE
Same as Hwi_restore()
 
Hwi_restoreInterrupt()  // module-wide

Restore a specific interrupt's enabled/disabled state

C synopsis target-domain
Void Hwi_restoreInterrupt(UInt intNum, UInt key);
 
ARGUMENTS
intNum — interrupt number to restore
key — key returned from enableInt or disableInt
DETAILS
Restores a specific interrupt identified by an interrupt number. restoreInterrupt is generally used to restore an interrupt to its state before disableInterrupt or enableInterrupt was invoked
 
Hwi_setPriority()  // module-wide

Set an interrupt's priority

C synopsis target-domain
Void Hwi_setPriority(UInt intNum, UInt priority);
 
ARGUMENTS
intNum — ID of interrupt
priority — priority
DETAILS
Not an instance function so that it can be used with non-dispatched interrupts.
 
Hwi_startup()  // module-wide

Initially enable interrupts

C synopsis target-domain
Void Hwi_startup();
 
DETAILS
Called within BIOS_start
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId Hwi_Module_id();
// Get this module's unique id
 
Bool Hwi_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle Hwi_Module_heap();
// The heap from which this module allocates memory
 
Bool Hwi_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 Hwi_Module_getMask();
// Returns the diagnostics mask for this module
 
Void Hwi_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct Hwi_Object Hwi_Object;
// Opaque internal representation of an instance object
 
typedef Hwi_Object *Hwi_Handle;
// Client reference to an instance object
 
typedef struct Hwi_Struct Hwi_Struct;
// Opaque client structure large enough to hold an instance object
 
Hwi_Handle Hwi_handle(Hwi_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
Hwi_Struct *Hwi_struct(Hwi_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct Hwi_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
    UArg arg;
    // ISR function argument. Default is 0
    Bool enableInt;
    // Enable this interrupt when object is created? Default is true
    Int eventId;
    // Interrupt event ID (Interrupt Selection Number)
    IHwi_MaskingOption maskSetting;
    // The interrupt controller is designed for priority based interrupts
    Int priority;
    // Hwi instance interrupt priority
    UInt targetProcList;
    // Set an interrupt's target processor list
    UInt triggerSensitivity;
    // Set an interrupt's trigger sensitivity
    Hwi_Type type;
    // Interrupt type (IRQ/FIQ). Default is IRQ
} Hwi_Params;
 
Void Hwi_Params_init(Hwi_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
 
config Hwi_Params.arg  // instance

ISR function argument. Default is 0

C synopsis target-domain
struct Hwi_Params {
      ...
    UArg arg;
 
 
config Hwi_Params.enableInt  // instance

Enable this interrupt when object is created? Default is true

C synopsis target-domain
struct Hwi_Params {
      ...
    Bool enableInt;
 
 
config Hwi_Params.eventId  // instance

Interrupt event ID (Interrupt Selection Number)

C synopsis target-domain
struct Hwi_Params {
      ...
    Int eventId;
 
DETAILS
Default is -1. Not all targets/devices support this instance parameter. On those that don't, this parameter is ignored.
 
config Hwi_Params.maskSetting  // instance

The interrupt controller is designed for priority based interrupts

C synopsis target-domain
struct Hwi_Params {
      ...
    IHwi_MaskingOption maskSetting;
 
 
config Hwi_Params.priority  // instance

Hwi instance interrupt priority

C synopsis target-domain
struct Hwi_Params {
      ...
    Int priority;
 
DETAILS
The default value of -1 is used as a flag to indicate the lowest (logical) device-specific priority value.
Not all targets/devices support this instance parameter. On those that don't, this parameter is ignored.
Valid priorities are device dependent and their nesting behaviors depend on the BPR setting.
See the ARM GIC Architecture Specification v2.0 document for more details.
 
config Hwi_Params.targetProcList  // instance

Set an interrupt's target processor list

C synopsis target-domain
struct Hwi_Params {
      ...
    UInt targetProcList;
 
DETAILS
This is an 8-bit CPU targets field that stores the list of target processors for the interrupt. That is, it holds the list of CPU interfaces to which the GIC Distributor will forward the interrupt if it is asserted and has sufficient priority.
Each bit in targetProcList refers to the corresponding processor. For instance, a value of 0x3 means the pending interrupt is forwarded to processor 0 and 1.
For more information please refer section 4.3.12 on Interrupt Processor Targets Registers (GICD_ITARGETSRn) in ARM Generic Interrupt Controller Architecure Spec v2.0
If running in SMP mode and both the targetProcList Hwi param as well as the intAffinity[] array entry for the intNum are set, targetProcList is given precedence and is used to configure the interrupt's target processors.
NOTE
Target processor list is read-only for the first 32 interrupts. Therefore, this field will have no effect for interrupt numbers less than 32 (intNum 0-31).
 
config Hwi_Params.triggerSensitivity  // instance

Set an interrupt's trigger sensitivity

C synopsis target-domain
struct Hwi_Params {
      ...
    UInt triggerSensitivity;
 
DETAILS
2-bit field that configures the trigger sensitivity of an interrupt.
On the Cortex-A15, all software generated interrupts (SGI) are edge-triggered (b10) and all private peripheral interrupts (PPI) are level-sensitive (b01). The trigger sensitivity of these interrupt types cannot be changed.
For shared peripheral interrupts (SPI), the LSB of the bit-pair is read only and is always 1. The MSB of the bit-pair can be altered to change trigger sensitivity.
Possible bit-pair encodings for Cortex-A15 SPIs: b01 Interrupt is active-High level-sensitive (default) b11 Interrupt is rising edge-sensitive
For more information please refer section 4.3.13 on Interrupt Configuration Registers (GICD_ICFGRn) in ARM Generic Interrupt Controller Architecure Spec v2.0
 
config Hwi_Params.type  // instance

Interrupt type (IRQ/FIQ). Default is IRQ

C synopsis target-domain
struct Hwi_Params {
      ...
    Hwi_Type type;
 
NOTE
FIQs are only supported when enableSecureMode is set to true.
Runtime Instance Creation

C synopsis target-domain
Hwi_Handle Hwi_create(Int intNum, IHwi_FuncPtr hwiFxn, const Hwi_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void Hwi_construct(Hwi_Struct *structP, Int intNum, IHwi_FuncPtr hwiFxn, const Hwi_Params *params, Error_Block *eb);
// Initialize a new instance object inside the provided structure
ARGUMENTS
intNum — interrupt number
hwiFxn — pointer to ISR function
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Hwi dispatcher table entry is created and filled with the function specified by the fxn parameter and the attributes specified by the params parameter.
If params is NULL, the Hwi's dispatcher properties are assigned a default set of values. Otherwise, the following properties are specified by a structure of type Hwi_Params.
  • The arg element is a generic argument that is passed to the plugged function as its only parameter. The default value is 0.
  • The enableInt element determines whether the interrupt should be enabled in the IER by create.
  • The maskSetting element defines the dispatcherAutoNestingSupport behavior of the interrupt.
Hwi_create returns a pointer to the created Hwi object.
Instance Deletion

C synopsis target-domain
Void Hwi_delete(Hwi_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void Hwi_destruct(Hwi_Struct *structP);
// Finalize the instance object inside the provided structure
 
Hwi_getFunc()  // instance

Get Hwi function and arg

C synopsis target-domain
IHwi_FuncPtr Hwi_getFunc(Hwi_Handle handle, UArg *arg);
 
ARGUMENTS
handle — handle of a previously-created Hwi instance object
arg — pointer for returning hwi's ISR function argument
RETURNS
hwi's ISR function
 
Hwi_getHookContext()  // instance

Get hook instance's context for a Hwi

C synopsis target-domain
Ptr Hwi_getHookContext(Hwi_Handle handle, Int id);
 
ARGUMENTS
handle — handle of a previously-created Hwi instance object
RETURNS
hook instance's context for hwi
 
Hwi_getIrp()  // instance

Get address of interrupted instruction

C synopsis target-domain
IHwi_Irp Hwi_getIrp(Hwi_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created Hwi instance object
RETURNS
most current IRP of a Hwi
 
Hwi_reconfig()  // instance

Reconfigure a dispatched interrupt

C synopsis target-domain
Void Hwi_reconfig(Hwi_Handle handle, Hwi_FuncPtr fxn, Hwi_Params *params);
 
ARGUMENTS
handle — handle of a previously-created Hwi instance object
 
Hwi_setFunc()  // instance

Overwrite Hwi function and arg

C synopsis target-domain
Void Hwi_setFunc(Hwi_Handle handle, IHwi_FuncPtr fxn, UArg arg);
 
ARGUMENTS
handle — handle of a previously-created Hwi instance object
fxn — pointer to ISR function
arg — argument to ISR function
DETAILS
Replaces a Hwi object's hwiFxn function originally provided in create.
CONSTRAINTS
Hwi_setFunc() is not thread safe. This means that the new value for for 'fxn' may be temporarily paired with the previous value for 'arg' if pre-emption occurs within the execution of Hwi_setFunc().
To guard against this condition, surround the Hwi_setFunc() call with calls to Hwi_disable() and Hwi_restore():
  key = Hwi_disable();

  Hwi_setFunc(newFunc, newArg);

  Hwi_restore(key);
 
Hwi_setHookContext()  // instance

Set hook instance's context for a Hwi

C synopsis target-domain
Void Hwi_setHookContext(Hwi_Handle handle, Int id, Ptr hookContext);
 
ARGUMENTS
handle — handle of a previously-created Hwi instance object
id — hook instance's ID
hookContext — value to write to context
Instance Convertors

C synopsis target-domain
IHwi_Handle Hwi_Handle_upCast(Hwi_Handle handle);
// unconditionally move one level up the inheritance hierarchy
 
Hwi_Handle Hwi_Handle_downCast(IHwi_Handle handle);
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins

C synopsis target-domain
Int Hwi_Object_count();
// The number of statically-created instance objects
 
Hwi_Handle Hwi_Object_get(Hwi_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
Hwi_Handle Hwi_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
Hwi_Handle Hwi_Object_next(Hwi_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle Hwi_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *Hwi_Handle_label(Hwi_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String Hwi_Handle_name(Hwi_Handle handle);
// The name of this instance object
 
Configuration settings sourced in ti/sysbios/family/arm/gic/Hwi.xdc
var Hwi = xdc.useModule('ti.sysbios.family.arm.gic.Hwi');
module-wide constants & types
        const Hwi.MaskingOption_NONE;
        const Hwi.MaskingOption_ALL;
        const Hwi.MaskingOption_SELF;
        const Hwi.MaskingOption_BITMASK;
        const Hwi.MaskingOption_LOWER;
 
        const Hwi.Type_IRQ// IRQ interrupt;
        const Hwi.Type_FIQ// FIQ interrupt;
 
        obj.CTLR// 0x0000 CPU Interface Control Register = UInt32  ...
        obj.PMR// 0x0004 Interrupt Priority Mask Register = UInt32  ...
        obj.BPR// 0x0008 Binary Point Register = UInt32  ...
        obj.IAR// 0x000C Interrupt Acknowledge Register = UInt32  ...
        obj.EOIR// 0x0010 End Of Interrupt Register = UInt32  ...
        obj.RPR// 0x0014 Running Priority Register = UInt32  ...
        obj.ABPR// 0x001C Aliased Binary Point Register = UInt32  ...
        obj.AIAR// 0x0020 Aliased IAR Register = UInt32  ...
        obj.AEOIR// 0x0024 Aliased EOI Register = UInt32  ...
        obj.AHPPIR// 0x0028 Aliased HPPI Register = UInt32  ...
        obj.hole0// 0x002C-0x00CC = UInt32[41]  ...
        obj.APR0// 0x00D0 Active Priority Register = UInt32  ...
        obj.hole1// 0x00D4-0x00DC = UInt32[3]  ...
        obj.NSAPR0// 0x00E0 Non-secure Active Priority Register = UInt32  ...
        obj.hole2// 0x00E4-0x00F8 = UInt32[6]  ...
        obj.IIDR// 0x00FC CPU Interface Id Register = UInt32  ...
        obj.hole3// 0x0100-0x0FFC = UInt32[960]  ...
        obj.DIR// 0x1000 Deactivate Interrupt Register = UInt32  ...
 
        obj.CTLR// 0x000 Distributor Control Register = UInt32  ...
        obj.TYPER// 0x004 Interrupt Controller Type Register = UInt32  ...
        obj.IIDR// 0x008 Distributor Implementor Id Register = UInt32  ...
        obj.hole0// 0x00C-0x07C = UInt32[29]  ...
        obj.IGROUPR// 0x080 Interrupt Group Registers = UInt32[32]  ...
        obj.ISENABLER// 0x100 Interrupt Set-Enable Registers = UInt32[32]  ...
        obj.ICENABLER// 0x180 Interrupt Clear-Enable Registers = UInt32[32]  ...
        obj.ISPENDR// 0x200 Interrupt Set-Pending Registers = UInt32[32]  ...
        obj.ICPENDR// 0x280 Interrupt Clear-Pending Registers = UInt32[32]  ...
        obj.ISACTIVER// 0x300 Interrupt Set-Active Registers = UInt32[32]  ...
        obj.ICACTIVER// 0x380 Interrupt Clear-Active Registers = UInt32[32]  ...
        obj.IPRIORITYR// 0x400 Interrupt Priority Registers = UInt32[255]  ...
        obj.hole1// 0x7FC = UInt32[1]  ...
        obj.ITARGETSR// 0x800 Interrupt Processor Targets Register = UInt32[255]  ...
        obj.hole2// 0xBFC = UInt32[1]  ...
        obj.ICFGR// 0xC00 Interrupt Configuration Registers = UInt32[64]  ...
        obj.PPISR// 0xD00 PPI Status Register = UInt32  ...
        obj.SPISR// 0xD04 SPI Status Registers = UInt32[7]  ...
        obj.hole3// 0xD20-0xEFC = UInt32[120]  ...
        obj.SGIR// 0xF00 Software Generated Interrupt Registers = UInt32  ...
        obj.hole4// 0xF04-0xF0C = UInt32[3]  ...
        obj.CPENDSGIR// 0xF10 SGI Clear-Pending Registers = UInt32[4]  ...
        obj.SPENDSGIR// 0xF20 SGI Set-Pending Registers = UInt32[4]  ...
        obj.hole5// 0xF30-0xFCC = UInt32[40]  ...
        obj.PIDR4// 0xFD0 Peripheral ID4 Register = UInt32  ...
        obj.PIDR5// 0xFD4 Peripheral ID5 Register = UInt32  ...
        obj.PIDR6// 0xFD8 Peripheral ID6 Register = UInt32  ...
        obj.PIDR7// 0xFDC Peripheral ID7 Register = UInt32  ...
        obj.PIDR0// 0xFE0 Peripheral ID0 Register = UInt32  ...
        obj.PIDR1// 0xFE4 Peripheral ID1 Register = UInt32  ...
        obj.PIDR2// 0xFE8 Peripheral ID2 Register = UInt32  ...
        obj.PIDR3// 0xFEC Peripheral ID3 Register = UInt32  ...
        obj.CIDR0// 0xFF0 Component ID0 Register = UInt32  ...
        obj.CIDR1// 0xFF4 Component ID1 Register = UInt32  ...
        obj.CIDR2// 0xFF8 Component ID2 Register = UInt32  ...
        obj.CIDR3// 0xFFC Component ID3 Register = UInt32  ...
 
        obj.registerFxn = Void(*)(Int)  ...
        obj.createFxn = Void(*)(IHwi.Handle,Error.Block*)  ...
        obj.beginFxn = Void(*)(IHwi.Handle)  ...
        obj.endFxn = Void(*)(IHwi.Handle)  ...
        obj.deleteFxn = Void(*)(IHwi.Handle)  ...
 
        obj.hwiStackPeak = SizeT  ...
        obj.hwiStackSize = SizeT  ...
        obj.hwiStackBase = Ptr  ...
module-wide config parameters
        msg: "A_badSGIIntNum: SGI intNum should be <= 15."
    };
    Hwi.BPR// GIC Binary Point Register value = UInt undefined;
        msg: "E_alreadyDefined: Hwi already defined, intnum: %d"
    };
        msg: "E_badIntNum, intnum: %d is out of range"
    };
        msg: "E_handleNotFound: Hwi handle not found: 0x%x"
    };
        msg: "E_undefined: Hwi undefined, intnum: %d"
    };
        mask: Diags.USER2,
        msg: "LD_end: hwi: 0x%x"
    };
        mask: Diags.USER1 | Diags.USER2,
        msg: "LM_begin: hwi: 0x%x, func: 0x%x, preThread: %d, intNum: %d, irp: 0x%x"
    };
 
    Hwi.fiqStacks//  = Ptr[] undefined;
    Hwi.resetFunc// Reset Handler. Default is _c_int00 = Void(*)(Void) undefined;
module-wide functions
per-instance config parameters
    var params = new Hwi.Params// Instance config-params object;
        params.arg// ISR function argument. Default is 0 = UArg 0;
        params.priority// Hwi instance interrupt priority = Int -1;
per-instance creation
    var inst = Hwi.create// Create an instance-object(Int intNum, Void(*)(UArg) hwiFxn, params);
 
 
enum Hwi.MaskingOption

Shorthand interrupt masking options

Configuration settings
values of type Hwi.MaskingOption
    const Hwi.MaskingOption_NONE;
    const Hwi.MaskingOption_ALL;
    const Hwi.MaskingOption_SELF;
    const Hwi.MaskingOption_BITMASK;
    const Hwi.MaskingOption_LOWER;
 
VALUES
MaskingOption_NONE — No interrupts are disabled
MaskingOption_ALL — All interrupts are disabled
MaskingOption_SELF — Only this interrupt is disabled
MaskingOption_BITMASK — User supplies interrupt enable masks
MaskingOption_LOWER — All current and lower priority interrupts are disabled.
Only a few targets/devices truly support this masking option. For those that don't, this setting is treated the same as MaskingOption_SELF.
C SYNOPSIS
 
enum Hwi.Type

Interrupt type. IRQ or FIQ

Configuration settings
values of type Hwi.Type
    const Hwi.Type_IRQ;
    // IRQ interrupt
    const Hwi.Type_FIQ;
    // FIQ interrupt
 
C SYNOPSIS
 
struct Hwi.Gicc

Generic Interrupt Controller CPU Interface. Symbol "Hwi_gicc" is a physical device

Configuration settings
var obj = new Hwi.Gicc;
 
    obj.CTLR = UInt32  ...
    // 0x0000 CPU Interface Control Register
    obj.PMR = UInt32  ...
    // 0x0004 Interrupt Priority Mask Register
    obj.BPR = UInt32  ...
    // 0x0008 Binary Point Register
    obj.IAR = UInt32  ...
    // 0x000C Interrupt Acknowledge Register
    obj.EOIR = UInt32  ...
    // 0x0010 End Of Interrupt Register
    obj.RPR = UInt32  ...
    // 0x0014 Running Priority Register
    obj.HPPIR = UInt32  ...
    // 0x0018 Highest Priority Pending Interrupt Register
    obj.ABPR = UInt32  ...
    // 0x001C Aliased Binary Point Register
    obj.AIAR = UInt32  ...
    // 0x0020 Aliased IAR Register
    obj.AEOIR = UInt32  ...
    // 0x0024 Aliased EOI Register
    obj.AHPPIR = UInt32  ...
    // 0x0028 Aliased HPPI Register
    obj.hole0 = UInt32[41]  ...
    // 0x002C-0x00CC
    obj.APR0 = UInt32  ...
    // 0x00D0 Active Priority Register
    obj.hole1 = UInt32[3]  ...
    // 0x00D4-0x00DC
    obj.NSAPR0 = UInt32  ...
    // 0x00E0 Non-secure Active Priority Register
    obj.hole2 = UInt32[6]  ...
    // 0x00E4-0x00F8
    obj.IIDR = UInt32  ...
    // 0x00FC CPU Interface Id Register
    obj.hole3 = UInt32[960]  ...
    // 0x0100-0x0FFC
    obj.DIR = UInt32  ...
    // 0x1000 Deactivate Interrupt Register
 
C SYNOPSIS
 
struct Hwi.Gicd

Generic Interrupt Controller Distributor. Symbol "Hwi_gicd" is a physical device

Configuration settings
var obj = new Hwi.Gicd;
 
    obj.CTLR = UInt32  ...
    // 0x000 Distributor Control Register
    obj.TYPER = UInt32  ...
    // 0x004 Interrupt Controller Type Register
    obj.IIDR = UInt32  ...
    // 0x008 Distributor Implementor Id Register
    obj.hole0 = UInt32[29]  ...
    // 0x00C-0x07C
    obj.IGROUPR = UInt32[32]  ...
    // 0x080 Interrupt Group Registers
    obj.ISENABLER = UInt32[32]  ...
    // 0x100 Interrupt Set-Enable Registers
    obj.ICENABLER = UInt32[32]  ...
    // 0x180 Interrupt Clear-Enable Registers
    obj.ISPENDR = UInt32[32]  ...
    // 0x200 Interrupt Set-Pending Registers
    obj.ICPENDR = UInt32[32]  ...
    // 0x280 Interrupt Clear-Pending Registers
    obj.ISACTIVER = UInt32[32]  ...
    // 0x300 Interrupt Set-Active Registers
    obj.ICACTIVER = UInt32[32]  ...
    // 0x380 Interrupt Clear-Active Registers
    obj.IPRIORITYR = UInt32[255]  ...
    // 0x400 Interrupt Priority Registers
    obj.hole1 = UInt32[1]  ...
    // 0x7FC
    obj.ITARGETSR = UInt32[255]  ...
    // 0x800 Interrupt Processor Targets Register
    obj.hole2 = UInt32[1]  ...
    // 0xBFC
    obj.ICFGR = UInt32[64]  ...
    // 0xC00 Interrupt Configuration Registers
    obj.PPISR = UInt32  ...
    // 0xD00 PPI Status Register
    obj.SPISR = UInt32[7]  ...
    // 0xD04 SPI Status Registers
    obj.hole3 = UInt32[120]  ...
    // 0xD20-0xEFC
    obj.SGIR = UInt32  ...
    // 0xF00 Software Generated Interrupt Registers
    obj.hole4 = UInt32[3]  ...
    // 0xF04-0xF0C
    obj.CPENDSGIR = UInt32[4]  ...
    // 0xF10 SGI Clear-Pending Registers
    obj.SPENDSGIR = UInt32[4]  ...
    // 0xF20 SGI Set-Pending Registers
    obj.hole5 = UInt32[40]  ...
    // 0xF30-0xFCC
    obj.PIDR4 = UInt32  ...
    // 0xFD0 Peripheral ID4 Register
    obj.PIDR5 = UInt32  ...
    // 0xFD4 Peripheral ID5 Register
    obj.PIDR6 = UInt32  ...
    // 0xFD8 Peripheral ID6 Register
    obj.PIDR7 = UInt32  ...
    // 0xFDC Peripheral ID7 Register
    obj.PIDR0 = UInt32  ...
    // 0xFE0 Peripheral ID0 Register
    obj.PIDR1 = UInt32  ...
    // 0xFE4 Peripheral ID1 Register
    obj.PIDR2 = UInt32  ...
    // 0xFE8 Peripheral ID2 Register
    obj.PIDR3 = UInt32  ...
    // 0xFEC Peripheral ID3 Register
    obj.CIDR0 = UInt32  ...
    // 0xFF0 Component ID0 Register
    obj.CIDR1 = UInt32  ...
    // 0xFF4 Component ID1 Register
    obj.CIDR2 = UInt32  ...
    // 0xFF8 Component ID2 Register
    obj.CIDR3 = UInt32  ...
    // 0xFFC Component ID3 Register
 
C SYNOPSIS
 
struct Hwi.HookSet

Hwi hook set type definition

Configuration settings
var obj = new Hwi.HookSet;
 
    obj.registerFxn = Void(*)(Int)  ...
    obj.createFxn = Void(*)(IHwi.Handle,Error.Block*)  ...
    obj.beginFxn = Void(*)(IHwi.Handle)  ...
    obj.endFxn = Void(*)(IHwi.Handle)  ...
    obj.deleteFxn = Void(*)(IHwi.Handle)  ...
 
DETAILS
The functions that make up a hookSet have certain restrictions. They cannot call any Hwi instance functions other than Hwi_getHookContext() and Hwi_setHookContext(). For all practical purposes, they should treat the Hwi_Handle passed to these functions as an opaque handle.
C SYNOPSIS
 
struct Hwi.StackInfo

Structure contains Hwi stack usage info

Configuration settings
var obj = new Hwi.StackInfo;
 
    obj.hwiStackPeak = SizeT  ...
    obj.hwiStackSize = SizeT  ...
    obj.hwiStackBase = Ptr  ...
 
DETAILS
Used by getStackInfo() and viewGetStackInfo() functions
C SYNOPSIS
 
config Hwi.ABPR  // module-wide

GIC Aliased Binary Point Register value for Grourp 1 interrupts

Configuration settings
Hwi.ABPR = UInt undefined;
 
DETAILS
Defines the point at which the priority value fields split into two parts, the group priority field and the sub-priority field. ABPR is used only when enableSecureMode set to true and is ignored when security mode is set to false. ABPR applies to Group 1 interrupts.
The group priority field determines interrupt preemption in case of nested interrupts whereas sub-priority field is used to determine priority within a group when multiple interrrupts belonging to the same group are pending.
Valid ABPR values are from 1-7 with the minimum value supported being implementation defined and in the range 1-4. Minimum ABPR value is 1 more than the minimum BPR value.
   --------------------------------------------------------
  | ABPR value | Group priority field | Sub-priority field |
   --------------------------------------------------------
  |     0      |          --          |         --         |
  |     1      |         [7:1]        |         [0]        |
  |     2      |         [7:2]        |        [1:0]       |
  |     3      |         [7:3]        |        [2:0]       |
  |     4      |         [7:4]        |        [3:0]       |
  |     5      |         [7:5]        |        [4:0]       |
  |     6      |         [7:6]        |        [5:0]       |
  |     7      |          [7]         |        [6:0]       |
   --------------------------------------------------------
C SYNOPSIS
 
config Hwi.A_badSGIIntNum  // module-wide

Assert raised when an interrupt number >= 16 is passed to Hwi_raiseSGI() function

Configuration settings
Hwi.A_badSGIIntNum = Assert.Desc {
    msg: "A_badSGIIntNum: SGI intNum should be <= 15."
};
 
C SYNOPSIS
 
config Hwi.BPR  // module-wide

GIC Binary Point Register value

Configuration settings
Hwi.BPR = UInt undefined;
 
DETAILS
Defines the point at which the priority value fields split into two parts, the group priority field and the sub-priority field. When running in SECURE mode, BPR applies to Group 0 interrupts and when running in NON-SECURE mode, BPR applies to Group 1 interrupts.
The group priority field determines interrupt preemption in case of nested interrupts whereas sub-priority field is used to determine priority within a group when multiple interrrupts belonging to the same group are pending.
Valid BPR values are from 0-7 with the minimum value supported being implementation defined and in the range 0-3.
   -------------------------------------------------------
  | BPR value | Group priority field | Sub-priority field |
   -------------------------------------------------------
  |     0     |         [7:1]        |         [0]        |
  |     1     |         [7:2]        |        [1:0]       |
  |     2     |         [7:3]        |        [2:0]       |
  |     3     |         [7:4]        |        [3:0]       |
  |     4     |         [7:5]        |        [4:0]       |
  |     5     |         [7:6]        |        [5:0]       |
  |     6     |          [7]         |        [6:0]       |
  |     7     |     No preemption    |        [7:0]       |
   -------------------------------------------------------
C SYNOPSIS
 
config Hwi.DEFAULT_INT_PRIORITY  // module-wide

Default Interrupt Priority

Configuration settings
Hwi.DEFAULT_INT_PRIORITY = UInt undefined;
 
DETAILS
Set to one level higher than minimum supported priority.
C SYNOPSIS
 
config Hwi.E_alreadyDefined  // module-wide

Error raised when an attempt is made to create a Hwi that has already been created

Configuration settings
Hwi.E_alreadyDefined = Error.Desc {
    msg: "E_alreadyDefined: Hwi already defined, intnum: %d"
};
 
C SYNOPSIS
 
config Hwi.E_badIntNum  // module-wide

Error raised if an attempt is made to create a Hwi with an interrupt number greater than Hwi_NUM_INTERRUPTS - 1

Configuration settings
Hwi.E_badIntNum = Error.Desc {
    msg: "E_badIntNum, intnum: %d is out of range"
};
 
C SYNOPSIS
 
config Hwi.E_handleNotFound  // module-wide

Error raised when Hwi handle referenced in Hwi_delete() is not found in the Hwi dispatch table

Configuration settings
Hwi.E_handleNotFound = Error.Desc {
    msg: "E_handleNotFound: Hwi handle not found: 0x%x"
};
 
C SYNOPSIS
 
config Hwi.E_undefined  // module-wide

Error raised when an undefined interrupt has fired

Configuration settings
Hwi.E_undefined = Error.Desc {
    msg: "E_undefined: Hwi undefined, intnum: %d"
};
 
C SYNOPSIS
 
config Hwi.LD_end  // module-wide

Issued just after return from Hwi function (with interrupts disabled)

Configuration settings
Hwi.LD_end = Log.EventDesc {
    mask: Diags.USER2,
    msg: "LD_end: hwi: 0x%x"
};
 
C SYNOPSIS
 
config Hwi.LM_begin  // module-wide

Issued just prior to Hwi function invocation (with interrupts disabled)

Configuration settings
Hwi.LM_begin = Log.EventDesc {
    mask: Diags.USER1 | Diags.USER2,
    msg: "LM_begin: hwi: 0x%x, func: 0x%x, preThread: %d, intNum: %d, irp: 0x%x"
};
 
C SYNOPSIS
 
config Hwi.MIN_INT_PRIORITY  // module-wide

Minimum Interrupt Priority

Configuration settings
Hwi.MIN_INT_PRIORITY = UInt undefined;
 
C SYNOPSIS
 
config Hwi.NUM_INTERRUPTS  // module-wide

Number of interrupts implemented in GIC

Configuration settings
Hwi.NUM_INTERRUPTS = UInt undefined;
 
DETAILS
On OMAP543x GIC implements 192 interrupts.
See the OMAP543x_ES1 Technical Reference Manual pg 5280 for more details.
C SYNOPSIS
 
config Hwi.NUM_PRIORITY_BITS  // module-wide

Number of Priority bits implemented

Configuration settings
Hwi.NUM_PRIORITY_BITS = UInt undefined;
 
DETAILS
On OMAP543x running in non-secure mode, only most significant 4 priority bits are available for use. The least significant 4 bits are always 0.
C SYNOPSIS
 
config Hwi.dispatcherAutoNestingSupport  // module-wide

Include interrupt nesting logic in interrupt dispatcher?

Configuration settings
Hwi.dispatcherAutoNestingSupport = Bool true;
 
DETAILS
Default is true.
This option provides the user with the ability to optimize interrupt dispatcher performance when support for interrupt nesting is not required.
Setting this parameter to false will disable the logic in the interrupt dispatcher that manipulates interrupt mask registers and enables and disables interrupts before and after invoking the user's Hwi function.
Set this parameter to false if you don't need interrupts enabled during the execution of your Hwi functions.
C SYNOPSIS
 
config Hwi.dispatcherIrpTrackingSupport  // module-wide

Controls whether the dispatcher retains the interrupted thread's return address

Configuration settings
Hwi.dispatcherIrpTrackingSupport = Bool true;
 
DETAILS
This option is enabled by default.
Setting this parameter to false will disable the logic in the interrupt dispatcher that keeps track of the interrupt's return address and provide a small savings in interrupt latency.
The application can get an interrupt's most recent return address using the getIrp API.
C SYNOPSIS
 
config Hwi.dispatcherSwiSupport  // module-wide

Include Swi scheduling logic in interrupt dispatcher?

Configuration settings
Hwi.dispatcherSwiSupport = Bool undefined;
 
DETAILS
Default is inherited from BIOS.swiEnabled, which is true by default.
This option provides the user with the ability to optimize interrupt dispatcher performance when it is known that Swis will not be posted from any of their Hwi threads.
WARNING
Setting this parameter to false will disable the logic in the interrupt dispatcher that invokes the Swi scheduler prior to returning from an interrupt. With this setting, Swis MUST NOT be posted from Hwi functions!
C SYNOPSIS
 
config Hwi.dispatcherTaskSupport  // module-wide

Include Task scheduling logic in interrupt dispatcher?

Configuration settings
Hwi.dispatcherTaskSupport = Bool undefined;
 
DETAILS
Default is inherited from BIOS.taskEnabled, which is true by default.
This option provides the user with the ability to optimize interrupt dispatcher performance when it is known that no Task scheduling APIs (ie Semaphore_post()) will be executed from any of their Hwi threads.
Setting this parameter to false will disable the logic in the interrupt dispatcher that invokes the Task scheduler prior to returning from an interrupt.
C SYNOPSIS
 
config Hwi.enableSecureMode  // module-wide

Security Mode

Configuration settings
Hwi.enableSecureMode = Bool false;
 
DETAILS
This field specifies the MPU's security mode. The MPU's security mode determines the type of accesses to the GIC i.e. if the MPU is in secure mode, all accesses to the GIC are secure and if the MPU is in non-secure mode, all accesses to the GIC are non-secure.
An exception to the above rule can be seen on certain devices like Keystone 2, where all GIC acceses are secure irrespective of the MPU's security state. enableSecureMode should be set to true for such devices.
C SYNOPSIS
 
config Hwi.initGicd  // module-wide

Initialize all GIC Distributor registers. True by default

Configuration settings
Hwi.initGicd = Bool true;
 
DETAILS
Flag determines whether to initialize certain global GIC distributor registers. It is set to false when running under a hypervisor and should be true if not running under a hypervisor.
C SYNOPSIS
 
metaonly config Hwi.common$  // module-wide

Common module configuration parameters

Configuration settings
Hwi.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly config Hwi.dataAbortFunc  // module-wide

Data abort exception handler. Default is an internal exception handler

Configuration settings
Hwi.dataAbortFunc = Void(*)(Void) undefined;
 
 
metaonly config Hwi.fiqFunc  // module-wide

FIQ interrupt handler. Default is internal exception handler

Configuration settings
Hwi.fiqFunc = Void(*)(Void) undefined;
 
 
metaonly config Hwi.fiqStackSection  // module-wide

Memory section used for FIQ stack Default is null

Configuration settings
Hwi.fiqStackSection = String null;
 
 
metaonly config Hwi.fiqStackSize  // module-wide

FIQ stack size in MAUs. Default is 1024 bytes

Configuration settings
Hwi.fiqStackSize = SizeT 1024;
 
DETAILS
If running in SMP mode, the FIQ stacks on all cores are set to this size.
 
metaonly config Hwi.fiqStacks  // module-wide
Configuration settings
Hwi.fiqStacks = Ptr[] undefined;
 
 
metaonly config Hwi.intAffinity  // module-wide

SMP Interrupt affinity mappings

Configuration settings
Hwi.intAffinity = UInt8[] undefined;
 
DETAILS
In SMP mode, this array maps an interrupt number to the coreId it is to be tied to. By default, all ints are mapped to core 0.
For example, to make Timer 1 from the ti.sysbios.timers.dmtimer.Timer module interrupt on core 1 rather than core 0, add the following to your config file:
     var Hwi = xdc.useModule('ti.sysbios.family.arm.gic.Hwi');
     Hwi.intAffinity[<intNum>] = 1;
CONSTRAINTS
Interrupt numbers below 32 are ignored. This config param only allows routing interrupt numbers greater than or equal to #32.
 
metaonly config Hwi.irqFunc  // module-wide

IRQ interrupt handler. Default is internal IRQ dispatcher

Configuration settings
Hwi.irqFunc = Void(*)(Void) undefined;
 
 
metaonly config Hwi.prefetchAbortFunc  // module-wide

Prefetch abort exception handler. Default is an internal exception handler

Configuration settings
Hwi.prefetchAbortFunc = Void(*)(Void) undefined;
 
 
metaonly config Hwi.reservedFunc  // module-wide

Reserved exception handler. Default is an internal exception handler

Configuration settings
Hwi.reservedFunc = Void(*)(Void) undefined;
 
 
metaonly config Hwi.resetFunc  // module-wide

Reset Handler. Default is _c_int00

Configuration settings
Hwi.resetFunc = Void(*)(Void) undefined;
 
 
metaonly config Hwi.svcFunc  // module-wide

SVC Handler. Supervisor Call exception handler. (previously called Software Interrupt or SWI) Default is an internal exception handler

Configuration settings
Hwi.svcFunc = Void(*)(Void) undefined;
 
 
metaonly config Hwi.undefinedInstFunc  // module-wide

Undefined instruction exception handler. Default is an internal exception handler

Configuration settings
Hwi.undefinedInstFunc = Void(*)(Void) undefined;
 
 
metaonly Hwi.addHookSet()  // module-wide

addHookSet is used in a config file to add a hook set (defined by struct HookSet)

Configuration settings
Hwi.addHookSet(IHwi.HookSet hook) returns Void
 
ARGUMENTS
hook — structure of type HookSet
DETAILS
HookSet structure elements may be omitted, in which case those elements will not exist.
Instance Config Parameters

Configuration settings
var params = new Hwi.Params;
// Instance config-params object
    params.arg = UArg 0;
    // ISR function argument. Default is 0
    params.enableInt = Bool true;
    // Enable this interrupt when object is created? Default is true
    params.eventId = Int -1;
    // Interrupt event ID (Interrupt Selection Number)
    params.maskSetting = IHwi.MaskingOption IHwi.MaskingOption_LOWER;
    // The interrupt controller is designed for priority based interrupts
    params.priority = Int -1;
    // Hwi instance interrupt priority
    params.targetProcList = UInt 0x0;
    // Set an interrupt's target processor list
    params.triggerSensitivity = UInt ~(0);
    // Set an interrupt's trigger sensitivity
    params.type = Hwi.Type Hwi.Type_IRQ;
    // Interrupt type (IRQ/FIQ). Default is IRQ
 
config Hwi.Params.arg  // instance

ISR function argument. Default is 0

Configuration settings
var params = new Hwi.Params;
  ...
params.arg = UArg 0;
 
C SYNOPSIS
 
config Hwi.Params.enableInt  // instance

Enable this interrupt when object is created? Default is true

Configuration settings
var params = new Hwi.Params;
  ...
params.enableInt = Bool true;
 
C SYNOPSIS
 
config Hwi.Params.eventId  // instance

Interrupt event ID (Interrupt Selection Number)

Configuration settings
var params = new Hwi.Params;
  ...
params.eventId = Int -1;
 
DETAILS
Default is -1. Not all targets/devices support this instance parameter. On those that don't, this parameter is ignored.
C SYNOPSIS
 
config Hwi.Params.maskSetting  // instance

The interrupt controller is designed for priority based interrupts

Configuration settings
var params = new Hwi.Params;
  ...
 
C SYNOPSIS
 
config Hwi.Params.priority  // instance

Hwi instance interrupt priority

Configuration settings
var params = new Hwi.Params;
  ...
params.priority = Int -1;
 
DETAILS
The default value of -1 is used as a flag to indicate the lowest (logical) device-specific priority value.
Not all targets/devices support this instance parameter. On those that don't, this parameter is ignored.
Valid priorities are device dependent and their nesting behaviors depend on the BPR setting.
See the ARM GIC Architecture Specification v2.0 document for more details.
C SYNOPSIS
 
config Hwi.Params.targetProcList  // instance

Set an interrupt's target processor list

Configuration settings
var params = new Hwi.Params;
  ...
params.targetProcList = UInt 0x0;
 
DETAILS
This is an 8-bit CPU targets field that stores the list of target processors for the interrupt. That is, it holds the list of CPU interfaces to which the GIC Distributor will forward the interrupt if it is asserted and has sufficient priority.
Each bit in targetProcList refers to the corresponding processor. For instance, a value of 0x3 means the pending interrupt is forwarded to processor 0 and 1.
For more information please refer section 4.3.12 on Interrupt Processor Targets Registers (GICD_ITARGETSRn) in ARM Generic Interrupt Controller Architecure Spec v2.0
If running in SMP mode and both the targetProcList Hwi param as well as the intAffinity[] array entry for the intNum are set, targetProcList is given precedence and is used to configure the interrupt's target processors.
NOTE
Target processor list is read-only for the first 32 interrupts. Therefore, this field will have no effect for interrupt numbers less than 32 (intNum 0-31).
C SYNOPSIS
 
config Hwi.Params.triggerSensitivity  // instance

Set an interrupt's trigger sensitivity

Configuration settings
var params = new Hwi.Params;
  ...
params.triggerSensitivity = UInt ~(0);
 
DETAILS
2-bit field that configures the trigger sensitivity of an interrupt.
On the Cortex-A15, all software generated interrupts (SGI) are edge-triggered (b10) and all private peripheral interrupts (PPI) are level-sensitive (b01). The trigger sensitivity of these interrupt types cannot be changed.
For shared peripheral interrupts (SPI), the LSB of the bit-pair is read only and is always 1. The MSB of the bit-pair can be altered to change trigger sensitivity.
Possible bit-pair encodings for Cortex-A15 SPIs: b01 Interrupt is active-High level-sensitive (default) b11 Interrupt is rising edge-sensitive
For more information please refer section 4.3.13 on Interrupt Configuration Registers (GICD_ICFGRn) in ARM Generic Interrupt Controller Architecure Spec v2.0
C SYNOPSIS
 
config Hwi.Params.type  // instance

Interrupt type (IRQ/FIQ). Default is IRQ

Configuration settings
var params = new Hwi.Params;
  ...
params.type = Hwi.Type Hwi.Type_IRQ;
 
NOTE
FIQs are only supported when enableSecureMode is set to true.
C SYNOPSIS
Static Instance Creation

Configuration settings
var params = new Hwi.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = Hwi.create(Int intNum, Void(*)(UArg) hwiFxn, params);
// Create an instance-object
ARGUMENTS
intNum — interrupt number
hwiFxn — pointer to ISR function
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Hwi dispatcher table entry is created and filled with the function specified by the fxn parameter and the attributes specified by the params parameter.
If params is NULL, the Hwi's dispatcher properties are assigned a default set of values. Otherwise, the following properties are specified by a structure of type Hwi_Params.
  • The arg element is a generic argument that is passed to the plugged function as its only parameter. The default value is 0.
  • The enableInt element determines whether the interrupt should be enabled in the IER by create.
  • The maskSetting element defines the dispatcherAutoNestingSupport behavior of the interrupt.
Hwi_create returns a pointer to the created Hwi object.
generated on Sat, 30 Jun 2018 01:22:37 GMT