module ti.sysbios.family.arm.m3.TimestampProvider

Cortex M3 TimestampProvider

Cortex M3 TimestampProvider delegate for use with xdc.runtime.Timestamp. [ more ... ]
C synopsis target-domain sourced in ti/sysbios/family/arm/m3/TimestampProvider.xdc
DETAILS
Cortex M3 TimestampProvider delegate for use with xdc.runtime.Timestamp.
The SysTick timer is used as the timestamp source.

Calling Context

Function Hwi Swi Task Main** Startup***
get32 Y Y Y Y N
get64 Y Y Y Y N
getFreq Y Y Y Y N
 
config TimestampProvider_configTimer  // module-wide
C synopsis target-domain
extern const Bool TimestampProvider_configTimer;
 
 
TimestampProvider_get32()  // module-wide

Return a 32-bit timestamp

C synopsis target-domain
Bits32 TimestampProvider_get32();
 
RETURNS
Returns a 32-bit timestamp value. Use getFreq to convert this value into units of real time.
Returns a 32-bit timestamp value. Use getFreq to convert this value into units of real time.
SEE
 
TimestampProvider_get64()  // module-wide

Return a 64-bit timestamp

C synopsis target-domain
Void TimestampProvider_get64(Types_Timestamp64 *result);
 
ARGUMENTS
result — pointer to 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide timestamp value where the current timestamp is written.
If the underlying hardware does not support 64-bit resolution, the hi field of result is always set to 0; see xdc.runtime.Types.Timestamp64. So, it is possible for the lo field to wrap around without any change to the hi field. Use getFreq to convert this value into units of real time.
pointer to 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide timestamp value where the current timestamp is written.
If the underlying hardware does not support 64-bit resolution, the hi field of result is always set to 0; see xdc.runtime.Types.Timestamp64. So, it is possible for the lo field to wrap around without any change to the hi field. Use getFreq to convert this value into units of real time.
SEE
 
TimestampProvider_getFreq()  // module-wide

Get the timestamp timer's frequency (in Hz)

C synopsis target-domain
Void TimestampProvider_getFreq(Types_FreqHz *freq);
 
ARGUMENTS
freq — pointer to a 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide frequency value where the timer's frequency (in Hz) is written; see xdc.runtime.Types.FreqHz. This function provides a way of converting timestamp values into units of real time.
pointer to a 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide frequency value where the timer's frequency (in Hz) is written; see xdc.runtime.Types.FreqHz. This function provides a way of converting timestamp values into units of real time.
SEE
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId TimestampProvider_Module_id();
// Get this module's unique id
 
Bool TimestampProvider_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle TimestampProvider_Module_heap();
// The heap from which this module allocates memory
 
Bool TimestampProvider_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 TimestampProvider_Module_getMask();
// Returns the diagnostics mask for this module
 
Void TimestampProvider_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/sysbios/family/arm/m3/TimestampProvider.xdc
var TimestampProvider = xdc.useModule('ti.sysbios.family.arm.m3.TimestampProvider');
module-wide config parameters
    TimestampProvider.configTimer//  = Bool false;
 
 
 
config TimestampProvider.configTimer  // module-wide
Configuration settings
TimestampProvider.configTimer = Bool false;
 
C SYNOPSIS
 
metaonly config TimestampProvider.common$  // module-wide

Common module configuration parameters

Configuration settings
TimestampProvider.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Wed, 15 Apr 2015 00:19:31 GMT