GateHwi uses disabling and enabling of interrupts as the resource locking
mechanism. Such a gate guarantees exclusive access to the CPU. This gate
can be used whenever the resource is being shared by Tasks, Swis, and/or
Hwis.
The duration between the enter and leave should be as short as possible
to minimize Hwi latency.
GateHwi inherits from xdc.runtime.IGateProvider, therefore supports nesting.
const GateHwi_Q_BLOCKING |
![](../../../Arrow_up.png) |
Blocking quality
#define GateHwi_Q_BLOCKING (Int)1
DETAILS
Gates with this "quality" may cause the calling thread to block;
i.e., suspend execution until another thread leaves the gate.
const GateHwi_Q_PREEMPTING |
![](../../../Arrow_up.png) |
Preempting quality
#define GateHwi_Q_PREEMPTING (Int)2
DETAILS
Gates with this "quality" allow other threads to preempt the thread
that has already entered the gate.
GateHwi_query() // module-wide |
![](../../../Arrow_up.png) |
Runtime test for a particular gate quality
Bool GateHwi_query(Int qual);
ARGUMENTS
qual
constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality,
and FALSE otherwise, which includes the case when the gate does not
recognize the constant describing the quality.
Module-Wide Built-Ins |
![](../../../Arrow_up.png) |
// Get this module's unique id
Bool GateHwi_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool GateHwi_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 GateHwi_Module_getMask();
// Returns the diagnostics mask for this module
Void GateHwi_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
![](../../../Arrow_up.png) |
typedef struct GateHwi_Object GateHwi_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct GateHwi_Struct GateHwi_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
![](../../../Arrow_up.png) |
typedef struct GateHwi_Params {
// Instance config-params structure
// Common per-instance configs
} GateHwi_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
Runtime Instance Creation |
![](../../../Arrow_up.png) |
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
Instance Deletion |
![](../../../Arrow_up.png) |
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
GateHwi_enter() // instance |
![](../../../Arrow_up.png) |
Enter this gate
ARGUMENTS
handle
handle of a previously-created GateHwi instance object
DETAILS
Each gate provider can implement mutual exclusion using different
algorithms; e.g., disabling all scheduling, disabling the scheduling
of all threads below a specified "priority level", suspending the
caller when the gate has been entered by another thread and
re-enabling it when the the other thread leaves the gate. However,
in all cases, after this method returns that caller has exclusive
access to the data protected by this gate.
A thread may reenter a gate without blocking or failing.
RETURNS
Returns a "key" that is used to
leave this gate; this
value is used to restore thread preemption to the state that
existed just prior to entering this gate.
GateHwi_leave() // instance |
![](../../../Arrow_up.png) |
Leave this gate
ARGUMENTS
handle
handle of a previously-created GateHwi instance object
key
the value returned by a matching call to
enter
DETAILS
This method is only called by threads that have previously entered
this gate via
enter. After this method returns, the
caller must not access the data structure protected by this gate
(unless the caller has entered the gate more than once and other
calls to
leave remain to balance the number of previous
calls to
enter).
Instance Convertors |
![](../../../Arrow_up.png) |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins |
![](../../../Arrow_up.png) |
Int GateHwi_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object