The
Common$ structure defined by the
Types module
is available for (or common to) all modules. Every field of the
Common$ structure is a configuration parameter that may be set within
a configuration script for any module (not just the
xdc.runtime modules). The fields of this structure are typically read
by the modules in the
xdc.runtime package at configuration time to
control the generation of data structures that are embedded in the
application and referenced by these modules at runtime.
Every module has a configuration parameter named
common$ that is of type
Common$. This allows the user
of any module to control the module's diagnostics, where its instances
are allocated, how they are allocated, and (for gated modules) what
gate it should use to protect critical sections.
Configuration example: The following configuration script specifies
that the instance objects managed by the Memory module in the
xdc.runtime package should be placed in the ".fast" memory section
and that ENTRY diagnostics should be available at runtime.
var Memory = xdc.useModule('xdc.runtime.Memory");
Memory.common$.instanceSection = ".fast";
Memory.common$.diags_ENTRY = Diags.RUNTIME_OFF
Note that by setting
Memory.common$.diags_ENTRY to
Diags.RUNTIME_OFF
we are both enabling
ENTRY events and specifying that they are initially
disabled; they must be explicitly enabled at runtime. See the
Diags modules for additional information.
enum Types_CreatePolicy |
![](../../Arrow_up.png) |
Instance creation policy
typedef enum Types_CreatePolicy {
Types_STATIC_POLICY,
// static creation only; no runtime create/delete
Types_CREATE_POLICY,
// dynamic creation, but no deletion
Types_DELETE_POLICY
// dynamic creation and deletion
} Types_CreatePolicy;
enum Types_OutputPolicy |
![](../../Arrow_up.png) |
Destination file for module's functions
typedef enum Types_OutputPolicy {
Types_COMMON_FILE,
// functions are in the common C file
Types_SEPARATE_FILE,
// module has its own separate file
Types_NO_FILE
// functions are not generated
} Types_OutputPolicy;
typedef Types_DiagsMask |
![](../../Arrow_up.png) |
typedef Bits16 Types_DiagsMask;
typedef Types_Event |
![](../../Arrow_up.png) |
ILogger event encoding
typedef Bits32 Types_Event;
DETAILS
Whereas a
Log.Event encodes an event ID and a mask, a
Types_Event encodes the same event ID and the module ID of the
module containing the call site that generated the
Types_Event.
typedef Types_ModuleId |
![](../../Arrow_up.png) |
Unique module identifier
typedef Bits16 Types_ModuleId;
DETAILS
Module IDs are assigned at configuration time based in the set
of modules that are "used" in the application. So, although each
module has a unique 16-bit ID at runtime this ID may vary between
configurations of the application.
To save precious data space, module names are managed by the
Text module and it is this table that is used to assign
module IDs. If the table is maintained on the target, the module ID
is an "index" into this table; otherwise, the module ID is simply
a unique integer less than the total number of modules in the
application.
Although module IDs are not independent of an application's
configuration, a module's ID may be compared to a runtime value
symbolically. Every module has a (generated) method that returns
the module's ID; e.g., a module named Task has a method named
Task_Module_id() which returns Task's module ID.
#include <xdc/runtime/Types.h>
#include <ti/sysbios/knl/Task.h>
:
void checkId(Types_ModuleId modId) {
if (Task_Module_id() == modId) {
System_printf("Task module");
}
}
struct Types_FreqHz |
![](../../Arrow_up.png) |
Frequency-in-hertz struct
typedef struct Types_FreqHz {
Bits32 hi;
// most significant 32-bits of frequency
Bits32 lo;
// least significant 32-bits of frequency
} Types_FreqHz;
struct Types_Label |
![](../../Arrow_up.png) |
Instance label struct
typedef struct Types_Label {
Ptr handle;
// instance object address
// corresponding module id
String iname;
// name supplied during instance creation
Bool named;
// true, if iname is available
} Types_Label;
DETAILS
Label structures are used to provide human readable names for
instance handles.
It is possible to initialize a Label from any instance handle. All
modules that support instances provide a method named
Mod_Handle_label() which, given an instance handle and a pointer to
a Label structure, initializes the structure with all available
information. For example, the following code fragment initializes a
Label from an instance of the HeapMin module.
HeapMin_Handle heap;
Types_Label label;
HeapMin_Handle_label(heap, &label);
Unless you explicitly disable it,
System_printf
can be used to convert a pointer to a
Label into an human readable
"instance name". Continuing with the example above, the following
line can be used to print the an instance's label.
System_printf("heap instance name: %$L\n", &label);
SEE
struct Types_RegDesc |
![](../../Arrow_up.png) |
Registry module descriptor
typedef struct Types_RegDesc {
CString modName;
} Types_RegDesc;
struct Types_Site |
![](../../Arrow_up.png) |
Error site description struct
typedef struct Types_Site {
// module id of this site
CString file;
// filename of this site
Int line;
// line number of this site
} Types_Site;
FIELDS
mod
the module id of the module containing the call site
file
the name of the file containing the call site or NULL;
some call sites omit the file name to save data space.
line
the line number within the file named
DETAILS
This structure describes the location of the line that raised
an error.
struct Types_Timestamp64 |
![](../../Arrow_up.png) |
64-bit timestamp struct
typedef struct Types_Timestamp64 {
Bits32 hi;
// most significant 32-bits of timestamp
Bits32 lo;
// least significant 32-bits of timestamp
} Types_Timestamp64;
DETAILS
Some platforms only support 32-bit timestamps. In this case,
the most significant 32-bits are always set to 0.
Types_getEventId() // module-wide |
![](../../Arrow_up.png) |
Get event ID of the specified event
ARGUMENTS
DETAILS
This method is used to get an ID that can be compared to other
"known" IDs. For example, after a
Types_Event is
generated, the following code determines if the event
corresponds to a
Log.L_create event:
Bool isCreateEvent(Types_Event evt) {
return (Log_getEventId(Log_L_create) == Types_getEventId(evt));
}
RETURNS
This function returns the event ID of a specified event.
Types_getModuleId() // module-wide |
![](../../Arrow_up.png) |
Get the module ID for the specified event
ARGUMENTS
RETURNS
This function returns the module ID of a specified event.
Types_makeEvent() // module-wide |
![](../../Arrow_up.png) |
Make an Event from an Event ID and a module ID
ARGUMENTS
id
ID of the event itself
callSite
the module from which this event originated
RETURNS
This function returns an event.
Module-Wide Built-Ins |
![](../../Arrow_up.png) |
// Get this module's unique id
Bool Types_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Types_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Types_Module_getMask();
// Returns the diagnostics mask for this module
Void Types_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
enum Types.CreatePolicy |
![](../../Arrow_up.png) |
Instance creation policy
values of type Types.CreatePolicy
const Types.STATIC_POLICY;
// static creation only; no runtime create/delete
const Types.CREATE_POLICY;
// dynamic creation, but no deletion
const Types.DELETE_POLICY;
// dynamic creation and deletion
C SYNOPSIS
enum Types.OutputPolicy |
![](../../Arrow_up.png) |
Destination file for module's functions
values of type Types.OutputPolicy
const Types.COMMON_FILE;
// functions are in the common C file
const Types.SEPARATE_FILE;
// module has its own separate file
const Types.NO_FILE;
// functions are not generated
C SYNOPSIS
metaonly struct Types.Common$ |
![](../../Arrow_up.png) |
Common module config struct
var obj = new Types.Common$;
// module's Diags assert mode
// module's function entry Diags mode
// module's function exit Diags mode
// module's internal assert mode
// module's instance lifecycle mode
// module's errors and warnings
// module's user1 Diags mode
// module's user2 Diags mode
// module's user3 Diags mode
// module's user4 Diags mode
// module's user5 Diags mode
// module's user6 Diags mode
// module's user7 Diags mode
// module's informational event mode
// module's user8 Diags mode
// module's Diags analysis mode
obj.fxntab = Bool ...
// module's gate
obj.gateParams = Ptr ...
// gate params for module created gates
// module's instance heap
obj.instanceSection = String ...
// memory section for module's instances
// module's logger
// destination file for module's code
// module's memory policy
obj.namedInstance = Bool ...
// true => instances have string names
obj.namedModule = Bool ...
// true => module's name is on target
obj.romPatchTable = Bool ...
FIELDS
diags_ASSERT
The Diags.ASSERT bit of a module's
diagnostics mask.
diags_ENTRY
The Diags.ENTRY category of a module's
diagnostics mask.
diags_EXIT
The Diags.EXIT category of a module's
diagnostics mask.
diags_INTERNAL
The Diags.INTERNAL bit of a module's
diagnostics mask.
diags_LIFECYCLE
The Diags.LIFECYCLE category of a
module's diagnostics mask.
diags_STATUS
The Diags.STATUS category of a module's
diagnostics mask.
diags_USER1
The Diags.USER1 category of a module's
diagnostics mask.
diags_USER2
The Diags.USER2 category of a module's
diagnostics mask.
diags_USER3
The Diags.USER3 category of a module's
diagnostics mask.
diags_USER4
The Diags.USER4 category of a module's
diagnostics mask.
diags_USER5
The Diags.USER5 category of a module's
diagnostics mask.
diags_USER6
The Diags.USER6 category of a module's
diagnostics mask.
diags_USER7
The Diags.USER7 category of a module's
diagnostics mask. The bit for this category has been repurposed for the
Diags.INFO category, so the use of USER7 has been deprecated.
diags_INFO
The Diags.INFO category of a module's
diagnostics mask.
diags_USER8
The Diags.USER8 category of a module's
diagnostics mask. The bit for this category has been repurposed for the
Diags.ANALYSIS category, so the use of USER8 has been
deprecated.
diags_ANALYSIS
The Diags.ANALYSIS category of a
module's diagnostics mask.
fxntab
This configurtation parameter is only applicable to modules that
inherit an interface and have instance objects. Setting fxntab
to false can save some data space but also prevents the
application from using instance objects through abstract interfaces.
Function tables are used whenever it's necessary to call a module's
methods via an abstract interface; e.g., the
Memory module
calls methods defined by the
IHeap interface but there may
be several distinct modules that implement this interface. In order
for this type of call to be possible, instance objects contain a
reference to a function table containing the instance module's
functions; the caller gets the module's function from the instance
object and calls through a function pointer. Every module that
inherits an interface has such a table and modules that do not
inherit an interface do not have a function table.
If this configuration parameter is set to false, the module's
instance objects will NOT be initialized with a reference to their
module's function table and, since the function table will not
be referenced by the application, the resulting executable will be
smaller. However, if this parameter is false you must never
attempt to use this module's instance objects via reference this
module through an abstract interface. Since this is often hard to
determine, especially as an application evolves over time, you should
only set this parameter to false when you are absolutely sure that
the module's functions are always only being directly called and you
need to absolutely minimize the data footprint of your application.
The default for this parameter is true.
gate
A handle to the module-level IGateProvider
instance to be used when this module calls functions from
Gate
gateParams
Gate parameters used by this module to create
the gates used when this module calls
Gate_allocInstance
instanceHeap
Identifies the heap from which this module
should allocate memory.
instanceSection
Identifies the section in which instances
created by this module should be placed.
logger
The handle of the logger instance used by the module.
All log events generated by the module are routed to this logger
instance. See ILogger for details on the logger interface.
See LoggerBuf and LoggerSys for two examples of
logger modules provided by the xdc.runtime package.
memoryPolicy
Specifies whether this module should allow
static object creation only (STATIC_POLICY),
dynamic object creation but not deletion
(CREATE_POLICY), or both dynamic object
creation and deletion (DELETE_POLICY).
namedInstance
If set to true, each instance object is
given an additional field to hold a string name that is used
when displaying information about an instance. Setting this to
true increases the size of the module's instance objects by a
single word but improves the usability of tools that display
instance objects. If set to false, assignments of instance
names are silently ignored. This allows one to remove instance
name support to save space without having to change any source code.
See IInstance.name for details.
namedModule
If set to true, this module's string name
is retained on the target so that it can be displayed as part
of Log and Error events. Setting this to false
saves data space in the application at the expense of readability
of log and error messages associated with this module.
Note: setting this to
false also prevents one from controlling the
module's diagnostics at runtime via
Diags.setMask().
This method uses the module's name to lookup the module's
diagnostics mask. It is still possible to control the module's
diagnostics at design-time from a configuration script.
DETAILS
Every module contains this structure during the configuration
phase. The fields of this structure are set in configuration scripts
and referenced by the modules in the
xdc.runtime package. For default
values of these fields, see
Defaults.
SEE
struct Types.FreqHz |
![](../../Arrow_up.png) |
Frequency-in-hertz struct
var obj = new Types.FreqHz;
obj.hi = Bits32 ...
// most significant 32-bits of frequency
obj.lo = Bits32 ...
// least significant 32-bits of frequency
C SYNOPSIS
struct Types.Label |
![](../../Arrow_up.png) |
Instance label struct
var obj = new Types.Label;
obj.handle = Ptr ...
// instance object address
obj.modId = Bits16 ...
// corresponding module id
obj.iname = String ...
// name supplied during instance creation
obj.named = Bool ...
// true, if iname is available
DETAILS
Label structures are used to provide human readable names for
instance handles.
It is possible to initialize a Label from any instance handle. All
modules that support instances provide a method named
Mod_Handle_label() which, given an instance handle and a pointer to
a Label structure, initializes the structure with all available
information. For example, the following code fragment initializes a
Label from an instance of the HeapMin module.
HeapMin_Handle heap;
Types_Label label;
HeapMin_Handle_label(heap, &label);
Unless you explicitly disable it,
System_printf
can be used to convert a pointer to a
Label into an human readable
"instance name". Continuing with the example above, the following
line can be used to print the an instance's label.
System_printf("heap instance name: %$L\n", &label);
SEE
C SYNOPSIS
struct Types.RegDesc |
![](../../Arrow_up.png) |
Registry module descriptor
var obj = new Types.RegDesc;
obj.modName = CString ...
obj.id = Bits16 ...
obj.mask = Bits16 ...
C SYNOPSIS
struct Types.Site |
![](../../Arrow_up.png) |
Error site description struct
var obj = new Types.Site;
obj.mod = Bits16 ...
// module id of this site
obj.file = CString ...
// filename of this site
obj.line = Int ...
// line number of this site
FIELDS
mod
the module id of the module containing the call site
file
the name of the file containing the call site or NULL;
some call sites omit the file name to save data space.
line
the line number within the file named
DETAILS
This structure describes the location of the line that raised
an error.
C SYNOPSIS
struct Types.Timestamp64 |
![](../../Arrow_up.png) |
64-bit timestamp struct
var obj = new Types.Timestamp64;
obj.hi = Bits32 ...
// most significant 32-bits of timestamp
obj.lo = Bits32 ...
// least significant 32-bits of timestamp
DETAILS
Some platforms only support 32-bit timestamps. In this case,
the most significant 32-bits are always set to 0.
C SYNOPSIS
metaonly config Types.common$ // module-wide |
![](../../Arrow_up.png) |
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.