module ti.sysbios.knl.Task

Task Manager

The Task module makes available a set of functions that manipulate task objects accessed through pointers of type Handle. Tasks represent independent threads of control that conceptually execute functions in parallel within a single C program; in reality, concurrency is achieved by switching the processor from one task to another. [ more ... ]
C synopsis target-domain sourced in ti/sysbios/knl/Task.xdc
#include <ti/sysbios/knl/Task.h>
Functions
Void
Void
Void
UInt 
Void 
UInt 
Ptr 
Ptr 
Int 
Void
Void 
macro Task_Handle 
UInt 
Void 
Void 
UInt 
Void 
Void 
Task_startCore// (UInt coreId);
Void 
Void 
Functions common to all target instances
Functions common to all target modules
Defines
#define
Typedefs
typedef Void 
typedef Void 
typedef Task_Object *
typedef struct
typedef enum
typedef struct
typedef struct
typedef struct
typedef struct
Constants
extern const Task_AllBlockedFuncPtr 
extern const Assert_Id 
extern const Assert_Id 
extern const Assert_Id 
extern const Assert_Id 
extern const Assert_Id 
extern const Assert_Id 
extern const Assert_Id 
extern const Assert_Id 
extern const IHeap_Handle 
extern const SizeT 
extern const Bool 
extern const Error_Id 
extern const Error_Id 
extern const Error_Id 
extern const Task_HookSet 
extern const Bool 
extern const Log_Event 
extern const Log_Event 
extern const Log_Event 
extern const Log_Event 
extern const Log_Event 
extern const Log_Event 
extern const Log_Event 
extern const Log_Event 
extern const Log_Event 
extern const Log_Event 
extern const UInt 
 
DETAILS
The Task module makes available a set of functions that manipulate task objects accessed through pointers of type Handle. Tasks represent independent threads of control that conceptually execute functions in parallel within a single C program; in reality, concurrency is achieved by switching the processor from one task to another.
When you create a task, it is provided with its own run-time stack, used for storing local variables as well as for further nesting of function calls. Each stack must be large enough to handle normal subroutine calls and one task preemption context. A task preemption context is the context that gets saved when one task preempts another as a result of an interrupt thread readying a higher-priority task.
All tasks executing within a single program share a common set of global variables, accessed according to the standard rules of scope defined for C functions.
Each task is in one of five modes of execution at any point in time: running, ready, blocked, terminated, or inactive. By design, there is always one (and only one) task currently running, even if it is only the idle task managed internally by Task. The current task can be suspended from execution by calling certain Task functions, as well as functions provided by other modules like the Semaphore or Event Modules. The current task can also terminate its own execution. In either case, the processor is switched to the highest priority task that is ready to run.
You can assign numeric priorities to tasks. Tasks are readied for execution in strict priority order; tasks of the same priority are scheduled on a first-come, first-served basis. The priority of the currently running task is never lower than the priority of any ready task. Conversely, the running task is preempted and re-scheduled for execution whenever there exists some ready task of higher priority.
TASK DELETION
Any dynamically created task that is not in the Task_Mode_RUNNING state (ie not the currently running task) can be deleted using the delete API.
Task_delete() removes the task from all internal queues and calls Memory_free() is used to free the task object and its stack. Memory_free() must acquire a lock to the memory before proceeding. If another task already holds a lock to the memory, then the thread performing the delete will be blocked until the memory is unlocked.
Note: Task_delete() should be called with extreme care. As mentioned above, the scope of Task_delete() is limited to freeing the Task object itself, freeing the task's stack memory if it was allocated at create time, and removing the task from any SYS/BIOS-internal state structures.
SYS/BIOS does not keep track of any resources the task may have acquired or used during its lifetime.
It is the application's responsibility to guarantee the integrity of a task's partnerships prior to deleting that task.
For example, if a task has obtained exclusive access to a resource, deleting that task will make the resource forever unavailable.
Task_delete() sets the referenced task handle to NULL. Any subsequent call to a Task instance API using that null task handle will behave unpredictably and will usually result in an application crash.
Assuming a task completely cleans up after itself prior to calling Task_exit() (or falling through the the bottom of the task function), it is then safest to use Task_delete() only when a task is in the 'Task_Mode_TERMINATED' state.
Delete hooks: You can specify application-wide Delete hook functions that run whenever a task is deleted. See the discussion of Hook Functions below for details.
Task_delete() constraints:
  • The task cannot be the currently executing task (Task_self()).
  • Task_delete cannot be called from a Swi or Hwi.
  • No check is performed to prevent Task_delete from being used on a statically-created object. If a program attempts to delete a task object that was created statically, the Memory_free() call will result in an assertion failure in its corresponding Heap manager, causing the application to exit.
STACK ALIGNMENT
Stack size parameters for both static and dynamic tasks are rounded up to the nearest integer multiple of a target-specific alignment requirement.
In the case of Task's which are created with a user-provided stack, both the base address and the stackSize are aligned. The base address is increased to the nearest aligned address. The stack size is decreased accordingly and then rounded down to the nearest integer multiple of the target-specific required alignment.
HOOK FUNCTIONS
Sets of hook functions can be specified for the Task module. Each set can contains these hook functions:
  • Register: A function called before any statically created tasks are initialized at runtime. The register hook is called at boot time before main() and before interrupts are enabled.
  • Create: A function that is called when a task is created. This includes tasks that are created statically and those created dynamically using create or construct. The create hook is called outside of a Task_disable/enable block and before the task has been added to the ready list.
  • Ready: A function that is called when a task becomes ready to run. The ready hook is called from within a Task_disable/enable block with interrupts enabled.
  • Switch: A function that is called just before a task switch occurs. The 'prev' and 'next' task handles are passed to the Switch hook. 'prev' is set to NULL for the initial task switch that occurs during SYS/BIOS startup. The Switch hook is called from within a Task_disable/enable block with interrupts enabled.
  • Exit: A function that is called when a task exits using exit. The exit hook is passed the handle of the exiting task. The exit hook is called outside of a Task_disable/enable block and before the task has been removed from the kernel lists.
  • Delete: A function that is called when any task is deleted at run-time with delete. The delete hook is called outside of a Task_disable/enable block.
Hook functions can only be configured statically.
If you define more than one set of hook functions, all the functions of a particular type will be run when a Swi triggers that type of hook.
Register Function
The Register function is provided to allow a hook set to store its hookset ID. This id can be passed to setHookContext and getHookContext to set or get hookset-specific context. The Register function must be specified if the hook implementation needs to use setHookContext or getHookContext. The registerFxn hook function is called during system initialization before interrupts have been enabled.
  Void myRegisterFxn(Int id);
Create and Delete Functions
The create and delete functions are called whenever a Task is created or deleted. They are called with interrupts enabled (unless called at boot time or from main()).
  Void myCreateFxn(Task_Handle task, Error_Block *eb);
  Void myDeleteFxn(Task_Handle task);
Switch Function
If a switch function is specified, it is invoked just before the new task is switched to. The switch function is called with interrupts enabled.
This function can be used to save/restore additional task context (for example, external hardware registers), to check for task stack overflow, to monitor the time used by each task, etc.
  Void mySwitchFxn(Task_Handle prev, Task_Handle next);
To properly handle the switch to the first task your switchFxn should check for "prev == NULL" before using prev:
  Void mySwitchFxn(Task_Handle prev, Task_Handle next)
  {
      if (prev != NULL) {
          ...
      }
      ...
  }
Ready Function
If a ready function is specified, it is invoked whenever a task is made ready to run. The ready function is called with interrupts enabled (unless called at boot time or from main()).
  Void myReadyFxn(Task_Handle task);
Exit Function
If an exit function is specified, it is invoked when a task exits (via call to Task_exit() or when a task returns from its' main function). The Exit Function is called with interrupts enabled.
  Void myExitFxn(Task_Handle task);

Calling Context

Function Hwi Swi Task Main Startup
create N N Y Y N
disable Y Y Y Y N
exit N N Y N N
getIdleTask Y Y Y Y N
Params_init Y Y Y Y Y
restore Y Y Y Y N
self Y Y Y Y N
sleep N N Y N N
yield Y Y Y N N
construct N N Y Y N
delete N N Y Y N
destruct N N Y Y N
getEnv Y Y Y Y N
getHookContext Y Y Y Y N
getMode Y Y Y Y N
getPri Y Y Y Y N
getFunc Y Y Y Y N
setEnv Y Y Y Y N
setHookContext Y Y Y Y N
setPri Y Y Y N N
stat Y Y Y Y N
Definitions:
  • Hwi: API is callable from a Hwi thread.
  • Swi: API is callable from a Swi thread.
  • Task: API is callable from a Task thread.
  • Main: API is callable during any of these phases:
    • In your module startup after this module is started (e.g. Task_Module_startupDone() returns TRUE).
    • During xdc.runtime.Startup.lastFxns.
    • During main().
    • During BIOS.startupFxns.
  • Startup: API is callable during any of these phases:
    • During xdc.runtime.Startup.firstFxns.
    • In your module startup before this module is started (e.g. Task_Module_startupDone() returns FALSE).
 
const Task_AFFINITY_NONE

"Don't care" task affinity

C synopsis target-domain
#define Task_AFFINITY_NONE (UInt)~(0)
 
 
enum Task_Mode

Task execution modes

C synopsis target-domain
typedef enum Task_Mode {
    Task_Mode_RUNNING,
    // Task is currently executing
    Task_Mode_READY,
    // Task is scheduled for execution
    Task_Mode_BLOCKED,
    // Task is suspended from execution
    Task_Mode_TERMINATED,
    // Task is terminated from execution
    Task_Mode_INACTIVE
    // Task is on inactive task list
} Task_Mode;
 
DETAILS
These enumerations are the range of modes or states that a task can be in. A task's current mode can be gotten using stat.
 
typedef Task_AllBlockedFuncPtr

"All Task Blocked" function type definition

C synopsis target-domain
typedef Void (*Task_AllBlockedFuncPtr)(Void);
 
 
typedef Task_FuncPtr

Task function type definition

C synopsis target-domain
typedef Void (*Task_FuncPtr)(UArg,UArg);
 
 
struct Task_HookSet

Task hook set type definition

C synopsis target-domain
typedef struct Task_HookSet {
    Void (*registerFxn)(Int);
    Void (*createFxn)(Task_Handle,Error_Block*);
    Void (*readyFxn)(Task_Handle);
    Void (*switchFxn)(Task_Handle,Task_Handle);
    Void (*exitFxn)(Task_Handle);
    Void (*deleteFxn)(Task_Handle);
} Task_HookSet;
 
DETAILS
Sets of hook functions can be specified for the Task module. See Hook Functions for details.
 
struct Task_Stat

Task Status Buffer

C synopsis target-domain
typedef struct Task_Stat {
    Int priority;
    // Task priority
    Ptr stack;
    // Task stack
    SizeT stackSize;
    // Task stack size
    IHeap_Handle stackHeap;
    // Heap used to alloc stack
    Ptr env;
    // Global environment struct
    Task_Mode mode;
    // Task's current mode
    Ptr sp;
    // Task's current stack pointer
    SizeT used;
    // max # of words used on stack
} Task_Stat;
 
DETAILS
Passed to and filled in by stat;
 
config Task_A_badAffinity  // module-wide

Asserted in Task_setAffinity

C synopsis target-domain
extern const Assert_Id Task_A_badAffinity;
 
 
config Task_A_badPriority  // module-wide

Asserted in Task_create

C synopsis target-domain
extern const Assert_Id Task_A_badPriority;
 
 
config Task_A_badTaskState  // module-wide

Asserted in Task_delete

C synopsis target-domain
extern const Assert_Id Task_A_badTaskState;
 
 
config Task_A_badThreadType  // module-wide

Asserted in Task_create and Task_delete

C synopsis target-domain
extern const Assert_Id Task_A_badThreadType;
 
 
config Task_A_badTimeout  // module-wide

Asserted in Task_sleep

C synopsis target-domain
extern const Assert_Id Task_A_badTimeout;
 
 
config Task_A_noPendElem  // module-wide

Asserted in Task_delete

C synopsis target-domain
extern const Assert_Id Task_A_noPendElem;
 
 
config Task_A_sleepTaskDisabled  // module-wide

Asserted in Task_sleep

C synopsis target-domain
extern const Assert_Id Task_A_sleepTaskDisabled;
 
 
config Task_A_taskDisabled  // module-wide

Asserted in Task_create

C synopsis target-domain
extern const Assert_Id Task_A_taskDisabled;
 
 
config Task_E_deleteNotAllowed  // module-wide
C synopsis target-domain
extern const Error_Id Task_E_deleteNotAllowed;
 
 
config Task_E_spOutOfBounds  // module-wide

Error raised when a task's stack pointer (SP) does not point somewhere within the task's stack

C synopsis target-domain
extern const Error_Id Task_E_spOutOfBounds;
 
DETAILS
This error is raised by kernel's stack checking function. This function checks the SPs before every task switch to make sure they point within the task's stack.
The stack checking logic is enabled by the initStackFlag and checkStackFlag configuration parameters. If both of these flags are set to true, the kernel will validate the stack pointers.
 
config Task_E_stackOverflow  // module-wide

Error raised when a stack overflow (or corruption) is detected

C synopsis target-domain
extern const Error_Id Task_E_stackOverflow;
 
DETAILS
This error is raised by kernel's stack checking function. This function checks the stacks before every task switch to make sure that reserved word at top of stack has not been modified.
The stack checking logic is enabled by the initStackFlag and checkStackFlag configuration parameters. If both of these flags are set to true, the kernel will validate the stacks.
 
config Task_LD_block  // module-wide

Logged when a task is blocked (ie Semaphore_pend())

C synopsis target-domain
extern const Log_Event Task_LD_block;
 
 
config Task_LD_exit  // module-wide

Logged when Task functions fall thru the bottom or when Task_exit() is explicitly called

C synopsis target-domain
extern const Log_Event Task_LD_exit;
 
 
config Task_LD_ready  // module-wide

Logged when a task is made ready to run (ie Semaphore_post())

C synopsis target-domain
extern const Log_Event Task_LD_ready;
 
 
config Task_LM_noWork  // module-wide

Logged when no scheduling work was found

C synopsis target-domain
extern const Log_Event Task_LM_noWork;
 
 
config Task_LM_schedule  // module-wide

Logged on every task schedule entry

C synopsis target-domain
extern const Log_Event Task_LM_schedule;
 
 
config Task_LM_setAffinity  // module-wide

Logged on calls to Task_setAffinity

C synopsis target-domain
extern const Log_Event Task_LM_setAffinity;
 
 
config Task_LM_setPri  // module-wide

Logged on calls to Task_setPri

C synopsis target-domain
extern const Log_Event Task_LM_setPri;
 
 
config Task_LM_sleep  // module-wide

Logged on calls to Task_sleep

C synopsis target-domain
extern const Log_Event Task_LM_sleep;
 
 
config Task_LM_switch  // module-wide

Logged on every task switch

C synopsis target-domain
extern const Log_Event Task_LM_switch;
 
 
config Task_LM_yield  // module-wide

Logged on calls to Task_yield

C synopsis target-domain
extern const Log_Event Task_LM_yield;
 
 
config Task_allBlockedFunc  // module-wide

Function to call while all tasks are blocked

C synopsis target-domain
extern const Task_AllBlockedFuncPtr Task_allBlockedFunc;
 
DETAILS
This function will be called repeatedly while no tasks are ready to run.
Ordinarily (in applications that have tasks ready to run at startup), the function will run in the context of the last task to block.
In an application where there are no tasks ready to run when BIOS_start() is called, the allBlockedFunc function is called within the BIOS_start() thread which runs on the system/ISR stack.
By default, allBlockedFunc is initialized to point to an internal function that simply returns.
By adding the following lines to the config script, the Idle functions will run whenever all tasks are blocked:
  Task.enableIdleTask = false;
  Task.allBlockedFunc = Idle.run;
SEE
CONSTRAINTS
The configured allBlockedFunc is designed to be called repeatedly. It must return in order for the task scheduler to check if all tasks are STILL blocked and if not, run the highest priority task currently ready to run.
The configured allBlockedFunc function is called with interrupts disabled. If your function must run with interrupts enabled, surround the body of your code with Hwi_enable()/Hwi_restore() function calls per the following example:
  Void yourFunc() {
      UInt hwiKey;

      hwiKey = Hwi_enable();

      ...         // your code here

      Hwi_restore(hwiKey);
  }
 
config Task_defaultStackHeap  // module-wide

Default Mem heap used for all dynamically created task stacks

C synopsis target-domain
extern const IHeap_Handle Task_defaultStackHeap;
 
DETAILS
Default is null.
 
config Task_defaultStackSize  // module-wide

Default stack size (in MAUs) used for all tasks

C synopsis target-domain
extern const SizeT Task_defaultStackSize;
 
DETAILS
Default is obtained from the family-specific TaskSupport module (e.g. ti.sysbios.family.arm.m3.TaskSupport, ti.sysbios.family.c62.TaskSupport).
 
config Task_deleteTerminatedTasks  // module-wide

Automatically delete terminated tasks

C synopsis target-domain
extern const Bool Task_deleteTerminatedTasks;
 
DETAILS
If this feature is enabled, an Idle function is installed that deletes dynamically created Tasks that have terminated either by falling through their task function or by explicitly calling Task_exit().
A list of terminated Tasks that were created dynmically is maintained internally. Each invocation of the installed Idle function deletes the first Task on this list. This one-at-a-time process continues until the list is empty.
NOTE
This feature is disabled by default.
WARNING
When this feature is enabled, an error will be raised if the user's application attempts to delete a terminated task. If a terminated task has already been automatically deleted and THEN the user's application attempts to delete it (ie: using a stale Task handle), the results are undefined and probably catastrophic!
 
config Task_hooks  // module-wide

Const array that holds the HookSet objects

C synopsis target-domain
extern const Task_HookSet Task_hooks[length];
 
DETAILS
See Hook Functions for details about HookSets.
 
config Task_initStackFlag  // module-wide

Initialize stack with known value for stack checking at runtime (see checkStackFlag)

C synopsis target-domain
extern const Bool Task_initStackFlag;
 
DETAILS
This is also useful for inspection of stack in debugger or core dump utilities. Default is true.
 
config Task_numPriorities  // module-wide

Number of Task priorities supported. Default is 16

C synopsis target-domain
extern const UInt Task_numPriorities;
 
DETAILS
The maximum number of priorities supported is target specific and depends on the number of bits in a UInt data type. For 6x and ARM devices the maximum number of priorities is therefore 32. For 28x, 55x, and MSP430 devices, the maximum number of priorities is 16.
 
Task_disable()  // module-wide

Disable the task scheduler

C synopsis target-domain
UInt Task_disable();
 
RETURNS
key for use with restore
DETAILS
disable and restore control Task scheduling. disable disables all other Tasks from running until restore is called. Hardware and Software interrupts can still run.
disable and restore allow you to ensure that statements that must be performed together during critical processing are not preempted by other Tasks.
The value of the key returned is opaque to applications and is meant to be passed to Task_restore().
In the following example, the critical section is not preempted by any Tasks.
  key = Task_disable();
      `critical section`
  Task_restore(key);
You can also use disable and restore to create several Tasks and allow them to be invoked in priority order.
disable calls can be nested.
CONSTRAINTS
Do not call any function that can cause the current task to block within a disable/restore block. For example, Semaphore_pend (if timeout is non-zero), sleep, yield, and Memory_alloc can all cause blocking.
 
Task_exit()  // module-wide

Terminate execution of the current task

C synopsis target-domain
Void Task_exit();
 
DETAILS
Task_exit terminates execution of the current task, changing its mode from Mode_RUNNING to Mode_TERMINATED. If all tasks have been terminated, or if all remaining tasks have their vitalTaskFlag attribute set to FALSE, then SYS/BIOS terminates the program as a whole by calling the function System_exit with a status code of 0.
Task_exit is automatically called whenever a task returns from its top-level function.
Exit Hooks (see exitFxn in HookSet) can be used to provide functions that run whenever a task is terminated. The exitFxn Hooks are called before the task has been blocked and marked Mode_TERMINATED. See Hook Functions for more information.
Any SYS/BIOS function can be called from an Exit Hook function.
Calling self within an Exit function returns the task being exited. Your Exit function declaration should be similar to the following:
  Void myExitFxn(Void);
A task switch occurs when calling Task_exit unless the program as a whole is terminated
CONSTRAINTS
Task_exit cannot be called from a Swi or Hwi.
Task_exit cannot be called from the program's main() function.
 
Task_restore()  // module-wide

Restore Task scheduling state

C synopsis target-domain
Void Task_restore(UInt key);
 
ARGUMENTS
key — key to restore previous Task scheduler state
DETAILS
disable and restore control Task scheduling disable disables all other Tasks from running until restore is called. Hardware and Software interrupts can still run.
disable and restore allow you to ensure that statements that must be performed together during critical processing are not preempted.
In the following example, the critical section is not preempted by any Tasks.
  key = Task_disable();
      `critical section`
  Task_restore(key);
You can also use disable and restore to create several Tasks and allow them to be performed in priority order.
disable calls can be nested.
restore returns with interrupts enabled if the key unlocks the scheduler
CONSTRAINTS
Do not call any function that can cause the current task to block within a disable/restore block. For example, Semaphore_pend() (if timeout is non-zero), sleep, yield, and Memory_alloc can all cause blocking.
restore internally calls Hwi_enable() if the key passed to it results in the unlocking of the Task scheduler (ie if this is root Task_disable/Task_restore pair).
 
Task_self()  // module-wide

Returns a handle to the currently executing Task object

C synopsis target-domain
Task_Handle Task_self();
 
RETURNS
address of currently executing task object
DETAILS
Task_self returns the object handle for the currently executing task. This function is useful when inspecting the object or when the current task changes its own priority through setPri.
No task switch occurs when calling Task_self.
Task_self will return NULL until Tasking is initiated at the end of BIOS_start().
 
Task_selfMacro()  // module-wide

Returns a handle to the currently executing Task object

C synopsis target-domain
macro Task_Handle Task_selfMacro();
 
RETURNS
address of currently executing task object
DETAILS
Task_selfMacro is identical to self but is implemented as and inline macro.
 
Task_sleep()  // module-wide

Delay execution of the current task

C synopsis target-domain
Void Task_sleep(UInt nticks);
 
ARGUMENTS
nticks — number of system clock ticks to sleep
DETAILS
Task_sleep changes the current task's mode from Mode_RUNNING to Mode_BLOCKED, and delays its execution for nticks increments of the system clock. The actual time delayed can be up to 1 system clock tick less than nticks due to granularity in system timekeeping and the time elapsed per tick is determined by Clock_tickPeriod.
After the specified period of time has elapsed, the task reverts to the Mode_READY mode and is scheduled for execution.
A task switch always occurs when calling Task_sleep if nticks > 0.
CONSTRAINTS
Task_sleep cannot be called from a Swi or Hwi, or within a disable / restore block.
Task_sleep cannot be called from the program's main() function.
Task_sleep should not be called from within an Idle function. Doing so prevents analysis tools from gathering run-time information.
nticks cannot be BIOS_WAIT_FOREVER.
 
Task_startCore()  // module-wide
C synopsis target-domain
Void Task_startCore(UInt coreId);
 
 
Task_yield()  // module-wide

Yield processor to equal priority task

C synopsis target-domain
Void Task_yield();
 
DETAILS
Task_yield yields the processor to another task of equal priority.
A task switch occurs when you call Task_yield if there is an equal priority task ready to run.
Tasks of higher priority preempt the currently running task without the need for a call to Task_yield. If only lower-priority tasks are ready to run when you call Task_yield, the current task continues to run. Control does not pass to a lower-priority task.
CONSTRAINTS
When called within an Hwi, the code sequence calling Task_yield must be invoked by the Hwi dispatcher.
Task_yield cannot be called from the program's main() function.
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId Task_Module_id();
// Get this module's unique id
 
Bool Task_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle Task_Module_heap();
// The heap from which this module allocates memory
 
Bool Task_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 Task_Module_getMask();
// Returns the diagnostics mask for this module
 
Void Task_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct Task_Object Task_Object;
// Opaque internal representation of an instance object
 
typedef Task_Object *Task_Handle;
// Client reference to an instance object
 
typedef struct Task_Struct Task_Struct;
// Opaque client structure large enough to hold an instance object
 
Task_Handle Task_handle(Task_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
Task_Struct *Task_struct(Task_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct Task_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
    UInt affinity;
    // The core which this task is to run on. Default is Task_AFFINITY_NONE
    UArg arg0;
    // Task function argument. Default is 0
    UArg arg1;
    // Task function argument. Default is 0
    Ptr env;
    // Environment data struct
    Int priority;
    // Task priority (0 to Task.numPriorities-1, or -1). Default is 1
    Ptr stack;
    // Task stack pointer. Default = null
    IHeap_Handle stackHeap;
    // Mem heap used for dynamically created task stack
    SizeT stackSize;
    // Task stack size in MAUs
    Bool vitalTaskFlag;
    // Exit system immediately when the last task with this flag set to TRUE has terminated
} Task_Params;
 
Void Task_Params_init(Task_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
 
config Task_affinity  // instance

The core which this task is to run on. Default is Task_AFFINITY_NONE

C synopsis target-domain
struct Task_Params {
      ...
    UInt affinity;
 
DETAILS
If there is a compelling reason for a task to be pinned to a particular core, then setting 'affinity' to the corresponding core id will force the task to only be run on that core.
The default affinity is inherited from Task.defaultAffinity which in turn defaults to Task_AFFINITY_NONE, which means the task can be run on either core.
Furthermore, Task_AFFINITY_NONE implies that the task can be moved from core to core as deemed necessary by the Task scheduler in order to keep the two highest priority ready tasks running simultaneously.
 
config Task_arg0  // instance

Task function argument. Default is 0

C synopsis target-domain
struct Task_Params {
      ...
    UArg arg0;
 
 
config Task_arg1  // instance

Task function argument. Default is 0

C synopsis target-domain
struct Task_Params {
      ...
    UArg arg1;
 
 
config Task_env  // instance

Environment data struct

C synopsis target-domain
struct Task_Params {
      ...
    Ptr env;
 
 
config Task_priority  // instance

Task priority (0 to Task.numPriorities-1, or -1). Default is 1

C synopsis target-domain
struct Task_Params {
      ...
    Int priority;
 
 
config Task_stack  // instance

Task stack pointer. Default = null

C synopsis target-domain
struct Task_Params {
      ...
    Ptr stack;
 
DETAILS
Null indicates that the stack is to be allocated by create().
Example: To statically initialize "tsk0"'s stack to a literal address, use the following syntax:
      Program.global.tsk0.stack = $addr(literal);
 
config Task_stackHeap  // instance

Mem heap used for dynamically created task stack

C synopsis target-domain
struct Task_Params {
      ...
    IHeap_Handle stackHeap;
 
DETAILS
The default value of NULL means that the module config defaultStackHeap is used.
 
config Task_stackSize  // instance

Task stack size in MAUs

C synopsis target-domain
struct Task_Params {
      ...
    SizeT stackSize;
 
DETAILS
The default value of 0 means that the module config defaultStackSize is used.
 
config Task_vitalTaskFlag  // instance

Exit system immediately when the last task with this flag set to TRUE has terminated

C synopsis target-domain
struct Task_Params {
      ...
    Bool vitalTaskFlag;
 
DETAILS
Default is true.
Instance Creation

C synopsis target-domain
Task_Handle Task_create(Task_FuncPtr fxn, const Task_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void Task_construct(Task_Struct *structP, Task_FuncPtr fxn, const Task_Params *params, Error_Block *eb);
// Initialize a new instance object inside the provided structure
ARGUMENTS
fxn — Task Function
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
Task_create creates a new task object. If successful, Task_create returns the handle of the new task object. If unsuccessful, Task_create returns NULL unless it aborts.
The fxn parameter uses the FuncPtr type to pass a pointer to the function the Task object should run. For example, if myFxn is a function in your program, your C code can create a Task object to call that function as follows:
  Task_Params taskParams;

  // Create task with priority 15
  Task_Params_init(&taskParams);
  taskParams.stackSize = 512;
  taskParams.priority = 15;
  Task_create((Task_FuncPtr)myFxn, &taskParams, &eb);
The following statements statically create a task in the configuration file:
  var params = new Task.Params;
  params.instance.name = "tsk0";
  params.arg0 = 1;
  params.arg1 = 2;
  params.priority = 1;
  Task.create('&tsk0_func', params);
If NULL is passed instead of a pointer to an actual Task_Params struct, a default set of parameters is used. The "eb" is an error block that you can use to handle errors that may occur during Task object creation.
The newly created task is placed in Mode_READY mode, and is scheduled to begin concurrent execution of the following function call:
  (*fxn)(arg1, arg2);
As a result of being made ready to run, the task runs any application-wide Ready functions that have been specified.
Task_exit is automatically called if and when the task returns from fxn.
Create Hook Functions
You can specify application-wide Create hook functions in your config file that run whenever a task is created. This includes tasks that are created statically and those created dynamically using Task_create.
For Task objects created statically, Create functions are called during the Task module initialization phase of the program startup process prior to main().
For Task objects created dynamically, Create functions are called after the task handle has been initialized but before the task has been placed on its ready queue.
Any SYS/BIOS function can be called from Create functions. SYS/BIOS passes the task handle of the task being created to each of the Create functions.
All Create function declarations should be similar to this:
  Void myCreateFxn(Task_Handle task);
CONSTRAINTS
  • The fxn parameter and the name attribute cannot be NULL.
  • The priority attribute must be less than or equal to (numPriorities - 1) and greater than or equal to one (1) (priority 0 is owned by the Idle task).
  • The priority can be set to -1 for tasks that will not execute until another task changes the priority to a positive value.
  • The stackHeap attribute must identify a valid memory Heap.
Instance Deletion

C synopsis target-domain
Void Task_delete(Task_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void Task_destruct(Task_Struct *structP);
// Finalize the instance object inside the provided structure
 
Task_getAffinity()  // instance

Return task's core affinity

C synopsis target-domain
UInt Task_getAffinity(Task_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created Task instance object
RETURNS
task's current core affinity
 
Task_getEnv()  // instance

Get task environment pointer

C synopsis target-domain
Ptr Task_getEnv(Task_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created Task instance object
RETURNS
task environment pointer
DETAILS
Task_getEnv returns the environment pointer of the specified task. The environment pointer references an arbitrary application-defined data structure.
If your program uses multiple hook sets, getHookContext allows you to get environment pointers you have set for a particular hook set and Task object combination.
 
Task_getFunc()  // instance

Get Task function and arguments

C synopsis target-domain
Task_FuncPtr Task_getFunc(Task_Handle handle, UArg *arg0, UArg *arg1);
 
ARGUMENTS
handle — handle of a previously-created Task instance object
arg0 — pointer for returning Task's first function argument
arg1 — pointer for returning Task's second function argument
RETURNS
Task function
DETAILS
If either arg0 or arg1 is NULL, then the corresponding argument is not returned.
 
Task_getHookContext()  // instance

Get hook set's context for a task

C synopsis target-domain
Ptr Task_getHookContext(Task_Handle handle, Int id);
 
ARGUMENTS
handle — handle of a previously-created Task instance object
id — hook set ID
RETURNS
hook set context for task
DETAILS
For example, this C code gets the HookContext, prints it, and sets a new value for the HookContext.
  Ptr pEnv;
  Task_Handle myTask;
  Int myHookSetId1;

  pEnv = Task_getHookContext(task, myHookSetId1);

  System_printf("myEnd1: pEnv = 0x%lx, time = %ld\n",
                (ULong)pEnv, (ULong)Timestamp_get32());

  Task_setHookContext(task, myHookSetId1, (Ptr)0xc0de1);
See Hook Functions for more details.
 
Task_getMode()  // instance

Retrieve the Mode of a task

C synopsis target-domain
Task_Mode Task_getMode(Task_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created Task instance object
 
Task_getPri()  // instance

Get task priority

C synopsis target-domain
Int Task_getPri(Task_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created Task instance object
RETURNS
task priority
DETAILS
Task_getPri returns the priority of the referenced task.
 
Task_setAffinity()  // instance

Set task's core affinity

C synopsis target-domain
UInt Task_setAffinity(Task_Handle handle, UInt coreId);
 
ARGUMENTS
handle — handle of a previously-created Task instance object
RETURNS
task's previous core affinity
DETAILS
If the new core ID is different than the current core affinity a reschedule will be performed immediately.
CONSTRAINTS
Must NOT be called with interrupts disabled (ie within a Hwi_disable()/Hwi_restore() block).
Must NOT be called with tasking disabled (ie within a Task_disable()/Task_restore() block).
 
Task_setEnv()  // instance

Set task environment

C synopsis target-domain
Void Task_setEnv(Task_Handle handle, Ptr env);
 
ARGUMENTS
handle — handle of a previously-created Task instance object
env — task environment pointer
DETAILS
Task_setEnv sets the task environment pointer to env. The environment pointer references an arbitrary application-defined data structure.
If your program uses multiple hook sets, setHookContext allows you to set environment pointers for any hook set and Task object combination.
 
Task_setHookContext()  // instance

Set hook instance's context for a task

C synopsis target-domain
Void Task_setHookContext(Task_Handle handle, Int id, Ptr hookContext);
 
ARGUMENTS
handle — handle of a previously-created Task instance object
id — hook set ID
hookContext — value to write to context
DETAILS
For example, this C code gets the HookContext, prints it, and sets a new value for the HookContext.
  Ptr pEnv;
  Task_Handle myTask;
  Int myHookSetId1;

  pEnv = Task_getHookContext(task, myHookSetId1);

  System_printf("myEnd1: pEnv = 0x%lx, time = %ld\n",
                (ULong)pEnv, (ULong)Timestamp_get32());

  Task_setHookContext(task, myHookSetId1, (Ptr)0xc0de1);
See Hook Functions for more details.
 
Task_setPri()  // instance

Set a task's priority

C synopsis target-domain
UInt Task_setPri(Task_Handle handle, Int newpri);
 
ARGUMENTS
handle — handle of a previously-created Task instance object
newpri — task's new priority
RETURNS
task's old priority
DETAILS
Task_setpri sets the execution priority of task to newpri, and returns that task's old priority value. Raising or lowering a task's priority does not necessarily force preemption and re-scheduling of the caller: tasks in the Mode_BLOCKED mode remain suspended despite a change in priority; and tasks in the Mode_READY mode gain control only if their new priority is greater than that of the currently executing task.
newpri should be set to a value greater than or equal to 1 and less than or equal to (numPriorities - 1). newpri can also be set to -1 which puts the the task into the INACTIVE state and the task will not run until its priority is raised at a later time by another task. Priority 0 is reserved for the idle task. If newpri equals (numPriorities - 1), execution of the task effectively locks out all other program activity, except for the handling of interrupts.
The current task can change its own priority (and possibly preempt its execution) by passing the output of self as the value of the task parameter.
A context switch occurs when calling Task_setpri if a currently running task priority is set lower than the priority of another currently ready task, or if another ready task is made to have a higher priority than the currently running task.
Task_setpri can be used for mutual exclusion.
If a task's new priority is different than its previous priority, then its relative placement in its new ready task priority queue can be different than the one it was removed from. This can effect the relative order in which it becomes the running task.
The effected task is placed at the head of its new priority queue if it is the currently running task. Otherwise it is placed at at the end of its new task priority queue.
CONSTRAINTS
newpri must be a value between 1 and (numPriorities - 1) or -1.
The task cannot be in the Mode_TERMINATED mode.
The new priority should not be zero (0). This priority level is reserved for the Idle task.
 
Task_stat()  // instance

Retrieve the status of a task

C synopsis target-domain
Void Task_stat(Task_Handle handle, Task_Stat *statbuf);
 
ARGUMENTS
handle — handle of a previously-created Task instance object
statbuf — pointer to task status structure
DETAILS
Task_stat retrieves attribute values and status information about a task.
Status information is returned through statbuf, which references a structure of type Stat.
When a task is preempted by a software or hardware interrupt, the task execution mode returned for that task by Task_stat is still Mode_RUNNING because the task runs when the preemption ends.
The current task can inquire about itself by passing the output of self as the first argument to Task_stat. However, the task stack pointer (sp) in the Stat structure is the value from the previous context switch.
Task_stat has a non-deterministic execution time. As such, it is not recommended to call this API from Swis or Hwis.
CONSTRAINTS
statbuf cannot be NULL;
Instance Built-Ins

C synopsis target-domain
Int Task_Object_count();
// The number of statically-created instance objects
 
Task_Handle Task_Object_get(Task_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
Task_Handle Task_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
Task_Handle Task_Object_next(Task_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle Task_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *Task_Handle_label(Task_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String Task_Handle_name(Task_Handle handle);
// The name of this instance object
 
Configuration settings sourced in ti/sysbios/knl/Task.xdc
var Task = xdc.useModule('ti.sysbios.knl.Task');
module-wide constants & types
 
    values of type Task.Mode// Task execution modes
 
        obj.registerFxn = Void(*)(Int)  ...
        obj.createFxn = Void(*)(Task.Handle,Error.Block*)  ...
        obj.readyFxn = Void(*)(Task.Handle)  ...
        obj.switchFxn = Void(*)(Task.Handle,Task.Handle)  ...
        obj.exitFxn = Void(*)(Task.Handle)  ...
        obj.deleteFxn = Void(*)(Task.Handle)  ...
 
    var obj = new Task.Stat// Task Status Buffer;
        obj.priority// Task priority = Int  ...
        obj.stack// Task stack = Ptr  ...
        obj.stackSize// Task stack size = SizeT  ...
        obj.env// Global environment struct = Ptr  ...
        obj.mode// Task's current mode = Task.Mode  ...
        obj.sp// Task's current stack pointer = Ptr  ...
        obj.used// max # of words used on stack = SizeT  ...
module-wide config parameters
        msg: "A_badAffinity: Invalid affinity."
    };
        msg: "A_badPriority: An invalid task priority was used."
    };
        msg: "A_badTaskState: Can't delete a task in RUNNING state."
    };
        msg: "A_badThreadType: Cannot create/delete a task from Hwi or Swi thread."
    };
        msg: "A_badTimeout: Can't sleep FOREVER."
    };
        msg: "A_noPendElem: Not enough info to delete BLOCKED task."
    };
        msg: "A_sleepTaskDisabled: Cannot call Task_sleep() while the Task scheduler is disabled."
    };
        msg: "A_taskDisabled: Cannot create a task when tasking is disabled."
    };
        msg: "E_deleteNotAllowed: Task 0x%x."
    };
        msg: "E_spOutOfBounds: Task 0x%x stack error, SP = 0x%x."
    };
        msg: "E_stackOverflow: Task 0x%x stack overflow."
    };
        mask: Diags.USER2,
        msg: "LD_block: tsk: 0x%x, func: 0x%x"
    };
        mask: Diags.USER2,
        msg: "LD_exit: tsk: 0x%x, func: 0x%x"
    };
        mask: Diags.USER2,
        msg: "LD_ready: tsk: 0x%x, func: 0x%x, pri: %d"
    };
        mask: Diags.USER3,
        msg: "LD_noWork: coreId: %d, curSetLocal: %d, curSetX: %d, curMaskLocal: %d"
    };
        mask: Diags.USER3,
        msg: "LD_schedule: coreId: %d, workFlag: %d, curSetLocal: %d, curSetX: %d, curMaskLocal: %d"
    };
        mask: Diags.USER1 | Diags.USER2,
        msg: "LM_setAffinity: tsk: 0x%x, func: 0x%x, oldCore: %d, oldAffinity %d, newAffinity %d"
    };
        mask: Diags.USER1 | Diags.USER2,
        msg: "LM_setPri: tsk: 0x%x, func: 0x%x, oldPri: %d, newPri %d"
    };
        mask: Diags.USER1 | Diags.USER2,
        msg: "LM_sleep: tsk: 0x%x, func: 0x%x, timeout: %d"
    };
        mask: Diags.USER1 | Diags.USER2,
        msg: "LM_switch: oldtsk: 0x%x, oldfunc: 0x%x, newtsk: 0x%x, newfunc: 0x%x"
    };
        mask: Diags.USER1 | Diags.USER2,
        msg: "LM_yield: tsk: 0x%x, func: 0x%x, currThread: %d"
    };
 
module-wide functions
    Task.getNickName// (Any tskView) returns String
per-instance config parameters
    var params = new Task.Params// Instance config-params object;
        params.arg0// Task function argument. Default is 0 = UArg 0;
        params.arg1// Task function argument. Default is 0 = UArg 0;
        params.env// Environment data struct = Ptr null;
        params.stack// Task stack pointer. Default = null = Ptr null;
        params.stackSection// Mem section used for statically created task stacks = String undefined;
        params.stackSize// Task stack size in MAUs = SizeT 0;
per-instance creation
    var inst = Task.create// Create an instance-object(Void(*)(UArg,UArg) fxn, params);
 
 
const Task.AFFINITY_NONE

"Don't care" task affinity

Configuration settings
const Task.AFFINITY_NONE = ~(0);
 
C SYNOPSIS
 
enum Task.Mode

Task execution modes

Configuration settings
values of type Task.Mode
    const Task.Mode_RUNNING;
    // Task is currently executing
    const Task.Mode_READY;
    // Task is scheduled for execution
    const Task.Mode_BLOCKED;
    // Task is suspended from execution
    const Task.Mode_TERMINATED;
    // Task is terminated from execution
    const Task.Mode_INACTIVE;
    // Task is on inactive task list
 
DETAILS
These enumerations are the range of modes or states that a task can be in. A task's current mode can be gotten using stat.
C SYNOPSIS
 
struct Task.HookSet

Task hook set type definition

Configuration settings
var obj = new Task.HookSet;
 
    obj.registerFxn = Void(*)(Int)  ...
    obj.createFxn = Void(*)(Task.Handle,Error.Block*)  ...
    obj.readyFxn = Void(*)(Task.Handle)  ...
    obj.switchFxn = Void(*)(Task.Handle,Task.Handle)  ...
    obj.exitFxn = Void(*)(Task.Handle)  ...
    obj.deleteFxn = Void(*)(Task.Handle)  ...
 
DETAILS
Sets of hook functions can be specified for the Task module. See Hook Functions for details.
C SYNOPSIS
 
struct Task.Stat

Task Status Buffer

Configuration settings
var obj = new Task.Stat;
 
    obj.priority = Int  ...
    // Task priority
    obj.stack = Ptr  ...
    // Task stack
    obj.stackSize = SizeT  ...
    // Task stack size
    obj.stackHeap = IHeap.Handle  ...
    // Heap used to alloc stack
    obj.env = Ptr  ...
    // Global environment struct
    obj.mode = Task.Mode  ...
    // Task's current mode
    obj.sp = Ptr  ...
    // Task's current stack pointer
    obj.used = SizeT  ...
    // max # of words used on stack
 
DETAILS
Passed to and filled in by stat;
C SYNOPSIS
 
config Task.A_badAffinity  // module-wide

Asserted in Task_setAffinity

Configuration settings
Task.A_badAffinity = Assert.Desc {
    msg: "A_badAffinity: Invalid affinity."
};
 
C SYNOPSIS
 
config Task.A_badPriority  // module-wide

Asserted in Task_create

Configuration settings
Task.A_badPriority = Assert.Desc {
    msg: "A_badPriority: An invalid task priority was used."
};
 
C SYNOPSIS
 
config Task.A_badTaskState  // module-wide

Asserted in Task_delete

Configuration settings
Task.A_badTaskState = Assert.Desc {
    msg: "A_badTaskState: Can't delete a task in RUNNING state."
};
 
C SYNOPSIS
 
config Task.A_badThreadType  // module-wide

Asserted in Task_create and Task_delete

Configuration settings
Task.A_badThreadType = Assert.Desc {
    msg: "A_badThreadType: Cannot create/delete a task from Hwi or Swi thread."
};
 
C SYNOPSIS
 
config Task.A_badTimeout  // module-wide

Asserted in Task_sleep

Configuration settings
Task.A_badTimeout = Assert.Desc {
    msg: "A_badTimeout: Can't sleep FOREVER."
};
 
C SYNOPSIS
 
config Task.A_noPendElem  // module-wide

Asserted in Task_delete

Configuration settings
Task.A_noPendElem = Assert.Desc {
    msg: "A_noPendElem: Not enough info to delete BLOCKED task."
};
 
C SYNOPSIS
 
config Task.A_sleepTaskDisabled  // module-wide

Asserted in Task_sleep

Configuration settings
Task.A_sleepTaskDisabled = Assert.Desc {
    msg: "A_sleepTaskDisabled: Cannot call Task_sleep() while the Task scheduler is disabled."
};
 
C SYNOPSIS
 
config Task.A_taskDisabled  // module-wide

Asserted in Task_create

Configuration settings
Task.A_taskDisabled = Assert.Desc {
    msg: "A_taskDisabled: Cannot create a task when tasking is disabled."
};
 
C SYNOPSIS
 
config Task.E_deleteNotAllowed  // module-wide
Configuration settings
Task.E_deleteNotAllowed = Error.Desc {
    msg: "E_deleteNotAllowed: Task 0x%x."
};
 
C SYNOPSIS
 
config Task.E_spOutOfBounds  // module-wide

Error raised when a task's stack pointer (SP) does not point somewhere within the task's stack

Configuration settings
Task.E_spOutOfBounds = Error.Desc {
    msg: "E_spOutOfBounds: Task 0x%x stack error, SP = 0x%x."
};
 
DETAILS
This error is raised by kernel's stack checking function. This function checks the SPs before every task switch to make sure they point within the task's stack.
The stack checking logic is enabled by the initStackFlag and checkStackFlag configuration parameters. If both of these flags are set to true, the kernel will validate the stack pointers.
C SYNOPSIS
 
config Task.E_stackOverflow  // module-wide

Error raised when a stack overflow (or corruption) is detected

Configuration settings
Task.E_stackOverflow = Error.Desc {
    msg: "E_stackOverflow: Task 0x%x stack overflow."
};
 
DETAILS
This error is raised by kernel's stack checking function. This function checks the stacks before every task switch to make sure that reserved word at top of stack has not been modified.
The stack checking logic is enabled by the initStackFlag and checkStackFlag configuration parameters. If both of these flags are set to true, the kernel will validate the stacks.
C SYNOPSIS
 
config Task.LD_block  // module-wide

Logged when a task is blocked (ie Semaphore_pend())

Configuration settings
Task.LD_block = Log.EventDesc {
    mask: Diags.USER2,
    msg: "LD_block: tsk: 0x%x, func: 0x%x"
};
 
C SYNOPSIS
 
config Task.LD_exit  // module-wide

Logged when Task functions fall thru the bottom or when Task_exit() is explicitly called

Configuration settings
Task.LD_exit = Log.EventDesc {
    mask: Diags.USER2,
    msg: "LD_exit: tsk: 0x%x, func: 0x%x"
};
 
C SYNOPSIS
 
config Task.LD_ready  // module-wide

Logged when a task is made ready to run (ie Semaphore_post())

Configuration settings
Task.LD_ready = Log.EventDesc {
    mask: Diags.USER2,
    msg: "LD_ready: tsk: 0x%x, func: 0x%x, pri: %d"
};
 
C SYNOPSIS
 
config Task.LM_noWork  // module-wide

Logged when no scheduling work was found

Configuration settings
Task.LM_noWork = Log.EventDesc {
    mask: Diags.USER3,
    msg: "LD_noWork: coreId: %d, curSetLocal: %d, curSetX: %d, curMaskLocal: %d"
};
 
C SYNOPSIS
 
config Task.LM_schedule  // module-wide

Logged on every task schedule entry

Configuration settings
Task.LM_schedule = Log.EventDesc {
    mask: Diags.USER3,
    msg: "LD_schedule: coreId: %d, workFlag: %d, curSetLocal: %d, curSetX: %d, curMaskLocal: %d"
};
 
C SYNOPSIS
 
config Task.LM_setAffinity  // module-wide

Logged on calls to Task_setAffinity

Configuration settings
Task.LM_setAffinity = Log.EventDesc {
    mask: Diags.USER1 | Diags.USER2,
    msg: "LM_setAffinity: tsk: 0x%x, func: 0x%x, oldCore: %d, oldAffinity %d, newAffinity %d"
};
 
C SYNOPSIS
 
config Task.LM_setPri  // module-wide

Logged on calls to Task_setPri

Configuration settings
Task.LM_setPri = Log.EventDesc {
    mask: Diags.USER1 | Diags.USER2,
    msg: "LM_setPri: tsk: 0x%x, func: 0x%x, oldPri: %d, newPri %d"
};
 
C SYNOPSIS
 
config Task.LM_sleep  // module-wide

Logged on calls to Task_sleep

Configuration settings
Task.LM_sleep = Log.EventDesc {
    mask: Diags.USER1 | Diags.USER2,
    msg: "LM_sleep: tsk: 0x%x, func: 0x%x, timeout: %d"
};
 
C SYNOPSIS
 
config Task.LM_switch  // module-wide

Logged on every task switch

Configuration settings
Task.LM_switch = Log.EventDesc {
    mask: Diags.USER1 | Diags.USER2,
    msg: "LM_switch: oldtsk: 0x%x, oldfunc: 0x%x, newtsk: 0x%x, newfunc: 0x%x"
};
 
C SYNOPSIS
 
config Task.LM_yield  // module-wide

Logged on calls to Task_yield

Configuration settings
Task.LM_yield = Log.EventDesc {
    mask: Diags.USER1 | Diags.USER2,
    msg: "LM_yield: tsk: 0x%x, func: 0x%x, currThread: %d"
};
 
C SYNOPSIS
 
config Task.allBlockedFunc  // module-wide

Function to call while all tasks are blocked

Configuration settings
Task.allBlockedFunc = Void(*)(Void) null;
 
DETAILS
This function will be called repeatedly while no tasks are ready to run.
Ordinarily (in applications that have tasks ready to run at startup), the function will run in the context of the last task to block.
In an application where there are no tasks ready to run when BIOS_start() is called, the allBlockedFunc function is called within the BIOS_start() thread which runs on the system/ISR stack.
By default, allBlockedFunc is initialized to point to an internal function that simply returns.
By adding the following lines to the config script, the Idle functions will run whenever all tasks are blocked:
  Task.enableIdleTask = false;
  Task.allBlockedFunc = Idle.run;
SEE
CONSTRAINTS
The configured allBlockedFunc is designed to be called repeatedly. It must return in order for the task scheduler to check if all tasks are STILL blocked and if not, run the highest priority task currently ready to run.
The configured allBlockedFunc function is called with interrupts disabled. If your function must run with interrupts enabled, surround the body of your code with Hwi_enable()/Hwi_restore() function calls per the following example:
  Void yourFunc() {
      UInt hwiKey;

      hwiKey = Hwi_enable();

      ...         // your code here

      Hwi_restore(hwiKey);
  }
C SYNOPSIS
 
config Task.defaultStackHeap  // module-wide

Default Mem heap used for all dynamically created task stacks

Configuration settings
Task.defaultStackHeap = IHeap.Handle undefined;
 
DETAILS
Default is null.
C SYNOPSIS
 
config Task.defaultStackSize  // module-wide

Default stack size (in MAUs) used for all tasks

Configuration settings
Task.defaultStackSize = SizeT undefined;
 
DETAILS
Default is obtained from the family-specific TaskSupport module (e.g. ti.sysbios.family.arm.m3.TaskSupport, ti.sysbios.family.c62.TaskSupport).
C SYNOPSIS
 
config Task.deleteTerminatedTasks  // module-wide

Automatically delete terminated tasks

Configuration settings
Task.deleteTerminatedTasks = Bool false;
 
DETAILS
If this feature is enabled, an Idle function is installed that deletes dynamically created Tasks that have terminated either by falling through their task function or by explicitly calling Task_exit().
A list of terminated Tasks that were created dynmically is maintained internally. Each invocation of the installed Idle function deletes the first Task on this list. This one-at-a-time process continues until the list is empty.
NOTE
This feature is disabled by default.
WARNING
When this feature is enabled, an error will be raised if the user's application attempts to delete a terminated task. If a terminated task has already been automatically deleted and THEN the user's application attempts to delete it (ie: using a stale Task handle), the results are undefined and probably catastrophic!
C SYNOPSIS
 
config Task.hooks  // module-wide

Const array that holds the HookSet objects

Configuration settings
Task.hooks = Task.HookSet[length] [ ];
 
DETAILS
See Hook Functions for details about HookSets.
C SYNOPSIS
 
config Task.initStackFlag  // module-wide

Initialize stack with known value for stack checking at runtime (see checkStackFlag)

Configuration settings
Task.initStackFlag = Bool true;
 
DETAILS
This is also useful for inspection of stack in debugger or core dump utilities. Default is true.
C SYNOPSIS
 
config Task.numPriorities  // module-wide

Number of Task priorities supported. Default is 16

Configuration settings
Task.numPriorities = UInt 16;
 
DETAILS
The maximum number of priorities supported is target specific and depends on the number of bits in a UInt data type. For 6x and ARM devices the maximum number of priorities is therefore 32. For 28x, 55x, and MSP430 devices, the maximum number of priorities is 16.
C SYNOPSIS
 
metaonly config Task.checkStackFlag  // module-wide

Check 'from' and 'to' task stacks before task context switch

Configuration settings
Task.checkStackFlag = Bool true;
 
DETAILS
The check consists of testing the top of stack value against its initial value (see initStackFlag). If it is no longer at this value, the assumption is that the task has overrun its stack. If the test fails, then the E_stackOverflow error is raised.
Runtime stack checking is only performed if initStackFlag is also true.
Default is true.
To enable or disable full stack checking, you should set both this flag and the ti.sysbios.hal.Hwi.checkStackFlag.
 
metaonly config Task.common$  // module-wide

Common module configuration parameters

Configuration settings
Task.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly config Task.defaultAffinity  // module-wide

Default core affinity for newly created tasks

Configuration settings
Task.defaultAffinity = UInt Task.AFFINITY_NONE;
 
DETAILS
Default is Task_AFFINITY_NONE, meaning don't care.
 
metaonly config Task.defaultStackSection  // module-wide

Default memory section used for all statically created task stacks

Configuration settings
Task.defaultStackSection = String undefined;
 
DETAILS
The default stack section name is target/device specific. For C6x targets it is ".far:taskStackSection". For C28x targets it is ".taskStackSection". For all other targets it is ".bss:taskStackSection".
By default, all statically created task stacks are grouped together into the defaultStackSection and placed where ever the target specific defaultStackSection base section name (ie .bss, .far, .ebss) is placed.
To place all task stacks into a different memory segment, add the following to your config script:
  Program.sectMap[Task.defaultStackSection] = new Program.SectionSpec();
  Program.sectMap[Task.defaultStackSection].loadSegment =
                   "yourMemorySegment";
To group all task stacks into a different section AND place that section into a specific memory segment, add the following to your config script:
  Task.defaultStackSection = ".yourSectionName";
  Program.sectMap[Task.defaultStackSection] = new Program.SectionSpec();
  Program.sectMap[Task.defaultStackSection].loadSegment =
                   "yourMemorySegment";
Where "yourSectionName" can be just about anything, and "yourMemorySegment" must be a memory segment defined for your board.
 
metaonly config Task.enableIdleTask  // module-wide

Create a task (of priority 0) to run the Idle functions in

Configuration settings
Task.enableIdleTask = Bool true;
 
DETAILS
When set to true, a task is created that continuously calls the Idle_run() function, which, in turn calls each of the configured Idle functions.
When set to false, no Idle Task is created and it is up to the user to call the Idle_run() function if the configured Idle functions need to be run. Or, by adding the following lines to the config script, the Idle functions will run whenever all tasks are blocked (Task.allBlockedFunc):
  Task.enableIdleTask = false;
  Task.allBlockedFunc = Idle.run;
Default is true.
SEE
 
metaonly config Task.idleTaskStackSection  // module-wide

Idle task stack section

Configuration settings
Task.idleTaskStackSection = String undefined;
 
DETAILS
Default is inherited from module config defaultStackSection;
 
metaonly config Task.idleTaskStackSize  // module-wide

Idle task stack size in MAUs

Configuration settings
Task.idleTaskStackSize = SizeT undefined;
 
DETAILS
Default is inherited from module config defaultStackSize.
 
metaonly config Task.idleTaskVitalTaskFlag  // module-wide

Idle task's vitalTaskFlag. (see vitalTaskFlag)

Configuration settings
Task.idleTaskVitalTaskFlag = Bool true;
 
DETAILS
Default is true.
 
metaonly Task.addHookSet()  // module-wide

addHookSet is used in a config file to add a hook set

Configuration settings
Task.addHookSet(Task.HookSet hook) returns Void
 
ARGUMENTS
hook — structure of type HookSet
DETAILS
Configures a set of hook functions for the Task module. Each set contains these hook functions:
  • Register: A function called before any statically created tasks are initialized at runtime. The register hook is called at boot time before main() and before interrupts are enabled.
  • Create: A function that is called when a task is created. This includes tasks that are created statically and those created dynamically using create or construct. The create hook is called outside of a Task_disable/enable block and before the task has been added to the ready list.
  • Ready: A function that is called when a task becomes ready to run. The ready hook is called from within a Task_disable/enable block with interrupts enabled.
  • Switch: A function that is called just before a task switch occurs. The 'prev' and 'next' task handles are passed to the Switch hook. 'prev' is set to NULL for the initial task switch that occurs during SYS/BIOS startup. The Switch hook is called from within a Task_disable/enable block with interrupts enabled.
  • Exit: A function that is called when a task exits using exit. The exit hook is passed the handle of the exiting task. The exit hook is called outside of a Task_disable/enable block and before the task has been removed from the kernel lists.
  • Delete: A function that is called when any task is deleted at run-time with delete. The delete hook is called outside of a Task_disable/enable block.
Hook functions can only be configured statically.
See Hook Functions for more details.
HookSet structure elements may be omitted, in which case those elements will not exist.
For example, the following configuration code defines a HookSet:
  // Hook Set 1
  Task.addHookSet({
     registerFxn: '&myRegister1',
     createFxn:   '&myCreate1',
     readyFxn:    '&myReady1',
     switchFxn:   '&mySwitch1',
     exitFxn:     '&myExit1',
     deleteFxn:   '&myDelete1'
  });
 
metaonly Task.getNickName()  // module-wide
Configuration settings
Task.getNickName(Any tskView) returns String
 
Instance Config Parameters

Configuration settings
var params = new Task.Params;
// Instance config-params object
    params.affinity = UInt undefined;
    // The core which this task is to run on. Default is Task_AFFINITY_NONE
    params.arg0 = UArg 0;
    // Task function argument. Default is 0
    params.arg1 = UArg 0;
    // Task function argument. Default is 0
    params.env = Ptr null;
    // Environment data struct
    params.priority = Int 1;
    // Task priority (0 to Task.numPriorities-1, or -1). Default is 1
    params.stack = Ptr null;
    // Task stack pointer. Default = null
    params.stackHeap = IHeap.Handle null;
    // Mem heap used for dynamically created task stack
    params.stackSection = String undefined;
    // Mem section used for statically created task stacks
    params.stackSize = SizeT 0;
    // Task stack size in MAUs
    params.vitalTaskFlag = Bool true;
    // Exit system immediately when the last task with this flag set to TRUE has terminated
 
config Task.affinity  // instance

The core which this task is to run on. Default is Task_AFFINITY_NONE

Configuration settings
var params = new Task.Params;
  ...
params.affinity = UInt undefined;
 
DETAILS
If there is a compelling reason for a task to be pinned to a particular core, then setting 'affinity' to the corresponding core id will force the task to only be run on that core.
The default affinity is inherited from Task.defaultAffinity which in turn defaults to Task_AFFINITY_NONE, which means the task can be run on either core.
Furthermore, Task_AFFINITY_NONE implies that the task can be moved from core to core as deemed necessary by the Task scheduler in order to keep the two highest priority ready tasks running simultaneously.
C SYNOPSIS
 
config Task.arg0  // instance

Task function argument. Default is 0

Configuration settings
var params = new Task.Params;
  ...
params.arg0 = UArg 0;
 
C SYNOPSIS
 
config Task.arg1  // instance

Task function argument. Default is 0

Configuration settings
var params = new Task.Params;
  ...
params.arg1 = UArg 0;
 
C SYNOPSIS
 
config Task.env  // instance

Environment data struct

Configuration settings
var params = new Task.Params;
  ...
params.env = Ptr null;
 
C SYNOPSIS
 
config Task.priority  // instance

Task priority (0 to Task.numPriorities-1, or -1). Default is 1

Configuration settings
var params = new Task.Params;
  ...
params.priority = Int 1;
 
C SYNOPSIS
 
config Task.stack  // instance

Task stack pointer. Default = null

Configuration settings
var params = new Task.Params;
  ...
params.stack = Ptr null;
 
DETAILS
Null indicates that the stack is to be allocated by create().
Example: To statically initialize "tsk0"'s stack to a literal address, use the following syntax:
      Program.global.tsk0.stack = $addr(literal);
C SYNOPSIS
 
config Task.stackHeap  // instance

Mem heap used for dynamically created task stack

Configuration settings
var params = new Task.Params;
  ...
params.stackHeap = IHeap.Handle null;
 
DETAILS
The default value of NULL means that the module config defaultStackHeap is used.
C SYNOPSIS
 
config Task.stackSize  // instance

Task stack size in MAUs

Configuration settings
var params = new Task.Params;
  ...
params.stackSize = SizeT 0;
 
DETAILS
The default value of 0 means that the module config defaultStackSize is used.
C SYNOPSIS
 
config Task.vitalTaskFlag  // instance

Exit system immediately when the last task with this flag set to TRUE has terminated

Configuration settings
var params = new Task.Params;
  ...
params.vitalTaskFlag = Bool true;
 
DETAILS
Default is true.
C SYNOPSIS
 
metaonly config Task.stackSection  // instance

Mem section used for statically created task stacks

Configuration settings
var params = new Task.Params;
  ...
params.stackSection = String undefined;
 
DETAILS
Default is inherited from module config defaultStackSection.
Instance Creation

Configuration settings
var params = new Task.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = Task.create(Void(*)(UArg,UArg) fxn, params);
// Create an instance-object
ARGUMENTS
fxn — Task Function
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
Task_create creates a new task object. If successful, Task_create returns the handle of the new task object. If unsuccessful, Task_create returns NULL unless it aborts.
The fxn parameter uses the FuncPtr type to pass a pointer to the function the Task object should run. For example, if myFxn is a function in your program, your C code can create a Task object to call that function as follows:
  Task_Params taskParams;

  // Create task with priority 15
  Task_Params_init(&taskParams);
  taskParams.stackSize = 512;
  taskParams.priority = 15;
  Task_create((Task_FuncPtr)myFxn, &taskParams, &eb);
The following statements statically create a task in the configuration file:
  var params = new Task.Params;
  params.instance.name = "tsk0";
  params.arg0 = 1;
  params.arg1 = 2;
  params.priority = 1;
  Task.create('&tsk0_func', params);
If NULL is passed instead of a pointer to an actual Task_Params struct, a default set of parameters is used. The "eb" is an error block that you can use to handle errors that may occur during Task object creation.
The newly created task is placed in Mode_READY mode, and is scheduled to begin concurrent execution of the following function call:
  (*fxn)(arg1, arg2);
As a result of being made ready to run, the task runs any application-wide Ready functions that have been specified.
Task_exit is automatically called if and when the task returns from fxn.
Create Hook Functions
You can specify application-wide Create hook functions in your config file that run whenever a task is created. This includes tasks that are created statically and those created dynamically using Task_create.
For Task objects created statically, Create functions are called during the Task module initialization phase of the program startup process prior to main().
For Task objects created dynamically, Create functions are called after the task handle has been initialized but before the task has been placed on its ready queue.
Any SYS/BIOS function can be called from Create functions. SYS/BIOS passes the task handle of the task being created to each of the Create functions.
All Create function declarations should be similar to this:
  Void myCreateFxn(Task_Handle task);
CONSTRAINTS
  • The fxn parameter and the name attribute cannot be NULL.
  • The priority attribute must be less than or equal to (numPriorities - 1) and greater than or equal to one (1) (priority 0 is owned by the Idle task).
  • The priority can be set to -1 for tasks that will not execute until another task changes the priority to a positive value.
  • The stackHeap attribute must identify a valid memory Heap.
generated on Fri, 03 Oct 2014 23:11:46 GMT