package ti.sysbios.family.arm.ducati |
![](../../../../../Arrow_right.png) |
Contains specifications for the Ducati device-specific SYS/BIOS functions
The two M3 cores share a number of hardware and software resources.
[
more ... ]
package ti.sysbios.family.arm.ducati [2, 0, 0, 0] {
// Counter Timer Module Device Definitions
// Core Identification Module
// A Gate for use by the two Ducati M3 cores to manage shared resources
// Hwi, Swi & Task Gate
// Ducati Cortex M3 Timer Peripherals Manager
// Wugen Module
}
DETAILS
The two M3 cores share a number of hardware and software resources.
The system software must carefully manage these resources when the
dynamic loading of applications is required.
Below is a list of the shared resources that SYS/BIOS modules utilize and
manage.
Shared resources:
AMMU
- Must be configured before unicache is enabled.
- Must have a page descriptor for EVERY memory address
accessed by either core before unicache is enabled.
- AMMU is configured statically, no runtime APIs to modify
the AMMU configuration are provided.
- Initialization is controlled by the
AMMU.configureAmmu flag.
- By default, this flag is true.
Unicache
- Must be configured and enabled.
- Runtime APIs use GateDualCore[0] to arbitrate shared unicache
register usage.
- Initialization is controlled by the
Cache.configureCache flag.
- By default this flag is false.
CTM 2,3,4,5 used for timestamping
- These counters are initialized by the
TimestampProvider module, which
is used by the xdc.runtime.Timestamp module to provide
timestamp services.
- Must be configured and started.
- Configured and started by whichever core comes up first
and detects (by testing register contents) that the CTM
hasn't been configured and started.
Reset Exception vector table (vectors 0-14)
- The address of the Reset Exception vector table is shared by
both cores.
- Vectors 0 and 1 at addresses 0x0 are fetched each time
a core is reset. At that time they must contain the SP and
address of c_int00 for the core being reset.
- Exception vectors 2-14 are used by each core until it has
successfully configured its NVIC's Vector Table Offset Register (VTOR)
to point to the vector table that will be used afterwards.
- The Reset Exception vectors are required to be valid and unique
to the core being reset in case an exception occurs prior to the
VTOR being configured.
- The Reset Exception vector table placement is controlled by the
Hwi.resetVectorAddress
config parameter.
- By default, both cores place their Reset Exception vector table
at 0x00000000.
- It is left to the system software design to guarantee
that only one core is climbing up at a time.
Runtime Exception and Interrupt vector table (vectors 0-79)
- The address of the Runtime Exception and Interrupt vector table
should be unique to each core.
- The Runtime Exception and Interrupt vector table
placement is controlled by the
Hwi.vectorTableAddress
config parameter.
- Default behavior is that core 0 places its runtime vector table
at 0x400 and core 1 places its runtime vector table at 0x800.
GateDualCore[0] is used by the unicache module.
GateDualCore[1-n] can be used by applications to manage shared hardware/software resources
- Initialization is controlled by the
GateDualCore.initGates flag.
- By default, core 0 initializes the gate objects.
generated on Tue, 12 Feb 2013 01:44:10 GMT