This Timer module manages the timer64 peripheral available on many devices.
It is supported on the ARM and c64x+ DSP targets. This module supports the
timer in '32-bit chained' and '32-bit unchained' mode. In the
'32-bit unchained' mode, specify the lower or upper half to be use.
The physical timer being used will be taken out of reset, only when
its specified to be the master.
For shared timers on a homogeneous multicore device (ie. c6472), each
core can create the timer, but only one core will initialize the timer
and take it out of reset. The core that does the initialization can be
specified by the module configuration parameter
timerSettings[].ownerCoreId in the *.cfg file.
By default, Core 0 is the owner for all shared timers.
Note: Creating a timer with 'Timer.ANY' specified as the id will not
return a shared timer on a homogeneous multicore device. To use
a shared timer, specify the timer id explicitly when creating it.
On these devices Timer.ANY specifies the local timer id. This
allows a single image to run on multiple cores since each core
will program a different local timer.
The following sample .cfg code sets core 1 to initialize a shared timer
with id 4.
The following sample .cfg code sets core 0 to initialize a shared timer
with id 4. It also configures the Clock module to use this timer.
This allows multiple cores to share timer 4 for the Clock module's
interrupt source.
const Timer_ANY |
|
Const used to specify any timer
#define Timer_ANY (UInt)~0
const Timer_MAX_PERIOD |
|
Max value of Timer period for PeriodType_COUNTS
#define Timer_MAX_PERIOD (UInt)0xffffffff
enum Timer_Half |
|
In 32-bit modes, used to specify which half of Timer to use
typedef enum Timer_Half {
Timer_Half_LOWER,
Timer_Half_UPPER,
Timer_Half_DEFAULT
} Timer_Half;
enum Timer_Mode |
|
The different modes of the Timer. These values match the TIMMODE
bit fields of the Timer Global Control Register
typedef enum Timer_Mode {
Timer_Mode_64BITGPTIMER,
Timer_Mode_UNCHAINED,
Timer_Mode_WATCHDOG,
Timer_Mode_CHAINED
} Timer_Mode;
enum Timer_PeriodType |
|
Timer period units
typedef enum Timer_PeriodType {
Timer_PeriodType_MICROSECS,
// period in microsecs
Timer_PeriodType_COUNTS
// period in counts
} Timer_PeriodType;
VALUES
PeriodType_MICROSECS
Period value is in microseconds.
PeriodType_COUNTS
Period value is in counts.
enum Timer_RunMode |
|
Timer Run Modes
typedef enum Timer_RunMode {
Timer_RunMode_CONTINUOUS,
// periodic and continuous
Timer_RunMode_ONESHOT,
// one-shot
Timer_RunMode_DYNAMIC
// dynamically reprogrammed
} Timer_RunMode;
VALUES
RunMode_CONTINUOUS
Timer is periodic and runs continuously.
RunMode_ONESHOT
Timer runs for a single period value and stops.
RunMode_DYNAMIC
Timer is dynamically reprogrammed for the next required tick.
enum Timer_StartMode |
|
Timer Start Modes
typedef enum Timer_StartMode {
Timer_StartMode_AUTO,
// timer starts automatically
Timer_StartMode_USER
// timer will be started by user
} Timer_StartMode;
VALUES
StartMode_AUTO
Statically created/constructed Timers will be started in BIOS_start().
Dynamically created Timers will start at create() time. This includes
timers created before BIOS_start().
StartMode_USER
Timer will be started by the user using start().
enum Timer_Status |
|
Timer Status
typedef enum Timer_Status {
Timer_Status_INUSE,
// timer in use
Timer_Status_FREE
// timer is free
} Timer_Status;
VALUES
Status_INUSE
Timer is in use. A timer is marked in use from the time it gets
created to the time it gets deleted.
Status_FREE
Timer is free and can be acquired using create.
typedef Timer_FuncPtr |
|
Timer tick function prototype
typedef Void (*Timer_FuncPtr)(UArg);
struct Timer_Control |
|
Timer Control Register struct
typedef struct Timer_Control {
Bits8 tien;
// 0=Clock not gated by TINP; 1=Clock gated
Bits8 invout;
// 0=Uninverted TSTAT drives TOUT; 1=Inverted TSTAT
Bits8 invin;
// 0=Uninverted TINP drives Timer; 1=Inverted TINP
UInt8 pwid;
// TSTATx goes inactive after pwid cycles (CP=0)
Bits8 cp;
// 0=pulse mode; 1=clock mode
} Timer_Control;
struct Timer_EmuMgt |
|
Timer Emulation Management Register struct
typedef struct Timer_EmuMgt {
Bool free;
// 0=suspend for emu halt; 1=don't suspend
Bool soft;
// 0=stop immediately; 1=stop when count==period
} Timer_EmuMgt;
struct Timer_GpioDatDir |
|
Timer GPIO Data and Direction Management Register struct
typedef struct Timer_GpioDatDir {
Bits8 gpio_dati12;
// 0=TINP12 is input; 1=TINP12 is output
Bits8 gpio_dato12;
// 0=TOUTP12 is input; 1=TOUTP12 is output
Bits8 gpio_dati34;
// 0=TINP34 is input; 1=TINP34 is output
Bits8 gpio_dato34;
// 0=TOUTP34 is input; 1=TOUTP34 is output
Bits8 gpio_diri12;
// 0=input as GPIO input; 1=input as GPIO output
Bits8 gpio_diro12;
// 0=output as GPIO input;1=output as GPIO output
Bits8 gpio_diri34;
// 0=input as GPIO input; 1=input as GPIO output
Bits8 gpio_diro34;
// 0=output as GPIO input;1=output as GPIO output
} Timer_GpioDatDir;
struct Timer_GpioIntEn |
|
Timer GPIO interrupt control and enable Management Register struct
typedef struct Timer_GpioIntEn {
Bits8 gpint12_eni;
// 0=source by timer; 1=input to source event
Bits8 gpint12_eno;
// 0=source by timer; 1=output to source event
Bits8 gpint12_invi;
// 0=don't invert invput; 1=invert input
Bits8 gpint12_invo;
// 0=don't invert output; 1=invert output
Bits8 gpint34_eni;
// 0=source by timer; 1=input to source event
Bits8 gpint34_eno;
// 0=source by timer; 1=output to source event
Bits8 gpint34_invi;
// 0=don't invert invput; 1=invert input
Bits8 gpint34_invo;
// 0=don't invert output; 1=invert output
Bits8 gpio_eni12;
// 0=TINP12 as timer input; 1=TINP12 as GPIO
Bits8 gpio_eno12;
// 0=TOUTP12 as timer output; 1=TOUTP12 as GPIO
Bits8 gpio_eni34;
// 0=TINP34 as timer input; 1=TINP34 as GPIO
Bits8 gpio_eno34;
// 0=TOUTP34 as timer output; 1=TOUTP12 as GPIO
} Timer_GpioIntEn;
struct Timer_TimerSetting |
|
Timer Settings
typedef struct Timer_TimerSetting {
// mode to put each Timer into
Bool master;
// for 'unchained' mode; 1=set mode and reset
UInt16 ownerCoreId;
// used only for homogeneous multicore DSPs
} Timer_TimerSetting;
config Timer_A_notAvailable // module-wide |
|
Assert raised when static created timer is not available
config Timer_E_cannotSupport // module-wide |
|
Error raised when period requested is not supported
extern const Error_Id Timer_E_cannotSupport;
config Timer_E_invalidTimer // module-wide |
|
Error raised when timer id specified is not supported
extern const Error_Id Timer_E_invalidTimer;
config Timer_E_notAvailable // module-wide |
|
Error raised when timer requested is in use
extern const Error_Id Timer_E_notAvailable;
config Timer_anyMask // module-wide |
|
Available mask to be used when select = Timer_ANY. Set in xs file
extern const Bits32 Timer_anyMask;
config Timer_defaultHalf // module-wide |
|
The default 32-bit half of the timer to be used
config Timer_timerSettings // module-wide |
|
Global Control configuration for each physical timer
DETAILS
mode: Mode_UNCHAINED 32-bit unchained mode.
master: TRUE If TRUE, release Timer from reset.
Timer_getNumTimers() // module-wide |
|
Returns number of timer peripherals on the platform
UInt Timer_getNumTimers();
RETURNS
Number of timer peripherals.
Timer_getStatus() // module-wide |
|
Returns timer status (free or in use)
RETURNS
timer status
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool Timer_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Timer_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Timer_Module_getMask();
// Returns the diagnostics mask for this module
Void Timer_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
|
typedef struct Timer_Object Timer_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct Timer_Struct Timer_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
|
typedef struct Timer_Params {
// Instance config-params structure
// Common per-instance configs
UArg arg;
// Argument for tick function
// Control configuration. Default is all fields 0 or false except:
// Emulation Management configuration. Default is:
// Timer frequency
// General Purpose IO data and direction Management configuration
The default is all fields is 0
// General Purpose IO interrupt control and enable Management
configuration. The default for all fields is 0
// In 32-bit unchained mode, this field is used to specify which half
of the timer to use
// Hwi Params for Hwi Object. Default is null
Int intNum;
// Hwi interrupt number to be used by Timer
UInt32 period;
// Period of a tick
// Period type
UInt prescalar;
// 32-bit pre-scalar to TIM12 in '32-bit chained' mode.
The default is 0
// Timer run mode
// Timer start mode
} Timer_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config Timer_arg // instance |
|
Argument for tick function
DETAILS
Default is null.
config Timer_controlInit // instance |
|
Control configuration. Default is all fields 0 or false except:
DETAILS
pwid: 1
config Timer_emuMgtInit // instance |
|
Emulation Management configuration. Default is:
DETAILS
free: 0
soft: 0
config Timer_extFreq // instance |
|
Timer frequency
DETAILS
This parameter is meaningfull only on platforms where the timer's
input clock can be changed. If value is left at zero, then input clock
to the timer clock is assumed.
This value is used to convert timer ticks to real time units; seconds,
milliseconds, etc.
config Timer_gpioDatDir // instance |
|
General Purpose IO data and direction Management configuration
The default is all fields is 0
config Timer_gpioIntEn // instance |
|
General Purpose IO interrupt control and enable Management
configuration. The default for all fields is 0
config Timer_half // instance |
|
In 32-bit unchained mode, this field is used to specify which half
of the timer to use
config Timer_hwiParams // instance |
|
Hwi Params for Hwi Object. Default is null
config Timer_intNum // instance |
|
Hwi interrupt number to be used by Timer
config Timer_period // instance |
|
Period of a tick
DETAILS
The period can be specified in timer counts or microseconds
and its default value is 0.
The implementation of ITimer will support a period of UInt32
timer counts and use pre-scalars if necessary.
config Timer_periodType // instance |
|
Period type
DETAILS
Default is PeriodType_MICROSECS
config Timer_prescalar // instance |
|
32-bit pre-scalar to TIM12 in '32-bit chained' mode.
The default is 0
config Timer_runMode // instance |
|
Timer run mode
DETAILS
config Timer_startMode // instance |
|
Timer start mode
DETAILS
Instance Creation |
|
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
id
Timer id ranging from 0 to a platform specific value,
or ANY
tickFxn
function that runs upon timer expiry.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
Create could fail if timer peripheral is unavailable. To
request any available timer use
ANY as the id.
TimerId's are logical ids. The family-specific implementations
map the ids to physical peripherals.
Instance Deletion |
|
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
Timer_getCount() // instance |
|
Read timer counter register
ARGUMENTS
handle
handle of a previously-created Timer instance object
RETURNS
timer counter value
Timer_getFreq() // instance |
|
Return timer frequency in Hz
ARGUMENTS
handle
handle of a previously-created Timer instance object
freq
frequency in Hz
DETAILS
This is the effective frequency of the clock incrementing the timer
counter register after all scaling factors are taken into account.
(including pre-scalars).
Timer_getFunc() // instance |
|
Get Timer function and arg
ARGUMENTS
handle
handle of a previously-created Timer instance object
arg
pointer for returning Timer's function argument
RETURNS
Timer's function
Timer_getPeriod() // instance |
|
Get timer period in timer counts
ARGUMENTS
handle
handle of a previously-created Timer instance object
RETURNS
period in timer counts
Timer_reconfig() // instance |
|
Used to modify static timer instances at runtime
ARGUMENTS
handle
handle of a previously-created Timer instance object
timerParams
timer Params
tickFxn
functions that runs when timer expires
Timer_setFunc() // instance |
|
Overwrite Timer function and arg
ARGUMENTS
handle
handle of a previously-created Timer instance object
fxn
pointer to function
arg
argument to function
DETAILS
Replaces a Timer object's tickFxn function originally
provided in
create.
Timer_setPeriod() // instance |
|
Set timer period specified in timer counts
ARGUMENTS
handle
handle of a previously-created Timer instance object
period
period in timer counts
DETAILS
Timer_setPeriod() invokes Timer_stop() prior to setting the period
and leaves the timer in the stopped state.
To dynamically change the period of a timer you must
protect against re-entrancy by disabling interrupts.
Use the following call sequence to guarantee proper results:
// disable interrupts if an interrupt could lead to
// another call to Timer_start().
key = Hwi_disable();
Timer_setPeriod(period);
Timer_start();
Hwi_restore(key);
ITimer implementation must support UInt32 and use pre-scalars whenever
necessary
SIDE EFFECTS
Calls Timer_stop(), and disables the timer's interrupt.
Timer_setPeriodMicroSecs() // instance |
|
Set timer period specified in microseconds
Bool Timer_setPeriodMicroSecs(
Timer_Handle handle,
UInt32 microsecs);
ARGUMENTS
handle
handle of a previously-created Timer instance object
period
period in microseconds
DETAILS
A best-effort method will be used to set the period register.
There might be a slight rounding error based on resolution of timer
period register. If the timer frequency cannot support the requested
period, i.e. the timer period register cannot support the requested
period, then this function returns false.
Timer_setPeriodMicroSecs() invokes Timer_stop() prior to setting
the period and leaves the timer in the stopped state.
To dynamically change the period of a timer you must
protect against re-entrancy by disabling interrupts.
Use the following call sequence to guarantee proper results:
// disable interrupts if an interrupt could lead to
// another call to Timer_start().
key = Hwi_disable();
Timer_setPeriodMicroSecs(period);
Timer_start();
Hwi_restore(key);
Timer_start() // instance |
|
Reload and start the timer
ARGUMENTS
handle
handle of a previously-created Timer instance object
DETAILS
Thread safety must be observed when using the
start
and
stop APIs to avoid possible miss-
configuration of the timers and unintended behaviors.
To protect against re-entrancy, surround the start/stop invocations
with
Hwi_disable() and
Hwi_restore() calls:
// disable interrupts if an interrupt could lead to
// another call to Timer_start().
key = Hwi_disable();
Timer_stop();
...
Timer_start();
Hwi_restore(key);
SIDE EFFECTS
Enables the timer's interrupt.
Timer_stop() // instance |
|
Stop the timer
ARGUMENTS
handle
handle of a previously-created Timer instance object
DETAILS
Thread safety must be observed when using the
start
and
stop APIs to avoid possible miss-
configuration of the timers and unintended behaviors.
To protect against re-entrancy, surround the start/stop invocations
with
Hwi_disable() and
Hwi_restore() calls:
// disable interrupts if an interrupt could lead to
// another call to Timer_start().
key = Hwi_disable();
Timer_stop();
...
Timer_start();
Hwi_restore(key);
SIDE EFFECTS
Disables the timer's interrupt.
Instance Convertors |
|
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins |
|
Int Timer_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
const Timer.ANY |
|
Const used to specify any timer
XDCscript usage |
meta-domain |
C SYNOPSIS
const Timer.MAX_PERIOD |
|
Max value of Timer period for PeriodType_COUNTS
XDCscript usage |
meta-domain |
const Timer.MAX_PERIOD = 0xffffffff;
C SYNOPSIS
enum Timer.Half |
|
In 32-bit modes, used to specify which half of Timer to use
XDCscript usage |
meta-domain |
values of type Timer.Half
const Timer.Half_LOWER;
const Timer.Half_UPPER;
const Timer.Half_DEFAULT;
C SYNOPSIS
enum Timer.Mode |
|
The different modes of the Timer. These values match the TIMMODE
bit fields of the Timer Global Control Register
XDCscript usage |
meta-domain |
values of type Timer.Mode
const Timer.Mode_64BITGPTIMER;
const Timer.Mode_UNCHAINED;
const Timer.Mode_WATCHDOG;
const Timer.Mode_CHAINED;
C SYNOPSIS
enum Timer.PeriodType |
|
Timer period units
XDCscript usage |
meta-domain |
values of type Timer.PeriodType
const Timer.PeriodType_MICROSECS;
// period in microsecs
const Timer.PeriodType_COUNTS;
// period in counts
VALUES
PeriodType_MICROSECS
Period value is in microseconds.
PeriodType_COUNTS
Period value is in counts.
C SYNOPSIS
enum Timer.RunMode |
|
Timer Run Modes
XDCscript usage |
meta-domain |
values of type Timer.RunMode
const Timer.RunMode_CONTINUOUS;
// periodic and continuous
const Timer.RunMode_ONESHOT;
// one-shot
const Timer.RunMode_DYNAMIC;
// dynamically reprogrammed
VALUES
RunMode_CONTINUOUS
Timer is periodic and runs continuously.
RunMode_ONESHOT
Timer runs for a single period value and stops.
RunMode_DYNAMIC
Timer is dynamically reprogrammed for the next required tick.
C SYNOPSIS
enum Timer.StartMode |
|
Timer Start Modes
XDCscript usage |
meta-domain |
values of type Timer.StartMode
const Timer.StartMode_AUTO;
// timer starts automatically
const Timer.StartMode_USER;
// timer will be started by user
VALUES
StartMode_AUTO
Statically created/constructed Timers will be started in BIOS_start().
Dynamically created Timers will start at create() time. This includes
timers created before BIOS_start().
StartMode_USER
Timer will be started by the user using start().
C SYNOPSIS
enum Timer.Status |
|
Timer Status
XDCscript usage |
meta-domain |
values of type Timer.Status
const Timer.Status_INUSE;
// timer in use
const Timer.Status_FREE;
// timer is free
VALUES
Status_INUSE
Timer is in use. A timer is marked in use from the time it gets
created to the time it gets deleted.
Status_FREE
Timer is free and can be acquired using create.
C SYNOPSIS
struct Timer.Control |
|
Timer Control Register struct
XDCscript usage |
meta-domain |
var obj = new Timer.Control;
obj.tien = Bits8 ...
// 0=Clock not gated by TINP; 1=Clock gated
obj.invout = Bits8 ...
// 0=Uninverted TSTAT drives TOUT; 1=Inverted TSTAT
obj.invin = Bits8 ...
// 0=Uninverted TINP drives Timer; 1=Inverted TINP
obj.pwid = UInt8 ...
// TSTATx goes inactive after pwid cycles (CP=0)
obj.cp = Bits8 ...
// 0=pulse mode; 1=clock mode
C SYNOPSIS
struct Timer.EmuMgt |
|
Timer Emulation Management Register struct
XDCscript usage |
meta-domain |
var obj = new Timer.EmuMgt;
obj.free = Bool ...
// 0=suspend for emu halt; 1=don't suspend
obj.soft = Bool ...
// 0=stop immediately; 1=stop when count==period
C SYNOPSIS
struct Timer.GpioDatDir |
|
Timer GPIO Data and Direction Management Register struct
XDCscript usage |
meta-domain |
var obj = new Timer.GpioDatDir;
obj.gpio_dati12 = Bits8 ...
// 0=TINP12 is input; 1=TINP12 is output
obj.gpio_dato12 = Bits8 ...
// 0=TOUTP12 is input; 1=TOUTP12 is output
obj.gpio_dati34 = Bits8 ...
// 0=TINP34 is input; 1=TINP34 is output
obj.gpio_dato34 = Bits8 ...
// 0=TOUTP34 is input; 1=TOUTP34 is output
obj.gpio_diri12 = Bits8 ...
// 0=input as GPIO input; 1=input as GPIO output
obj.gpio_diro12 = Bits8 ...
// 0=output as GPIO input;1=output as GPIO output
obj.gpio_diri34 = Bits8 ...
// 0=input as GPIO input; 1=input as GPIO output
obj.gpio_diro34 = Bits8 ...
// 0=output as GPIO input;1=output as GPIO output
C SYNOPSIS
struct Timer.GpioIntEn |
|
Timer GPIO interrupt control and enable Management Register struct
XDCscript usage |
meta-domain |
var obj = new Timer.GpioIntEn;
obj.gpint12_eni = Bits8 ...
// 0=source by timer; 1=input to source event
obj.gpint12_eno = Bits8 ...
// 0=source by timer; 1=output to source event
obj.gpint12_invi = Bits8 ...
// 0=don't invert invput; 1=invert input
obj.gpint12_invo = Bits8 ...
// 0=don't invert output; 1=invert output
obj.gpint34_eni = Bits8 ...
// 0=source by timer; 1=input to source event
obj.gpint34_eno = Bits8 ...
// 0=source by timer; 1=output to source event
obj.gpint34_invi = Bits8 ...
// 0=don't invert invput; 1=invert input
obj.gpint34_invo = Bits8 ...
// 0=don't invert output; 1=invert output
obj.gpio_eni12 = Bits8 ...
// 0=TINP12 as timer input; 1=TINP12 as GPIO
obj.gpio_eno12 = Bits8 ...
// 0=TOUTP12 as timer output; 1=TOUTP12 as GPIO
obj.gpio_eni34 = Bits8 ...
// 0=TINP34 as timer input; 1=TINP34 as GPIO
obj.gpio_eno34 = Bits8 ...
// 0=TOUTP34 as timer output; 1=TOUTP12 as GPIO
C SYNOPSIS
struct Timer.TimerSetting |
|
Timer Settings
XDCscript usage |
meta-domain |
var obj = new Timer.TimerSetting;
// mode to put each Timer into
obj.master = Bool ...
// for 'unchained' mode; 1=set mode and reset
obj.ownerCoreId = UInt16 ...
// used only for homogeneous multicore DSPs
C SYNOPSIS
config Timer.A_notAvailable // module-wide |
|
Assert raised when static created timer is not available
XDCscript usage |
meta-domain |
msg: "A_notAvailable: static created timer not available"
};
C SYNOPSIS
config Timer.E_cannotSupport // module-wide |
|
Error raised when period requested is not supported
XDCscript usage |
meta-domain |
msg: "E_cannotSupport: Timer cannot support requested period %d"
};
C SYNOPSIS
config Timer.E_invalidTimer // module-wide |
|
Error raised when timer id specified is not supported
XDCscript usage |
meta-domain |
msg: "E_invalidTimer: Invalid Timer Id %d"
};
C SYNOPSIS
config Timer.E_notAvailable // module-wide |
|
Error raised when timer requested is in use
XDCscript usage |
meta-domain |
msg: "E_notAvailable: Timer not available %d"
};
C SYNOPSIS
config Timer.anyMask // module-wide |
|
Available mask to be used when select = Timer_ANY. Set in xs file
XDCscript usage |
meta-domain |
Timer.anyMask = Bits32 undefined;
C SYNOPSIS
config Timer.defaultHalf // module-wide |
|
The default 32-bit half of the timer to be used
XDCscript usage |
meta-domain |
C SYNOPSIS
config Timer.timerSettings // module-wide |
|
Global Control configuration for each physical timer
XDCscript usage |
meta-domain |
DETAILS
mode: Mode_UNCHAINED 32-bit unchained mode.
master: TRUE If TRUE, release Timer from reset.
C SYNOPSIS
metaonly config Timer.common$ // module-wide |
|
Common module configuration parameters
XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly config Timer.intFreqs // module-wide |
|
Internal frequency for Timers
XDCscript usage |
meta-domain |
Instance Config Parameters |
|
XDCscript usage |
meta-domain |
var params = new Timer.Params;
// Instance config-params object
params.arg = UArg null;
// Argument for tick function
// Control configuration. Default is all fields 0 or false except:
tien: 0,
invout: 0,
invin: 0,
pwid: 1,
cp: 0
};
// Emulation Management configuration. Default is:
free: 0,
soft: 0
};
// Timer frequency
lo: 0,
hi: 0
};
// General Purpose IO data and direction Management configuration
The default is all fields is 0
gpio_dati12: 0,
gpio_dato12: 0,
gpio_dati34: 0,
gpio_dato34: 0,
gpio_diri12: 0,
gpio_diro12: 0,
gpio_diri34: 0,
gpio_diro34: 0
};
// General Purpose IO interrupt control and enable Management
configuration. The default for all fields is 0
gpint12_eni: 0,
gpint12_eno: 0,
gpint12_invi: 0,
gpint12_invo: 0,
gpint34_eni: 0,
gpint34_eno: 0,
gpint34_invi: 0,
gpint34_invo: 0,
gpio_eni12: 0,
gpio_eno12: 0,
gpio_eni34: 0,
gpio_eno34: 0
};
// In 32-bit unchained mode, this field is used to specify which half
of the timer to use
// Hwi Params for Hwi Object. Default is null
params.intNum = Int -1;
// Hwi interrupt number to be used by Timer
params.period = UInt32 0;
// Period of a tick
// Period type
params.prescalar = UInt 0;
// 32-bit pre-scalar to TIM12 in '32-bit chained' mode.
The default is 0
// Timer run mode
// Timer start mode
config Timer.arg // instance |
|
Argument for tick function
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
params.arg = UArg null;
DETAILS
Default is null.
C SYNOPSIS
config Timer.controlInit // instance |
|
Control configuration. Default is all fields 0 or false except:
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
tien: 0,
invout: 0,
invin: 0,
pwid: 1,
cp: 0
};
DETAILS
pwid: 1
C SYNOPSIS
config Timer.emuMgtInit // instance |
|
Emulation Management configuration. Default is:
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
free: 0,
soft: 0
};
DETAILS
free: 0
soft: 0
C SYNOPSIS
config Timer.extFreq // instance |
|
Timer frequency
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
lo: 0,
hi: 0
};
DETAILS
This parameter is meaningfull only on platforms where the timer's
input clock can be changed. If value is left at zero, then input clock
to the timer clock is assumed.
This value is used to convert timer ticks to real time units; seconds,
milliseconds, etc.
C SYNOPSIS
config Timer.gpioDatDir // instance |
|
General Purpose IO data and direction Management configuration
The default is all fields is 0
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
gpio_dati12: 0,
gpio_dato12: 0,
gpio_dati34: 0,
gpio_dato34: 0,
gpio_diri12: 0,
gpio_diro12: 0,
gpio_diri34: 0,
gpio_diro34: 0
};
C SYNOPSIS
config Timer.gpioIntEn // instance |
|
General Purpose IO interrupt control and enable Management
configuration. The default for all fields is 0
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
gpint12_eni: 0,
gpint12_eno: 0,
gpint12_invi: 0,
gpint12_invo: 0,
gpint34_eni: 0,
gpint34_eno: 0,
gpint34_invi: 0,
gpint34_invo: 0,
gpio_eni12: 0,
gpio_eno12: 0,
gpio_eni34: 0,
gpio_eno34: 0
};
C SYNOPSIS
config Timer.half // instance |
|
In 32-bit unchained mode, this field is used to specify which half
of the timer to use
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
C SYNOPSIS
config Timer.hwiParams // instance |
|
Hwi Params for Hwi Object. Default is null
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
C SYNOPSIS
config Timer.intNum // instance |
|
Hwi interrupt number to be used by Timer
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
params.intNum = Int -1;
C SYNOPSIS
config Timer.period // instance |
|
Period of a tick
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
params.period = UInt32 0;
DETAILS
The period can be specified in timer counts or microseconds
and its default value is 0.
The implementation of ITimer will support a period of UInt32
timer counts and use pre-scalars if necessary.
C SYNOPSIS
config Timer.periodType // instance |
|
Period type
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
DETAILS
Default is PeriodType_MICROSECS
C SYNOPSIS
config Timer.prescalar // instance |
|
32-bit pre-scalar to TIM12 in '32-bit chained' mode.
The default is 0
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
params.prescalar = UInt 0;
C SYNOPSIS
config Timer.runMode // instance |
|
Timer run mode
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
DETAILS
C SYNOPSIS
config Timer.startMode // instance |
|
Timer start mode
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
DETAILS
C SYNOPSIS
Instance Creation |
|
XDCscript usage |
meta-domain |
var params =
new Timer.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = Timer.create(Int id, Void(*)(UArg) tickFxn, params);
// Create an instance-object
ARGUMENTS
id
Timer id ranging from 0 to a platform specific value,
or ANY
tickFxn
function that runs upon timer expiry.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
Create could fail if timer peripheral is unavailable. To
request any available timer use
ANY as the id.
TimerId's are logical ids. The family-specific implementations
map the ids to physical peripherals.