const Timer_ANY |
![](../../../../Arrow_up.png) |
Const used to specify any timer
#define Timer_ANY (UInt)~0
const Timer_MAX_PERIOD |
![](../../../../Arrow_up.png) |
Max value of Timer period for PeriodType_COUNTS
#define Timer_MAX_PERIOD (UInt)0xffffffff
const Timer_NUM_TIMER_DEVICES |
![](../../../../Arrow_up.png) |
Emulation supports 2 timers
#define Timer_NUM_TIMER_DEVICES (Int)2
enum Timer_PeriodType |
![](../../../../Arrow_up.png) |
PeriodType
typedef enum Timer_PeriodType {
Timer_PeriodType_MICROSECS,
// period in microsecs
Timer_PeriodType_COUNTS
// period in counts
} Timer_PeriodType;
VALUES
PeriodType_MICROSECS
Period value is in microseconds.
PeriodType_COUNTS
Period value is in counts.
enum Timer_RunMode |
![](../../../../Arrow_up.png) |
Timer Run Modes
typedef enum Timer_RunMode {
Timer_RunMode_CONTINUOUS,
// periodic and continuous
Timer_RunMode_ONESHOT
// one-shot
} Timer_RunMode;
VALUES
RunMode_CONTINUOUS
Timer is periodic and runs continuously.
RunMode_ONESHOT
Timer runs for a single period value and stops
enum Timer_StartMode |
![](../../../../Arrow_up.png) |
Timer Start Modes
typedef enum Timer_StartMode {
Timer_StartMode_AUTO,
// timer starts automatically
Timer_StartMode_USER
// timer will be started by user
} Timer_StartMode;
VALUES
StartMode_AUTO
Statically created/constructed Timers will be started in BIOS_start().
Dynamically created Timers will start at create() time. This includes
timers created before BIOS_start().
StartMode_USER
Timer will be started by the user using start().
enum Timer_Status |
![](../../../../Arrow_up.png) |
Timer Status
typedef enum Timer_Status {
Timer_Status_INUSE,
// timer in use
Timer_Status_FREE
// timer is free
} Timer_Status;
VALUES
Status_INUSE
Timer is in use. A timer is marked in use from the time it gets
created to the time it gets deleted.
Status_FREE
Timer is free and can be acquired using create.
typedef Timer_FuncPtr |
![](../../../../Arrow_up.png) |
Timer tick function prototype
typedef Void (*Timer_FuncPtr)(UArg);
config Timer_E_calloc // module-wide |
![](../../../../Arrow_up.png) |
Error: memory allocation request failed
DETAILS
A request into the Windows runtime library for memory has failed.
RAISED_IN
config Timer_E_cannotSupport // module-wide |
![](../../../../Arrow_up.png) |
Error: unsupported timer period
extern const Error_Id Timer_E_cannotSupport;
DETAILS
On Windows, the timer period cannot be less than one millisecond.
However, the actual minimum timer period (even when set to one
millisecond) is 10 - 15 milliseconds. This latency results from the
Windows clock ticking at 10 milliseconds with additional delays in
the Windows kernel.
RAISED_IN
config Timer_E_event // module-wide |
![](../../../../Arrow_up.png) |
Error: CreateEvent failed
DETAILS
A CreateEvent call into the Win32 API has failed.
RAISED_IN
config Timer_E_invalidTimer // module-wide |
![](../../../../Arrow_up.png) |
Error: Invalid timer specified
extern const Error_Id Timer_E_invalidTimer;
DETAILS
An invalid timer id was specified. Timer id must be in the range
0 to (
NUM_TIMER_DEVICES - 1). In the
create() call,
an id of -1 may be used to request any available timer.
RAISED_IN
config Timer_E_noneAvailable // module-wide |
![](../../../../Arrow_up.png) |
Error: no timers available
extern const Error_Id Timer_E_noneAvailable;
DETAILS
A request was made for any available timer, but there are none
available at this time.
RAISED_IN
config Timer_E_notAvailable // module-wide |
![](../../../../Arrow_up.png) |
Error: requested timer not available
extern const Error_Id Timer_E_notAvailable;
DETAILS
A request was made for a timer, but it is not available at this time.
It is currently in use.
RAISED_IN
config Timer_E_notSupported // module-wide |
![](../../../../Arrow_up.png) |
Error: API not supported on Windows
extern const Error_Id Timer_E_notSupported;
DETAILS
This timer API is not supported on Windows.
RAISED_IN
config Timer_E_thread // module-wide |
![](../../../../Arrow_up.png) |
Error: CreateThread failed
DETAILS
A CreateThread call into the Win32 API has failed.
RAISED_IN
config Timer_E_wait // module-wide |
![](../../../../Arrow_up.png) |
Error: WaitForSingleObject failed
DETAILS
A WaitForSingleObject call into the Win32 API has failed.
RAISED_IN
config Timer_anyMask // module-wide |
![](../../../../Arrow_up.png) |
Available mask to be used when select = TIMER_ANY
extern const UInt Timer_anyMask;
Timer_getNumTimers() // module-wide |
![](../../../../Arrow_up.png) |
Returns number of timer peripherals on the platform
UInt Timer_getNumTimers();
RETURNS
Number of timer peripherals.
Timer_getStatus() // module-wide |
![](../../../../Arrow_up.png) |
Returns timer status (free or in use)
RETURNS
timer status
Module-Wide Built-Ins |
![](../../../../Arrow_up.png) |
// Get this module's unique id
Bool Timer_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Timer_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Timer_Module_getMask();
// Returns the diagnostics mask for this module
Void Timer_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
![](../../../../Arrow_up.png) |
typedef struct Timer_Object Timer_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct Timer_Struct Timer_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
![](../../../../Arrow_up.png) |
typedef struct Timer_Params {
// Instance config-params structure
// Common per-instance configs
UArg arg;
// Argument for tick function. Default is null
// Timer frequency
UInt32 period;
// Period of tick. Can be specified in timer counts or microseconds.
Default is 0
// Period Type. Default is PeriodType_MICROSECS
} Timer_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config Timer_arg // instance |
![](../../../../Arrow_up.png) |
Argument for tick function. Default is null
config Timer_extFreq // instance |
![](../../../../Arrow_up.png) |
Timer frequency
DETAILS
This parameter is meaningfull only on platforms where the timer clock
can be changed. If value is left at zero, then default hookup of timer
clock is assumed.
config Timer_period // instance |
![](../../../../Arrow_up.png) |
Period of tick. Can be specified in timer counts or microseconds.
Default is 0
DETAILS
The implementation of ITimer will support a period of UInt32
timer counts and use pre-scalars if necessary.
config Timer_periodType // instance |
![](../../../../Arrow_up.png) |
Period Type. Default is PeriodType_MICROSECS
config Timer_runMode // instance |
![](../../../../Arrow_up.png) |
Timer run mode. Default is RunMode_CONTINUOUS
config Timer_startMode // instance |
![](../../../../Arrow_up.png) |
Start mode. Default is StartMode_AUTO
Instance Creation |
![](../../../../Arrow_up.png) |
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
id
Timer id ranging from 0 to a platform specific value
tickFxn
function that runs upon timer expiry.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
Create could fail if timer peripheral is unavailable. To
request any available timer use
ANY as the id.
TimerId's are logical ids. The family-specific implementations
map the ids to physical peripherals.
Instance Deletion |
![](../../../../Arrow_up.png) |
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
Timer_getCount() // instance |
![](../../../../Arrow_up.png) |
Reads timer counter register
ARGUMENTS
handle
handle of a previously-created Timer instance object
RETURNS
timer counter value
Timer_getFreq() // instance |
![](../../../../Arrow_up.png) |
Returns timer frequency in Hz
ARGUMENTS
handle
handle of a previously-created Timer instance object
freq
frequency in Hz
DETAILS
This is the effective frequency of the clock incrementing the timer
counter register after all scaling factors are taken into account.
(including pre-scalars).
Timer_getFunc() // instance |
![](../../../../Arrow_up.png) |
Get Timer function and arg
ARGUMENTS
handle
handle of a previously-created Timer instance object
arg
pointer for returning Timer's function argument
RETURNS
Timer's function
Timer_getPeriod() // instance |
![](../../../../Arrow_up.png) |
Gets timer period in timer counts
ARGUMENTS
handle
handle of a previously-created Timer instance object
RETURNS
period in timer counts
Timer_setFunc() // instance |
![](../../../../Arrow_up.png) |
Overwrite Timer function and arg
ARGUMENTS
handle
handle of a previously-created Timer instance object
fxn
pointer to function
arg
argument to function
DETAILS
Replaces a Timer object's tickFxn function originally
provided in
create.
Timer_setPeriod() // instance |
![](../../../../Arrow_up.png) |
Sets timer period specified in timer counts
ARGUMENTS
handle
handle of a previously-created Timer instance object
period
period in timer counts
DETAILS
Timer_setPeriod() invokes Timer_stop() prior to setting the period
and leaves the timer in the stopped state.
To dynamically change the period of a timer you must
protect against re-entrancy by disabling interrupts.
Use the following call sequence to guarantee proper results:
// disable interrupts if an interrupt could lead to
// another call to Timer_start().
key = Hwi_disable();
Timer_setPeriod(period);
Timer_start();
Hwi_restore(key);
ITimer implementation must support UInt32 and use pre-scalars whenever
necessary
SIDE EFFECTS
Calls Timer_stop(), and disables the timer's interrupt.
Timer_setPeriodMicroSecs() // instance |
![](../../../../Arrow_up.png) |
Sets timer period specified in microseconds
Bool Timer_setPeriodMicroSecs(
Timer_Handle handle,
UInt32 microsecs);
ARGUMENTS
handle
handle of a previously-created Timer instance object
period
period in microseconds
DETAILS
A best-effort method will be used to set the period register.
There might be a slight rounding error based on resolution of timer
period register. If the timer frequency cannot support the requested
period, ie the timer period register cannot support the requested
period, then this function returns false.
Timer_setPeriodMicroSecs() invokes Timer_stop() prior to setting
the period and leaves the timer in the stopped state.
To dynamically change the period of a timer you must
protect against re-entrancy by disabling interrupts.
Use the following call sequence to guarantee proper results:
// disable interrupts if an interrupt could lead to
// another call to Timer_start().
key = Hwi_disable();
Timer_setPeriodMicroSecs(period);
Timer_start();
Hwi_restore(key);
Timer_start() // instance |
![](../../../../Arrow_up.png) |
Reloads and starts the timer
ARGUMENTS
handle
handle of a previously-created Timer instance object
DETAILS
Thread safety must be observed when using the
start
and
stop APIs to avoid possible miss-
configuration of the timers and unintended behaviors.
To protect against re-entrancy, surround the start/stop invocations
with
Hwi_disable() and
Hwi_restore() calls:
// disable interrupts if an interrupt could lead to
// another call to Timer_start().
key = Hwi_disable();
Timer_stop();
...
Timer_start();
Hwi_restore(key);
SIDE EFFECTS
Enables the timer's interrupt.
Timer_stop() // instance |
![](../../../../Arrow_up.png) |
Stop the timer
ARGUMENTS
handle
handle of a previously-created Timer instance object
DETAILS
Thread safety must be observed when using the
start
and
stop APIs to avoid possible miss-
configuration of the timers and unintended behaviors.
To protect against re-entrancy, surround the start/stop invocations
with
Hwi_disable() and
Hwi_restore() calls:
// disable interrupts if an interrupt could lead to
// another call to Timer_start().
key = Hwi_disable();
Timer_stop();
...
Timer_start();
Hwi_restore(key);
SIDE EFFECTS
Disables the timer's interrupt.
Instance Convertors |
![](../../../../Arrow_up.png) |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins |
![](../../../../Arrow_up.png) |
Int Timer_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
const Timer.ANY |
![](../../../../Arrow_up.png) |
Const used to specify any timer
XDCscript usage |
meta-domain |
C SYNOPSIS
const Timer.MAX_PERIOD |
![](../../../../Arrow_up.png) |
Max value of Timer period for PeriodType_COUNTS
XDCscript usage |
meta-domain |
const Timer.MAX_PERIOD = 0xffffffff;
C SYNOPSIS
const Timer.NUM_TIMER_DEVICES |
![](../../../../Arrow_up.png) |
Emulation supports 2 timers
XDCscript usage |
meta-domain |
const Timer.NUM_TIMER_DEVICES = 2;
C SYNOPSIS
enum Timer.PeriodType |
![](../../../../Arrow_up.png) |
PeriodType
XDCscript usage |
meta-domain |
values of type Timer.PeriodType
const Timer.PeriodType_MICROSECS;
// period in microsecs
const Timer.PeriodType_COUNTS;
// period in counts
VALUES
PeriodType_MICROSECS
Period value is in microseconds.
PeriodType_COUNTS
Period value is in counts.
C SYNOPSIS
enum Timer.RunMode |
![](../../../../Arrow_up.png) |
Timer Run Modes
XDCscript usage |
meta-domain |
values of type Timer.RunMode
const Timer.RunMode_CONTINUOUS;
// periodic and continuous
const Timer.RunMode_ONESHOT;
// one-shot
VALUES
RunMode_CONTINUOUS
Timer is periodic and runs continuously.
RunMode_ONESHOT
Timer runs for a single period value and stops
C SYNOPSIS
enum Timer.StartMode |
![](../../../../Arrow_up.png) |
Timer Start Modes
XDCscript usage |
meta-domain |
values of type Timer.StartMode
const Timer.StartMode_AUTO;
// timer starts automatically
const Timer.StartMode_USER;
// timer will be started by user
VALUES
StartMode_AUTO
Statically created/constructed Timers will be started in BIOS_start().
Dynamically created Timers will start at create() time. This includes
timers created before BIOS_start().
StartMode_USER
Timer will be started by the user using start().
C SYNOPSIS
enum Timer.Status |
![](../../../../Arrow_up.png) |
Timer Status
XDCscript usage |
meta-domain |
values of type Timer.Status
const Timer.Status_INUSE;
// timer in use
const Timer.Status_FREE;
// timer is free
VALUES
Status_INUSE
Timer is in use. A timer is marked in use from the time it gets
created to the time it gets deleted.
Status_FREE
Timer is free and can be acquired using create.
C SYNOPSIS
config Timer.E_calloc // module-wide |
![](../../../../Arrow_up.png) |
Error: memory allocation request failed
XDCscript usage |
meta-domain |
DETAILS
A request into the Windows runtime library for memory has failed.
RAISED_IN
C SYNOPSIS
config Timer.E_cannotSupport // module-wide |
![](../../../../Arrow_up.png) |
Error: unsupported timer period
XDCscript usage |
meta-domain |
msg: "Timer cannot support requested period %d"
};
DETAILS
On Windows, the timer period cannot be less than one millisecond.
However, the actual minimum timer period (even when set to one
millisecond) is 10 - 15 milliseconds. This latency results from the
Windows clock ticking at 10 milliseconds with additional delays in
the Windows kernel.
RAISED_IN
C SYNOPSIS
config Timer.E_event // module-wide |
![](../../../../Arrow_up.png) |
Error: CreateEvent failed
XDCscript usage |
meta-domain |
msg: "CreateEvent failed"
};
DETAILS
A CreateEvent call into the Win32 API has failed.
RAISED_IN
C SYNOPSIS
config Timer.E_invalidTimer // module-wide |
![](../../../../Arrow_up.png) |
Error: Invalid timer specified
XDCscript usage |
meta-domain |
msg: "E_invalidTimer: Invalid Timer Id %d"
};
DETAILS
An invalid timer id was specified. Timer id must be in the range
0 to (
NUM_TIMER_DEVICES - 1). In the
create() call,
an id of -1 may be used to request any available timer.
RAISED_IN
C SYNOPSIS
config Timer.E_noneAvailable // module-wide |
![](../../../../Arrow_up.png) |
Error: no timers available
XDCscript usage |
meta-domain |
msg: "no available timer"
};
DETAILS
A request was made for any available timer, but there are none
available at this time.
RAISED_IN
C SYNOPSIS
config Timer.E_notAvailable // module-wide |
![](../../../../Arrow_up.png) |
Error: requested timer not available
XDCscript usage |
meta-domain |
msg: "E_notAvailable: Timer not available %d"
};
DETAILS
A request was made for a timer, but it is not available at this time.
It is currently in use.
RAISED_IN
C SYNOPSIS
config Timer.E_notSupported // module-wide |
![](../../../../Arrow_up.png) |
Error: API not supported on Windows
XDCscript usage |
meta-domain |
msg: "API not supported on Windows"
};
DETAILS
This timer API is not supported on Windows.
RAISED_IN
C SYNOPSIS
config Timer.E_thread // module-wide |
![](../../../../Arrow_up.png) |
Error: CreateThread failed
XDCscript usage |
meta-domain |
msg: "CreateThread failed"
};
DETAILS
A CreateThread call into the Win32 API has failed.
RAISED_IN
C SYNOPSIS
config Timer.E_wait // module-wide |
![](../../../../Arrow_up.png) |
Error: WaitForSingleObject failed
XDCscript usage |
meta-domain |
msg: "WaitForSingleObject failed"
};
DETAILS
A WaitForSingleObject call into the Win32 API has failed.
RAISED_IN
C SYNOPSIS
config Timer.anyMask // module-wide |
![](../../../../Arrow_up.png) |
Available mask to be used when select = TIMER_ANY
XDCscript usage |
meta-domain |
Timer.anyMask = UInt 0x3;
C SYNOPSIS
metaonly config Timer.common$ // module-wide |
![](../../../../Arrow_up.png) |
Common module configuration parameters
XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
Instance Config Parameters |
![](../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new Timer.Params;
// Instance config-params object
params.arg = UArg null;
// Argument for tick function. Default is null
// Timer frequency
lo: 0,
hi: 0
};
params.period = UInt32 0;
// Period of tick. Can be specified in timer counts or microseconds.
Default is 0
// Period Type. Default is PeriodType_MICROSECS
config Timer.arg // instance |
![](../../../../Arrow_up.png) |
Argument for tick function. Default is null
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
params.arg = UArg null;
C SYNOPSIS
config Timer.extFreq // instance |
![](../../../../Arrow_up.png) |
Timer frequency
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
lo: 0,
hi: 0
};
DETAILS
This parameter is meaningfull only on platforms where the timer clock
can be changed. If value is left at zero, then default hookup of timer
clock is assumed.
C SYNOPSIS
config Timer.period // instance |
![](../../../../Arrow_up.png) |
Period of tick. Can be specified in timer counts or microseconds.
Default is 0
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
params.period = UInt32 0;
DETAILS
The implementation of ITimer will support a period of UInt32
timer counts and use pre-scalars if necessary.
C SYNOPSIS
config Timer.periodType // instance |
![](../../../../Arrow_up.png) |
Period Type. Default is PeriodType_MICROSECS
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
C SYNOPSIS
config Timer.runMode // instance |
![](../../../../Arrow_up.png) |
Timer run mode. Default is RunMode_CONTINUOUS
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
C SYNOPSIS
config Timer.startMode // instance |
![](../../../../Arrow_up.png) |
Start mode. Default is StartMode_AUTO
XDCscript usage |
meta-domain |
var params = new Timer.Params;
...
C SYNOPSIS
Instance Creation |
![](../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params =
new Timer.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = Timer.create(Int id, Void(*)(UArg) tickFxn, params);
// Create an instance-object
ARGUMENTS
id
Timer id ranging from 0 to a platform specific value
tickFxn
function that runs upon timer expiry.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
Create could fail if timer peripheral is unavailable. To
request any available timer use
ANY as the id.
TimerId's are logical ids. The family-specific implementations
map the ids to physical peripherals.