module ti.sysbios.family.c64p.EventCombiner |
![](../../../../Arrow_left.png) |
![](../../../../Arrow_up.png) |
![](../../../../Arrow_right.png) |
Event Combiner Manager module
The event combiner allows the user to combine up to 32 system events
into a single combined event. The events 0, 1, 2, and 3 are the events
associated with the event combiner. Using the EventCombiner module
along with the Hwi module, allows the user to route a combined event
to any of the 12 maskable CPU interrupts available on GEM. The
EventCombiner supports up to 128 system events. Users can specify
a function and an argument for each system event and can choose to
enable whichever system events they want.
[
more ... ]
#include <ti/sysbios/family/c64p/EventCombiner.h>
Functions |
Void | |
Void | |
Void | |
Void | |
Functions common to all target modules |
|
|
Defines |
#define | |
Typedefs |
typedef Void | |
Constants |
extern const Bits32 | |
| |
DETAILS
The event combiner allows the user to combine up to 32 system events
into a single combined event. The events 0, 1, 2, and 3 are the events
associated with the event combiner. Using the EventCombiner module
along with the Hwi module, allows the user to route a combined event
to any of the 12 maskable CPU interrupts available on GEM. The
EventCombiner supports up to 128 system events. Users can specify
a function and an argument for each system event and can choose to
enable whichever system events they want.
Calling Context
Function | Hwi | Swi | Task | Main | Startup |
disableEvent | Y | Y | Y | Y | Y |
dispatch | Y | N | N | N | N |
dispatchPlug | Y | Y | Y | Y | Y |
enableEvent | Y | Y | Y | Y | Y |
Definitions:
- Hwi: API is callable from a Hwi thread.
- Swi: API is callable from a Swi thread.
- Task: API is callable from a Task thread.
- Main: API is callable during any of these phases:
- In your module startup after this module is started (e.g. EventCombiner_Module_startupDone() returns TRUE).
- During xdc.runtime.Startup.lastFxns.
- During main().
- During BIOS.startupFxns.
- Startup: API is callable during any of these phases:
- During xdc.runtime.Startup.firstFxns.
- In your module startup before this module is started (e.g. EventCombiner_Module_startupDone() returns FALSE).
|
const EventCombiner_NUM_EVENTS |
![](../../../../Arrow_up.png) |
C64+ supports 128 events
#define EventCombiner_NUM_EVENTS (Int)128
typedef EventCombiner_FuncPtr |
![](../../../../Arrow_up.png) |
Event Combiner dispatcher function type definition
typedef Void (*EventCombiner_FuncPtr)(UArg);
config EventCombiner_EVTMASK // module-wide |
![](../../../../Arrow_up.png) |
Holds the initialization values for the C64+ EVTMASK registers (0-3)
extern const Bits32 EventCombiner_EVTMASK[4];
DETAILS
It is assigned values based on the 'unmask' member of the 'events'
configuration array. It can also be assigned manually in the program
configuration script.
config EventCombiner_E_unpluggedEvent // module-wide |
![](../../../../Arrow_up.png) |
Error raised when an unplug Event is executed
extern const Error_Id EventCombiner_E_unpluggedEvent;
EventCombiner_disableEvent() // module-wide |
![](../../../../Arrow_up.png) |
Disables 'evt' from contributing to its combined event group
Void EventCombiner_disableEvent(UInt evt);
DETAILS
It accomplishes this by setting the corresponding
bit in the C64+ EVTMASK array to 1 (to mask it).
EventCombiner_dispatch() // module-wide |
![](../../../../Arrow_up.png) |
The Event Combiner dispatcher
Void EventCombiner_dispatch(UInt evt);
DETAILS
It is mostly used internally, but can be used directly by the user.
EventCombiner_dispatchPlug() // module-wide |
![](../../../../Arrow_up.png) |
Used to configure a dispatcher entry for 'evt'
DETAILS
The parameters correspond to the same ones for static configuration
in EventObj. dispatchPlug does not map the corresponding combined
event group to an Hwi interrupt - such an action needs to be
performed either using the event combiner configuration or using the Hwi
module.
EventCombiner_enableEvent() // module-wide |
![](../../../../Arrow_up.png) |
Enables 'evt' to contribute to its combined event group
Void EventCombiner_enableEvent(UInt evt);
DETAILS
It accomplishes this by setting the corresponding
bit in the C64+ EVTMASK array to 0 (to unmask it).
Module-Wide Built-Ins |
![](../../../../Arrow_up.png) |
// Get this module's unique id
Bool EventCombiner_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool EventCombiner_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 EventCombiner_Module_getMask();
// Returns the diagnostics mask for this module
Void EventCombiner_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var EventCombiner = xdc.useModule('ti.sysbios.family.c64p.EventCombiner');
module-wide constants & types
obj.
fxn =
Void(*)(UArg) ...
module-wide config parameters
msg: "E_unpluggedEvent: Event# %d is unplugged"
};
module-wide functions
generated on Fri, 21 Jan 2011 00:18:54 GMT