Additional C28 device-specific APIs are also provided.
ISRs specified with Hwi_plug will not go through the dispatcher; the
ISR function will be directly plugged into the vector table. Hwi_plug can
be used for any ISR which does not call any SYS/BIOS APIs.
ISRs can be plugged or created statically in the configuration script or
dynamically at runtime.
const Hwi_NUM_INTERRUPTS |
|
C28 supports 32 interrupts
#define Hwi_NUM_INTERRUPTS (Int)32
const Hwi_NUM_INTERRUPTS_ALL |
|
const Hwi_NUM_INTERRUPTS_PIE |
|
C28 supports 96 PIE interrupts
#define Hwi_NUM_INTERRUPTS_PIE (Int)96
enum Hwi_MaskingOption |
|
Shorthand interrupt masking options
typedef enum Hwi_MaskingOption {
Hwi_MaskingOption_NONE,
// No interrupts are disabled
Hwi_MaskingOption_ALL,
// All interrupts are disabled
Hwi_MaskingOption_SELF,
// Only this interrupt is disabled
Hwi_MaskingOption_BITMASK,
// User supplies IER masks
Hwi_MaskingOption_LOWER
// All current and lower priority
interrupts are disabled. Only a few
targets/devices truly support this
masking option. For those that don't,
this setting is treated the same as
MaskingOption_SELF
} Hwi_MaskingOption;
typedef Hwi_FuncPtr |
|
Hwi create function type definition
typedef Void (*Hwi_FuncPtr)(UArg);
typedef Hwi_Irp |
|
Interrupt Return Pointer.
This is the address of the interrupted instruction
typedef Hwi_PlugFuncPtr |
|
Hwi plug function type definition, which doesn't take an arg
typedef Void (*Hwi_PlugFuncPtr)(Void);
struct Hwi_HookSet |
|
Hwi hook set type definition
typedef struct Hwi_HookSet {
Void (*registerFxn)(Int);
} Hwi_HookSet;
DETAILS
The functions that make up a hookSet have certain restrictions. They
cannot call any Hwi instance functions other than Hwi_getHookContext()
and Hwi_setHookContext(). For all practical purposes, they should treat
the Hwi_Handle passed to these functions as an opaque handle.
config Hwi_A_badIntNum // module-wide |
|
Assert raised when an invalid interrupt number is passed to a Hwi call
config Hwi_A_invalidArg // module-wide |
|
Assert raised when an invalid argument has been passed to a function
config Hwi_A_zeroLatencyConflict // module-wide |
|
Assert raised when there is a conflict with the zero latency IER mask
extern const Assert_Id Hwi_A_zeroLatencyConflict;
DETAILS
This assert is raised when trying to create a Hwi with an intNum that
conflicts with the supplied zero latency IER mask.
config Hwi_E_alreadyDefined // module-wide |
|
Error raised when Hwi is already defined
extern const Error_Id Hwi_E_alreadyDefined;
config Hwi_E_unpluggedInterrupt // module-wide |
|
Error raised when an unplugged interrupt is flagged
extern const Error_Id Hwi_E_unpluggedInterrupt;
config Hwi_LD_end // module-wide |
|
Issued just after return from Hwi function (with interrupts disabled)
config Hwi_LM_begin // module-wide |
|
Issued just prior to Hwi function invocation (with interrupts disabled)
config Hwi_dispatcherAutoNestingSupport // module-wide |
|
Include interrupt nesting logic in interrupt dispatcher?
extern const Bool Hwi_dispatcherAutoNestingSupport;
DETAILS
Default is true.
This option provides the user with the ability to optimize
interrupt dispatcher performance when support for interrupt
nesting is not required.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that manipulates interrupt mask
registers and enables and disables interrupts before and
after invoking the user's Hwi function.
Set this parameter to false if you don't need interrupts
enabled during the execution of your Hwi functions.
config Hwi_dispatcherIrpTrackingSupport // module-wide |
|
Controls whether the
dispatcher retains the interrupted thread's return address
extern const Bool Hwi_dispatcherIrpTrackingSupport;
DETAILS
This option is enabled by default.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that keeps track of the interrupt's
return address and provide a small savings in interrupt latency.
The application can get an interrupt's most recent return
address using the
getIrp API.
config Hwi_dispatcherSwiSupport // module-wide |
|
Include Swi scheduling logic in interrupt dispatcher?
extern const Bool Hwi_dispatcherSwiSupport;
DETAILS
Default is inherited from
BIOS.swiEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that Swis
will not be posted from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Swi scheduler
prior to returning from an interrupt.
config Hwi_dispatcherTaskSupport // module-wide |
|
Include Task scheduling logic in interrupt dispatcher?
extern const Bool Hwi_dispatcherTaskSupport;
DETAILS
Default is inherited from
BIOS.taskEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that no
Task scheduling APIs (ie
Semaphore_post()) will be executed from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Task scheduler
prior to returning from an interrupt.
config Hwi_zeroLatencyIERMask // module-wide |
|
Zero Latency IER Mask
extern const Bits16 Hwi_zeroLatencyIERMask;
DETAILS
CPU interrupts specified in this mask (which corresponds to the 16-bit
IER register) will never be disabled. This means that the
disable,
enable, and
restore calls leave the
zero latency CPU interrupts enabled after being called. Zero latency
operation may be used to ensure minimal interrupt-to-ISR time for
non-BIOS interrupt handlers in applications that demand low latency.
It is important to note that zero latency and non-zero latency PIE
interrupts may not share a common PIE group. The entire PIE group whose
bit is set in the zeroLatencyIERMask will be treated as zero latency.
Enabling zero latency mode (specifying a non-zero zeroLatencyIERMask)
generates alternate (and slower) code used to disable, enable and
restore interrupts. This alternate code will maintain a shadow copy
of interrupt state (IER register and global interrupt state).
disableIER,
enableIER and
restoreIER will update
both the IER register and its shadow. The
disable call
will copy the zero latency IER mask (supplied here) into the IER
register. The
enable call will copy the contents of the
shadow IER register into the actual register. The
restore
call may either disable or enable the non-zero-latency interrupts.
It is important to be aware of the performance penalty associated with
using zero latency interrupts before using this feature.
Example:
var Hwi = xdc.useModule('ti.sysbios.family.c28.Hwi');
Hwi.zeroLatencyIERMask = 0x0010;
// PIE group 5 classified as zero latency
Hwi_clearInterrupt() // module-wide |
|
Clear a specific interrupt
Void Hwi_clearInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to clear
DETAILS
Clears a specific interrupt's pending status.
The implementation is family-specific.
HWI
The behavior of clearInterrupt depends on whether the intNum
is a PIE interrupt number. If so, the corresponding PIEIFR bit is
cleared. If not (1 <= intNum <= 14), the corresponding IFR bit is
cleared.
Hwi_disable() // module-wide |
|
Globally disable interrupts
RETURNS
opaque key for use by Hwi_restore()
DETAILS
Hwi_disable globally disables hardware interrupts and returns an
opaque key indicating whether interrupts were globally enabled or
disabled on entry to Hwi_disable().
The actual value of the key is target/device specific and is meant
to be passed to Hwi_restore().
Call Hwi_disable before a portion of a function that needs
to run without interruption. When critical processing is complete, call
Hwi_restore or Hwi_enable to reenable hardware interrupts.
Servicing of interrupts that occur while interrupts are disabled is
postponed until interrupts are reenabled. However, if the same type
of interrupt occurs several times while interrupts are disabled,
the interrupt's function is executed only once when interrupts are
reenabled.
A context switch can occur when calling Hwi_enable or Hwi_restore if
an enabled interrupt occurred while interrupts are disabled.
Hwi_disable may be called from main(). However, since Hwi interrupts
are already disabled in main(), such a call has no effect.
CONSTRAINTS
If a Task switching API such as
Semaphore_pend(),
Semaphore_post(),
Task_sleep(), or
Task_yield()
is invoked which results in a context switch while
interrupts are disabled, an embedded call to
Hwi_enable occurs
on the way to the new thread context which unconditionally re-enables
interrupts. Interrupts will remain enabled until a subsequent
Hwi_disable
invocation.
Swis always run with interrupts enabled.
See
Swi_post() for a discussion Swis and
interrupts.
Hwi_disableIER() // module-wide |
|
Disable certain maskable interrupts
Bits16 Hwi_disableIER(Bits16 mask);
ARGUMENTS
mask
bitmask of interrupts to disable
RETURNS
previous IER settings bitmask
DETAILS
Atomically disables specific interrupts by clearing the bits
specified by mask in the Interrupt Enable Register (IER).
The IER bits to be cleared should be set to 1 in the mask.
Hwi_disableInterrupt() // module-wide |
|
Disable a specific interrupt
UInt Hwi_disableInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to disable
RETURNS
key to restore previous enable/disable state
DETAILS
Disable a specific interrupt identified by an interrupt number.
HWI
The behavior of Hwi_disableInterrupt depends on whether the intNum
is a PIE interrupt number. If so, the appropriate bit in its group's
PIEIER register is cleared. Note that, unlike
enableInterrupt, disableInterrupt does not touch IER bits
when operating upon a PIE interrupt number. If intNum is a non-PIE
interrupt (1 <= intNum <= 14), then the corresponding bit in the IER
register is cleared.
The return value is a key whose value reflects the previous state of
the PIEIER bit.
Hwi_disablePIEIER() // module-wide |
|
Disable interrupts in a PIE group
Bits16 Hwi_disablePIEIER(UInt groupNum, Bits16 pieMask);
ARGUMENTS
groupNum
PIE group number
pieMask
PIEIER disable mask for group
RETURNS
Previous PIEIER settings bitmask
DETAILS
Atomically disable PIE interrupts in a single PIE group
according to supplied PIEIER bitmask
Hwi_enable() // module-wide |
|
Globally enable interrupts
RETURNS
opaque key for use by Hwi_restore()
DETAILS
Hwi_enable globally enables hardware interrupts and returns an
opaque key indicating whether interrupts were globally enabled or
disabled on entry to Hwi_enable().
The actual value of the key is target/device specific and is meant
to be passed to Hwi_restore().
This function is
called as part of SYS/BIOS Startup_POST_APP_MAIN phase.
Hardware interrupts are enabled unless a call to Hwi_disable disables
them.
Servicing of interrupts that occur while interrupts are disabled is
postponed until interrupts are reenabled. However, if the same type
of interrupt occurs several times while interrupts are disabled,
the interrupt's function is executed only once when interrupts are
reenabled.
A context switch can occur when calling Hwi_enable or Hwi_restore if
an enabled interrupt occurred while interrupts are disabled.
Any call to Hwi_enable enables interrupts, even if Hwi_disable has
been called several times.
Hwi_enable must not be called from main().
Hwi_enableIER() // module-wide |
|
Enable certain maskable interrupts
Bits16 Hwi_enableIER(Bits16 mask);
ARGUMENTS
mask
Bitmask of interrupts to enable
RETURNS
Previous IER settings bitmask
DETAILS
Atomically enables specific interrupts by setting the bits
specified by mask in the Interrupt Enable Register (IER).
The IER bits to be set should be set to 1 in the mask.
Hwi_enableInterrupt() // module-wide |
|
Enable a specific interrupt
UInt Hwi_enableInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to enable
RETURNS
key to restore previous enable/disable state
DETAILS
Enables a specific interrupt identified by an interrupt number.
HWI
The behavior of enableInterrupt depends on whether the intNum
is a PIE interrupt number. If so, two operations are
performed. The IER bit for intNum's PIE group is set and the
appropriate bit in its group's PIEIER register is also set. However,
if intNum is a non-PIE interrupt (1 <= intNum <= 14), then the
corresponding bit in the IER register is set.
The return value is a key whose value reflects the previous state of
the PIEIER bit. Note that the key does not reflect
the IER register's previous state even if its state is modified by this
call.
Hwi_enablePIEIER() // module-wide |
|
Enable interrupts in a PIE group
Bits16 Hwi_enablePIEIER(UInt groupNum, Bits16 pieMask);
ARGUMENTS
groupNum
PIE group number
pieMask
PIEIER enable mask for group
RETURNS
Previous PIEIER settings bitmask
DETAILS
Atomically enable PIE interrupts in a single PIE group
according to supplied PIEIER bitmask
Hwi_getHandle() // module-wide |
|
Returns Hwi handle associated with intNum
ARGUMENTS
intNum
Interrupt number
RETURNS
Hwi handle associated with intNum
Hwi_plug() // module-wide |
|
Plug an interrupt vector with an ISR address
ARGUMENTS
intNum
interrupt number
fxn
pointer to ISR function
DETAILS
plug hooks up the specified function as the branch target for a
hardware interrupt (fielded by the CPU) at the vector address
corresponding to intNum. plug does not enable the interrupt. Use
Hwi_enableIER to enable specific interrupts.
This API can plug the full set of vectors supported by the PIE (0-127).
Hwi_restore() // module-wide |
|
Globally restore interrupts
Void Hwi_restore(UInt key);
ARGUMENTS
key
enable/disable state to restore
DETAILS
Hwi_restore globally restores interrupts to the state determined
by the key argument provided by a previous invocation of Hwi_disable.
A context switch may occur when calling Hwi_restore if Hwi_restore
reenables interrupts and another Hwi occurred while interrupts were
disabled.
Hwi_restore may be called from main(). However, since Hwi_enable
cannot be called from main(), interrupts are always disabled in
main(), and a call to Hwi_restore has no effect.
Hwi_restoreIER() // module-wide |
|
Restore maskable interrupts
Bits16 Hwi_restoreIER(Bits16 mask);
ARGUMENTS
mask
Bitmask of interrupts to restore
RETURNS
Previous IER settings bitmask
DETAILS
Restores maskable interrupts to the state they were in
when either disableIER() or enableIER() was called.
Atomically writes the given mask to the IER register. Typically used
to restore the IER register to the state returned from a call to
either
disableIER() or
enableIER().
Hwi_restoreInterrupt() // module-wide |
|
Restore a specific interrupt's enabled/disabled state
Void Hwi_restoreInterrupt(UInt intNum, UInt key);
ARGUMENTS
intNum
interrupt number to restore
key
key returned from enableInt or disableInt
DETAILS
Restores a specific interrupt identified by an interrupt number.
restoreInterrupt is generally used to restore an interrupt to its state
before
disableInterrupt or
enableInterrupt was
invoked
HWI
The behavior of restoreInterrupt depends on whether the intNum
is a PIE interrupt number. If so, the supplied key returned by an
earlier call to
disableInterrupt and
enableInterrupt
is used to restore the corresponding PIEIER bit to its state before
the earlier call.
However, if intNum is a non-PIE interrupt (1 <= intNum <= 14), then the
corresponding bit in the IER register is restored using the key.
Hwi_restorePIEIER() // module-wide |
|
Restores interrupts in a PIE group
Bits16 Hwi_restorePIEIER(UInt groupNum, Bits16 pieMask);
ARGUMENTS
groupNum
PIE group number
pieMask
PIEIER restore mask for group
RETURNS
Previous PIEIER settings bitmask
DETAILS
Atomically restore PIE interrupts in a single PIE group
according to supplied PIEIER bitmask
Hwi_startup() // module-wide |
|
Initially enable interrupts
DETAILS
Called within BIOS_start
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool Hwi_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Hwi_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Hwi_Module_getMask();
// Returns the diagnostics mask for this module
Void Hwi_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
|
typedef struct Hwi_Object Hwi_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct Hwi_Struct Hwi_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
|
typedef struct Hwi_Params {
// Instance config-params structure
// Common per-instance configs
UArg arg;
// ISR function argument. Default is 0
Bits16 disableMask;
// Dispatcher auto-nesting interrupt disable mask
Bool enableAck;
// Enable automatic acknowledgement of PIE interrupts by the Hwi interrupt
dispatcher
Bool enableInt;
// Enable this interrupt now? Default is true
Int eventId;
// Interrupt event ID (Interrupt Selection Number)
Default is -1.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored
Int priority;
// Interrupt priority. Not supported on this target
Bits16 restoreMask;
// Dispatcher auto-nesting interrupt restore mask
} Hwi_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config Hwi_arg // instance |
|
ISR function argument. Default is 0
config Hwi_disableMask // instance |
|
Dispatcher auto-nesting interrupt disable mask
DETAILS
When the dispatcher's auto interrupt nesting support feature
is enabled (see
dispatcherAutoNestingSupport),
this mask defines which IER bits are disabled prior to invoking
the user's ISR function with GIE = 1.
disableMask bits set to 1 correspond to IER bits that will be cleared
prior to invoking the ISR.
The value of this mask is normally auto-calculated based on the
value of the maskSetting. However, manual setting of this
mask is enabled by setting the maskSetting to
MaskingOption_BITMASK.
The default value is derived from the
MaskingOption_SELF
maskSetting.
config Hwi_enableAck // instance |
|
Enable automatic acknowledgement of PIE interrupts by the Hwi interrupt
dispatcher
config Hwi_enableInt // instance |
|
Enable this interrupt now? Default is true
config Hwi_eventId // instance |
|
Interrupt event ID (Interrupt Selection Number)
Default is -1.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored
config Hwi_maskSetting // instance |
|
maskSetting. Default is Hwi_MaskingOption_SELF
config Hwi_priority // instance |
|
Interrupt priority. Not supported on this target
config Hwi_restoreMask // instance |
|
Dispatcher auto-nesting interrupt restore mask
DETAILS
When the dispatcher's auto interrupt nesting support feature
is enabled (see
dispatcherAutoNestingSupport),
this mask defines which IER bits are restored to their previous
setting upon return from the user's ISR function.
restoreMask bits set to 1 correspond to IER bits that will be restored.
The value of this mask is normally auto-calculated based on the
value of the maskSetting. However, manual setting of this
mask is enabled by setting the maskSetting to
MaskingOption_BITMASK.
The default value is derived from the
MaskingOption_SELF
maskSetting.
Instance Creation |
|
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
intNum
interrupt number
hwiFxn
pointer to ISR function
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Hwi dispatcher table entry is created and filled with the
function specified by the fxn parameter and the attributes
specified by the params parameter.
If params is NULL, the Hwi's dispatcher properties are assigned a
default set of values. Otherwise, the following properties
are specified by a structure of type Hwi_Params.
- The arg element is a generic argument that is passed to the plugged
function as its only parameter. The default value is 0.
- The enableInt element determines whether the interrupt should be
enabled in the IER by create.
- The maskSetting element defines the dispatcherAutoNestingSupport
behavior of the interrupt.
Hwi_create returns a pointer to the created Hwi object.
Instance Deletion |
|
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
Hwi_getFunc() // instance |
|
Get Hwi function and arg
ARGUMENTS
handle
handle of a previously-created Hwi instance object
arg
pointer for returning hwi's ISR function argument
RETURNS
hwi's ISR function
Hwi_getHookContext() // instance |
|
Get hook instance's context for a Hwi
Ptr Hwi_getHookContext(
Hwi_Handle handle,
Int id);
ARGUMENTS
handle
handle of a previously-created Hwi instance object
RETURNS
hook instance's context for hwi
Hwi_getIrp() // instance |
|
Get address of interrupted instruction
ARGUMENTS
handle
handle of a previously-created Hwi instance object
RETURNS
most current IRP of a Hwi
Hwi_reconfig() // instance |
|
Reconfigure a dispatched interrupt
ARGUMENTS
handle
handle of a previously-created Hwi instance object
Hwi_setFunc() // instance |
|
Overwrite Hwi function and arg
ARGUMENTS
handle
handle of a previously-created Hwi instance object
fxn
pointer to ISR function
arg
argument to ISR function
DETAILS
Replaces a Hwi object's hwiFxn function originally
provided in
create.
Hwi_setHookContext() // instance |
|
Set hook instance's context for a Hwi
Void Hwi_setHookContext(
Hwi_Handle handle,
Int id,
Ptr hookContext);
ARGUMENTS
handle
handle of a previously-created Hwi instance object
id
hook instance's ID
hookContext
value to write to context
Instance Convertors |
|
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins |
|
Int Hwi_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
const Hwi.NUM_INTERRUPTS |
|
C28 supports 32 interrupts
XDCscript usage |
meta-domain |
const Hwi.NUM_INTERRUPTS = 32;
C SYNOPSIS
const Hwi.NUM_INTERRUPTS_ALL |
|
XDCscript usage |
meta-domain |
C SYNOPSIS
const Hwi.NUM_INTERRUPTS_PIE |
|
C28 supports 96 PIE interrupts
XDCscript usage |
meta-domain |
const Hwi.NUM_INTERRUPTS_PIE = 96;
C SYNOPSIS
enum Hwi.MaskingOption |
|
Shorthand interrupt masking options
XDCscript usage |
meta-domain |
values of type Hwi.MaskingOption
const Hwi.MaskingOption_NONE;
// No interrupts are disabled
const Hwi.MaskingOption_ALL;
// All interrupts are disabled
const Hwi.MaskingOption_SELF;
// Only this interrupt is disabled
const Hwi.MaskingOption_BITMASK;
// User supplies IER masks
const Hwi.MaskingOption_LOWER;
// All current and lower priority
interrupts are disabled. Only a few
targets/devices truly support this
masking option. For those that don't,
this setting is treated the same as
MaskingOption_SELF
C SYNOPSIS
struct Hwi.HookSet |
|
Hwi hook set type definition
XDCscript usage |
meta-domain |
var obj = new Hwi.HookSet;
obj.registerFxn = Void(*)(Int) ...
DETAILS
The functions that make up a hookSet have certain restrictions. They
cannot call any Hwi instance functions other than Hwi_getHookContext()
and Hwi_setHookContext(). For all practical purposes, they should treat
the Hwi_Handle passed to these functions as an opaque handle.
C SYNOPSIS
metaonly struct Hwi.NonDispatchedInterrupt |
|
Non-dispatched interrupt object
XDCscript usage |
meta-domain |
var obj = new Hwi.NonDispatchedInterrupt;
obj.intNum = Int ...
obj.fxn = Void(*)(Void) ...
obj.enableInt = Bool ...
FIELDS
intNum
Interrupt number
fxn
Non-dispatched interrupt service routine (ISR)
enableInt
Enable the interrupt after plugging the vector
DETAILS
Provided so that XGCONF users can easily plug non-dispatched interrupts
config Hwi.A_badIntNum // module-wide |
|
Assert raised when an invalid interrupt number is passed to a Hwi call
XDCscript usage |
meta-domain |
msg: "A_badIntNum: Invalid interrupt number"
};
C SYNOPSIS
config Hwi.A_invalidArg // module-wide |
|
Assert raised when an invalid argument has been passed to a function
XDCscript usage |
meta-domain |
msg: "A_invalidArg: Invalid argument"
};
C SYNOPSIS
config Hwi.A_zeroLatencyConflict // module-wide |
|
Assert raised when there is a conflict with the zero latency IER mask
XDCscript usage |
meta-domain |
msg: "A_zeroLatencyConflict: Conflict with zero latency IER mask"
};
DETAILS
This assert is raised when trying to create a Hwi with an intNum that
conflicts with the supplied zero latency IER mask.
C SYNOPSIS
config Hwi.E_alreadyDefined // module-wide |
|
Error raised when Hwi is already defined
XDCscript usage |
meta-domain |
msg: "E_alreadyDefined: Hwi already defined: intr# %d"
};
C SYNOPSIS
config Hwi.E_unpluggedInterrupt // module-wide |
|
Error raised when an unplugged interrupt is flagged
XDCscript usage |
meta-domain |
msg: "E_unpluggedInterrupt: Unplugged interrupt flagged: intr# %d"
};
C SYNOPSIS
config Hwi.LD_end // module-wide |
|
Issued just after return from Hwi function (with interrupts disabled)
XDCscript usage |
meta-domain |
msg: "LD_end: hwi: 0x%x"
};
C SYNOPSIS
config Hwi.LM_begin // module-wide |
|
Issued just prior to Hwi function invocation (with interrupts disabled)
XDCscript usage |
meta-domain |
msg: "LM_begin: hwi: 0x%x, func: 0x%x, preThread: %d, intNum: %d, irp: 0x%x"
};
C SYNOPSIS
config Hwi.dispatcherAutoNestingSupport // module-wide |
|
Include interrupt nesting logic in interrupt dispatcher?
XDCscript usage |
meta-domain |
Hwi.dispatcherAutoNestingSupport = Bool true;
DETAILS
Default is true.
This option provides the user with the ability to optimize
interrupt dispatcher performance when support for interrupt
nesting is not required.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that manipulates interrupt mask
registers and enables and disables interrupts before and
after invoking the user's Hwi function.
Set this parameter to false if you don't need interrupts
enabled during the execution of your Hwi functions.
C SYNOPSIS
config Hwi.dispatcherIrpTrackingSupport // module-wide |
|
Controls whether the
dispatcher retains the interrupted thread's return address
XDCscript usage |
meta-domain |
Hwi.dispatcherIrpTrackingSupport = Bool true;
DETAILS
This option is enabled by default.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that keeps track of the interrupt's
return address and provide a small savings in interrupt latency.
The application can get an interrupt's most recent return
address using the
getIrp API.
C SYNOPSIS
config Hwi.dispatcherSwiSupport // module-wide |
|
Include Swi scheduling logic in interrupt dispatcher?
XDCscript usage |
meta-domain |
Hwi.dispatcherSwiSupport = Bool undefined;
DETAILS
Default is inherited from
BIOS.swiEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that Swis
will not be posted from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Swi scheduler
prior to returning from an interrupt.
C SYNOPSIS
config Hwi.dispatcherTaskSupport // module-wide |
|
Include Task scheduling logic in interrupt dispatcher?
XDCscript usage |
meta-domain |
Hwi.dispatcherTaskSupport = Bool undefined;
DETAILS
Default is inherited from
BIOS.taskEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that no
Task scheduling APIs (ie
Semaphore_post()) will be executed from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Task scheduler
prior to returning from an interrupt.
C SYNOPSIS
config Hwi.zeroLatencyIERMask // module-wide |
|
Zero Latency IER Mask
XDCscript usage |
meta-domain |
Hwi.zeroLatencyIERMask = Bits16 0x0;
DETAILS
CPU interrupts specified in this mask (which corresponds to the 16-bit
IER register) will never be disabled. This means that the
disable,
enable, and
restore calls leave the
zero latency CPU interrupts enabled after being called. Zero latency
operation may be used to ensure minimal interrupt-to-ISR time for
non-BIOS interrupt handlers in applications that demand low latency.
It is important to note that zero latency and non-zero latency PIE
interrupts may not share a common PIE group. The entire PIE group whose
bit is set in the zeroLatencyIERMask will be treated as zero latency.
Enabling zero latency mode (specifying a non-zero zeroLatencyIERMask)
generates alternate (and slower) code used to disable, enable and
restore interrupts. This alternate code will maintain a shadow copy
of interrupt state (IER register and global interrupt state).
disableIER,
enableIER and
restoreIER will update
both the IER register and its shadow. The
disable call
will copy the zero latency IER mask (supplied here) into the IER
register. The
enable call will copy the contents of the
shadow IER register into the actual register. The
restore
call may either disable or enable the non-zero-latency interrupts.
It is important to be aware of the performance penalty associated with
using zero latency interrupts before using this feature.
Example:
var Hwi = xdc.useModule('ti.sysbios.family.c28.Hwi');
Hwi.zeroLatencyIERMask = 0x0010;
// PIE group 5 classified as zero latency
C SYNOPSIS
metaonly config Hwi.common$ // module-wide |
|
Common module configuration parameters
XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly config Hwi.nonDispatchedInterrupts // module-wide |
|
Non-dispatched interrupt array
XDCscript usage |
meta-domain |
DETAILS
Provided so that XGCONF users can easily plug non-dispatched interrupts
metaonly config Hwi.rovViewInfo // module-wide |
|
XDCscript usage |
meta-domain |
metaonly Hwi.addHookSet() // module-wide |
|
addHookSet is used in a config file to add a hook set (defined
by struct HookSet)
XDCscript usage |
meta-domain |
ARGUMENTS
hook
structure of type HookSet
DETAILS
HookSet structure elements may be omitted, in which case those
elements will not exist.
metaonly Hwi.plugMeta() // module-wide |
|
Statically plug an interrupt vector with an ISR address
XDCscript usage |
meta-domain |
Hwi.plugMeta(UInt intNum, Void(*)(Void) fxn) returns Void
ARGUMENTS
intNum
Interrupt number
fxn
Pointer to ISR function
Instance Config Parameters |
|
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
// Instance config-params object
params.arg = UArg 0;
// ISR function argument. Default is 0
params.disableMask = Bits16 0;
// Dispatcher auto-nesting interrupt disable mask
params.enableAck = Bool true;
// Enable automatic acknowledgement of PIE interrupts by the Hwi interrupt
dispatcher
params.enableInt = Bool true;
// Enable this interrupt now? Default is true
params.eventId = Int -1;
// Interrupt event ID (Interrupt Selection Number)
Default is -1.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored
params.priority = Int 0;
// Interrupt priority. Not supported on this target
params.restoreMask = Bits16 0;
// Dispatcher auto-nesting interrupt restore mask
config Hwi.arg // instance |
|
ISR function argument. Default is 0
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.arg = UArg 0;
C SYNOPSIS
config Hwi.disableMask // instance |
|
Dispatcher auto-nesting interrupt disable mask
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.disableMask = Bits16 0;
DETAILS
When the dispatcher's auto interrupt nesting support feature
is enabled (see
dispatcherAutoNestingSupport),
this mask defines which IER bits are disabled prior to invoking
the user's ISR function with GIE = 1.
disableMask bits set to 1 correspond to IER bits that will be cleared
prior to invoking the ISR.
The value of this mask is normally auto-calculated based on the
value of the maskSetting. However, manual setting of this
mask is enabled by setting the maskSetting to
MaskingOption_BITMASK.
The default value is derived from the
MaskingOption_SELF
maskSetting.
C SYNOPSIS
config Hwi.enableAck // instance |
|
Enable automatic acknowledgement of PIE interrupts by the Hwi interrupt
dispatcher
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.enableAck = Bool true;
C SYNOPSIS
config Hwi.enableInt // instance |
|
Enable this interrupt now? Default is true
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.enableInt = Bool true;
C SYNOPSIS
config Hwi.eventId // instance |
|
Interrupt event ID (Interrupt Selection Number)
Default is -1.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.eventId = Int -1;
C SYNOPSIS
config Hwi.maskSetting // instance |
|
maskSetting. Default is Hwi_MaskingOption_SELF
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
C SYNOPSIS
config Hwi.priority // instance |
|
Interrupt priority. Not supported on this target
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.priority = Int 0;
C SYNOPSIS
config Hwi.restoreMask // instance |
|
Dispatcher auto-nesting interrupt restore mask
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.restoreMask = Bits16 0;
DETAILS
When the dispatcher's auto interrupt nesting support feature
is enabled (see
dispatcherAutoNestingSupport),
this mask defines which IER bits are restored to their previous
setting upon return from the user's ISR function.
restoreMask bits set to 1 correspond to IER bits that will be restored.
The value of this mask is normally auto-calculated based on the
value of the maskSetting. However, manual setting of this
mask is enabled by setting the maskSetting to
MaskingOption_BITMASK.
The default value is derived from the
MaskingOption_SELF
maskSetting.
C SYNOPSIS
Instance Creation |
|
XDCscript usage |
meta-domain |
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = Hwi.create(Int intNum, Void(*)(UArg) hwiFxn, params);
// Create an instance-object
ARGUMENTS
intNum
interrupt number
hwiFxn
pointer to ISR function
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Hwi dispatcher table entry is created and filled with the
function specified by the fxn parameter and the attributes
specified by the params parameter.
If params is NULL, the Hwi's dispatcher properties are assigned a
default set of values. Otherwise, the following properties
are specified by a structure of type Hwi_Params.
- The arg element is a generic argument that is passed to the plugged
function as its only parameter. The default value is 0.
- The enableInt element determines whether the interrupt should be
enabled in the IER by create.
- The maskSetting element defines the dispatcherAutoNestingSupport
behavior of the interrupt.
Hwi_create returns a pointer to the created Hwi object.