![]() |
![]() |
#include <dsplink.h>
#include <mplistdefs.h>
Go to the source code of this file.
Functions | |
DLLEXPORT DSP_STATUS | MPLIST_create (IN ProcessorId procId, IN Char8 *name, IN MPLIST_List *mplistObj, IN MPLIST_Attrs *attrs) |
Allocates and initializes a doubly linked circular list in shared memory. The memory for the object may or may not be provided by the user. Uses POOl api to allocate a list object. The list object contains a MPCS object and a single element and initializes that element to indicate that it is the "end of the list" (i.e., the list is empty). An entry is added in the shared memory control structure for the list. | |
DLLEXPORT DSP_STATUS | MPLIST_delete (IN ProcessorId procId, IN Char8 *name) |
Removes a list by freeing its control structure's memory space. Must ONLY be used for empty lists, because it does not delete the list elements. Calling this function on a non-empty list will cause a memory leak. | |
DLLEXPORT DSP_STATUS | MPLIST_open (IN ProcessorId procId, IN Char8 *name, OUT MPLIST_Handle *mplistHandle) |
This function opens an MPLIST object specified by its name and gets a handle to the object. Every process that needs to use the MPLIST object must get a handle to the object by calling this API. | |
DLLEXPORT DSP_STATUS | MPLIST_close (IN MPLIST_Handle mplistHandle) |
This function closes an MPLIST instance. | |
DLLEXPORT Bool | MPLIST_isEmpty (IN MPLIST_Handle mplistHandle) |
Check for an empty list. | |
DLLEXPORT DSP_STATUS | MPLIST_insertBefore (IN MPLIST_Handle mplistHandle, IN MPLIST_Elem insertElement, IN MPLIST_Elem existingElement) |
Inserts the element before the existing element. | |
DLLEXPORT DSP_STATUS | MPLIST_putTail (IN MPLIST_Handle mplistHandle, IN MPLIST_Elem element) |
Adds the specified element to the tail of the list. | |
DLLEXPORT DSP_STATUS | MPLIST_removeElement (IN MPLIST_Handle mplistHandle, IN MPLIST_Elem element) |
Removes (unlinks) the given element from the list, if the list is not empty. Does not free the list element. | |
DLLEXPORT DSP_STATUS | MPLIST_first (IN MPLIST_Handle mplistHandle, OUT MPLIST_Elem *element) |
Returns a pointer to the first element of the list, or NULL if the list is empty. | |
DLLEXPORT DSP_STATUS | MPLIST_next (IN MPLIST_Handle mplistHandle, IN MPLIST_Elem currentElement, OUT MPLIST_Elem *nextElement) |
Returns a pointer to the next element of the list, or NULL if the next element is the head of the list or the list is empty. | |
DLLEXPORT DSP_STATUS | MPLIST_getHead (IN MPLIST_Handle mplistHandle, OUT MPLIST_Elem *element) |
Pops the head off the list and returns a pointer to it. If the list is empty, returns NULL. |
DLLEXPORT DSP_STATUS MPLIST_create | ( | IN ProcessorId | procId, |
IN Char8 * | name, | ||
IN MPLIST_List * | mplistObj, | ||
IN MPLIST_Attrs * | attrs | ||
) |
Allocates and initializes a doubly linked circular list in shared memory. The memory for the object may or may not be provided by the user. Uses POOl api to allocate a list object. The list object contains a MPCS object and a single element and initializes that element to indicate that it is the "end of the list" (i.e., the list is empty). An entry is added in the shared memory control structure for the list.
============================================================================
procId | Processor id of the processor making this create call. |
mplistObj | Pointer to the shared MPLIST object. If memory for the MPLIST object is provided by the user, the MPLIST object handle is not NULL. Otherwise, if the memory is to be allocated by the MPLIST component, the MPLIST object handle can be specified as NULL. |
name | Name of the list to be created. |
attrs | Attributes of the list to be created. |
DLLEXPORT DSP_STATUS MPLIST_delete | ( | IN ProcessorId | procId, |
IN Char8 * | name | ||
) |
Removes a list by freeing its control structure's memory space. Must ONLY be used for empty lists, because it does not delete the list elements. Calling this function on a non-empty list will cause a memory leak.
============================================================================
procId | Processor id of the processor making this delete call. |
name | Name of the list to be deleted. |
DLLEXPORT DSP_STATUS MPLIST_open | ( | IN ProcessorId | procId, |
IN Char8 * | name, | ||
OUT MPLIST_Handle * | mplistHandle | ||
) |
This function opens an MPLIST object specified by its name and gets a handle to the object. Every process that needs to use the MPLIST object must get a handle to the object by calling this API.
============================================================================
procId | Processor id of the processor making the open call. |
name | Name of the list to be opened. |
mplistHandle | Handle of list which has been opened. |
DLLEXPORT DSP_STATUS MPLIST_close | ( | IN MPLIST_Handle | mplistHandle ) |
This function closes an MPLIST instance.
============================================================================
mplistHandle | Handle for list operations. |
DLLEXPORT Bool MPLIST_isEmpty | ( | IN MPLIST_Handle | mplistHandle ) |
Check for an empty list.
============================================================================
mplistHandle | Handle for list operations. |
DLLEXPORT DSP_STATUS MPLIST_insertBefore | ( | IN MPLIST_Handle | mplistHandle, |
IN MPLIST_Elem | insertElement, | ||
IN MPLIST_Elem | existingElement | ||
) |
Inserts the element before the existing element.
============================================================================
mplistHandle | Handle for list operations. |
insertElement | Pointer to element in list to insert. |
existingElement | Pointer to existing list element. |
DLLEXPORT DSP_STATUS MPLIST_putTail | ( | IN MPLIST_Handle | mplistHandle, |
IN MPLIST_Elem | element | ||
) |
Adds the specified element to the tail of the list.
============================================================================
mplistHandle | Handle for list operations. |
element | Pointer to list element to be added. |
DLLEXPORT DSP_STATUS MPLIST_removeElement | ( | IN MPLIST_Handle | mplistHandle, |
IN MPLIST_Elem | element | ||
) |
Removes (unlinks) the given element from the list, if the list is not empty. Does not free the list element.
============================================================================
mplistHandle | Handle for list operations. |
element | Pointer to element in list to remove. |
DLLEXPORT DSP_STATUS MPLIST_first | ( | IN MPLIST_Handle | mplistHandle, |
OUT MPLIST_Elem * | element | ||
) |
Returns a pointer to the first element of the list, or NULL if the list is empty.
============================================================================
mplistHandle | Handle for list operations. |
element | OUT parameter for holding the first element. |
DLLEXPORT DSP_STATUS MPLIST_next | ( | IN MPLIST_Handle | mplistHandle, |
IN MPLIST_Elem | currentElement, | ||
OUT MPLIST_Elem * | nextElement | ||
) |
Returns a pointer to the next element of the list, or NULL if the next element is the head of the list or the list is empty.
============================================================================
mplistHandle | Handle for list operations. |
currentElement | Pointer to element in list to remove. |
nextElement | OUT parameter to hold the next element. |
DLLEXPORT DSP_STATUS MPLIST_getHead | ( | IN MPLIST_Handle | mplistHandle, |
OUT MPLIST_Elem * | element | ||
) |
Pops the head off the list and returns a pointer to it. If the list is empty, returns NULL.
============================================================================
mplistHandle | Handle for list operations. |
element | OUT Parameter to hold the head element. |