#include <que.h>
#include <pool.h>
#include <platform.h>
#include <version.h>
Go to the source code of this file.
Defines |
#define | IN |
| Argument specification syntax ============================================================================.
|
#define | OUT |
#define | CONST const |
#define | DSP_MAX_STRLEN 32 |
| Maximum length of string. ============================================================================.
|
#define | MAX_IPS 16 |
#define | DSPLINK_TERMINATE_EVT (-1) |
#define | DSPLINK_DRIVER_NAME "/dsplink" |
| DSPLINK driver name ============================================================================.
|
#define | MAX_DRIVER_NAME_LEN 16 |
| Maximum length of the driver name. ============================================================================.
|
Typedefs |
typedef Void(* | DSPLINK_TerminateFxn )(Void) |
Variables |
far DSPLINK_TerminateFxn | DSPLINK_terminateFxn |
POOL |
POOL variable defined by MSGQ module. This is temporary until this definition is exported by DSP/BIOS configuration tool. ============================================================================
============================================================================
|
POOL_Config * | POOL |
Void | DSPLINK_init (Void) |
| This function initializes DSP/BIOS LINK.
|
Define Documentation
Argument specification syntax ============================================================================.
============================================================================
- Macro:
- IN/OUT/CONST
#define DSP_MAX_STRLEN 32 |
Maximum length of string. ============================================================================.
============================================================================
- Constant:
- DSP_MAX_STRLEN
#define DSPLINK_TERMINATE_EVT (-1) |
#define DSPLINK_DRIVER_NAME "/dsplink" |
DSPLINK driver name ============================================================================.
============================================================================
- Constant:
- DSPLINK_DRIVER_NAME
#define MAX_DRIVER_NAME_LEN 16 |
Maximum length of the driver name. ============================================================================.
============================================================================
- Constant:
- MAX_DRIVER_NAME_LEN
Typedef Documentation
Function Documentation
Void DSPLINK_init |
( |
Void |
) |
|
This function initializes DSP/BIOS LINK.
============================================================================
- Function:
- DSPLINK_init
- Parameters:
-
- Returns:
- None.
- Precondition:
- None.
- Postcondition:
- None.
- See also:
- None. ============================================================================
Variable Documentation