Data Fields

DM648_ddrRegs Struct Reference

#include <dm648_hal_pci.h>

Data Fields

volatile Uint32 MIDR
volatile Uint32 SDSTAT
volatile Uint32 SDCFG
volatile Uint32 SDREF
volatile Uint32 SDTIM1
volatile Uint32 SDTIM2
volatile Uint8 RSVD0 [8]
volatile Uint32 BPRIO
volatile Uint8 RSVD1 [192]
volatile Uint32 DDRCTL
volatile Uint32 PHYSTAT

Field Documentation

volatile Uint8 DM648_ddrRegs::RSVD1[192]

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated