![]() |
![]() |
#include <dsplink.h>
#include <mpcsdefs.h>
Go to the source code of this file.
Data Structures | |||||||||||||||||
struct | MPLIST_Attrs_tag | ||||||||||||||||
struct | MPLIST_Header_tag | ||||||||||||||||
struct | MPLIST_List_tag | ||||||||||||||||
struct | MPLIST_Entry_tag | ||||||||||||||||
struct | MPLIST_Ctrl_tag | ||||||||||||||||
struct | MPLIST_MemInfo_tag | ||||||||||||||||
Typedefs | |||||||||||||||||
MPLIST_Attrs | |||||||||||||||||
This structure defines the MPLIST Creation Parameters. ============================================================================
| |||||||||||||||||
typedef struct MPLIST_Attrs_tag | MPLIST_Attrs | ||||||||||||||||
MPLIST_Handle | |||||||||||||||||
Handle to the MPLIST object. ============================================================================ ============================================================================ | |||||||||||||||||
typedef void * | MPLIST_Handle | ||||||||||||||||
MPLIST_Header | |||||||||||||||||
An element of a list. ============================================================================
| |||||||||||||||||
typedef struct MPLIST_Header_tag | MPLIST_Header | ||||||||||||||||
MPLIST_Elem | |||||||||||||||||
This type is used for the handle to the shared list entry structure. ============================================================================ ============================================================================ | |||||||||||||||||
typedef MPLIST_Header * | MPLIST_Elem | ||||||||||||||||
MPLIST_List | |||||||||||||||||
Definition of a MPLIST. ============================================================================
| |||||||||||||||||
typedef struct MPLIST_List_tag | MPLIST_List | ||||||||||||||||
MPLIST_Entry | |||||||||||||||||
MPLIST descriptor entry for each MPLIST in the system. ============================================================================
| |||||||||||||||||
typedef struct MPLIST_Entry_tag | MPLIST_Entry | ||||||||||||||||
MPLIST_Ctrl | |||||||||||||||||
This structure defines the control structure required by the MPLIST component. It contains information about all MPLIST objects shared between the GPP and a specific DSP. ============================================================================
| |||||||||||||||||
typedef struct MPLIST_Ctrl_tag | MPLIST_Ctrl | ||||||||||||||||
MPLIST_MemInfo | |||||||||||||||||
Entry structure for the MpList data transport ============================================================================
| |||||||||||||||||
typedef struct MPLIST_MemInfo_tag | MPLIST_MemInfo |
typedef struct MPLIST_Attrs_tag MPLIST_Attrs |
typedef void* MPLIST_Handle |
typedef struct MPLIST_Header_tag MPLIST_Header |
typedef MPLIST_Header* MPLIST_Elem |
typedef struct MPLIST_List_tag MPLIST_List |
typedef struct MPLIST_Entry_tag MPLIST_Entry |
typedef struct MPLIST_Ctrl_tag MPLIST_Ctrl |
typedef struct MPLIST_MemInfo_tag MPLIST_MemInfo |