Data Fields

OMAP3530_HalObj_tag Struct Reference

#include <omap3530_hal.h>

Collaboration diagram for OMAP3530_HalObj_tag:
Collaboration graph
[legend]

Data Fields

HAL_Interfaceinterface
IsrObject * isrObject
Uint32 generalCtrlBase
Uint32 iva2CmBase
Uint32 coreCmBase
Uint32 perCmBase
Uint32 iva2PrmBase
Uint32 mailboxBase
Uint32 mmuBase
Uint32 tlbIndex
Uint32 procId
Bool type

Field Documentation


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated