Functions

mplist.h File Reference

#include <dsplink.h>
#include <mplistdefs.h>
Include dependency graph for gpp/inc/mplist.h:

Go to the source code of this file.

Functions

DLLEXPORT DSP_STATUS MPLIST_create (IN ProcessorId procId, IN Char8 *name, IN MPLIST_List *mplistObj, IN MPLIST_Attrs *attrs)
 Allocates and initializes a doubly linked circular list in shared memory. The memory for the object may or may not be provided by the user. Uses POOl api to allocate a list object. The list object contains a MPCS object and a single element and initializes that element to indicate that it is the "end of the list" (i.e., the list is empty). An entry is added in the shared memory control structure for the list.
DLLEXPORT DSP_STATUS MPLIST_delete (IN ProcessorId procId, IN Char8 *name)
 Removes a list by freeing its control structure's memory space. Must ONLY be used for empty lists, because it does not delete the list elements. Calling this function on a non-empty list will cause a memory leak.
DLLEXPORT DSP_STATUS MPLIST_open (IN ProcessorId procId, IN Char8 *name, OUT MPLIST_Handle *mplistHandle)
 This function opens an MPLIST object specified by its name and gets a handle to the object. Every process that needs to use the MPLIST object must get a handle to the object by calling this API.
DLLEXPORT DSP_STATUS MPLIST_close (IN MPLIST_Handle mplistHandle)
 This function closes an MPLIST instance.
DLLEXPORT Bool MPLIST_isEmpty (IN MPLIST_Handle mplistHandle)
 Check for an empty list.
DLLEXPORT DSP_STATUS MPLIST_insertBefore (IN MPLIST_Handle mplistHandle, IN MPLIST_Elem insertElement, IN MPLIST_Elem existingElement)
 Inserts the element before the existing element.
DLLEXPORT DSP_STATUS MPLIST_putTail (IN MPLIST_Handle mplistHandle, IN MPLIST_Elem element)
 Adds the specified element to the tail of the list.
DLLEXPORT DSP_STATUS MPLIST_removeElement (IN MPLIST_Handle mplistHandle, IN MPLIST_Elem element)
 Removes (unlinks) the given element from the list, if the list is not empty. Does not free the list element.
DLLEXPORT DSP_STATUS MPLIST_first (IN MPLIST_Handle mplistHandle, OUT MPLIST_Elem *element)
 Returns a pointer to the first element of the list, or NULL if the list is empty.
DLLEXPORT DSP_STATUS MPLIST_next (IN MPLIST_Handle mplistHandle, IN MPLIST_Elem currentElement, OUT MPLIST_Elem *nextElement)
 Returns a pointer to the next element of the list, or NULL if the next element is the head of the list or the list is empty.
DLLEXPORT DSP_STATUS MPLIST_getHead (IN MPLIST_Handle mplistHandle, OUT MPLIST_Elem *element)
 Pops the head off the list and returns a pointer to it. If the list is empty, returns NULL.

Function Documentation

DLLEXPORT DSP_STATUS MPLIST_create ( IN ProcessorId  procId,
IN Char8 name,
IN MPLIST_List mplistObj,
IN MPLIST_Attrs attrs 
)

Allocates and initializes a doubly linked circular list in shared memory. The memory for the object may or may not be provided by the user. Uses POOl api to allocate a list object. The list object contains a MPCS object and a single element and initializes that element to indicate that it is the "end of the list" (i.e., the list is empty). An entry is added in the shared memory control structure for the list.

============================================================================

Function:
MPLIST_create
Parameters:
procIdProcessor id of the processor making this create call.
mplistObjPointer to the shared MPLIST object. If memory for the MPLIST object is provided by the user, the MPLIST object handle is not NULL. Otherwise, if the memory is to be allocated by the MPLIST component, the MPLIST object handle can be specified as NULL.
nameName of the list to be created.
attrsAttributes of the list to be created.
Returns:
DSP_SOK Operation successfully completed. DSP_EINVALIDARG Invalid arguments. DSP_EMEMORY Operation failed due to a memory error. DSP_EALREADYEXISTS The specified MPLIST name is already in use. DSP_ERESOURCE All MPLIST entries are currently in use. DSP_EACCESSDENIED The MPLIST component has not been initialized. DSP_ENOTFOUND Information about specified POOL buffer was not available. DSP_EFAIL General failure.
Precondition:
Processor id must be valid. MPLIST name must be valid. MPLIST creation attributes must be a valid. PROC_attach has been successful. POOL has been configured according to application specification.
Postcondition:
None
See also:
MPLIST_delete ============================================================================
DLLEXPORT DSP_STATUS MPLIST_delete ( IN ProcessorId  procId,
IN Char8 name 
)

Removes a list by freeing its control structure's memory space. Must ONLY be used for empty lists, because it does not delete the list elements. Calling this function on a non-empty list will cause a memory leak.

============================================================================

Function:
MPLIST_delete
Parameters:
procIdProcessor id of the processor making this delete call.
nameName of the list to be deleted.
Returns:
DSP_SOK Operation successfully completed. DSP_EINVALIDARG Invalid arguments. DSP_EACCESSDENIED The MPLIST component has not been initialized. DSP_ENOTFOUND The MPLIST to be deleted is not present. Information about specified POOL buffer was not available. DSP_EFAIL General Failure.
Precondition:
Processor Id must be valid. MPLIST name must be valid. All MPLIST operations on that MP_LIST are complete.
Postcondition:
None
See also:
MPLIST_create ============================================================================
DLLEXPORT DSP_STATUS MPLIST_open ( IN ProcessorId  procId,
IN Char8 name,
OUT MPLIST_Handle mplistHandle 
)

This function opens an MPLIST object specified by its name and gets a handle to the object. Every process that needs to use the MPLIST object must get a handle to the object by calling this API.

============================================================================

Function:
MPLIST_open
Parameters:
procIdProcessor id of the processor making the open call.
nameName of the list to be opened.
mplistHandleHandle of list which has been opened.
Returns:
DSP_SOK Operation successfully completed. DSP_EINVALIDARG Invalid arguments. DSP_EFAIL General Failure. DSP_EACCESSDENIED The MPLIST component has not been initialized. DSP_ENOTFOUND The MPLIST to be deleted is not present. Information about specified POOL buffer was not available. DSP_EACCESSDENIED The MPLIST component has not been initialized.
Precondition:
mplistHandle must be a valid pointer. name must be a valid pointer. MPLIST_create has been successful.
Postcondition:
None
See also:
MPLIST_close ============================================================================
DLLEXPORT DSP_STATUS MPLIST_close ( IN MPLIST_Handle  mplistHandle )

This function closes an MPLIST instance.

============================================================================

Function:
MPLIST_close
Parameters:
mplistHandleHandle for list operations.
Returns:
DSP_SOK Operation successfully completed. DSP_SFREE Resource has been freed successfully. DSP_EINVALIDARG Invalid arguments. DSP_EACCESSDENIED The MPLIST component has not been initialized. DSP_EFAIL General Failure.
Precondition:
mplistHandle must be a valid pointer. All MPLIST operations are successful.
Postcondition:
None
See also:
MPLIST_open
Modifies:
None ============================================================================
DLLEXPORT Bool MPLIST_isEmpty ( IN MPLIST_Handle  mplistHandle )

Check for an empty list.

============================================================================

Function:
MPLIST_isEmpty
Parameters:
mplistHandleHandle for list operations.
Returns:
TRUE List is empty. FALSE List is not empty.
Precondition:
mplistHandle must be a valid pointer. MPLIST_create has been successful.
Postcondition:
None
See also:
None ============================================================================
DLLEXPORT DSP_STATUS MPLIST_insertBefore ( IN MPLIST_Handle  mplistHandle,
IN MPLIST_Elem  insertElement,
IN MPLIST_Elem  existingElement 
)

Inserts the element before the existing element.

============================================================================

Function:
MPLIST_insertBefore
Parameters:
mplistHandleHandle for list operations.
insertElementPointer to element in list to insert.
existingElementPointer to existing list element.
Returns:
DSP_SOK Operation successfully completed. DSP_EINVALIDARG Invalid arguments. DSP_ENOTFOUND Information about specified POOL buffer was not available. DSP_EFAIL General Failure.
Precondition:
mplistHandle must be a valid pointer. insertElement must be a valid pointer. existingElement must be a valid pointer. MPLIST_open has been successful.
Postcondition:
None
See also:
MPLIST_create, MPLIST_putTail ============================================================================
DLLEXPORT DSP_STATUS MPLIST_putTail ( IN MPLIST_Handle  mplistHandle,
IN MPLIST_Elem  element 
)

Adds the specified element to the tail of the list.

============================================================================

Function:
MPLIST_putTail
Parameters:
mplistHandleHandle for list operations.
elementPointer to list element to be added.
Returns:
DSP_SOK Operation successfully completed. DSP_EINVALIDARG Invalid arguments. DSP_ENOTFOUND Information about specified POOL buffer was not available. DSP_EFAIL General Failure.
Precondition:
mplistHandle must be a valid pointer. element must be a valid pointer. MPLIST_open has been successful.
Postcondition:
None
See also:
MPLIST_insertBefore ============================================================================
DLLEXPORT DSP_STATUS MPLIST_removeElement ( IN MPLIST_Handle  mplistHandle,
IN MPLIST_Elem  element 
)

Removes (unlinks) the given element from the list, if the list is not empty. Does not free the list element.

============================================================================

Function:
MPLIST_removeElement
Parameters:
mplistHandleHandle for list operations.
elementPointer to element in list to remove.
Returns:
DSP_SOK Operation successfully completed. DSP_EINVALIDARG Invalid arguments. DSP_EFAIL General Failure.
Precondition:
mplistHandle must be a valid pointer. element be a valid pointer. MPLIST_open has been successful.
Postcondition:
None
See also:
MPLIST_insertBefore, MPLIST_create, MPLIST_putTail ============================================================================
DLLEXPORT DSP_STATUS MPLIST_first ( IN MPLIST_Handle  mplistHandle,
OUT MPLIST_Elem element 
)

Returns a pointer to the first element of the list, or NULL if the list is empty.

============================================================================

Function:
MPLIST_first
Parameters:
mplistHandleHandle for list operations.
elementOUT parameter for holding the first element.
Returns:
DSP_SOK Operation successfully completed. DSP_EINVALIDARG Invalid arguments. DSP_EFAIL General Failure.
Precondition:
mplistHandle must be a valid pointer. element be a valid pointer. MPLIST_open has been successful.
Postcondition:
None
See also:
MPLIST_create, MPLIST_puttail, MPLIST_insertbefore ============================================================================
DLLEXPORT DSP_STATUS MPLIST_next ( IN MPLIST_Handle  mplistHandle,
IN MPLIST_Elem  currentElement,
OUT MPLIST_Elem nextElement 
)

Returns a pointer to the next element of the list, or NULL if the next element is the head of the list or the list is empty.

============================================================================

Function:
MPLIST_next
Parameters:
mplistHandleHandle for list operations.
currentElementPointer to element in list to remove.
nextElementOUT parameter to hold the next element.
Returns:
DSP_SOK Operation successfully completed. DSP_EINVALIDARG Invalid arguments. DSP_EFAIL General Failure.
Precondition:
mplistHandle must be a valid pointer. currentElement be a valid pointer. nextElement be a valid pointer. MPLIST_open has been successful.
Postcondition:
None
See also:
MPLIST_insertBefore, MPLIST_putTail ============================================================================
DLLEXPORT DSP_STATUS MPLIST_getHead ( IN MPLIST_Handle  mplistHandle,
OUT MPLIST_Elem element 
)

Pops the head off the list and returns a pointer to it. If the list is empty, returns NULL.

============================================================================

Function:
MPLIST_getHead
Parameters:
mplistHandleHandle for list operations.
elementOUT Parameter to hold the head element.
Returns:
DSP_SOK Operation successfully completed. DSP_EINVALIDARG Invalid arguments. DSP_ENOTFOUND Information about specified POOL buffer was not available. DSP_EFAIL General Failure.
Precondition:
mplistHandle must be a valid pointer. element be a valid pointer. MPLIST_open has been successful.
Postcondition:
None
See also:
MPLIST_puttail, MPLIST_insertbefore ============================================================================
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated