![]() |
![]() |
#include <gpptypes.h>
#include <constants.h>
#include <errbase.h>
#include <archdefs.h>
#include <linkcfgdefs.h>
Go to the source code of this file.
Defines | |
#define | MAX_IPS 16u |
#define | WAIT_FOREVER (~((Uint32) 0u)) |
Wait indefinitely. ============================================================================. | |
#define | WAIT_NONE ((Uint32) 0u) |
Do not wait. ============================================================================. | |
#define | IS_GPPID(id) (id == ID_GPP) |
Is the GPP ID valid. ============================================================================. |
#define MAX_IPS 16u |
#define WAIT_FOREVER (~((Uint32) 0u)) |
Wait indefinitely. ============================================================================.
============================================================================
#define WAIT_NONE ((Uint32) 0u) |
Do not wait. ============================================================================.
============================================================================
#define IS_GPPID | ( | id ) | (id == ID_GPP) |
Is the GPP ID valid. ============================================================================.
============================================================================