Data Structures | Defines

chnldefs.h File Reference


Detailed Description

Defines data types and structures used by CHNL component.

============================================================================

Path:
/gpp/inc/usr/
Version:
1.65.01.06 ============================================================================
Copyright:
Copyright (C) 2002-2009, Texas Instruments Incorporated - https://www.ti.com/

Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

* Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.

* Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.

* Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. ============================================================================

#include <dsplink.h>
#include <procdefs.h>
Include dependency graph for chnldefs.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  ChannelAttrs_tag
struct  ChannelIOInfo_tag

Defines

#define MAX_ALLOC_BUFFERS   1000u
 Maximum number of buffers that can be allocated through CHNL_AllocateBuffer. ============================================================================.
#define MAX_CHANNELS   16u
 Maximum number of channels that can be created for each DSP. ============================================================================.
#define IS_VALID_CHNLID(dspId, chnlId)   FALSE

Typedefs

ChannelAttrs

Channel Attributes.

============================================================================

Parameters:
endianismEndiannism information currently not used.
modeMode of channel (Input or output).
sizeSize of data sent on channel (16 bits or 32 bits). ============================================================================
typedef struct ChannelAttrs_tag ChannelAttrs
ChannelIOInfo

Information for adding or reclaiming a IO request.

============================================================================

Parameters:
bufferBuffer pointer.
sizeSize of buffer.
argArgument to receive or send. ============================================================================
typedef struct ChannelIOInfo_tag ChannelIOInfo

Enumerations

ChannelMode

Mode of a channel.

============================================================================

Parameters:
ChannelMode_InputIndicates the channel as an Input channel (from DSP to GPP).
ChannelMode_OutputIndicates the channel as an Output channel (from GPP to DSP). ============================================================================
enum  ChannelMode {
  ChannelMode_Input = 0x1u,
  ChannelMode_Output = 0x2u
}
ChannelDataSize

Width of data being sent on channel.

============================================================================

Parameters:
ChannelDataSize_16bitsIndicates the data to be transferred through the channel as 16 bit data.
ChannelDataSize_32bitsIndicates the data to be transferred through the channel as 32 bit data. ============================================================================
enum  ChannelDataSize {
  ChannelDataSize_16bits = 1u,
  ChannelDataSize_32bits = 2u
}

Define Documentation

#define MAX_ALLOC_BUFFERS   1000u

Maximum number of buffers that can be allocated through CHNL_AllocateBuffer. ============================================================================.

============================================================================

Constant:
MAX_ALLOC_BUFFERS
#define MAX_CHANNELS   16u

Maximum number of channels that can be created for each DSP. ============================================================================.

============================================================================

Constant:
MAX_CHANNELS
#define IS_VALID_CHNLID (   dspId,
  chnlId 
)    FALSE

Typedef Documentation


Enumeration Type Documentation

Enumerator:
ChannelMode_Input 
ChannelMode_Output 
Enumerator:
ChannelDataSize_16bits 
ChannelDataSize_32bits 
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated