Platform
Legend
|
Package Name |
The name of the application or files |
|
Version |
Version of the application or files |
|
License |
Name of the license or licenses that apply to the Package. |
|
Location |
The directory name and path on the media (or in an archive) where the Package is located. |
|
Delivered As |
This field will either be “Source”, “Binary” or “Source and Binary” and is the form the content of the Package is delivered in. If the Package is delivered in an archive format, this field applies to the contents of the archive. If the word Limited is used with Source, as in “Limited Source” or “Limited Source and Binary” then only portions of the Source for the application are provided. |
|
Modified |
This field will either be “Yes” or “No”. A “Yes” means TI had made changes to the Package. A “No” means TI has not made any changes. |
|
This field specifies where TI obtained the Package from. It may be a URL to an Open Source site, a 3rd party company name or TI. If this field contains a link to an Open Source package, the date it was downloaded is also recorded. |
Manifest
Note: Replace MM.mm.pp.bb in
the directory path below with the PSP release version you are using.
Wherever component versions are different(as
indicated by X.X.X.X) replace with the appropriate version from
"Version" column.
|
Package Name |
Version |
License |
Delivered As |
Modified |
|
|
|
Open Source Linux (based on linux-omap
GIT) |
2.6.37 |
GPLv2 |
Source and Binary |
Yes |
Location |
Source at AM35x-OMAP35x-LINUX-PSP-MM.mm.pp.bb/src/kernel/linux-MM.mm.pp.bb.tar.gz. AM35x-OMAP35x-LINUX-PSP-MM.mm.pp.bb/images/kernel/am3517/uImage AM35x-OMAP35x-LINUX-PSP-MM.mm.pp.bb/images/kernel/beagle/uImage |
|
Obtained from[1] |
Kernel 2.6.37 from linux-omap pm branch (commit 2b3ea6aa16956e15f1ba8e7b70898aaacbec2237) |
|||||
|
Bootstrapper |
1.51 |
GPLv2 |
Source and Binary |
Yes |
Location |
Source at AM35x-OMAP35x-LINUX-PSP-MM.mm.pp.bb/src/boot-strap/x-loader-MM.mm.pp.bb.tar.gz AM35x-OMAP35x-LINUX-PSP-MM.mm.pp.bb/images/boot-strap/beagle/x-load.bin.ift |
|
Obtained
from[1] |
Derived from U-boot project. |
|||||
|
U-Boot |
2010.06 |
GPLv2 |
Source and Binary |
Yes |
Location |
Source at AM35x-OMAP35x-LINUX-PSP-MM.mm.pp.bb/src/u-boot/u-boot-MM.mm.pp.bb.tar.gz AM35x-OMAP35x-LINUX-PSP-MM.mm.pp.bb/images/u-boot/am3517/u-boot.bin. AM35x-OMAP35x-LINUX-PSP-MM.mm.pp.bb/images/u-boot/beagle/u-boot.bin |
|
Obtained from[1] |
U-Boot 2010.06 from u-boot ( commit v2010.06 ). |
|||||
|
Sample Code(video, audio) |
NA |
BSD |
Source |
NA |
Location |
AM35x-OMAP35x-LINUX-PSP-MM.mm.pp.bb/src/examples/examples.tar.gz |
|
Obtained from[1] |
TI |
|||||
|
Image Signing Utility |
NA |
BSD |
Source and Binary |
NA |
Location |
Source at AM35x-OMAP35x-LINUX-PSP-MM.mm.pp.bb/host-tools/src/signGP.c Binary at AM35x-OMAP35x-LINUX-PSP-MM.mm.pp.bb/host-tools/linux/signGP |
|
Obtained from[1] |
TI |
|||||
|
|
|
|
|
|
|
|
[1] Any links appearing on this manifest
were verified at the time it was created. TI makes no guarantee that they will
remain active in the future.