10.5.2. Constants in Linker Command Files

You can specify constants with either of two syntax schemes: the scheme used for specifying decimal, octal, or hexadecimal constants (but not binary constants) used in the assembler (see Accessing Assembly Language Constants, Character String Constants, or the scheme used for integer constants in C syntax.

Examples:

Format

Decimal

Octal

Hexadecimal

Assembler format

32

40q

020h

C format

32

040

0x20