15.14. Control Hex Conversion Utility Diagnostics¶
The hex conversion utility uses certain C/C++ compiler options to control hex-converter-generated diagnostics.
- --diag_error¶
Syntax: --diag_error=id
Categorizes the diagnostic identified by id as an error. To determine the numeric identifier of a diagnostic message, use the --display_error_number option first in a separate link. Then use --diag_error=id to recategorize the diagnostic as an error. You can only alter the severity of discretionary diagnostics.
- --diag_remark¶
Syntax: --diag_remark=id
Categorizes the diagnostic identified by id as a remark. To determine the numeric identifier of a diagnostic message, use the --display_error_number option first in a separate link. Then use --diag_remark=id to recategorize the diagnostic as a remark. You can only alter the severity of discretionary diagnostics.
- --diag_suppress¶
Syntax: --diag_suppress=id
Suppresses the diagnostic identified by id. To determine the numeric identifier of a diagnostic message, use the --display_error_number option first in a separate link. Then use --diag_suppress=id to suppress the diagnostic. You can only suppress discretionary diagnostics.
- --diag_warning¶
Syntax: --diag_warning=id
Categorizes the diagnostic identified by id as a warning. To determine the numeric identifier of a diagnostic message, use the --display_error_number option first in a separate link. Then use --diag_warning=id to recategorize the diagnostic as a warning. You can only alter the severity of discretionary diagnostics.
- --display_error_number¶
Syntax: --display_error_number
Displays a diagnostic message’s numeric identifier along with its text. Use this option in determining which arguments you need to supply to the diagnostic suppression options (--diag_suppress, --diag_error, --diag_remark, and --diag_warning). This option also indicates whether a diagnostic is discretionary. A discretionary diagnostic is one whose severity can be overridden. A discretionary diagnostic includes the suffix -D; otherwise, no suffix is present. See Diagnostic Options for more information on diagnostic messages.
- --issue_remarks¶
Syntax: --issue_remarks
Issues remarks (nonserious warnings), which are suppressed by default.
- --no_warnings¶
Syntax: --no_warnings
Suppresses warning diagnostics (errors are still issued).
- --set_error_limit¶
Syntax: --set_error_limit=count
Sets the error limit to count, which can be any decimal value. The linker abandons linking after this number of errors. (The default is 100.)
- --verbose_diagnostics¶
Syntax: --verbose_diagnostics
Provides verbose diagnostics that display the original source with line-wrap and indicate the position of the error in the source line.