10.11.3. Setting the Size of the Stack and Heap Sections¶
The C/C++ language uses two uninitialized sections called .sysmemand .stack for the memory pool used by the malloc( ) functions and the run-time stacks, respectively. You can set the size of these by using the --heap_sizeor --stack_size option and specifying the size of the section as a 4-byteconstant immediately after the option. If the options are not used, the default size of the heap is 2K bytes and the default size of the stack is 2K bytes.
See Define Heap Size (--heap_size Option) for setting heap sizes and Define Stack Size (--stack_size Option) for setting stack sizes.