3.3. Using the Time-Stamp Counter (TSC) RegisterΒΆ
The C7000 Compiler Tools provide a way to access the Time-Stamp Counter (TSC) register on the device. The value in the 64-bit Time-Stamp Counter Register is incremented by one on every clock cycle. The following program shows use of the __TSC register.
1#include <stdio.h>
2#include <c7x.h>
3
4int main()
5{
6 unsigned long start_time = __TSC;
7
8 // Print out numbers 1 through 5
9 for (int i = 1; i <= 5; i++)
10 printf("%d\n", i);
11
12 unsigned long stop_time = __TSC;
13
14 // Calculate and display the # cycles taken
15 printf("Number of clock cycles elapsed is %lu\n",
16 stop_time - start_time);
17
18 return 0;
19}