9. Revision History

Changes from May 16, 2024 to present

  • Added a new section on vector programming and the scalable vector programming model

  • Added an examples chapter

  • Additional material added to Streaming Engine and Streaming Address Generator sections

  • Added additional possible user techniques to ameliorate register pressure issues in software pipelined loops

Changes from December 15, 2023 to May 15, 2024

  • Extensive reorganization and additions.

Changes from January 21, 2022 to December 15, 2023 (from Revision B (January 2022) to Revision C (December 2023))

Changes from March 15, 2021 to January 21, 2022 (from Revision A (March 2021) to Revision B (January 2022))

Changes from May 1, 2020 to March 15, 2021 (from Revision -- (May 2020) to Revision A (March 2021))

  • Vector predicated stores generated by the compiler may trigger page fault exceptions in certain situations. This issue can be corrected in the linker command file. See Vectorization and Vector Predication.