8.5.1. Reserved Names in Linker Command Files¶
The following names (in both uppercase and lowercase) are reserved as keywords for linker directives. Do not use them as symbol or section names in a command file.
ADDRESS_MASK
ALGORITHM
ALIAS
ALIGN
ATTR
BLOCK
COMPRESSION
COPY
CRC_TABLE
DSECT
ECC
END
f
FILL
GROUP
HAMMING_MASK
HIGH
INPUT_PAGE
INPUT_RANGE
l (lowercase L)
LAST
LEN
LENGTH
LOAD
LOAD_END
LOAD_SIZE
LOAD_START
MEMORY
MIRRORING
NOINIT
NOLOAD
o
ORG
ORIGIN
PAGE
PALIGN
PARITY_MASK
RUN
RUN_END
RUN_SIZE
RUN_START
SECTIONS
SIZE
START
TABLE
TYPE
UNION
UNORDERED
VFILL
In addition, any section names used by the TI tools are reserved from being used as the prefix for other names, unless the section will be a subsection of the section name used by the TI tools. For example, section names may not begin with .debug.