8.5.2. Constants in Linker Command Files¶
You can specify constants with either of two syntax schemes: the scheme used for specifying decimal, octal, or hexadecimal constants (but not binary constants) used internally by the assembler or the scheme used for integer constants in C syntax.
Examples:
Format |
Decimal |
Octal |
Hexadecimal |
---|---|---|---|
Assembler format |
32 |
40q |
020h |
C format |
32 |
040 |
0x20 |