UniFlash 6.0.0 Release Notes
Table of Contents
Overview
Universal Flash Programmer for Texas Instruments devices. Provides a single interface for programming Flash memory and executing Flash based operations on supported targets.
Please read the Known Issue(s) section for issues we are currently working on, and the Issues Reporting section for information on how to report issues you come across.
- Release Date: April 20, 2020
- Build Version: 6.0.0.2710
What’s new for v6.0.0
- Device Support Update
- Synced up with CCS10.0.0
- Support for new MSP430 devices (On-Chip and Bootloader)(MSP430FR6005, MSP430FR6007, MSP430FR2672, MSP430FR2673)
- Bug Fixes
System Requirements
- Free Disk Space - 600MB (2GB recommended)
- Memory - 2GB
- OS - Windows 7/8/10 (64-bit), 64-bit Linux Distribution based on CCS requirements here, MacOS
Installation Instructions
Download the CCS UniFlash v6.0.0 build at the following locations:
(Note: there is a known issue with the Mac installer that in some cases adds an extra blank checkbox/option at the end of installation page; please ignore the option)
Getting Started
- For MCU On-Chip Flash programming, please refer to the Quick Start Guide
- For CC32xx Image Creator support, please read the Image Creator User Guide
- For mmWave (AWR/IWR) device support, please read the UniFlash User Guide for mmWave Devices (PDF)
- For select AM and K2G device support, please refer to Board Utils section in Processor SDK documentation
- For MSP and SimpleLink Bootloader Programming Using UniFlash, please refer to the User Guide
List of Supported Devices
C2000™ 32-bit Real-time Control MCUs
| Device Series | Part # | Device List |
|---|---|---|
| C2000 Real-Time Control MCUs | TMS320F280x, TMS320F281x, TMS320F2801x, TMS320F28044, TMS320F2823x TMS320F2833x, TMS320F2837xD. TMS320F2837xS (Including F065 variants.) TMS320F2802x, TMS320F2803x, TMS320F2805x, TMS320F2806x, TMS320F2807x, TMS320F28004x, TMS320F28002x F28M35x, F28M36x, F2838x |
TI Product Page |
Hercules™ ARM® Safety MCUs
| Device Series | Part # | Device List |
|---|---|---|
| TMS470M ARM Cortex-M3 Series | TMS470Mx | TI Product Page |
| TMS570 ARM Cortex-R4 Series | TMS570LS20xxx/10xxx TMS570LS31x/21x/11x TMS570LS1227 TMS570LS04x/03x |
TI Product Page |
| RM4 ARM Cortex-R4 Series | RM48xxx RM46xxx RM42xxx |
TI Product Page |
MSP430™ Ultra-Low Power 16-bit Microcontroller
| Device Series | Part # | Device List |
|---|---|---|
| All MSP430 Series | MSP430 | TI Product Page |
MSP432™ Cortex M4 Microcontroller
| Device Series | Part # | Device List |
|---|---|---|
| All MSP432 Series | MSP432 | TI Product Page |
Tiva™ ARM® Cortex™-M Microcontrollers
| Device Series | Part # | Device List |
|---|---|---|
| Tiva™ C Series MCUs | TM4Cx | TI Product Page |
| Tiva™ E Series MCUs | TM4Ex | N/A |
Wireless Connectivity CCxxxx Cortex™-M Devices
| Device Series | Part # | Device List |
|---|---|---|
| CC13xx | CC13xx | TI Product Page |
| CC253x | CC2538 | TI Product Page |
| CC26xx | CC26xx | TI Product Page |
| CC32xx/CC31xx | CC32xx/CC31xx | TI Product Page |
UCD Digital Power Controllers
| Device Series | Part # | Device List |
|---|---|---|
| UCD31xx | UCD31xx | TI Product Page |
PGA Sensor Signal Conditioners
| Device Series | Part # | Device List |
|---|---|---|
| PGA9xx | PGA9xx | TI Product Page |
mmWave Sensors
| Device Series | Part # | Device List |
|---|---|---|
| AWR | AWRxxxx | TI Product Page |
| IWR | IWRxxxx | TI Product Page |
Sitara and K2G
| Device Series | Part # | Device List |
|---|---|---|
| Sitara | AM335x AM437x AM571x AM572x AM574x K2G |
TI Product Page |
List of Communication Interface (Emulator) Support
- XDS100v2 and XDS100v3 Debug Probes (all manufacturers)
- XDS110 Debug Probe
- XDS200-class Debug Probes (all manufacturers)
- Stellaris In-Circuit Debug Interface (ICDI)
- MSP-FET430UIF (for MSP430 devices only)
- MSP-FET (for MSP430 devices only)
List of Supported File Types
Loading:
- TI COFF
- TI ELF
- Intel Hex
- Motorola S-Record
- Tektronix Hex
- TI-TXT
- Binary
Saving/Exporting:
- TI COFF
- Binary
Issues Reporting
Please report all bugs, issues and enhancement requests in the following forum: https://e2e.ti.com/support/development_tools/code_composer_studio/default.aspx
Where to Get Help
Read the Getting Started section
Please post questions about the product in the following forum: https://e2e.ti.com/support/development_tools/code_composer_studio/default.aspx
Known Issue(s)
| ID | Description | Targeted Release |
|---|---|---|
| N/A | On some C2000 devices, if the device is locked, a “Verify Image” operation will fail since it does not perform an unlock operation before it tries to reads/verify memory. A workaround is to keep the core connected, unlock the core by providing the correct password, and then executing the verify operation. | N/A |
| UNIFLASH-570 | On flash devices, it is recommnded that you do not load to both RAM and flash memory in the same program, as the RAM memory can be overwritten by RAM needed by the flash algorithm. | N/A |
| UNIFLASH-1309 | On some C2000 devices, clicking on “Fill Security Fields from Target” button may not reflect correct values for LINKPOINTERS | N/A |
| CCBT-2603 | On C2000 F28004x/F28002x devices, after programming any new DCSM setting, a lock/unlock GUI sequence will fail to unlock the device. A debug reset needs to be issued for the unlock to work. | N/A |
| BLPROG-01 | Serial port is not closed properly when an unsupported file format is loaded using MSP430, CC13xx, and CC26xx bootloader programming. This causes any operation on the serial port to become unresponsive. The workaround is to disconnect and reconnect the USB cable to reset the serial port connection. Note: The supported firmware image format for these devices are Intel Hex and TI TXT file format. | UniFlash 6.1 |
Release Archive
All released versions and download links are available HERE