10. Frequently Asked Questions¶
This chapter answers some of the frequently asked questions (FAQs) about CCStudio™ IDE.
- 10.1. General
- 10.1.1. Is CCStudio™ IDE based on VS Code?
- 10.1.2. What are the differences between the Theia IDE and VS Code?
- 10.1.3. What happened to CCStudio Theia and how is it different from CCStudio IDE 20.x+?
- 10.1.4. Does CCStudio IDE come with an AI Code Assistant?
- 10.1.5. Is my device supported by the new Theia IDE based CCStudio IDE?
- 10.1.6. Which operating systems are supported by CCStudio IDE?
- 10.1.7. Why do I need to avoid non-alphanumeric (unicode) characters in my paths?
- 10.1.8. Are non-alphanumeric (unicode) characters supported?
- 10.1.9. What kind of safety certification does CCStudio IDE have?
- 10.1.10. What is the best way to look up a bug?
- 10.1.11. Where can I get more information on CCStudio IDE?
- 10.2. Installation
- 10.3. Licensing
- 10.4. Updates
- 10.5. AI Assistants
- 10.5.1. What should I know about data privacy when using AI assistants with CCStudio IDE?
- 10.5.2. What actions are being done when the AI Assistant Configurator is used to enable AI support in CCStudio IDE?
- 10.5.3. Does CCStudio IDE provide free AI model access, or do I need my own?
- 10.5.4. Do I need to have git installed?
- 10.5.5. Can I use a different model provider other than the ones listed in the AI Assistant Configurator?
- 10.5.6. Is Copilot supported?
- 10.5.7. I get an error message saying Failed to configure AI assistant. Failed to install <Extension>.. How can I resolve this?
- 10.5.8. Claude Code chat is not finding my existing configuration. How can I resolve this?
- 10.5.9. Claude Code chat is slow on initial startup. How can I speed it up?
- 10.5.10. Claude Code chat is returning various 400/403 errors. How can I resolve this?
- 10.6. General IDE
- 10.6.1. I get a dialog box asking me Do you trust the authors of the files in this folder? when I open a workspace or folder. What does this mean and what should I select?
- 10.6.2. Can I use any VS Code extension?
- 10.6.3. What is this "ENOTFOUND" error when trying to browse for extensions?
- 10.6.4. How do I use the themes I installed as an extension?
- 10.6.5. I want to restart CCStudio IDE with a fresh environment. How do I do this?
- 10.6.6. I see constant references to "TI Cloud Agent" when running CCStudio IDE on my local environment. What is this and do I need it?
- 10.6.7. How do I start up CCStudio IDE with a specific workspace?
- 10.7. Projects
- 10.7.1. How do I create a new project from scratch?
- 10.7.2. The Project Wizard does not find any examples for my selected device. Does that mean that my device is not supported by CCStudio IDE?
- 10.7.3. During project build, a ccsLinker.opt file sometimes gets passed to the linker instead of the list of object files. What is this file and when is it used?
- 10.7.4. How can I improve build speed?
- 10.7.5. How can I resolve build error #10234-D: unresolved symbols remain?
- 10.7.6. The Eclipse WORKSPACE_LOC variable is not pointing to my workspace folder. How do I resolve this?
- 10.8. Debug
- 10.8.1. Why are my breakpoints greyed out even though they are enabled?
- 10.8.2. Why can't I source step?
- 10.8.3. How do I access the debugger/flash properties when in a debug session?
- 10.8.4. Which scripting solution (legacy or new) should I use?
- 10.8.5. I get Data Verification errors when loading my program. What does it mean?
- 10.8.6. Why isn't printf working when running code in CCStudio IDE?
- 10.8.7. Do I have to use an XDS110 debug probe to debug a secure device?
- 10.8.8. Is Pin Trace Supported?