10.1. General

10.1.1. Is CCStudio™ IDE based on VS Code?

Starting with version 20.0.0, CCStudio IDE™ leverages the Theia IDE open source software framework. Theia IDE is very similar to Visual Studio (VS) Code but there are some differences.

10.1.2. What are the differences between the Theia IDE and VS Code?

See: https://eclipsesource.com/blogs/2024/07/12/vs-code-vs-theia-ide/

10.1.3. What happened to CCStudio Theia and how is it different from CCStudio IDE 20.x+?

Please see FAQ #7 of: https://software-dl.ti.com/ccs/esd/CCSv20/#faq/

10.1.4. Does CCStudio IDE come with an AI Code Assistant?

Please see the AI Assistants chapter for more information.

10.1.5. Is my device supported by the new Theia IDE based CCStudio IDE?

The new Theia IDE based CCStudio IDE will support most of the devices supported by CCStudio IDE 12.x with the exception of the below device families:

  • C55x

  • CC32xx

  • DaVinci

  • OMAP

10.1.6. Which operating systems are supported by CCStudio IDE?

Please see the related section in the Overview chapter.

10.1.7. Why do I need to avoid non-alphanumeric (unicode) characters in my paths?

Prior to CCStudio IDE 20.4, paths with non-alphanumeric characters caused various project management, build, and debug issues. Hence it was recommended to avoid using non-alphanumeric characters in paths such as the installation path, workspace path, project path, and ccxml file path.

However, starting with version 20.4, CCStudio IDE now provides support for non-alphanumeric characters in various paths (with some caveats). Please see the related FAQ below for more information.

10.1.8. Are non-alphanumeric (unicode) characters supported?

Starting with version 20.4, the CCStudio IDE will provide some limited support for non-alphanumeric characters in various paths.

  • Windows: The option Use Unicode UTF-8 for worldwide language support must be enabled.

  • Linux: There is a known issue with version 20.4.x with launching a debug session if either the ccxml file or the CCStudio IDE installation path contains non-alphanumeric characters. This issue has been resolved in version 20.5.0.

  • macOS: There are no known issues with non-alphanumeric characters in paths beyond the limitation with the compiler mentioned below.

Warning

Note that older non-clang based TI compilers will not run if installed in a directory with non-alphanumeric characters in paths. If CCStudio IDE is installed in such a path, then of the compilers that come bundled with CCStudio IDE, only the clang based compilers will work. The workaround is to install standalone versions of the older non-clang based compilers in paths without non-alphanumeric characters.

10.1.9. What kind of safety certification does CCStudio IDE have?

The overall CCStudio IDE environment does not have safety certificate documentation. In general, when attempting to meet these types of certifications, it is specific tools like the compiler that are required to meet the specified standards.

The Safety Compiler Qualification Kit was developed to assist customers in qualifying their use of the TI ARM, C6000, C7000 or C2000/CLA C/C++ Compiler to functional safety standards such as IEC 61508 and ISO 26262.

10.1.10. What is the best way to look up a bug?

Visit the TI Bug and Enhancement System. Enter the bug ID in the search box on the upper right. If the search fails, please surround the bug ID with "quotes" and try again.

10.1.11. Where can I get more information on CCStudio IDE?

All users are recommended to explore the CCStudio™ IDE Academy for additional information.

10.2. Installation

10.2.1. Can I install multiple versions of CCStudio IDE on my computer?

Yes. Multiple versions of CCStudio IDE can be installed on the same machine as long as they are installed in different directories.

10.3. Licensing

10.3.1. What is the licensing policy for CCStudio IDE?

There is no license fee associated with CCStudio IDE. Users are free to download and install CCStudio IDE without having to purchase a license.

For more details on the license, please refer to Licensing chapter.

10.4. Updates

10.4.1. How do I get updates to CCStudio IDE?

Please refer to the Updating CCStudio IDE section.

10.5. AI Assistants

10.5.1. What should I know about data privacy when using AI assistants with CCStudio IDE?

CCStudio IDE processes your code and queries locally. When you send queries to an AI assistant, the data handling depends on your configuration:

  • Third-Party Providers: Your queries and code are transmitted to the third-party AI model provider you have configured (such as Anthropic, OpenAI, or others). Texas Instruments does not act as an intermediary in these communications.

  • Locally Hosted Models: If you configure a locally hosted AI model, your queries and code remain on your local network and are not sent to external providers, providing enhanced data privacy.

For comprehensive details about data flow, privacy considerations, and information about locally hosted models, please refer to the Data Privacy and Information Handling section in the AI Assistants chapter.

10.5.2. What actions are being done when the AI Assistant Configurator is used to enable AI support in CCStudio IDE?

While the exact actions can vary depending on the agent and provider selected, the following actions are typically done:

  • The necessary extension for the selected AI agent is installed if it is not already installed.

  • The necessary connection settings for the selected AI agent are applied. This may include settings such as API keys, model provider URLs, and other relevant settings.

  • (If selected), the CCStudio IDE MCP servers are configured and enabled to allow the selected AI support to connect to the AI model provider and function properly. Note that MCP servers are only enabled when CCStudio IDE is running. It is automatically started when CCStudio IDE starts and automatically stopped when CCStudio IDE is closed.

  • The agent is granted permission to the paths of all discovered products and compilers shown in the CCStudio IDE Settings. This allows the agent to access the necessary SDK/product files and resources to provide relevant responses to user queries.

10.5.3. Does CCStudio IDE provide free AI model access, or do I need my own?

You must have existing access to an AI model — whether through a subscription, API key, or other means. Texas Instruments does not provide any AI model access, API keys, subscriptions, or credentials for any providers.

10.5.4. Do I need to have git installed?

Yes. Git is required for supported AI agents to manage the local repository that it uses to store the conversation history and other relevant data. If Git is not installed, the agent will not be able to function properly. Please install Git and make sure it is added to your system's PATH environment variable.

10.5.5. Can I use a different model provider other than the ones listed in the AI Assistant Configurator?

Note that while agents such as Claude Code are designed to use specific models (i.e. Anthropic models for Claude Code), it is possible to use models from other vendors with supported agents in CCStudio IDE using workarounds via LLM proxy and routers such as LiteLLM and OpenRouter.

Another option is to use an agent such as Cline, which is designed to work with multiple model providers. A Cline extension is available in the Open VSX Registry, allowing you to use it directly within CCStudio IDE.

10.5.6. Is Copilot supported?

Not directly. Copilot is not supported by the AI Assistant Configurator and integrating the associated VS Code Copilot extension directly into CCStudio IDE is currently not possible.

However, there are workarounds. It is possible to have Copilot interact with CCStudio IDE from the Copilot CLI. See the Copilot secton of this article for an example video.

It is also possible to connect the recommended Claude Code extension to GitHub Copilot models using an LLM proxy such as LiteLLM. For further details please refer to the document: Using GitHub Copilot Models with Claude Code in CCStudio™ IDE via LiteLLM.

Using CCStudio for VS Code is another option if your device is supported. Since it plugs into your existing VS Code environment, native Copilot support can be used.

10.5.7. I get an error message saying Failed to configure AI assistant. Failed to install <Extension>.. How can I resolve this?

The most common reason for this error is that the IDE was unable to download the extension from the Open VSX registry. If running on a network that requires a proxy server to access the internet, make sure the CCStudio IDE proxy settings are properly configured.

10.5.8. Claude Code chat is not finding my existing configuration. How can I resolve this?

If you have an valid existing configuration for Claude Code chat but it is not being detected, try closing and reopening the Claude Code chat view. If that does not work, try restarting CCStudio IDE. If the issue persists, try reapplying the configuration settings in the AI Assistant Configuratior view and then restart CCStudio IDE.

10.5.9. Claude Code chat is slow on initial startup. How can I speed it up?

The initial startup of the Claude Code chat may take some time as it needs to initialize the connection to the AI model provider and set up the necessary resources for the chat functionality. To speed up the initial startup, ensure that you have a stable and fast internet connection, as this can help reduce the time it takes to establish the connection to the AI model provider.

Another suggestion is to disable telemetry and other non-essential data collection using one of the following environment variables:

  • CLAUDE_CODE_DISABLE_NONESSENTIAL_TRAFFIC=1: This variable is a comprehensive option that disables all non-essential traffic, including operational metrics (telemetry), error reporting (Sentry), and the /bug command.

  • DISABLE_TELEMETRY=1: This variable specifically targets the operational metrics sent to the Statsig service, which logs latency, reliability, and usage patterns without including code or file paths.

10.5.10. Claude Code chat is returning various 400/403 errors. How can I resolve this?

If you are encountering 400/403 errors when using the Claude Code chat, it is likely due to an issue with the API key or the permissions associated with the API key. Other possible reasons for this error are issues with the Claude Code extension or issues with the connection to the AI model provider.

Some steps to try to resolve this issue include:

  • DISABLE_PROMPT_CACHING=1: This variable disables prompt caching, which can help resolve issues related to stale or corrupted cached prompts that may be causing errors.

  • CLAUDE_CODE_DISABLE_EXPERIMENTAL_BETAS=1: This variable disables experimental beta features in the Claude Code extension, which can help resolve issues that may be caused by bugs or instability in these features.

If issues still occur, rolling back to an older version of the Claude Code extension may help resolve the issue if it is caused by a recent update to the extension. To do this, go to the Extensions view in CCStudio IDE, search for "Claude Code", click on the extension in the search results, and press the "gear" button next to the Uninstall button and select the Install Specific Version... open in the menu to select an older version of the extension to install.

10.6. General IDE

10.6.1. I get a dialog box asking me Do you trust the authors of the files in this folder? when I open a workspace or folder. What does this mean and what should I select?

When a folder is opened in CCStudio IDE for the first time, a trust dialog will appear as below:

_images/ccs_workspace-trust.png

Please see the Workspaces section for more information.

10.6.2. Can I use any VS Code extension?

Not all VS Code extensions are compatible with Theia IDE, which CCStudio IDE is based on. The ones that are published to Open VSX are supported by Theia IDE and validated by the extension author. VS Code extensions that have been downloaded from the Visual Studio Code Market may be installed in CCStudio IDE, but there is no guarantee that they are compatible. One thing to look for is to check the API requirement for the extension and compare it with the VS Code API version in the Help → About dialog in CCStudio IDE.

10.6.3. What is this "ENOTFOUND" error when trying to browse for extensions?

If CCStudio IDE is unable to access the internet when browsing for extensions, the below error can occur:

_images/ccs_faq-extensions-proxy.png

Check your internet access. If the issue is specific to just CCStudio IDE and you are on an internal network that requires the use of a proxy server to access the internet, check the proxy settings in CCStudio IDE.

10.6.4. How do I use the themes I installed as an extension?

The color theme can be configured by going to File > Preferences > Color Theme. The themes that you have installed as extensions should appear in the list of available themes.

10.6.5. I want to restart CCStudio IDE with a fresh environment. How do I do this?

CCStudio IDE caches many files in the user's home folder. To clear these caches. delete:

Windows:

  • [USER HOME]\AppData\Local\Texas Instruments\CCS\.ccs-server

  • [USER HOME]\AppData\Local\Texas Instruments\CCS\[CCS INSTALL FOLDER NAME]

Linux:

  • [USER HOME]/.config/Texas Instruments/CCS/.ccs-server

  • [USER HOME]/.config/Local/Texas Instruments/CCS/[CCS INSTALL FOLDER NAME]

macOS:

  • [USER HOME]/Library/Application Support/Texas Instruments/CCS/.ccs-server

  • [USER HOME]/Library/Application Support/Texas Instruments/CCS/[CCS INSTALL FOLDER NAME]

Clearing these caches can also be helpful to resolve instability issues with the IDE.

Deleting additional debug cache files can also help resolve issues with debug instability. See Delete Debug Cache Files for more information.

Note that the default workspace folder workspace_ccstheia can also be found in the user's home folder. The workspace folder contains the projects imported to workspace in addition to the .theia/launch.json and .theia/settings.json file for the workspace. Deleting this folder would delete the projects contained within, hence you may want to back up your projects first. Another option is to just delete the .theia folder inside the workspace folder.

Warning

Deleting these caches will restore the IDE back to the original default state. Any custom user settings will be lost.

10.6.6. I see constant references to "TI Cloud Agent" when running CCStudio IDE on my local environment. What is this and do I need it?

TI Cloud Agent is a small local application that manages the communication between the host computer and the TI hardware devices for a variety of tools such as CCStudio IDE Desktop and Cloud IDE, UniFlash, GUI Composer, etc. Despite the name, it is not a cloud-based application and runs locally on the user's machine.

10.6.7. How do I start up CCStudio IDE with a specific workspace?

CCStudio IDE will start up with the last workspace used. For new installations, the default workspace is typically set to a folder named "workspace_ccstheia" in the user's home directory. To start up CCStudio IDE with a specific workspace, you can use the command line to run the CCStudio IDE executable (in [CCS INSTALL DIR]\ccs\theia) and specify the path to the desired workspace.

Example:

C:\ti\ccs2050\ccs\theia\ccstudio.exe C:\path\to\my\workspace_folder

10.7. Projects

10.7.1. How do I create a new project from scratch?

Starting with version 21.0.0, it is possible to create a new project from "scratch" with the Create a new empty project wizard. Please see Creating a New Empty CCStudio IDE Project.

New Static Library and System projects can also be created with this wizard.

10.7.2. The Project Wizard does not find any examples for my selected device. Does that mean that my device is not supported by CCStudio IDE?

The Project Wizard will only show examples from SDKs that are available from Resource Explorer. If an SDK is not available from Resource Explorer, then no example projects will be found. This does not necessarily mean that your device is not supported by CCStudio IDE, just that there are no available SDK examples from Resource Explorer. An existing project local to the user's environment will need to be manually imported.

10.7.3. During project build, a ccsLinker.opt file sometimes gets passed to the linker instead of the list of object files. What is this file and when is it used?

The ccsLinker.opt file is generated by CCStudio IDE and passed to the linker if the list of linker options and input files on the linker command line exceeds the maximum command line length of the host operating system. A project with a large number of object files (.obj) may pass the linker options and input files to the linker via the ccsLinker.opt file rather than directly on the command line.

10.7.4. How can I improve build speed?

Build speed can be affected by many factors such as the size of the project, the number of files being built, the performance of the machine, and other software running on the machine.

One of the biggest bottlenecks are antivirus/security and/or disk encryption software running on the machine. However, it is often not possible to disable these types of software due to company policies. One workaround is to add the CCStudio IDE installation folder and workspace folder to the exclusion list of the antivirus/security software.

Another thing that can help is to set the build output to minimal. This can be done from the CCStudio IDE Settings. See the information on Build-output verbosity.

10.7.5. How can I resolve build error #10234-D: unresolved symbols remain?

This article contains more information about the error and how to resolve it.

In summary, the error is generated by the linker when it is unable to find the definition for the symbol. This typically happens if an object file or library containing the definition for the symbol was not provided to the linker. The build output in the CCS build console should provide information on which object files and libraries are passed to the linker.

To resolve the error, locate the source file or library that contains the definition for the symbol and make sure that it is part of the project.

10.7.6. The Eclipse WORKSPACE_LOC variable is not pointing to my workspace folder. How do I resolve this?

WORKSPACE_LOC points to the default .metadata location (ex. on Windows: [USER HOME]\AppData\Local\Texas Instruments\CCS\.ccs-server\workspace) and not the folder that contains your projects (ex. workspace_ccstheia). Note that while this is the case in CCStudio IDE Theia, CCStudio IDE Eclipse worked differently in that both .metadata and project folders typically resided in the same "workspace" folder. This difference is important to keep in mind when importing CCStudio IDE Eclipse projects to CCStudio IDE Theia since some CCStudio IDE Eclipse projects will use WORKSPACE_LOC with the expectation that it is pointing to the root folder location of the CCStudio IDE projects copied to the workspace folder. WORKSPACE_LOC should be replaced with the new CCS_WORKSPACE_DIR variable in CCStudio IDE Theia since this variable points to the folder containing your projects.

10.8. Debug

10.8.1. Why are my breakpoints greyed out even though they are enabled?

If a breakpoint appears as greyed out in the Breakpoints View, this indicates that the debugger set the breakpoint but was unable to activate it. This is commonly due to a lack of hardware breakpoint resources. To confirm this, hover over the checkbox for the breakpoint and check to see if a pop-up message such as the one below appears:

_images/ccs_faq-breakpoint-grey.png

10.8.2. Why can't I source step?

If you are unable to source step, check the Debug Output View to see if error messages such as the below appear:

  • Breakpoint Manager: There are not enough resources available

  • Breakpoint Manager: _JobHardwareBreakpoint::ARM_DEBUG_V6M_bpu_add_breakpoint: FPB : All resources are in use.[22062]

If so, then the reason why source stepping is not working is because many source stepping operations require a hardware breakpoint resource and there are no more available resources. Please disable/remove some existing breakpoints or disable other tools that may be using a breakpoint like the Profile Clock.

10.8.3. How do I access the debugger/flash properties when in a debug session?

See: Debug Properties.

10.8.4. Which scripting solution (legacy or new) should I use?

A new scripting solution (CCS Scripting) is available. Both the legacy (DSS) and the new scripting (CCS Scripting) solution is available for use. New users have the option to use either. Since DSS has been deprecated in support, new users are recommended to use CCS Scripting.

10.8.5. I get Data Verification errors when loading my program. What does it mean?

See this article on Data Verification Errors

10.8.6. Why isn't printf working when running code in CCStudio IDE?

Two common errors are running out of heap, and running out of stack. For other errors that cause printf to fail, and how to address them, please see the article Tips For Using Printf.

10.8.7. Do I have to use an XDS110 debug probe to debug a secure device?

Yes. Only the XDS110 is capable of handling the secure debug features on supported devices such as CC234x and CC27x5.

10.8.8. Is Pin Trace Supported?

Pin trace is no longer supported. See the Trace section for more details on the types of core trace supported.