8.8.1.1.2.2.17. Target¶
- class Target¶
- connect() None¶
Connect or reconnect the debugger to the target.
# connects and disconnects from the target session.target.connect() session.target.disconnect()
- Return type:
None
- disconnect() None¶
Disconnect the debugger from the target
# connects and disconnects from the target session.target.connect() session.target.disconnect()
- Return type:
None
- isConnected() bool¶
Query if the target is connected
session.target.connect() status = session.target.isConnected() # will be True session.target.disconnect() status = session.target.isConnected() # will be False
- Return type:
bool
- getResets() dict[str, bool]¶
Query the target's available reset types. These can be performed using
reset()# Get a list of the resets which can currently be performed resets = session.target.getResets() # This might look like # resets = { # "CPU Reset": True, # "Board Reset": False # } allowedResets = [reset for reset, allowed in resets.items() if allowed] # allowedResets = ["CPU Reset"]
- Returns:
A mapping where the keys are the reset types, and the associated values indicate whether it is currently valid to issue a reset of this type.
- Return type:
dict[str, bool]
- reset(resetType=None) None¶
Issue the specified reset on the target
# Issue the System Reset (possible reset types vary by target) session.target.reset("System Reset")
- Parameters:
resetType (str) -- (optional) The type of reset to be issued. If not provided, the default reset is issued. You can query the available resets using
getResets()- Return type:
None
- run(waitForHalt=None) None¶
Issue a run command to the target, and wait until it has halted.
# run to foo session.breakpoints.add("foo") session.target.run() # run and return once the target is running session.target.run(False)
- Parameters:
waitForHalt (bool) -- (optional) Whether the command should wait until the target halts. Defaults to true.
- Return type:
None
- halt() None¶
Halt the target.
session.target.halt()
- Return type:
None
- waitForHalt() None¶
Waits until the target has halted for any reason.
# run the target and separately wait until it is halted session.target.run(False) session.target.waitForHalt()
- Return type:
None
- isHalted() bool¶
Query if the target is halted.
session.target.halt() status = session.target.isHalted() # will be True session.target.run(False) status = session.target.isHalted() # will be False
- Return type:
bool
- stepInto(explicitlyAsm=None) None¶
Steps the target, stepping into function calls. Returns once the step operation is completed and the target is once again halted.
If symbol information is loaded for the location at which the target is currently halted, then a source step is performed. Otherwise, or if explicitly ordered to do so, an assembly step is performed.
# source step into (assuming symbol information is loaded for the target's current location) session.target.stepInto() # explicit assembly step into session.target.stepInto(True)
- Parameters:
explicitlyAsm (bool) -- (optional) If true, an assembly step into operation will always be performed regardless of loaded symbols. Defaults to false.
- Return type:
None
- stepOver(explicitlyAsm=None) None¶
Steps the target, stepping over function calls. Returns once the step operation is completed and the target is once again halted.
If symbol information is loaded for the location at which the target is currently halted, then a source step is performed. Otherwise, or if explicitly ordered to do so, an assembly step is performed.
# source step over (assuming symbol information is loaded for the target's current location) session.target.stepOver() # explicit assembly step over session.target.stepOver(True)
- Parameters:
explicitlyAsm (bool) -- (optional) If true, an assembly step over operation will always be performed regardless of loaded symbols. Defaults to false.
- Return type:
None
- stepOut() None¶
Steps the target, stepping out of the current function. Returns once the step operation is completed and the target is once again halted.
session.target.stepOut()
- Return type:
None
- restart() None¶
Restart the target.
A restart sets the PC to the entry point, calls the OnRestart GEL callback, and, if configured in the settings, runs to a label (usually main). Returns once the step operation is completed and the target is once again halted.
session.target.restart()
- Return type:
None