8.8.1.1.2.2.12. Registers

class Registers
getRegisterGroups(groupId) → RegistersGroupsResult

Returns the registers and groups under the specified group.

# Reads the top level groups
topLevel = session.registers.getRegisterGroups()
# Reads the registers and subgroups of group "adc0"
adc0 = session.registers.getRegisterGroups("adc0")
groups, registers = adc0['groups'], adc0['registers']

# One can build an object representing the whole register tree recursively calling this
# The 'root' parameter is the id of top level group to start from
def queryRegisterTree(session, root):
       children = session.registers.getRegisterGroups(root)
       groups = { grp['name']: queryRegisterTree(session, grp['id']) for grp in children['groups'] }
       regs = { reg['name']: reg for reg in children['registers'] }
       return { 'groups': groups, 'registers': regs }

registerTree = queryRegisterTree(session, 'adc0')
Parameters:

groupId (str | None) -- The id of the group to fetch the subgroups of. If unset or is ""(empty string), fetch the root groups.

Returns:

Two lists of registers and groups under the specified group, or a list of the top level groups and empty list if groupId is blank.

Return type:

RegistersGroupsResult

getBitfields(registerId) → list[RegisterBitfield]

Returns the bitfields under a register.

# get the bitfields of the register 'adc0_ADC0_SCOMP1'
scopm1 = session.registers.getBitfields('adc0_ADC0_SCOMP1')
print(f"id: {scopm1['id']}")
print(f"name: {scopm1['name']}")
print(f"start: {scopm1['start']}")
print(f"end: {scopm1['end']}")
print(f"readable: {scopm1['readable']}")
print(f"writable: {scopm1['writable']}")
Parameters:

registerId (str) -- The id of the register whose bitfields will be fetched.

Returns:

A list of the bitfields, each entry containing the id, name, start and end of the bitfield, and whether it is readable/writable.

Return type:

list[RegisterBitfield]

read(registerName) → int | str

Reads the specified register.

# Reads the PC register
value = session.registers.read("PC")
Parameters:

registerName (str) -- The name of the register to be read.

Returns:

The value of the register.

Return type:

int | str

write(registerName, value) → None

Write to the specified register.

# Writes 0x12345 to the PC register
session.registers.write("PC", 0x12345)
# Writes -1 to the R0 register
session.registers.write("R0", -1)
Parameters:
  • registerName (str) -- The name of the register to be written to.

  • value (int | str) -- The value to be written to the register. Can be an integer, or an integer represented as a string. When using JavaScript, both standard (floating point) numbers and BigInts are accepted. The latter is recommended to avoid accuracy issues with large values.

Return type:

None

exportAsJson(groupIds, filePath, style=None) → None

Recursively reads all the register under the specified group and returns the data in a tree structure.

# Export the core registers and the group "adc0" to "/user/dump.json"
session.registers.exportAsJson(["Core Registers", "adc0"], "/user/dump.json")

# Export the core registers to "/user/dump.json" in one line
session.registers.exportAsJson("Core Registers", "/user/dump.json", False)
# equivalently
session.registers.exportAsJson([""], "/user/dump.json")

# Export all the registers to "/user/dump.json" in styled format
session.registers.exportAsJson("", "/user/dump.json", True)
Parameters:
  • groupIds (list[str]) -- The ids of the groups to read registers from. Can be a single id, or an array of ids. Use ""(empty string) to read all the groups.

  • filePath (str) -- The full path of the file to write the data to.

  • style (bool) -- (optional) If true, write the data string in a tree structure. If false, write the data string in one line. Default is false.

Return type:

None

importFromJson(filePath) → None

Recursively writes all the register under the specified group from a file.

# Import from "/user/dump.json"
session.registers.importFromJson("/user/dump.json")
Parameters:

filePath (str) -- The full path of the file to write the data to.

Return type:

None