7.5.4. List of importProject Options

Note that the available options can vary depending on the CCStudio™ IDE version used. For the list of options available for your specific CCStudio™ IDE version, run the command with the '-ccs.help' option:

ccs-server-cli -noSplash -workspace "<workspace_dir>" -application com.ti.ccs.apps.projectImport -ccs.help

Full list of projectImport options:

-ccs.location '<path>'
        Absolute or relative path to the location containing the project.
        Relative paths will be assumed to be relative to the working directory.

-ccs.device <id>
        The device-variant ID. Applicable only when '-ccs.location' flag resolves to a .projectspec file.

-ccs.definePathVariable <name> <value> [@scope (global|project)]
        Defines the given path-variable for resolving portable linked file paths (optional)
        (also defines a global build-macro with the same name and value).
        Optionally, specify the scope (defaults to 'global').

-ccs.copyIntoWorkspace
        Copy project folder and contents into the workspace directory (optional).
        Defaults to 'false'.

-ccs.renameTo <name>
        Rename the imported project to the specified name.

-ccs.overwrite
        Forces overwrite of existing file-system resources (optional).

-ccs.autoBuild
        Performs an incremental build on the imported/created project (optional).

-ccs.autoImportReferencedProjects
        If 'true', an attempt is made to automatically import any referenced projects found in the same parent directory as the main project.

-ccs.autoRenameReferencedProjects
        If 'true', and iff the '-ccs.renameTo' flag is present, any imported referenced projects will also be renamed automatically.

-ccs.referencedProjectSearchDirectory
        Directory to search for referenced projects. Applicable only when '-ccs.autoImportReferencedProjects' flag is present.

-ccs.captureCopiedFileOrigins
        Capture the original locations of all resources copied into the project during the import. These will be captured into a text file named 'copiedFileOrigins.txt'.

-ccs.captureProjectspecApplicability
        Capture the list of devices that the imported projectspec is applicable to. These will be captured into a text file named 'projectSpecApplicability.txt'.

-ccs.defaultImportDestination '<dir>'
        Default import-destination. This is the workspace where user-projects will be created/imported by default.

-ccs.args '<file>'
        File containing any extra arguments (optional).

-ccs.help
        Print this help message.