7.5.3. List of buildProject Options

Note that the available options can vary depending on the CCStudio™ IDE version used. For the list of options available for your specific CCStudio™ IDE version, run the command with the '-ccs.help' option:

ccs-server-cli -noSplash -workspace "<workspace_dir>" -application com.ti.ccs.apps.projectBuild -ccs.help

Full list of projectBuild options:

-ccs.projects [<name> ]+
        Space-separated list of project-names to build.

-ccs.locations [<path> ]+
        Space-separated list of locations to build.

-ccs.workspace
        Build entire workspace.

-ccs.buildType (incremental | full | clean)
        The type of build to perform (optional).
        Defaults to 'incremental'.

-ccs.configuration <name>
        The build-configuration to build (optional).
        Defaults to active build-configuration.

-ccs.listErrors
        List all errors after build completes (optional).

-ccs.listProblems
        List all errors and warnings after build completes (optional).

-ccs.autoImport
        Automatically import projects at their original locations (optional).

-ccs.autoOpen
        Automatically open any closed projects (this option has been deprecated and has no effect).

-ccs.defaultImportDestination '<dir>'
        Default import-destination. This is the workspace where user-projects will be created/imported by default.

-ccs.args '<file>'
        File containing any extra arguments (optional).

-ccs.help
        Print this help message.