11.1. Installation

11.1.1. General Tips for Installing Code Composer Studio™

  • Clean out all prior failed or incomplete installations (by deleting the install directory) before attempting a new one to the same directory.

  • If possible, disable anti-virus/security software (certain such software are known to cause problems).

  • It is recommended to have a username that does not have any non-alphanumeric characters, and that you are installing Code Composer Studio to a directory that does not have any non-alphanumeric characters.

11.2. General IDE

11.2.1. Delete Workspace Cache

Code Composer Studio caches various user information in separate folders located in the user's home directory. The contents of this folder can get corrupted over time, causing various instability and strange behavior with the IDE. Clearing this cache can help resolve these issues.

Warning

Deleting this cache will restore the IDE back to the original default state. Any custom user settings will be lost.

11.2.2. Unable to Connect to the Internet

If Code Composer Studio is running on a network that requires a proxy server to access the internet, it may be required to set the proxy settings for Code Composer Studio. This can be done from the General Settings:

_images/ccs_ts-proxy.png

An alternative to the above is to set the http_proxy and/or https_proxy system environment variables instead. Code Composer Studio will use the value of those variables if one is not set in the General Settings.

11.2.3. Poor Performance with Multiple XDS110 Debug Probes Connected

When multiple XDS110 debug probes are connected to the same system, there may be performance issues with auto-detect. This can cause performance degradation in various parts of the IDE, including debug launch. To resolve this issue, it is recommended to disconnect any unnecessary XDS110 debug probes from the system. Another option is to disable auto-detect with the Detect Probe On Launch setting in the General Settings under Extensions → CCS.

11.3. Resource Explorer

11.3.1. Check your Internet Connection

A poor internet connection may cause Resource Explorer to timeout when attempting to sync with the server. Try again when you have more bandwidth available.

11.3.2. Check the Proxy Setting

If Resource Explorer is unable to connect to the internet it may be an issue with the proxy settings. Check that your proxy settings in Code Composer Studio and for the system.

11.3.3. No Content Displayed

There is a known limitation with Resource Explorer inside the Code Composer Studio IDE not being able to display certain content properly or at all. The root cause is often not Resource Explorer itself but the internal web browser that is used by the IDE. If this happens, navigate to the relevant node in the left panel and then choose the option to Open in System Browser. This will open the page outside of the IDE in your default system web browser.

_images/ccs_ts-rex-system-browser.png

In some cases, an additional message will appear explicitly mentioning that the content must be opened in an external browser (such as above), while in other cases it will simply display invalid content. Regardless, the Open in System Browser button should be available in the upper right corner if the correct node is selected.

11.3.4. Video Playback Error

There is a known limitation with Resource Explorer inside the Code Composer Studio IDE not being able to playback certain video formats. This is common with many videos from the TI video library

_images/ccs_ts-rex-system-browser-codec.png

The root cause and workaround is the same as mentioned in the "No Content Displayed" FAQ above.

11.4. Projects

11.4.1. Unable to Build or Debug Projects

If the option to build or debug a project is unavailable, try restarting Code Composer Studio.

11.4.2. Project Build Hangs

If the build appears to hang or get "stuck, try clearing the following folders from the <CCS INSTALL DIR>/ccs/eclipse/configuration directory:

  • org.eclipse.core.runtime

  • org.eclipse.equinox.app

  • org.eclipse.osgi

11.5. Debug

11.5.1. Delete the Launch Configuration

Invalid information in the launch.json file can cause issues with the debug session. Clearing the contents of this file (or deleting it completely) can help resolve these issues.

11.5.2. Delete Debug Cache Files

Code Composer Studio caches various user information in separate folders located in the user's home directory. The contents of this folder can get corrupted over time, causing various instability and strange behavior with the IDE. Clearing this cache can help resolve these issues.

Warning

Deleting this cache will restore the IDE back to the original default state. Any custom user settings will be lost.

11.5.3. JTAG Connectivity Issues

If an error occurs during the process of launching the debugger or any JTAG-specific issues, see: Debugging JTAG Connectivity Problems.

Warning

If running Code Composer Studio on a Linux host, please make sure the driver install script is run as superuser using sudo after installation. See: Post Installation Step

11.5.4. Data Verification Issues

If a data verification error occurs when loading a program, see: Troubleshooting Code Composer Studio - Data Verification Errors.

11.5.5. Unable to Enable Trace

If the options to enable trace are unavailable, check the status of the Trace Server in the Trace view. It may be offline. If so, please restart Code Composer Studio.

11.5.6. Flash programming fails with Target did not enter SACI after pin reset error

This issue will occur when attempting to flash a program on a device with secure debug features using a non-XDS110 based debug probe. To resolve this issue, use an XDS110 based debug probe.

11.5.7. Debug launch fails with No matching COM port found error

It is unknown what the exact cause of this issue is. However, a workaround is to disable auto-detect with the Detect Probe On Launch setting in the General Settings under Extensions → CCS.

11.6. Getting Support

If the troubleshooting tips mentioned above do not help resolve the issue, please check the Support dialog under Help → Support for a link to the support forum and access to diagnostic logs.

_images/ccs_ide-support.png