3.1. Important Installation Information

3.1.1. Installation Types

Currently Code Composer Studio™ has a single installer package that includes core components. Additional device support, which can include Chip Support Packages, CGTs and SDKs, can be installed once your device is selected (if applicable).

3.1.2. System Requirements

Each version of Code Composer Studio describes its list of System Requirements. If your system does not meet these requirements you may experience poor performance, or the inability to run the application.

The System Requirements section in the Overview chapter has more information on the requirements for this release.

3.1.3. Security Software

During the installation of Code Composer Studio there may be packages downloaded from the internet and installed. Some anti-virus and security software detects this and will block the installation. As a result it is recommended that such software be disabled during installation of Code Composer Studio Theia. This is not a requirement but if the installation fails it is recommended to try again with the security software disabled.

3.1.4. Permissions

Depending on what debug probes are selected during installation there will be device drivers that need to be installed on the system. In order to complete this step the appropriate permissions on the system will be required. On Linux this involves running an installation script as sudo at the end of the installation.

3.1.5. Unicode Characters

Code Composer Studio supports environments using unicode characters in various folder names, with some caveats. Please see the FAQ on unicode support for more information.

3.2. Installation Process

Overall the installation process is the same across Windows, Linux and macOS. Where there are differences this will be noted in the installation steps.

3.2.1. Download

The installation images for Code Composer Studio can be obtained form the below site:

3.2.2. Running the Installer

Note that most of the installers are provided inside archive files such as a zip file. It is necessary to extract the archive file before proceeding with installation.

For Linux users it is recommended to install as a normal user and not sudo/root.

3.2.2.1. Dependencies

The Code Composer Studio installation is dependent on other software packages. For Windows and macOS users these packages will be installed automatically as part of the installation. For Linux users the installer will attempt to identify which packages are missing and display this list. See the System Check section below for more information.

3.2.3. Steps

3.2.3.1. License Agreement

The end user license agreement is displayed. The agreement can be printed if desired. The license agreement must be accepted to continue.

End User License Agreement

3.2.3.2. System Check

The installer will check the system to see if it meets the requirements for installation. Any issues that need to be addressed will be displayed. Disabling security software is recommended but optional.

Example on Windows host OS:

System Check (Windows)

Example on Ubuntu 22.04 LTS host OS:

System Check (Linux)

Please exit the installer and resolve any missing dependencies before trying again.

Note that some dependencies are optional and only required for specific use cases:

  • libpython3.9.so.1.0 is only required when working with mmWave radar sensor devices. Otherwise this dependency can be ignored.

  • libtinfo.so.5 is only required when using older versions of the TI Arm Clang Compiler. See the section below for more information. Note that the dependency check for this library may not occur with more recent Code Composer Studio versions that come with newer versions of the TI Arm Clang Compiler.

  • libusb-0.1.so is only required if a non-XDS110 debug probe is being used. Otherwise this dependency can be ignored.

  • libc6-i386 is only required when trying to install additional older compilers that use a 32-bit installer. Otherwise this dependency can be ignored.

3.2.3.2.1. Ubuntu 24.04

Note that Ubuntu 24.04 comes with libtinfo6. Older versions of the TI Arm Clang Compiler before 4.x requires libtinfo5, which is obsolete with Ubuntu 24.04. This package can be obtained from the Ubuntu 22.04 package repo and the .deb file can be installed manually. Note that Code Composer Studio 20.4.0 and later versions come with TI Arm Clang Compiler 4.x, which does not require libtinfo5, so this dependency can be ignored if you are installing Code Composer Studio 20.4.0 or later and do not plan to install older versions of the TI Arm Clang Compiler.

3.2.3.3. Installation Location

Choose a location to install Code Composer Studio. This location must not already contain a Code Composer Studio or Code Composer Studio installation. If multiple versions of Code Composer Studio or Code Composer Studio will be installed then it is recommended to install them in versioned folders.

Location for installation

3.2.3.4. Device Support

Choose the desired device families to install support for.

Device support selection

3.2.3.5. Progress

As the installation proceeds the progress screen will show what the installer is doing. Depending on how many device families were selected the installation may take a significant amount of time.

Installation progress bar

3.2.3.6. Completion

The last screen shown during installation is the successful completion screen. This screen provides options to launch Code Composer Studio and create a desktop shortcut.

Installation complete

The dialog will look different on Linux hosts, with an additional message regarding an additional step needed to enable the drivers for the debug probes.

Installation complete (Linux)

3.2.3.7. Post Installation Step (Linux Only)

If Code Composer Studio was installed as user, then it is necessary to run the driver install script after the installation is complete. Run <CCS_INSTALL_DIR>/ccs/install_scripts/install_drivers.sh with sudo as instructed by the installer.

install_drivers.sh

Warning

This step is essential not only to support debugging, but also to run the IDE on current Ubuntu environments. DO NOT SKIP THIS STEP!

3.2.3.7.1. Ubuntu 24.04

Note

The following steps are not required if the install_drivers.sh script is successfully executed.

If Ubuntu 24.04 is being used, the following additional steps may be required:

Browse to: <CCS_INSTALL_DIR>/ccs/theia and run the following commands:

sudo chown root chrome-sandbox
sudo chmod 4755 chrome-sandbox

3.3. Uninstalling Code Composer Studio

To uninstall Code Composer Studio: exit Code Composer Studio, navigate to <CCS_INSTALL_DIR>/ccs directory, and run the uninstall_ccs executable.

3.4. Command Line Installation

To install Code Composer Studio from the command line, run the installer executable with the desired options. The available options are listed below:

Usage:

--help                                      Display the list of valid options

--version                                   Display product information

--unattendedmodeui <unattendedmodeui>       Unattended Mode UI (only when running in unattended mode)
                                             Default: none
                                             Allowed: none minimal minimalWithDialogs

--optionfile <optionfile>                   Installation option file
                                             Default:

--debuglevel <debuglevel>                   Debug information level of verbosity
                                             Default: 2
                                             Allowed: 0 1 2 3 4

--mode <mode>                               Installation mode
                                             Default: [Run with --help to see os-specific default]
                                             Allowed: [Run with --help to see os-specific default] unattended

--debugtrace <debugtrace>                   Debug filename
                                             Default:

--enable-components <enable-components>     Comma-separated list of components
                                             Default: PF_AM13X,PF_SITARA_MCU,PF_ARM_MPU,PF_C28,PF_C6000SC,PF_HERCULES,PF_MMWAVE,PF_MSP430,PF_MSPM0,PF_MSPM33,PF_OMAPL,PF_PGA,PF_MSP432,PF_AUTO,PF_TM4C,PF_DIGITAL_POWER,PF_WCONN
                                             Allowed: PF_AM13X PF_SITARA_MCU PF_ARM_MPU PF_C28 PF_C6000SC PF_HERCULES PF_MMWAVE PF_MSP430 PF_MSPM0 PF_MSPM33 PF_OMAPL PF_PGA PF_MSP432 PF_AUTO PF_TM4C PF_DIGITAL_POWER PF_WCONN

--disable-components <disable-components>   Comma-separated list of components
                                             Default:
                                             Allowed: PF_AM13X PF_SITARA_MCU PF_ARM_MPU PF_C28 PF_C6000SC PF_HERCULES PF_MMWAVE PF_MSP430 PF_MSPM0 PF_MSPM33 PF_OMAPL PF_PGA PF_MSP432 PF_AUTO PF_TM4C PF_DIGITAL_POWER PF_WCONN

--installer-language <installer-language>   Language selection
                                             Default: en
                                             Allowed: en

--prefix <prefix>                           Installation Directory
                                             Default: [Run with --help to see default installation directory]

--errortrace <errortrace>                   Error trace filename
                                             Default:

Example for installing the MSP430 and MSPM0 components in c:\ti\mydir:

ccs_setup_<version>.exe --prefix c:\ti\mydir --enable-components PF_MSP430,PF_MSPM0

Example for installing the AM13x component in c:\ti\mydir without asking the user for any input (silent unattended installation):

ccs_setup_<version>.exe --prefix c:\ti\mydir --enable-components PF_AM13X --mode unattended

3.4.1. Product Families

The available components (device families) that can be installed are listed below:

  • PF_AM13X: AM13x Arm-based microcontrollers

  • PF_SITARA_MCU: AM2x Arm-based high performance microcontrollers

  • PF_ARM_MPU: Arm-based processors

  • PF_C28: C2000 real-time microcontrollers

  • PF_C6000SC: C6000 Power-Optimized DSP

  • PF_HERCULES: Hercules Safety MCUs

  • PF_MMWAVE: mmWave Sensors

  • PF_MSP430: MSP430 microcontrollers

  • PF_MSPM0: MSPM0 Arm Cortex-M0+ microcontrollers

  • PF_MSPM33: MSPM33 Arm Cortex-M33 microcontrollers

  • PF_OMAPL: OMAP-L1x DSP + Arm9 Processor

  • PF_PGA: PGA Sensor Signal Conditioners

  • PF_MSP432: SimpleLink MSP432 low power + performance MCUs

  • PF_AUTO: TDAx Driver Assistance SoCs & Jacinto DRAx Infotainment SoCs

  • PF_TM4C: TM4C12x Arm Cortex-M4F MCUs

  • PF_DIGITAL_POWER: UCD Digital Power Controllers

  • PF_WCONN: Wireless Connectivity

3.5. Updating Code Composer Studio

To initiate an update check, go to Help → Check for Updates... from the main Code Composer Studio menu. This will parse all the pre-configured update sites and display a list of available updates:

Software update dialog

Each listed update will also show the Current version installed and the Latest version available with the update.

Select the updates you want to install and click the Install button to continue. This will take you through the update process.